Design Name C:/srf04/Agama/Agama_EM_Designs/CC1352REM-XS169-XS24/Cadence/allegro/CC1352REM-XS169-XS24.brd
Date Fri Mar 13 21:06:00 2020

Note: This report identifies the unused B/B vias associated with a via stack structure. A stack structure can consist of coincidently placed micro, B/B vias or a combination. As an example of what the report detects, consider the stack Micro1-2, BB2-7, Micro7-8; if a trace connects to the stack on Layers 3 and 6, Micro1-2 and Micro7-8 would be identified as "unused". Click on the hyperlink to navigate to their location.

Unused Blind/Buried Vias
Net Name Padstack Name Start/Stop Layer Location (x y)