DMM Wsn Node + BLE Remote Display
Table of Contents
- Introduction
- Hardware Prerequisites
- Software Prerequisites
- Dynamic Multi-protocol Manager
- Usage
- Switching to SLR mode
- BLE Multi-Connections
- DMM Limitations
Introduction
The dmm_wsnnode_remote_display project showcases a dynamic multi-protocol example which enables concurrent proprietary Sub-1G and BLE5. This example implements a Sub-1G Wireless Sensor Network Node with a BLE Remote Display, using TI's DMM (Dynamic Multi-protocol Manager) to enable the multi-protocol and dual band features of the CC1352.
The BLE remote display allows a SmartPhone App to provision the Sub-1G node and to see data on the Sub-1G network.
This project has the following app configurations available:
| App Build Configuration | Description |
|---|---|
| FlashROM_Release (default) | All TI-RTOS debug features disabled but application-logging to UART remains enabled. The application uses the config file ble_release.cfg and the defines are in <app name>_FlashROM_Release.opt. |
All application configurations use the stack library configuration, FlashROM_Library. This build configuration will yield additional flash footprint optimizations by the linker since the application and stack can share contiguous flash pages. This configuration is further discussed in the Stack Library Configuration section of the BLE5-Stack User's Guide provided in the SDK.
This document discusses the procedure for using the Wsn Node Remote Display application when the FlashROM_Release configuration is used.
Hardware Prerequisites
The default Simple Peripheral configuration uses the LAUNCHXL-CC1352R. This hardware configuration is shown in the below image:
For custom hardware, see the Running the SDK on Custom Boards section of the BLE5-Stack User's Guide.
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the dependencies section of the Release Notes located in the root folder of the SDK.
For information on how to import this project into your IDE workspace and build/run, please refer to the device's Platform section in the BLE5-Stack Quick Start Guide.
Note: If you are running an OAD example, be sure to first build and flash a BIM project located in
/examples/nortos/<BOARD>/bim. For more instructions on how to do this, please refer to the BLE5-Stack Quick Start Guide.
Service/Profile Table
This project contains 1 service, which has 5 characteristics.
Note that BLE Scanner may report 128 bit UUIDs, but the project is generating 16 bit UUIDs.
| Characteristic | UUID | Format | Properties | Profile Source |
|---|---|---|---|---|
| Node Data | 1181 | 1 Byte Integer | Read/Notify | peripheral.c/remote_display_gatt_profile.c |
| Node Report Interval | 1182 | 1 Byte Integer | Read/Write | peripheral.c/remote_display_gatt_profile.c |
| Conc LED Identify | 1183 | 1 Byte Integer | Read/Write | peripheral.c/remote_display_gatt_profile.c |
| Node Address | 1184 | 1 Byte Integer | Auth Read/Write | peripheral.c/remote_display_gatt_profile.c |
Dynamic Multi-protocol Manager
The DMM uses 2 main components to dynamically arbitrate the RF resource.
- A Policy Manager
- A Scheduler
TI CC1352 devices are capable of dual band operation, the CC1352 Launchpad (TI development platform) has a dual band antenna which performs well in the 868/916MHz band as well as the 2.4GHz band. Using the DMM on a CC1352 device enables not only multi protocol, but also dual band. The below diagram shows how the DMM allows 2 stacks to run on the same device, which was previously only possible on 2 devices. In the diagram the Stack 1 is shown functioning along side Stack 2, this could be a BLE stack and a proprietary Sub1G stack (called Wireless Sensor Network) or a 15.4 Stack. The Stacks used are defined by the developer.
Single mode setup:
DMM Setup:
The DMM makes scheduling decisions based on Application Level information, Stack Level information, and the Global Priority Table (GPT).
The Stack Level information is embedded in each RF command and it includes: Start Type, Start Time, AllowDelay, Priority, Activity, etc.
The Global Priority Table (GPT) defines relative priorities of the two stacks
based on the activity and priority of RF commands. For details of the GPT,
refer to <SDK_DIR>\source\ti\common\dmm\dmm_priority_ble_wsn.c/h.
The Application Level information is the user defined information via the policy
table and inludes: Application State Name, Weight, AppliedActivity, Pause, etc;
the policy table can have multiple policies. A policy defines a specific state
of the DMM application where the user wants to apply different priority based on
an action. A simplified policy table is shown below, it defines the behavior
when Stack 1 is performing an OAD and does not take into account the specific
state of the stack 2 (i.e. any state). It specifies that when Stack 1 is in an
OAD state, the priority of the BLE_CONNECTION, in this case, is increased by
25. If any RF scheduling conflicts happen during the OAD, they will be resolved
by taking into account the modified priority defined in the policy.
| Stack 1 State Name | Stack 2 State Name | Weight | Applied Activity | Description |
|---|---|---|---|---|
| OAD | Any | 25 | CONNECTION | Increase the priority of CONNECTION activity of Stack 1 by 25 during OAD operation |
The policy used in this example is more complex than the illustration above. For
details of the actual policy used refer to
<SDK_DIR>\source\ti\common\dmm\policy.h and ti_dmm_application_policy.c/h as
generated by the SysConfig tool.
The DMM also supports pausing/resuming stacks based on a policy change. This is achieved by an application callback, which is called from the DMM policy manager when a policy change requiring a stack to pause operation is entire. An example of pausing the Zigbee stack during a BLE_OAD is provided in the DMM Zigbee Coordinator Switch + BLE OAD example.
See the DMM chapter in your protocol stack user's guide for more information about DMM.
Usage
This example should be used in conjunction with the EasyLink rfWsnConcentrator. It is advised that you use the LAUNCHXL_CC1352R1 rfWsnConcentrator located at ../easylink/rfWsnConcentrator. Alternatively a different CC13x2 concentrator can be used, however some features may not be available.
This application uses the UART peripheral to provide an interface for the application. The UART is only used for display messages.
This document will use Teraterm to serve as the display for the output of the CC1352 LaunchPad. The BLE Scanner smartphone application will act as the BLE Central device that will connect to the Remote Display service in this example. The BLE Scanner smartphone application is available on App Store and Google Play. Note that any other serial terminal and smart phone BLE application can be used. The following default parameters are used for the UART peripheral for display:
| UART Param | Default Values |
|---|---|
| Baud Rate | 115200 |
| Data length | 8 bits |
| Parity | None |
| Stop bits | 1 bit |
| Flow Control | None |
Note: If you are using a smartphone as the BLE central device and the same CC1352 LaunchPad was used previously with a different DMM or BLE example then you may need to forget the device in the smartphone BLE settings, then disable and enable BLE. Not doing this could result in the smartphone application displaying incorrect services and characteristics
Once the Wsn Node Remote Display application starts, the output to the terminal will report its address and the fact that it is advertising, as shown below:
The WsnConcentrator should be outputting the Sub-1G sensor as shown below:
The default reporting interval is 1s.
Advertising is enabled by default upon startup, so there is no need to physically press a button to start advertising. Using BLE Scanner to scan for the device, you should see a device with the name of Node Remote Display (note that the navigation might be slightly different depending on your mobile application):
If there is more than 1 device called Node Remote Display, the RSSI value under the strength bars on the left can be used to find which device you are trying to connect to. Press the "connect" button to connect to the device. When prompted enter the pairing code "123456".
Once connected, the terminal window will show the address of the connected device (smartphone):
In BLE Scanner, you should be able to see various information about the Node Remote Display device:
You should see 1 service, which is labeled as "CUSTOM SERVICE" (this may be slightly different for other smartphone applications). It will also provide its UUID. Clicking on this service will display the 3 characteristics that it contains, with information about each characteristic:
Scrolling down should show all 3 characteristics. The following sections detail the functions and operations of each of the characteristics.
Node Data Characteristic (UUID: 1181)
This characteristic demonstrates read only and notify properties, and it contains a 1-byte-long value indicating the Sub-1G node data. By default the BLE Scanner application enables the notifications (this may be different with other apps or versions of this app), notice that the value is updating every 1s. Click on the "Read, Notify" item to see more information about the characteristic. From here you can disable the notifications and read the characteristic manually.
If you disable notifications then make sure you re-enable them as this will be useful when changing the report interval later.
Node Report Interval Characteristic (UUID: 1182)
This characteristic demonstrates read and write properties, it contains a 1-byte-long value indicating the Sub-1G report interval in seconds.
This application consists of an Sensor Controller Engine, SCE, Task which samples the ADC. On initialization the CM3 application sets the minimum report interval and the minimum change value which is used by the SCE task to wake up the CM3. The ADC task on the SCE checks the ADC value once per second. If the ADC value has changed by the minimum change amount since the last time it notified the CM3, it wakes it up again. If the change is less than the masked value, then it does not wake up the CM3 unless the minimum report interval time has expired. This 1s update can also be seen on the BLE Scanner app when notifications are enabled. In the BLE Scanner application scroll down to the second characteristic of the "CUSTOM SERVICE", then Click on the "Read, Write" item of the Node Report Interval characteristic to see more information about the characteristic. From here you can read and write the report interval. When a value is written the rate at which node data is updated changes to reflect the new value.
Concetrator LED Identify (UUID: 1183)
This characteristic demonstrates read and write properties, it contains a 1-byte-long value used to make the Sub1GHz Wireless Sensor Network Concentrator blink its LED. Writing 1 to this characteristic will cause the Node Remote Display device to send a message over the Sub1GHz network to the network Concentrator instructing it to blink its LED. The network concentrator LED will blink 5 time when this message is received. The Characteristics value will reset back to 0 when the Concentrator acknowledges it has received the message. In the BLE Scanner application scroll down to the 3rd characteristic of the CUSTOM SERVICE, then click on the "Read, Write" item of the Concentrator LED Identify characteristic to see more information about the characteristic. From here you can write 01 to send a concentrator identify message.
Node Address Characteristic 3 (UUID: 1184)
This characteristic has read and write properties. Reading the chracteristic shows the node address reported by the concentrator. Writing to the characteristics will cause a new node with that address to appear on the concentrator's display.
Disabling Common User Interface
The common user interface (CUI) is a UART based interface that allows users to control and receive updates regarding the application. For various reasons, including reducing the memory footprint, the user is able to disable the common user interface (CUI). To disable the CUI, the following variable must be defined in the dmm_wsnnode_remote_display_app.opts:
-DCUI_DISABLE
Please Note: particular features that are dependednt on the CUI wil be unavailable when this feature is enabled.
Switching to SLR Mode
The following steps will allow you to use the easylink network on a SLR (Simplelink Long Range) PHY.
Change the PHY for the Node Application:
Modify the RADIO_EASYLINK_MODULATION in RadioProtocol.h. Use EasyLink_PHY_5KBPSSLLR instead of EasyLink_PHY_Custom.
Change the PHY for the Concentrator Application:
Modify the RADIO_EASYLINK_MODULATION in RadioProtocol.h. Use EasyLink_PHY_5KBPSSLLR instead of EasyLink_PHY_Custom.
Modify the NORERADIO_ACK_TIMEOUT_TIME_MS in ConcentratorRadioTask.c. Use '500' instead of '160'
Rebuild both the DMM Application and the Concentrator Application with these changes.
BLE Multi-Connections
This project is configured by default to make use of Multiple (4) BLE Connections. This means that the DMM project will be able to support 4 BLE connections on top of the secondary stack network.
Updating Multi-Connection Settings
The Multi-Connection Settings can easily be changed via the Sysconfig tool. No application changes are required by the user to go from 1 connection to 4 connections.
As always, with network configuration changes, it's important to recognize that the update will change the maximum bandwidth required by the BLE Stack. When moving from the default settings to something new, you as the developer should take time to consider how this will effect your network requirements.
DMM Limitations
The following limitations exist in the DMM implementation:
- Sub-1G SLR Phy not supported.
- Connection intervals lower than 60ms will result in high sub1G packet loss when BLE is connected.
- When connecting to a central device Sub-1G packet loss may be experienced until the update parameters are sent 1s after connection. This will be dependent on the initial connection interval of the BLE central devices.
- Only 1 BLE connection is supported. The number of concurrent BLE connections is set in the application .opt file, located in the project workspace under the TOOLS folder.