nvsexternal
Example Summary
This example shows how to use the Non-Volatile Storage (NVS) driver to read and write data to off-chip external flash memory. The external SPI flash is accessed by the NVS SPI driver.
Peripherals & Pin Assignments
When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.
CONFIG_NVSEXTERNAL- Non-volatile storage used by a NVS driver instance.
BoosterPacks, Board Resources & Jumper Settings
For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.
If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.
The Board.html can also be found in your SDK installation:
<SDK_INSTALL_DIR>/source/ti/boards/<BOARD>
Example Usage
Example output is generated through use of Display driver APIs. Refer to the Display driver documentation found in the SimpleLink MCU SDK User’s Guide.
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port. The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
The connection will have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example.
The example will output the region attributes as defined by
CONFIG_NVSEXTERNAL.- The example checks if the string, “SimpleLink SDK Non-Volatile Storage (NVS) Example” is present in non-volatile storage.
- If present, the string is displayed to the UART console. The entire flash sector is then erased.
- If not present, the string is written to the non-volatile storage.
Disconnect the device from the debug session.
When prompted, reset the device. This will cause the application to start over.
The sector size and region size will vary depending on the device specific definitions in the board file.
The following is example output assuming the string was not present in non-volatile storage:
Sector Size: 0x1000
Region Size: 0x4000
Writing signature to SPI flash...
Reset the device.
==================================================
The following is example output assuming the string is present in non-volatile storage:
Sector Size: 0x1000
Region Size: 0x4000
SimpleLink SDK Non-Volatile Storage (NVS) SPI Example.
Erasing SPI flash sector...
Reset the device.
==================================================
Application Design Details
The application utilizes a single thread to demonstrate using the non-volatile storage region defined by
CONFIG_NVSEXTERNAL.CONFIG_NVSEXTERNALdefines non-volatile storage located on an off-chip external flash memory location. The memory definitions may be found in the board file. AfterNVS_open(), thenvsHandleis associated with the memory region defined byCONFIG_NVSEXTERNAL.- A block of memory equal to the size of
signaturebytes is read from external flash and copied into RAM (buffer). This is performed through SPI transactions with the external flash device all contained inside the NVS SPI driver. The contents copied intobufferare compared tosignature. - If equal, the application displays the signature to the UART console. It is important to note that the string was copied into RAM (
buffer) duringNVS_read(). This example displays the copied string stored inbuffer. After the string is output to the UART console, the first sector in the NVS region is erased. If not equal, the application writes the string,
signatureto the NVS region. This is performed through SPI transactions with the external flash device all contained inside the NVS SPI driver.At the end of execution, the application prompts the user to reset the device. Upon a reset, the contents of volatile memory (RAM) are lost. The example application restarts.
The
NVS_WRITE_ERASEflag is used with theNVS_write()API to ensure the flash sector is erased prior to performing a write. This flag will eraseNVS_Attrs.sectorSizebytes of memory starting at the offset specified withNVS_write().The
NVS_WRITE_POST_VERIFYflag is also used with theNVS_write()API to ensure the flash memory was successfully written.
TI-RTOS:
- When building in Code Composer Studio, the kernel configuration project will be imported along with the example. The kernel configuration project is referenced by the example, so it will be built first. The “release” kernel configuration is the default project used. It has many debug features disabled. These feature include assert checking, logging and runtime stack checks. For a detailed difference between the “release” and “debug” kernel configurations and how to switch between them, please refer to the SimpleLink MCU SDK User’s Guide. The “release” and “debug” kernel configuration projects can be found under <SDK_INSTALL_DIR>/kernel/tirtos/builds/<BOARD>/(release|debug)/(ccs|gcc).
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.