#******************************************************************************
#
# Doxyfile - Doxygen configuration file.
#
# Copyright (c) 2005 Texas Instruments Incorporated.  All rights reserved.
# TI Information - Selective Disclosure
#
#******************************************************************************

# Doxyfile 1.4.2

# This file describes the settings to be used by the documentation system
# doxygen (www.doxygen.org) for a project
#
# All text after a hash (#) is considered a comment and will be ignored
# The format is:
#       TAG = value [value, ...]
# For lists items can also be appended using:
#       TAG += value [value, ...]
# Values that contain spaces should be placed between quotes (" ")

#---------------------------------------------------------------------------
# Project related configuration options
#---------------------------------------------------------------------------

# The PROJECT_NAME tag is a single word (or a sequence of words surrounded
# by quotes) that should identify the project.

PROJECT_NAME           =  "CC2538 Peripheral Driver Library"

# The PROJECT_NUMBER tag can be used to enter a project or revision number.
# This could be handy for archiving the generated documentation or
# if some version control system is used.

PROJECT_NUMBER         =  __REVISION__

# The OUTPUT_DIRECTORY tag is used to specify the (relative or absolute)
# base path where the generated documentation will be put.
# If a relative path is entered, it will be relative to the location
# where doxygen was started. If left blank the current directory will be used.

OUTPUT_DIRECTORY       =

# If the CREATE_SUBDIRS tag is set to YES, then doxygen will create
# 4096 sub-directories (in 2 levels) under the output directory of each output
# format and will distribute the generated files over these directories.
# Enabling this option can be useful when feeding doxygen a huge amount of
# source files, where putting all generated files in the same directory would
# otherwise cause performance problems for the file system.

CREATE_SUBDIRS         = NO

# The OUTPUT_LANGUAGE tag is used to specify the language in which all
# documentation generated by doxygen is written. Doxygen will use this
# information to generate all constant output in the proper language.
# The default language is English, other supported languages are:
# Brazilian, Catalan, Chinese, Chinese-Traditional, Croatian, Czech, Danish,
# Dutch, Finnish, French, German, Greek, Hungarian, Italian, Japanese,
# Japanese-en (Japanese with English messages), Korean, Korean-en, Norwegian,
# Polish, Portuguese, Romanian, Russian, Serbian, Slovak, Slovene, Spanish,
# Swedish, and Ukrainian.

OUTPUT_LANGUAGE        = English

# This tag can be used to specify the encoding used in the generated output.
# The encoding is not always determined by the language that is chosen,
# but also whether or not the output is meant for Windows or non-Windows users.
# In case there is a difference, setting the USE_WINDOWS_ENCODING tag to YES
# forces the Windows encoding (this is the default for the Windows binary),
# whereas setting the tag to NO uses a Unix-style encoding (the default for
# all platforms other than Windows).

USE_WINDOWS_ENCODING   = NO

# If the BRIEF_MEMBER_DESC tag is set to YES (the default) Doxygen will
# include brief member descriptions after the members that are listed in
# the file and class documentation (similar to JavaDoc).
# Set to NO to disable this.

BRIEF_MEMBER_DESC      = NO

# If the REPEAT_BRIEF tag is set to YES (the default) Doxygen will prepend
# the brief description of a member or function before the detailed description.
# Note: if both HIDE_UNDOC_MEMBERS and BRIEF_MEMBER_DESC are set to NO, the
# brief descriptions will be completely suppressed.

REPEAT_BRIEF           = YES

# This tag implements a quasi-intelligent brief description abbreviator
# that is used to form the text in various listings. Each string
# in this list, if found as the leading text of the brief description, will be
# stripped from the text and the result after processing the whole list, is
# used as the annotated text. Otherwise, the brief description is used as-is.
# If left blank, the following values are used ("$name" is automatically
# replaced with the name of the entity): "The $name class" "The $name widget"
# "The $name file" "is" "provides" "specifies" "contains"
# "represents" "a" "an" "the"

ABBREVIATE_BRIEF       =

# If the ALWAYS_DETAILED_SEC and REPEAT_BRIEF tags are both set to YES then
# Doxygen will generate a detailed section even if there is only a brief
# description.

ALWAYS_DETAILED_SEC    = NO

# If the INLINE_INHERITED_MEMB tag is set to YES, doxygen will show all
# inherited members of a class in the documentation of that class as if those
# members were ordinary class members. Constructors, destructors and assignment
# operators of the base classes will not be shown.

INLINE_INHERITED_MEMB  = NO

# If the FULL_PATH_NAMES tag is set to YES then Doxygen will prepend the full
# path before files name in the file list and in the header files. If set
# to NO the shortest path that makes the file name unique will be used.

FULL_PATH_NAMES        = NO

# If the FULL_PATH_NAMES tag is set to YES then the STRIP_FROM_PATH tag
# can be used to strip a user-defined part of the path. Stripping is
# only done if one of the specified strings matches the left-hand part of
# the path. The tag can be used to show relative paths in the file list.
# If left blank the directory from which doxygen is run is used as the
# path to strip.

STRIP_FROM_PATH        =

# The STRIP_FROM_INC_PATH tag can be used to strip a user-defined part of
# the path mentioned in the documentation of a class, which tells
# the reader which header file to include in order to use a class.
# If left blank only the name of the header file containing the class
# definition is used. Otherwise one should specify the include paths that
# are normally passed to the compiler using the -I flag.

STRIP_FROM_INC_PATH    =

# If the SHORT_NAMES tag is set to YES, doxygen will generate much shorter
# (but less readable) file names. This can be useful is your file systems
# doesn't support long names like on DOS, Mac, or CD-ROM.

SHORT_NAMES            = NO

# If the JAVADOC_AUTOBRIEF tag is set to YES then Doxygen
# will interpret the first line (until the first dot) of a JavaDoc-style
# comment as the brief description. If set to NO, the JavaDoc
# comments will behave just like the Qt-style comments (thus requiring an
# explicit @brief command for a brief description.

JAVADOC_AUTOBRIEF      = NO

# The MULTILINE_CPP_IS_BRIEF tag can be set to YES to make Doxygen
# treat a multi-line C++ special comment block (i.e. a block of //! or ///
# comments) as a brief description. This used to be the default behaviour.
# The new default is to treat a multi-line C++ comment block as a detailed
# description. Set this tag to YES if you prefer the old behaviour instead.

MULTILINE_CPP_IS_BRIEF = NO

# If the DETAILS_AT_TOP tag is set to YES then Doxygen
# will output the detailed description near the top, like JavaDoc.
# If set to NO, the detailed description appears after the member
# documentation.

DETAILS_AT_TOP         = NO

# If the INHERIT_DOCS tag is set to YES (the default) then an undocumented
# member inherits the documentation from any documented member that it
# re-implements.

INHERIT_DOCS           = YES

# If member grouping is used in the documentation and the DISTRIBUTE_GROUP_DOC
# tag is set to YES, then doxygen will reuse the documentation of the first
# member in the group (if any) for the other members of the group. By default
# all members of a group must be documented explicitly.

DISTRIBUTE_GROUP_DOC   = NO

# If the SEPARATE_MEMBER_PAGES tag is set to YES, then doxygen will produce
# a new page for each member. If set to NO, the documentation of a member will
# be part of the file/class/namespace that contains it.

SEPARATE_MEMBER_PAGES  = NO

# The TAB_SIZE tag can be used to set the number of spaces in a tab.
# Doxygen uses this value to replace tabs by spaces in code fragments.

TAB_SIZE               = 8

# This tag can be used to specify a number of aliases that acts
# as commands in the documentation. An alias has the form "name=value".
# For example adding "sideeffect=\par Side Effects:\n" will allow you to
# put the command \sideeffect (or @sideeffect) in the documentation, which
# will result in a user-defined paragraph with heading "Side Effects:".
# You can put \n's in the value part of an alias to insert newlines.

ALIASES                =
##### INTERNAL BEGIN #####
ALIASES                = "proposed=\latexonly{\color{red}\texttt{<< << << PROPOSED API >> >> >>}}\\\\\endlatexonly"
##### INTERNAL END #####

# Set the OPTIMIZE_OUTPUT_FOR_C tag to YES if your project consists of C
# sources only. Doxygen will then generate output that is more tailored for C.
# For instance, some of the names that are used will be different. The list
# of all members will be omitted, etc.

OPTIMIZE_OUTPUT_FOR_C  = YES

# Set the OPTIMIZE_OUTPUT_JAVA tag to YES if your project consists of Java sources
# only. Doxygen will then generate output that is more tailored for Java.
# For instance, namespaces will be presented as packages, qualified scopes
# will look different, etc.

OPTIMIZE_OUTPUT_JAVA   = NO

# Set the SUBGROUPING tag to YES (the default) to allow class member groups of
# the same type (for instance a group of public functions) to be put as a
# subgroup of that type (e.g. under the Public Functions section). Set it to
# NO to prevent subgrouping. Alternatively, this can be done per class using
# the \nosubgrouping command.

SUBGROUPING            = YES

#---------------------------------------------------------------------------
# Build related configuration options
#---------------------------------------------------------------------------

# If the EXTRACT_ALL tag is set to YES doxygen will assume all entities in
# documentation are documented, even if no documentation was available.
# Private class members and static file members will be hidden unless
# the EXTRACT_PRIVATE and EXTRACT_STATIC tags are set to YES

EXTRACT_ALL            = NO

# If the EXTRACT_PRIVATE tag is set to YES all private members of a class
# will be included in the documentation.

EXTRACT_PRIVATE        = NO

# If the EXTRACT_STATIC tag is set to YES all static members of a file
# will be included in the documentation.

EXTRACT_STATIC         = NO

# If the EXTRACT_LOCAL_CLASSES tag is set to YES classes (and structs)
# defined locally in source files will be included in the documentation.
# If set to NO only classes defined in header files are included.

EXTRACT_LOCAL_CLASSES  = NO

# This flag is only useful for Objective-C code. When set to YES local
# methods, which are defined in the implementation section but not in
# the interface are included in the documentation.
# If set to NO (the default) only methods in the interface are included.

EXTRACT_LOCAL_METHODS  = NO

# If the HIDE_UNDOC_MEMBERS tag is set to YES, Doxygen will hide all
# undocumented members of documented classes, files or namespaces.
# If set to NO (the default) these members will be included in the
# various overviews, but no documentation section is generated.
# This option has no effect if EXTRACT_ALL is enabled.

HIDE_UNDOC_MEMBERS     = YES

# If the HIDE_UNDOC_CLASSES tag is set to YES, Doxygen will hide all
# undocumented classes that are normally visible in the class hierarchy.
# If set to NO (the default) these classes will be included in the various
# overviews. This option has no effect if EXTRACT_ALL is enabled.

HIDE_UNDOC_CLASSES     = YES

# If the HIDE_FRIEND_COMPOUNDS tag is set to YES, Doxygen will hide all
# friend (class|struct|union) declarations.
# If set to NO (the default) these declarations will be included in the
# documentation.

HIDE_FRIEND_COMPOUNDS  = YES

# If the HIDE_IN_BODY_DOCS tag is set to YES, Doxygen will hide any
# documentation blocks found inside the body of a function.
# If set to NO (the default) these blocks will be appended to the
# function's detailed documentation block.

HIDE_IN_BODY_DOCS      = NO

# The INTERNAL_DOCS tag determines if documentation
# that is typed after a \internal command is included. If the tag is set
# to NO (the default) then the documentation will be excluded.
# Set it to YES to include the internal documentation.

INTERNAL_DOCS          = NO

# If the CASE_SENSE_NAMES tag is set to NO then Doxygen will only generate
# file names in lower-case letters. If set to YES upper-case letters are also
# allowed. This is useful if you have classes or files whose names only differ
# in case and if your file system supports case sensitive file names. Windows
# and Mac users are advised to set this option to NO.

CASE_SENSE_NAMES       = YES

# If the HIDE_SCOPE_NAMES tag is set to NO (the default) then Doxygen
# will show members with their full class and namespace scopes in the
# documentation. If set to YES the scope will be hidden.

HIDE_SCOPE_NAMES       = NO

# If the SHOW_INCLUDE_FILES tag is set to YES (the default) then Doxygen
# will put a list of the files that are included by a file in the documentation
# of that file.

SHOW_INCLUDE_FILES     = YES

# If the INLINE_INFO tag is set to YES (the default) then a tag [inline]
# is inserted in the documentation for inline members.

INLINE_INFO            = YES

# If the SORT_MEMBER_DOCS tag is set to YES (the default) then doxygen
# will sort the (detailed) documentation of file and class members
# alphabetically by member name. If set to NO the members will appear in
# declaration order.

SORT_MEMBER_DOCS       = YES

# If the SORT_BRIEF_DOCS tag is set to YES then doxygen will sort the
# brief documentation of file, namespace and class members alphabetically
# by member name. If set to NO (the default) the members will appear in
# declaration order.

SORT_BRIEF_DOCS        = YES

# If the SORT_BY_SCOPE_NAME tag is set to YES, the class list will be
# sorted by fully-qualified names, including namespaces. If set to
# NO (the default), the class list will be sorted only by class name,
# not including the namespace part.
# Note: This option is not very useful if HIDE_SCOPE_NAMES is set to YES.
# Note: This option applies only to the class list, not to the
# alphabetical list.

SORT_BY_SCOPE_NAME     = NO

# The GENERATE_TODOLIST tag can be used to enable (YES) or
# disable (NO) the todo list. This list is created by putting \todo
# commands in the documentation.

GENERATE_TODOLIST      = YES

# The GENERATE_TESTLIST tag can be used to enable (YES) or
# disable (NO) the test list. This list is created by putting \test
# commands in the documentation.

GENERATE_TESTLIST      = YES

# The GENERATE_BUGLIST tag can be used to enable (YES) or
# disable (NO) the bug list. This list is created by putting \bug
# commands in the documentation.

GENERATE_BUGLIST       = YES

# The GENERATE_DEPRECATEDLIST tag can be used to enable (YES) or
# disable (NO) the deprecated list. This list is created by putting
# \deprecated commands in the documentation.

GENERATE_DEPRECATEDLIST= YES

# The ENABLED_SECTIONS tag can be used to enable conditional
# documentation sections, marked by \if sectionname ... \endif.

  # This is the internal build of the document, which includes internal and
  # unannounced material.
ENABLED_SECTIONS       = LMI CODERED IAR KEIL CCS NOTCODERED NOTIAR NOTKEIL INTERNAL
  # The public build of the document for the LMI release.
#ENABLED_SECTIONS       = LMI CODERED IAR KEIL NOTCODERED NOTIAR NOTKEIL
  # The public build of the document for the Keil release.
#ENABLED_SECTIONS       = NOTLMI KEIL NOTCODERED NOTIAR
  # The public build of the document for the IAR release.
#ENABLED_SECTIONS       = NOTLMI IAR NOTCODERED NOTKEIL
  # The public build of the document for the code_red release.
#ENABLED_SECTIONS       = NOTLMI CODERED NOTIAR NOTKEIL

# The MAX_INITIALIZER_LINES tag determines the maximum number of lines
# the initial value of a variable or define consists of for it to appear in
# the documentation. If the initializer consists of more lines than specified
# here it will be hidden. Use a value of 0 to hide initializers completely.
# The appearance of the initializer of individual variables and defines in the
# documentation can be controlled using \showinitializer or \hideinitializer
# command in the documentation regardless of this setting.

MAX_INITIALIZER_LINES  = 0

# Set the SHOW_USED_FILES tag to NO to disable the list of files generated
# at the bottom of the documentation of classes and structs. If set to YES the
# list will mention the files that were used to generate the documentation.

SHOW_USED_FILES        = YES

# If the sources in your project are distributed over multiple directories
# then setting the SHOW_DIRECTORIES tag to YES will show the directory hierarchy
# in the documentation.

SHOW_DIRECTORIES       = NO

# The FILE_VERSION_FILTER tag can be used to specify a program or script that
# doxygen should invoke to get the current version for each file (typically from the
# version control system). Doxygen will invoke the program by executing (via
# popen()) the command <command> <input-file>, where <command> is the value of
# the FILE_VERSION_FILTER tag, and <input-file> is the name of an input file
# provided by doxygen. Whatever the progam writes to standard output
# is used as the file version. See the manual for examples.

FILE_VERSION_FILTER    =

#---------------------------------------------------------------------------
# configuration options related to warning and progress messages
#---------------------------------------------------------------------------

# The QUIET tag can be used to turn on/off the messages that are generated
# by doxygen. Possible values are YES and NO. If left blank NO is used.

QUIET                  = YES

# The WARNINGS tag can be used to turn on/off the warning messages that are
# generated by doxygen. Possible values are YES and NO. If left blank
# NO is used.

WARNINGS               = YES

# If WARN_IF_UNDOCUMENTED is set to YES, then doxygen will generate warnings
# for undocumented members. If EXTRACT_ALL is set to YES then this flag will
# automatically be disabled.

WARN_IF_UNDOCUMENTED   = YES

# If WARN_IF_DOC_ERROR is set to YES, doxygen will generate warnings for
# potential errors in the documentation, such as not documenting some
# parameters in a documented function, or documenting parameters that
# don't exist or using markup commands wrongly.

WARN_IF_DOC_ERROR      = YES

# This WARN_NO_PARAMDOC option can be abled to get warnings for
# functions that are documented, but have no documentation for their parameters
# or return value. If set to NO (the default) doxygen will only warn about
# wrong or incomplete parameter documentation, but not about the absence of
# documentation.

WARN_NO_PARAMDOC       = YES

# The WARN_FORMAT tag determines the format of the warning messages that
# doxygen can produce. The string should contain the $file, $line, and $text
# tags, which will be replaced by the file and line number from which the
# warning originated and the warning text. Optionally the format may contain
# $version, which will be replaced by the version of the file (if it could
# be obtained via FILE_VERSION_FILTER)

WARN_FORMAT            = "$file:$line: $text"

# The WARN_LOGFILE tag can be used to specify a file to which warning
# and error messages should be written. If left blank the output is written
# to stderr.

WARN_LOGFILE           =

#---------------------------------------------------------------------------
# configuration options related to the input files
#---------------------------------------------------------------------------

# The INPUT tag can be used to specify the files and/or directories that contain
# documented source files. You may enter file names like "myfile.cpp" or
# directories like "/usr/src/myproject". Separate the files or directories
# with spaces.

INPUT                  = . ../source

# If the value of the INPUT tag contains directories, you can use the
# FILE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp
# and *.h) to filter out the source-files in the directories. If left
# blank the following patterns are tested:
# *.c *.cc *.cxx *.cpp *.c++ *.java *.ii *.ixx *.ipp *.i++ *.inl *.h *.hh *.hxx
# *.hpp *.h++ *.idl *.odl *.cs *.php *.php3 *.inc *.m *.mm

FILE_PATTERNS          = *.c *.h *.dox

# The RECURSIVE tag can be used to turn specify whether or not subdirectories
# should be searched for input files as well. Possible values are YES and NO.
# If left blank NO is used.

RECURSIVE              = NO

# The EXCLUDE tag can be used to specify files and/or directories that should
# excluded from the INPUT source files. This way you can easily exclude a
# subdirectory from a directory tree whose root is specified with the INPUT tag.

EXCLUDE                =

# The EXCLUDE_SYMLINKS tag can be used select whether or not files or
# directories that are symbolic links (a Unix filesystem feature) are excluded
# from the input.

EXCLUDE_SYMLINKS       = NO

# If the value of the INPUT tag contains directories, you can use the
# EXCLUDE_PATTERNS tag to specify one or more wildcard patterns to exclude
# certain files from those directories.

EXCLUDE_PATTERNS       =

# The EXAMPLE_PATH tag can be used to specify one or more files or
# directories that contain example code fragments that are included (see
# the \include command).

EXAMPLE_PATH           = .

# If the value of the EXAMPLE_PATH tag contains directories, you can use the
# EXAMPLE_PATTERNS tag to specify one or more wildcard pattern (like *.cpp
# and *.h) to filter out the source-files in the directories. If left
# blank all files are included.

EXAMPLE_PATTERNS       =

# If the EXAMPLE_RECURSIVE tag is set to YES then subdirectories will be
# searched for input files to be used with the \include or \dontinclude
# commands irrespective of the value of the RECURSIVE tag.
# Possible values are YES and NO. If left blank NO is used.

EXAMPLE_RECURSIVE      = NO

# The IMAGE_PATH tag can be used to specify one or more files or
# directories that contain image that are included in the documentation (see
# the \image command).

IMAGE_PATH             =

# The INPUT_FILTER tag can be used to specify a program that doxygen should
# invoke to filter for each input file. Doxygen will invoke the filter program
# by executing (via popen()) the command <filter> <input-file>, where <filter>
# is the value of the INPUT_FILTER tag, and <input-file> is the name of an
# input file. Doxygen will then use the output that the filter program writes
# to standard output.  If FILTER_PATTERNS is specified, this tag will be
# ignored.

INPUT_FILTER           =

# The FILTER_PATTERNS tag can be used to specify filters on a per file pattern
# basis.  Doxygen will compare the file name with each pattern and apply the
# filter if there is a match.  The filters are a list of the form:
# pattern=filter (like *.cpp=my_cpp_filter). See INPUT_FILTER for further
# info on how filters are used. If FILTER_PATTERNS is empty, INPUT_FILTER
# is applied to all files.

FILTER_PATTERNS        =

# If the FILTER_SOURCE_FILES tag is set to YES, the input filter (if set using
# INPUT_FILTER) will be used to filter the input files when producing source
# files to browse (i.e. when SOURCE_BROWSER is set to YES).

FILTER_SOURCE_FILES    = NO

#---------------------------------------------------------------------------
# configuration options related to source browsing
#---------------------------------------------------------------------------

# If the SOURCE_BROWSER tag is set to YES then a list of source files will
# be generated. Documented entities will be cross-referenced with these sources.
# Note: To get rid of all source code in the generated output, make sure also
# VERBATIM_HEADERS is set to NO.

SOURCE_BROWSER         = NO

# Setting the INLINE_SOURCES tag to YES will include the body
# of functions and classes directly in the documentation.

INLINE_SOURCES         = NO

# Setting the STRIP_CODE_COMMENTS tag to YES (the default) will instruct
# doxygen to hide any special comment blocks from generated source code
# fragments. Normal C and C++ comments will always remain visible.

STRIP_CODE_COMMENTS    = YES

# If the REFERENCED_BY_RELATION tag is set to YES (the default)
# then for each documented function all documented
# functions referencing it will be listed.

REFERENCED_BY_RELATION = YES

# If the REFERENCES_RELATION tag is set to YES (the default)
# then for each documented function all documented entities
# called/used by that function will be listed.

REFERENCES_RELATION    = YES

# If the VERBATIM_HEADERS tag is set to YES (the default) then Doxygen
# will generate a verbatim copy of the header file for each class for
# which an include is specified. Set to NO to disable this.

VERBATIM_HEADERS       = NO

#---------------------------------------------------------------------------
# configuration options related to the alphabetical class index
#---------------------------------------------------------------------------

# If the ALPHABETICAL_INDEX tag is set to YES, an alphabetical index
# of all compounds will be generated. Enable this if the project
# contains a lot of classes, structs, unions or interfaces.

ALPHABETICAL_INDEX     = NO

# If the alphabetical index is enabled (see ALPHABETICAL_INDEX) then
# the COLS_IN_ALPHA_INDEX tag can be used to specify the number of columns
# in which this list will be split (can be a number in the range [1..20])

COLS_IN_ALPHA_INDEX    = 5

# In case all classes in a project start with a common prefix, all
# classes will be put under the same header in the alphabetical index.
# The IGNORE_PREFIX tag can be used to specify one or more prefixes that
# should be ignored while generating the index headers.

IGNORE_PREFIX          =

#---------------------------------------------------------------------------
# configuration options related to the HTML output
#---------------------------------------------------------------------------

# If the GENERATE_HTML tag is set to YES (the default) Doxygen will
# generate HTML output.

GENERATE_HTML          = NO

# The HTML_OUTPUT tag is used to specify where the HTML docs will be put.
# If a relative path is entered the value of OUTPUT_DIRECTORY will be
# put in front of it. If left blank `html' will be used as the default path.

HTML_OUTPUT            = html

# The HTML_FILE_EXTENSION tag can be used to specify the file extension for
# each generated HTML page (for example: .htm,.php,.asp). If it is left blank
# doxygen will generate files with .html extension.

HTML_FILE_EXTENSION    = .html

# The HTML_HEADER tag can be used to specify a personal HTML header for
# each generated HTML page. If it is left blank doxygen will generate a
# standard header.

HTML_HEADER            =

# The HTML_FOOTER tag can be used to specify a personal HTML footer for
# each generated HTML page. If it is left blank doxygen will generate a
# standard footer.

HTML_FOOTER            =

# The HTML_STYLESHEET tag can be used to specify a user-defined cascading
# style sheet that is used by each HTML page. It can be used to
# fine-tune the look of the HTML output. If the tag is left blank doxygen
# will generate a default style sheet. Note that doxygen will try to copy
# the style sheet file to the HTML output directory, so don't put your own
# stylesheet in the HTML output directory as well, or it will be erased!

HTML_STYLESHEET        =

# If the HTML_ALIGN_MEMBERS tag is set to YES, the members of classes,
# files or namespaces will be aligned in HTML using tables. If set to
# NO a bullet list will be used.

HTML_ALIGN_MEMBERS     = YES

# If the GENERATE_HTMLHELP tag is set to YES, additional index files
# will be generated that can be used as input for tools like the
# Microsoft HTML help workshop to generate a compressed HTML help file (.chm)
# of the generated HTML documentation.

GENERATE_HTMLHELP      = NO

# If the GENERATE_HTMLHELP tag is set to YES, the CHM_FILE tag can
# be used to specify the file name of the resulting .chm file. You
# can add a path in front of the file if the result should not be
# written to the html output directory.

CHM_FILE               =

# If the GENERATE_HTMLHELP tag is set to YES, the HHC_LOCATION tag can
# be used to specify the location (absolute path including file name) of
# the HTML help compiler (hhc.exe). If non-empty doxygen will try to run
# the HTML help compiler on the generated index.hhp.

HHC_LOCATION           =

# If the GENERATE_HTMLHELP tag is set to YES, the GENERATE_CHI flag
# controls if a separate .chi index file is generated (YES) or that
# it should be included in the master .chm file (NO).

GENERATE_CHI           = NO

# If the GENERATE_HTMLHELP tag is set to YES, the BINARY_TOC flag
# controls whether a binary table of contents is generated (YES) or a
# normal table of contents (NO) in the .chm file.

BINARY_TOC             = NO

# The TOC_EXPAND flag can be set to YES to add extra items for group members
# to the contents of the HTML help documentation and to the tree view.

TOC_EXPAND             = NO

# The DISABLE_INDEX tag can be used to turn on/off the condensed index at
# top of each HTML page. The value NO (the default) enables the index and
# the value YES disables it.

DISABLE_INDEX          = YES

# This tag can be used to set the number of enum values (range [1..20])
# that doxygen will group on one line in the generated HTML documentation.

ENUM_VALUES_PER_LINE   = 4

# If the GENERATE_TREEVIEW tag is set to YES, a side panel will be
# generated containing a tree-like index structure (just like the one that
# is generated for HTML Help). For this to work a browser that supports
# JavaScript, DHTML, CSS and frames is required (for instance Mozilla 1.0+,
# Netscape 6.0+, Internet explorer 5.0+, or Konqueror). Windows users are
# probably better off using the HTML help feature.

GENERATE_TREEVIEW      = NO

# If the treeview is enabled (see GENERATE_TREEVIEW) then this tag can be
# used to set the initial width (in pixels) of the frame in which the tree
# is shown.

TREEVIEW_WIDTH         = 250

#---------------------------------------------------------------------------
# configuration options related to the LaTeX output
#---------------------------------------------------------------------------

# If the GENERATE_LATEX tag is set to YES (the default) Doxygen will
# generate Latex output.

GENERATE_LATEX         = YES

# The LATEX_OUTPUT tag is used to specify where the LaTeX docs will be put.
# If a relative path is entered the value of OUTPUT_DIRECTORY will be
# put in front of it. If left blank `latex' will be used as the default path.

LATEX_OUTPUT           = latex

# The LATEX_CMD_NAME tag can be used to specify the LaTeX command name to be
# invoked. If left blank `latex' will be used as the default command name.

LATEX_CMD_NAME         = latex

# The MAKEINDEX_CMD_NAME tag can be used to specify the command name to
# generate index for LaTeX. If left blank `makeindex' will be used as the
# default command name.

MAKEINDEX_CMD_NAME     = makeindex

# If the COMPACT_LATEX tag is set to YES Doxygen generates more compact
# LaTeX documents. This may be useful for small projects and may help to
# save some trees in general.

COMPACT_LATEX          = NO

# The PAPER_TYPE tag can be used to set the paper type that is used
# by the printer. Possible values are: a4, a4wide, letter, legal and
# executive. If left blank a4wide will be used.

PAPER_TYPE             = letter

# The EXTRA_PACKAGES tag can be to specify one or more names of LaTeX
# packages that should be included in the LaTeX output.

EXTRA_PACKAGES         =

# The LATEX_HEADER tag can be used to specify a personal LaTeX header for
# the generated latex document. The header should contain everything until
# the first chapter. If it is left blank doxygen will generate a
# standard header. Notice: only use this tag if you know what you are doing!

LATEX_HEADER           =

# If the PDF_HYPERLINKS tag is set to YES, the LaTeX that is generated
# is prepared for conversion to pdf (using ps2pdf). The pdf file will
# contain links (just like the HTML output) instead of page references
# This makes the output suitable for online browsing using a pdf viewer.

PDF_HYPERLINKS         = YES

# If the USE_PDFLATEX tag is set to YES, pdflatex will be used instead of
# plain latex in the generated Makefile. Set this option to YES to get a
# higher quality PDF documentation.

USE_PDFLATEX           = YES

# If the LATEX_BATCHMODE tag is set to YES, doxygen will add the \\batchmode.
# command to the generated LaTeX files. This will instruct LaTeX to keep
# running if errors occur, instead of asking the user for help.
# This option is also used when generating formulas in HTML.

LATEX_BATCHMODE        = NO

# If LATEX_HIDE_INDICES is set to YES then doxygen will not
# include the index chapters (such as File Index, Compound Index, etc.)
# in the output.

LATEX_HIDE_INDICES     = YES

#---------------------------------------------------------------------------
# configuration options related to the RTF output
#---------------------------------------------------------------------------

# If the GENERATE_RTF tag is set to YES Doxygen will generate RTF output
# The RTF output is optimized for Word 97 and may not look very pretty with
# other RTF readers or editors.

GENERATE_RTF           = NO

# The RTF_OUTPUT tag is used to specify where the RTF docs will be put.
# If a relative path is entered the value of OUTPUT_DIRECTORY will be
# put in front of it. If left blank `rtf' will be used as the default path.

RTF_OUTPUT             = rtf

# If the COMPACT_RTF tag is set to YES Doxygen generates more compact
# RTF documents. This may be useful for small projects and may help to
# save some trees in general.

COMPACT_RTF            = NO

# If the RTF_HYPERLINKS tag is set to YES, the RTF that is generated
# will contain hyperlink fields. The RTF file will
# contain links (just like the HTML output) instead of page references.
# This makes the output suitable for online browsing using WORD or other
# programs which support those fields.
# Note: wordpad (write) and others do not support links.

RTF_HYPERLINKS         = NO

# Load stylesheet definitions from file. Syntax is similar to doxygen's
# config file, i.e. a series of assignments. You only have to provide
# replacements, missing definitions are set to their default value.

RTF_STYLESHEET_FILE    =

# Set optional variables used in the generation of an rtf document.
# Syntax is similar to doxygen's config file.

RTF_EXTENSIONS_FILE    =

#---------------------------------------------------------------------------
# configuration options related to the man page output
#---------------------------------------------------------------------------

# If the GENERATE_MAN tag is set to YES (the default) Doxygen will
# generate man pages

GENERATE_MAN           = NO

# The MAN_OUTPUT tag is used to specify where the man pages will be put.
# If a relative path is entered the value of OUTPUT_DIRECTORY will be
# put in front of it. If left blank `man' will be used as the default path.

MAN_OUTPUT             = man

# The MAN_EXTENSION tag determines the extension that is added to
# the generated man pages (default is the subroutine's section .3)

MAN_EXTENSION          = .3

# If the MAN_LINKS tag is set to YES and Doxygen generates man output,
# then it will generate one additional man file for each entity
# documented in the real man page(s). These additional files
# only source the real man page, but without them the man command
# would be unable to find the correct page. The default is NO.

MAN_LINKS              = NO

#---------------------------------------------------------------------------
# configuration options related to the XML output
#---------------------------------------------------------------------------

# If the GENERATE_XML tag is set to YES Doxygen will
# generate an XML file that captures the structure of
# the code including all documentation.

GENERATE_XML           = YES

# The XML_OUTPUT tag is used to specify where the XML pages will be put.
# If a relative path is entered the value of OUTPUT_DIRECTORY will be
# put in front of it. If left blank `xml' will be used as the default path.

XML_OUTPUT             = xml

# The XML_SCHEMA tag can be used to specify an XML schema,
# which can be used by a validating XML parser to check the
# syntax of the XML files.

XML_SCHEMA             =

# The XML_DTD tag can be used to specify an XML DTD,
# which can be used by a validating XML parser to check the
# syntax of the XML files.

XML_DTD                =

# If the XML_PROGRAMLISTING tag is set to YES Doxygen will
# dump the program listings (including syntax highlighting
# and cross-referencing information) to the XML output. Note that
# enabling this will significantly increase the size of the XML output.

XML_PROGRAMLISTING     = NO

#---------------------------------------------------------------------------
# configuration options for the AutoGen Definitions output
#---------------------------------------------------------------------------

# If the GENERATE_AUTOGEN_DEF tag is set to YES Doxygen will
# generate an AutoGen Definitions (see autogen.sf.net) file
# that captures the structure of the code including all
# documentation. Note that this feature is still experimental
# and incomplete at the moment.

GENERATE_AUTOGEN_DEF   = NO

#---------------------------------------------------------------------------
# configuration options related to the Perl module output
#---------------------------------------------------------------------------

# If the GENERATE_PERLMOD tag is set to YES Doxygen will
# generate a Perl module file that captures the structure of
# the code including all documentation. Note that this
# feature is still experimental and incomplete at the
# moment.

GENERATE_PERLMOD       = NO

# If the PERLMOD_LATEX tag is set to YES Doxygen will generate
# the necessary Makefile rules, Perl scripts and LaTeX code to be able
# to generate PDF and DVI output from the Perl module output.

PERLMOD_LATEX          = NO

# If the PERLMOD_PRETTY tag is set to YES the Perl module output will be
# nicely formatted so it can be parsed by a human reader.  This is useful
# if you want to understand what is going on.  On the other hand, if this
# tag is set to NO the size of the Perl module output will be much smaller
# and Perl will parse it just the same.

PERLMOD_PRETTY         = YES

# The names of the make variables in the generated doxyrules.make file
# are prefixed with the string contained in PERLMOD_MAKEVAR_PREFIX.
# This is useful so different doxyrules.make files included by the same
# Makefile don't overwrite each other's variables.

PERLMOD_MAKEVAR_PREFIX =

#---------------------------------------------------------------------------
# Configuration options related to the preprocessor
#---------------------------------------------------------------------------

# If the ENABLE_PREPROCESSING tag is set to YES (the default) Doxygen will
# evaluate all C-preprocessor directives found in the sources and include
# files.

ENABLE_PREPROCESSING   = YES

# If the MACRO_EXPANSION tag is set to YES Doxygen will expand all macro
# names in the source code. If set to NO (the default) only conditional
# compilation will be performed. Macro expansion can be done in a controlled
# way by setting EXPAND_ONLY_PREDEF to YES.

MACRO_EXPANSION        = YES

# If the EXPAND_ONLY_PREDEF and MACRO_EXPANSION tags are both set to YES
# then the macro expansion is limited to the macros specified with the
# PREDEFINED and EXPAND_AS_PREDEFINED tags.

EXPAND_ONLY_PREDEF     = YES

# If the SEARCH_INCLUDES tag is set to YES (the default) the includes files
# in the INCLUDE_PATH (see below) will be search if a #include is found.

SEARCH_INCLUDES        = YES

# The INCLUDE_PATH tag can be used to specify one or more directories that
# contain include files that are not input files but should be processed by
# the preprocessor.

INCLUDE_PATH           =

# You can use the INCLUDE_FILE_PATTERNS tag to specify one or more wildcard
# patterns (like *.h and *.hpp) to filter out the header-files in the
# directories. If left blank, the patterns specified with FILE_PATTERNS will
# be used.

INCLUDE_FILE_PATTERNS  =

# The PREDEFINED tag can be used to specify one or more macro names that
# are defined before the preprocessor is started (similar to the -D option of
# gcc). The argument of the tag is a list of macros of the form: name
# or name=definition (no spaces). If the definition and the = are
# omitted =1 is assumed. To prevent a macro definition from being
# undefined via #undef or recursively expanded use the := operator
# instead of the = operator.

PREDEFINED             = DOXYGEN __attribute__(x)=static

# If the MACRO_EXPANSION and EXPAND_ONLY_PREDEF tags are set to YES then
# this tag can be used to specify a list of macro names that should be expanded.
# The macro definition that is found in the sources will be used.
# Use the PREDEFINED tag if you want to use a different macro definition.

EXPAND_AS_DEFINED      = __attribute__

# If the SKIP_FUNCTION_MACROS tag is set to YES (the default) then
# doxygen's preprocessor will remove all function-like macros that are alone
# on a line, have an all uppercase name, and do not end with a semicolon. Such
# function macros are typically used for boiler-plate code, and will confuse
# the parser if not removed.

SKIP_FUNCTION_MACROS   = YES

#---------------------------------------------------------------------------
# Configuration::additions related to external references
#---------------------------------------------------------------------------

# The TAGFILES option can be used to specify one or more tagfiles.
# Optionally an initial location of the external documentation
# can be added for each tagfile. The format of a tag file without
# this location is as follows:
#   TAGFILES = file1 file2 ...
# Adding location for the tag files is done as follows:
#   TAGFILES = file1=loc1 "file2 = loc2" ...
# where "loc1" and "loc2" can be relative or absolute paths or
# URLs. If a location is present for each tag, the installdox tool
# does not have to be run to correct the links.
# Note that each tag file must have a unique name
# (where the name does NOT include the path)
# If a tag file is not located in the directory in which doxygen
# is run, you must also specify the path to the tagfile here.

TAGFILES               =

# When a file name is specified after GENERATE_TAGFILE, doxygen will create
# a tag file that is based on the input files it reads.

GENERATE_TAGFILE       =

# If the ALLEXTERNALS tag is set to YES all external classes will be listed
# in the class index. If set to NO only the inherited external classes
# will be listed.

ALLEXTERNALS           = NO

# If the EXTERNAL_GROUPS tag is set to YES all external groups will be listed
# in the modules index. If set to NO, only the current project's groups will
# be listed.

EXTERNAL_GROUPS        = YES

# The PERL_PATH should be the absolute path and name of the perl script
# interpreter (i.e. the result of `which perl').

PERL_PATH              = /usr/bin/perl

#---------------------------------------------------------------------------
# Configuration options related to the dot tool
#---------------------------------------------------------------------------

# If the CLASS_DIAGRAMS tag is set to YES (the default) Doxygen will
# generate a inheritance diagram (in HTML, RTF and LaTeX) for classes with base
# or super classes. Setting the tag to NO turns the diagrams off. Note that
# this option is superseded by the HAVE_DOT option below. This is only a
# fallback. It is recommended to install and use dot, since it yields more
# powerful graphs.

CLASS_DIAGRAMS         = YES

# If set to YES, the inheritance and collaboration graphs will hide
# inheritance and usage relations if the target is undocumented
# or is not a class.

HIDE_UNDOC_RELATIONS   = YES

# If you set the HAVE_DOT tag to YES then doxygen will assume the dot tool is
# available from the path. This tool is part of Graphviz, a graph visualization
# toolkit from AT&T and Lucent Bell Labs. The other options in this section
# have no effect if this option is set to NO (the default)

HAVE_DOT               = NO

# If the CLASS_GRAPH and HAVE_DOT tags are set to YES then doxygen
# will generate a graph for each documented class showing the direct and
# indirect inheritance relations. Setting this tag to YES will force the
# the CLASS_DIAGRAMS tag to NO.

CLASS_GRAPH            = YES

# If the COLLABORATION_GRAPH and HAVE_DOT tags are set to YES then doxygen
# will generate a graph for each documented class showing the direct and
# indirect implementation dependencies (inheritance, containment, and
# class references variables) of the class with other documented classes.

COLLABORATION_GRAPH    = YES

# If the GROUP_GRAPHS and HAVE_DOT tags are set to YES then doxygen
# will generate a graph for groups, showing the direct groups dependencies

GROUP_GRAPHS           = YES

# If the UML_LOOK tag is set to YES doxygen will generate inheritance and
# collaboration diagrams in a style similar to the OMG's Unified Modeling
# Language.

UML_LOOK               = NO

# If set to YES, the inheritance and collaboration graphs will show the
# relations between templates and their instances.

TEMPLATE_RELATIONS     = NO

# If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDE_GRAPH, and HAVE_DOT
# tags are set to YES then doxygen will generate a graph for each documented
# file showing the direct and indirect include dependencies of the file with
# other documented files.

INCLUDE_GRAPH          = YES

# If the ENABLE_PREPROCESSING, SEARCH_INCLUDES, INCLUDED_BY_GRAPH, and
# HAVE_DOT tags are set to YES then doxygen will generate a graph for each
# documented header file showing the documented files that directly or
# indirectly include this file.

INCLUDED_BY_GRAPH      = YES

# If the CALL_GRAPH and HAVE_DOT tags are set to YES then doxygen will
# generate a call dependency graph for every global function or class method.
# Note that enabling this option will significantly increase the time of a run.
# So in most cases it will be better to enable call graphs for selected
# functions only using the \callgraph command.

CALL_GRAPH             = NO

# If the GRAPHICAL_HIERARCHY and HAVE_DOT tags are set to YES then doxygen
# will graphical hierarchy of all classes instead of a textual one.

GRAPHICAL_HIERARCHY    = YES

# If the DIRECTORY_GRAPH, SHOW_DIRECTORIES and HAVE_DOT tags are set to YES
# then doxygen will show the dependencies a directory has on other directories
# in a graphical way. The dependency relations are determined by the #include
# relations between the files in the directories.

DIRECTORY_GRAPH        = YES

# The DOT_IMAGE_FORMAT tag can be used to set the image format of the images
# generated by dot. Possible values are png, jpg, or gif
# If left blank png will be used.

DOT_IMAGE_FORMAT       = png

# The tag DOT_PATH can be used to specify the path where the dot tool can be
# found. If left blank, it is assumed the dot tool can be found in the path.

DOT_PATH               =

# The DOTFILE_DIRS tag can be used to specify one or more directories that
# contain dot files that are included in the documentation (see the
# \dotfile command).

DOTFILE_DIRS           =

# The MAX_DOT_GRAPH_WIDTH tag can be used to set the maximum allowed width
# (in pixels) of the graphs generated by dot. If a graph becomes larger than
# this value, doxygen will try to truncate the graph, so that it fits within
# the specified constraint. Beware that most browsers cannot cope with very
# large images.

MAX_DOT_GRAPH_WIDTH    = 1024

# The MAX_DOT_GRAPH_HEIGHT tag can be used to set the maximum allows height
# (in pixels) of the graphs generated by dot. If a graph becomes larger than
# this value, doxygen will try to truncate the graph, so that it fits within
# the specified constraint. Beware that most browsers cannot cope with very
# large images.

MAX_DOT_GRAPH_HEIGHT   = 1024

# The MAX_DOT_GRAPH_DEPTH tag can be used to set the maximum depth of the
# graphs generated by dot. A depth value of 3 means that only nodes reachable
# from the root by following a path via at most 3 edges will be shown. Nodes
# that lay further from the root node will be omitted. Note that setting this
# option to 1 or 2 may greatly reduce the computation time needed for large
# code bases. Also note that a graph may be further truncated if the graph's
# image dimensions are not sufficient to fit the graph (see MAX_DOT_GRAPH_WIDTH
# and MAX_DOT_GRAPH_HEIGHT). If 0 is used for the depth value (the default),
# the graph is not depth-constrained.

MAX_DOT_GRAPH_DEPTH    = 0

# Set the DOT_TRANSPARENT tag to YES to generate images with a transparent
# background. This is disabled by default, which results in a white background.
# Warning: Depending on the platform used, enabling this option may lead to
# badly anti-aliased labels on the edges of a graph (i.e. they become hard to
# read).

DOT_TRANSPARENT        = NO

# Set the DOT_MULTI_TARGETS tag to YES allow dot to generate multiple output
# files in one run (i.e. multiple -o and -T options on the command line). This
# makes dot run faster, but since only newer versions of dot (>1.8.10)
# support this, this feature is disabled by default.

DOT_MULTI_TARGETS      = NO

# If the GENERATE_LEGEND tag is set to YES (the default) Doxygen will
# generate a legend page explaining the meaning of the various boxes and
# arrows in the dot generated graphs.

GENERATE_LEGEND        = YES

# If the DOT_CLEANUP tag is set to YES (the default) Doxygen will
# remove the intermediate dot files that are used to generate
# the various graphs.

DOT_CLEANUP            = YES

#---------------------------------------------------------------------------
# Configuration::additions related to the search engine
#---------------------------------------------------------------------------

# The SEARCHENGINE tag specifies whether or not a search engine should be
# used. If set to NO the values of all tags below this one will be ignored.

SEARCHENGINE           = NO