Project Summary
This project contains settings to disable the standard debug features in TI-RTOS.
Project Usage
This project is intended to be used by applications that need a “production” TI-RTOS configuration that does not include debug features. Multiple applications can use this project.
This project is the default configuration used by most of the SimpleLink examples. It was selected as the default to minimize code size.
Please refer to the TI-RTOS Kernel section in the SimpleLink MCU SDK User’s Guide for the details on how applications use this project.