/********************************************************************* * INCLUDES */ #include "ZComDef.h" #include "OSAL.h" #include "AF.h" #include "ZDApp.h" #include "ZDObject.h" #include "MT_SYS.h" #include "nwk_util.h" #include "zcl.h" #include "zcl_general.h" #include "zcl_ha.h" #include "zcl_ezmode.h" #include "zcl_diagnostic.h" #include "zcl_samplelight.h" #include "onboard.h" /* HAL */ #include "hal_lcd.h" //#include "hal_led.h" #include "hal_key.h" #if ( defined (ZGP_DEVICE_TARGET) || defined (ZGP_DEVICE_TARGETPLUS) \ || defined (ZGP_DEVICE_COMBO) || defined (ZGP_DEVICE_COMBO_MIN) ) #include "zgp_translationtable.h" #if (SUPPORTED_S_FEATURE(SUPP_ZGP_FEATURE_TRANSLATION_TABLE)) #define ZGP_AUTO_TT #endif #endif #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) #include "math.h" #include "hal_timer.h" #endif #include "NLMEDE.h" /********************************************************************* * MACROS */ /********************************************************************* * CONSTANTS */ #if (defined HAL_BOARD_ZLIGHT) #define LEVEL_MAX 0xFE #define LEVEL_MIN 0x0 #define GAMMA_VALUE 2 #define PWM_FULL_DUTY_CYCLE 1000 #elif (defined HAL_PWM) #define LEVEL_MAX 0xFE #define LEVEL_MIN 0x0 #define GAMMA_VALUE 2 #define PWM_FULL_DUTY_CYCLE 100 #endif /********************************************************************* * TYPEDEFS */ /********************************************************************* * GLOBAL VARIABLES */ byte zclSampleLight_TaskID; uint8 zclSampleLightSeqNum; /********************************************************************* * GLOBAL FUNCTIONS */ /********************************************************************* * LOCAL VARIABLES */ afAddrType_t zclSampleLight_DstAddr; #ifdef ZCL_EZMODE static void zclSampleLight_ProcessZDOMsgs( zdoIncomingMsg_t *pMsg ); static void zclSampleLight_EZModeCB( zlcEZMode_State_t state, zclEZMode_CBData_t *pData ); // register EZ-Mode with task information (timeout events, callback, etc...) static const zclEZMode_RegisterData_t zclSampleLight_RegisterEZModeData = { &zclSampleLight_TaskID, SAMPLELIGHT_EZMODE_NEXTSTATE_EVT, SAMPLELIGHT_EZMODE_TIMEOUT_EVT, &zclSampleLightSeqNum, zclSampleLight_EZModeCB }; #else uint16 bindingInClusters[] = { ZCL_CLUSTER_ID_GEN_ON_OFF #ifdef ZCL_LEVEL_CTRL , ZCL_CLUSTER_ID_GEN_LEVEL_CONTROL #endif }; #define ZCLSAMPLELIGHT_BINDINGLIST (sizeof(bindingInClusters) / sizeof(bindingInClusters[0])) #endif // ZCL_EZMODE // Test Endpoint to allow SYS_APP_MSGs static endPointDesc_t sampleLight_TestEp = { SAMPLELIGHT_ENDPOINT, &zclSampleLight_TaskID, (SimpleDescriptionFormat_t *)NULL, // No Simple description for this test endpoint (afNetworkLatencyReq_t)0 // No Network Latency req }; uint8 giLightScreenMode = LIGHT_MAINMODE; // display the main screen mode first uint8 gPermitDuration = 0; // permit joining default to disabled devStates_t zclSampleLight_NwkState = DEV_INIT; #if ZCL_LEVEL_CTRL uint8 zclSampleLight_WithOnOff; // set to TRUE if state machine should set light on/off uint8 zclSampleLight_NewLevel; // new level when done moving bool zclSampleLight_NewLevelUp; // is direction to new level up or down? int32 zclSampleLight_CurrentLevel32; // current level, fixed point (e.g. 192.456) int32 zclSampleLight_Rate32; // rate in units, fixed point (e.g. 16.123) uint8 zclSampleLight_LevelLastLevel; // to save the Current Level before the light was turned OFF #endif /********************************************************************* * LOCAL FUNCTIONS */ static void zclSampleLight_HandleKeys( byte shift, byte keys ); static void zclSampleLight_BasicResetCB( void ); static void zclSampleLight_IdentifyCB( zclIdentify_t *pCmd ); static void zclSampleLight_IdentifyQueryRspCB( zclIdentifyQueryRsp_t *pRsp ); static void zclSampleLight_OnOffCB( uint8 cmd ); static void zclSampleLight_ProcessIdentifyTimeChange( void ); #ifdef ZCL_LEVEL_CTRL static void zclSampleLight_LevelControlMoveToLevelCB( zclLCMoveToLevel_t *pCmd ); static void zclSampleLight_LevelControlMoveCB( zclLCMove_t *pCmd ); static void zclSampleLight_LevelControlStepCB( zclLCStep_t *pCmd ); static void zclSampleLight_LevelControlStopCB( void ); static void zclSampleLight_DefaultMove( void ); static uint32 zclSampleLight_TimeRateHelper( uint8 newLevel ); static uint16 zclSampleLight_GetTime ( uint8 level, uint16 time ); static void zclSampleLight_MoveBasedOnRate( uint8 newLevel, uint32 rate ); static void zclSampleLight_MoveBasedOnTime( uint8 newLevel, uint16 time ); static void zclSampleLight_AdjustLightLevel( void ); #endif // app display functions static void zclSampleLight_LcdDisplayUpdate( void ); #ifdef LCD_SUPPORTED static void zclSampleLight_LcdDisplayMainMode( void ); static void zclSampleLight_LcdDisplayHelpMode( void ); #endif static void zclSampleLight_DisplayLight( void ); #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) void zclSampleLight_UpdateLampLevel( uint8 level ); #endif // Functions to process ZCL Foundation incoming Command/Response messages static void zclSampleLight_ProcessIncomingMsg( zclIncomingMsg_t *msg ); #ifdef ZCL_READ static uint8 zclSampleLight_ProcessInReadRspCmd( zclIncomingMsg_t *pInMsg ); #endif #ifdef ZCL_WRITE static uint8 zclSampleLight_ProcessInWriteRspCmd( zclIncomingMsg_t *pInMsg ); #endif static uint8 zclSampleLight_ProcessInDefaultRspCmd( zclIncomingMsg_t *pInMsg ); #ifdef ZCL_DISCOVER static uint8 zclSampleLight_ProcessInDiscCmdsRspCmd( zclIncomingMsg_t *pInMsg ); static uint8 zclSampleLight_ProcessInDiscAttrsRspCmd( zclIncomingMsg_t *pInMsg ); static uint8 zclSampleLight_ProcessInDiscAttrsExtRspCmd( zclIncomingMsg_t *pInMsg ); #endif /********************************************************************* * STATUS STRINGS */ #ifdef LCD_SUPPORTED const char sDeviceName[] = " Sample Light"; const char sClearLine[] = " "; const char sSwLight[] = "SW1: ToggleLight"; // 16 chars max const char sSwEZMode[] = "SW2: EZ-Mode"; char sSwHelp[] = "SW5: Help "; // last character is * if NWK open const char sLightOn[] = " LIGHT ON "; const char sLightOff[] = " LIGHT OFF"; #if ZCL_LEVEL_CTRL char sLightLevel[] = " LEVEL ###"; // displays level 1-254 #endif #endif /********************************************************************* * ZCL General Profile Callback table */ static zclGeneral_AppCallbacks_t zclSampleLight_CmdCallbacks = { zclSampleLight_BasicResetCB, // Basic Cluster Reset command zclSampleLight_IdentifyCB, // Identify command #ifdef ZCL_EZMODE NULL, // Identify EZ-Mode Invoke command NULL, // Identify Update Commission State command #endif NULL, // Identify Trigger Effect command zclSampleLight_IdentifyQueryRspCB, // Identify Query Response command zclSampleLight_OnOffCB, // On/Off cluster commands NULL, // On/Off cluster enhanced command Off with Effect NULL, // On/Off cluster enhanced command On with Recall Global Scene NULL, // On/Off cluster enhanced command On with Timed Off #ifdef ZCL_LEVEL_CTRL zclSampleLight_LevelControlMoveToLevelCB, // Level Control Move to Level command zclSampleLight_LevelControlMoveCB, // Level Control Move command zclSampleLight_LevelControlStepCB, // Level Control Step command zclSampleLight_LevelControlStopCB, // Level Control Stop command #endif #ifdef ZCL_GROUPS NULL, // Group Response commands #endif #ifdef ZCL_SCENES NULL, // Scene Store Request command NULL, // Scene Recall Request command NULL, // Scene Response command #endif #ifdef ZCL_ALARMS NULL, // Alarm (Response) commands #endif #ifdef SE_UK_EXT NULL, // Get Event Log command NULL, // Publish Event Log command #endif NULL, // RSSI Location command NULL // RSSI Location Response command }; /********************************************************************* * @fn zclSampleLight_Init * * @brief Initialization function for the zclGeneral layer. * * @param none * * @return none */ //uint16 adc_ain2 = 0; #define DATA_PIN P0_5 #define forward P0_7 #define backward P0_6 #define pin P0_3 #define time 110 static int no = 0; #define PERIODIC_EVT 0x4000 #define PERIODIC_EVT2 0x0001 void zclSampleLight_Init( byte task_id ) { zclSampleLight_TaskID = task_id; osal_start_timerEx( zclSampleLight_TaskID, PERIODIC_EVT, 10 ); osal_start_timerEx( zclSampleLight_TaskID, PERIODIC_EVT2, 10 ); // Set destination address to indirect zclSampleLight_DstAddr.addrMode = (afAddrMode_t)AddrNotPresent; zclSampleLight_DstAddr.endPoint = 0; zclSampleLight_DstAddr.addr.shortAddr = 0; // This app is part of the Home Automation Profile zclHA_Init( &zclSampleLight_SimpleDesc ); // Register the ZCL General Cluster Library callback functions zclGeneral_RegisterCmdCallbacks( SAMPLELIGHT_ENDPOINT, &zclSampleLight_CmdCallbacks ); // Register the application's attribute list zcl_registerAttrList( SAMPLELIGHT_ENDPOINT, zclSampleLight_NumAttributes, zclSampleLight_Attrs ); // Register the Application to receive the unprocessed Foundation command/response messages zcl_registerForMsg( zclSampleLight_TaskID ); #ifdef ZCL_DISCOVER // Register the application's command list zcl_registerCmdList( SAMPLELIGHT_ENDPOINT, zclCmdsArraySize, zclSampleLight_Cmds ); #endif // Register for all key events - This app will handle all key events RegisterForKeys( zclSampleLight_TaskID ); // Register for a test endpoint afRegister( &sampleLight_TestEp ); #ifdef ZCL_EZMODE // Register EZ-Mode zcl_RegisterEZMode( &zclSampleLight_RegisterEZModeData ); // Register with the ZDO to receive Match Descriptor Responses ZDO_RegisterForZDOMsg(task_id, Match_Desc_rsp); #endif #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) HalTimer1Init( 0 ); halTimer1SetChannelDuty( WHITE_LED, 0 ); halTimer1SetChannelDuty( RED_LED, 0 ); halTimer1SetChannelDuty( BLUE_LED, 0 ); halTimer1SetChannelDuty( GREEN_LED, 0 ); // find if we are already on a network from NV_RESTORE uint8 state; NLME_GetRequest( nwkNwkState, 0, &state ); if ( state < NWK_ENDDEVICE ) { // Start EZMode on Start up to avoid button press osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_START_EZMODE_EVT, 500 ); } #if ZCL_LEVEL_CTRL zclSampleLight_DefaultMove(); #endif #endif // #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) #ifdef ZCL_DIAGNOSTIC // Register the application's callback function to read/write attribute data. // This is only required when the attribute data format is unknown to ZCL. zcl_registerReadWriteCB( SAMPLELIGHT_ENDPOINT, zclDiagnostic_ReadWriteAttrCB, NULL ); if ( zclDiagnostic_InitStats() == ZSuccess ) { // Here the user could start the timer to save Diagnostics to NV } #endif #ifdef LCD_SUPPORTED HalLcdWriteString ( (char *)sDeviceName, HAL_LCD_LINE_3 ); #endif // LCD_SUPPORTED #ifdef ZGP_AUTO_TT zgpTranslationTable_RegisterEP ( &zclSampleLight_SimpleDesc ); #endif ZDApp_ChangeState(DEV_NWK_DISC); // Restart scan for rejoin ZDApp_StartJoiningCycle(); osal_stop_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF ); osal_start_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF, zgDefaultRejoinScan ); /*P0SEL &= ~BV(3); P0DIR |= BV(3); pin = 1;*/ P0DIR |= 0x20; //P1DIR |= 0x3f; P0SEL &= ~BV(7); P0DIR |= BV(7); P0SEL &= ~BV(6); P0DIR |= BV(6); DATA_PIN = 0; forward = 0; backward = 1; for(int i=0; i #define KEYHOLD_EVT 0x0100 //define event for key hold int KeyPressCnt=0; uint16 adc_ain2=0; #define HAL_ADC_REF_125V 0x00 /* Internal 1.25V Reference */ #define HAL_ADC_DEC_064 0x00 /* Decimate by 64 : 8-bit resolution */ #define HAL_ADC_DEC_128 0x10 /* Decimate by 128 : 10-bit resolution */ #define HAL_ADC_DEC_512 0x30 /* Decimate by 512 : 14-bit resolution */ #define HAL_ADC_CHN_VDD3 0x0f /* Input channel: VDD/3 */ #define HAL_ADC_CHN_TEMP 0x0e /* Temperature sensor */ uint16 value_bat; uint32 next; halIntState_t intState; uint8 ret; #define TURNOFF_MOTOR_EVT 0x0400 uint16 zclSampleLight_event_loop( uint8 task_id, uint16 events ) { /*if( events & TURNOFF_MOTOR_EVT ) { forward = 0; backward = 0; DATA_PIN = 1; return (events ^ TURNOFF_MOTOR_EVT); } */ /*if ( events & KEYHOLD_EVT ) { if ( P2_0==1 ) { if (KeyPressCnt>50){ KeyPressCnt=0; extern void ZDApp_ResetTimerStart( uint16 delay ); zgWriteStartupOptions(ZG_STARTUP_SET, (ZCD_STARTOPT_DEFAULT_NETWORK_STATE | ZCD_STARTOPT_DEFAULT_CONFIG_STATE) ); //ZDApp_ResetTimerStart(100); ZDApp_ChangeState(DEV_NWK_DISC); // Restart scan for rejoin ZDApp_StartJoiningCycle(); osal_stop_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF ); osal_start_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF, zgDefaultRejoinScan ); } else{ KeyPressCnt++; osal_start_timerEx( zclSampleLight_TaskID, KEYHOLD_EVT, 100); ret=osal_start_timerEx( zclSampleLight_TaskID, KEYHOLD_EVT, 100); } } return ( events ^ KEYHOLD_EVT ); }*/ ////////////////////////////////////////////////////// /*if( events & PERIODIC_EVT2 ) { #ifdef ZCL_EZMODE { // Invoke EZ-Mode zclEZMode_InvokeData_t ezModeData; // Invoke EZ-Mode ezModeData.endpoint = SAMPLELIGHT_ENDPOINT; // endpoint on which to invoke EZ-Mode if ( (zclSampleLight_NwkState == DEV_ZB_COORD) || (zclSampleLight_NwkState == DEV_ROUTER) || (zclSampleLight_NwkState == DEV_END_DEVICE) ) { ezModeData.onNetwork = TRUE; // node is already on the network } else { ezModeData.onNetwork = FALSE; // node is not yet on the network } ezModeData.initiator = FALSE; // OnOffLight is a target ezModeData.numActiveOutClusters = 0; ezModeData.pActiveOutClusterIDs = NULL; ezModeData.numActiveInClusters = 0; ezModeData.pActiveOutClusterIDs = NULL; zcl_InvokeEZMode( &ezModeData ); } #endif // ZCL_EZMODE osal_start_timerEx( zclSampleLight_TaskID, PERIODIC_EVT2, 50000 ); return (events ^ PERIODIC_EVT2); }*/ ////////////////////////////////////////////////////////// if( events & PERIODIC_EVT ) { /*// Hold off interrupts. HAL_ENTER_CRITICAL_SECTION( intState ); // Get next time-out next = osal_next_timeout(); // Re-enable interrupts. HAL_EXIT_CRITICAL_SECTION( intState ); // Put the processor into sleep mode OSAL_SET_CPU_INTO_SLEEP( 50000 );*/ return (events ^ PERIODIC_EVT); } ////////////////////////////////////////////////////////// afIncomingMSGPacket_t *MSGpkt; (void)task_id; // Intentionally unreferenced parameter if ( events & SYS_EVENT_MSG ) { while ( (MSGpkt = (afIncomingMSGPacket_t *)osal_msg_receive( zclSampleLight_TaskID )) ) { switch ( MSGpkt->hdr.event ) { #ifdef ZCL_EZMODE case ZDO_CB_MSG: zclSampleLight_ProcessZDOMsgs( (zdoIncomingMsg_t *)MSGpkt ); break; #endif case ZCL_INCOMING_MSG: // Incoming ZCL Foundation command/response messages zclSampleLight_ProcessIncomingMsg( (zclIncomingMsg_t *)MSGpkt ); break; case KEY_CHANGE: zclSampleLight_HandleKeys( ((keyChange_t *)MSGpkt)->state, ((keyChange_t *)MSGpkt)->keys ); break; case ZDO_STATE_CHANGE: zclSampleLight_NwkState = (devStates_t)(MSGpkt->hdr.status); // now on the network if ( (zclSampleLight_NwkState == DEV_ZB_COORD) || (zclSampleLight_NwkState == DEV_ROUTER) || (zclSampleLight_NwkState == DEV_END_DEVICE) ) { giLightScreenMode = LIGHT_MAINMODE; zclSampleLight_LcdDisplayUpdate(); #ifdef ZCL_EZMODE zcl_EZModeAction( EZMODE_ACTION_NETWORK_STARTED, NULL ); #endif // ZCL_EZMODE } break; default: break; } // Release the memory osal_msg_deallocate( (uint8 *)MSGpkt ); } // return unprocessed events return (events ^ SYS_EVENT_MSG); } if ( events & SAMPLELIGHT_IDENTIFY_TIMEOUT_EVT ) { if ( zclSampleLight_IdentifyTime > 0 ) zclSampleLight_IdentifyTime--; zclSampleLight_ProcessIdentifyTimeChange(); return ( events ^ SAMPLELIGHT_IDENTIFY_TIMEOUT_EVT ); } if ( events & SAMPLELIGHT_MAIN_SCREEN_EVT ) { giLightScreenMode = LIGHT_MAINMODE; zclSampleLight_LcdDisplayUpdate(); return ( events ^ SAMPLELIGHT_MAIN_SCREEN_EVT ); } #ifdef ZCL_EZMODE #if (defined HAL_BOARD_ZLIGHT) // event to start EZMode on startup with a delay if ( events & SAMPLELIGHT_START_EZMODE_EVT ) { // Invoke EZ-Mode zclEZMode_InvokeData_t ezModeData; // Invoke EZ-Mode ezModeData.endpoint = SAMPLELIGHT_ENDPOINT; // endpoint on which to invoke EZ-Mode if ( (zclSampleLight_NwkState == DEV_ZB_COORD) || (zclSampleLight_NwkState == DEV_ROUTER) || (zclSampleLight_NwkState == DEV_END_DEVICE) ) { ezModeData.onNetwork = TRUE; // node is already on the network } else { ezModeData.onNetwork = FALSE; // node is not yet on the network } ezModeData.initiator = FALSE; // OnOffLight is a target ezModeData.numActiveOutClusters = 0; ezModeData.pActiveOutClusterIDs = NULL; ezModeData.numActiveInClusters = 0; ezModeData.pActiveOutClusterIDs = NULL; zcl_InvokeEZMode( &ezModeData ); return ( events ^ SAMPLELIGHT_START_EZMODE_EVT ); } #endif // #if (defined HAL_BOARD_ZLIGHT) // going on to next state if ( events & SAMPLELIGHT_EZMODE_NEXTSTATE_EVT ) { zcl_EZModeAction ( EZMODE_ACTION_PROCESS, NULL ); // going on to next state return ( events ^ SAMPLELIGHT_EZMODE_NEXTSTATE_EVT ); } // the overall EZMode timer expired, so we timed out if ( events & SAMPLELIGHT_EZMODE_TIMEOUT_EVT ) { zcl_EZModeAction ( EZMODE_ACTION_TIMED_OUT, NULL ); // EZ-Mode timed out return ( events ^ SAMPLELIGHT_EZMODE_TIMEOUT_EVT ); } #endif // ZLC_EZMODE #ifdef ZCL_LEVEL_CTRL if ( events & SAMPLELIGHT_LEVEL_CTRL_EVT ) { zclSampleLight_AdjustLightLevel(); return ( events ^ SAMPLELIGHT_LEVEL_CTRL_EVT ); } #endif // Discard unknown events return 0; } /********************************************************************* * @fn zclSampleLight_HandleKeys * * @brief Handles all key events for this device. * * @param shift - true if in shift/alt. * @param keys - bit field for key events. Valid entries: * HAL_KEY_SW_5 * HAL_KEY_SW_4 * HAL_KEY_SW_2 * HAL_KEY_SW_1 * * @return none */ static void zclSampleLight_HandleKeys( byte shift, byte keys ) { /*if ( (keys & HAL_KEY_SW_2) ) { forward = 0; backward = 0; DATA_PIN = 1; }*/ if ( keys & HAL_KEY_SW_6 ) { //osal_start_timerEx( zclSampleLight_TaskID, PERIODIC_EVT, 5000 ); /*ZDApp_ChangeState(DEV_NWK_DISC); // Restart scan for rejoin ZDApp_StartJoiningCycle(); osal_stop_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF ); osal_start_timerEx( ZDAppTaskID, ZDO_REJOIN_BACKOFF, zgDefaultRejoinScan );*/ /*osal_stop_timerEx( zclSampleLight_TaskID, TURNOFF_MOTOR_EVT); osal_start_timerEx( zclSampleLight_TaskID, TURNOFF_MOTOR_EVT, 5000); KeyPressCnt=0; osal_start_timerEx( zclSampleLight_TaskID, KEYHOLD_EVT, 100); // toggle local light immediately zclSampleLight_OnOff = zclSampleLight_OnOff ? LIGHT_OFF : LIGHT_ON;*/ } /*if ( keys & HAL_KEY_SW_3 ) { NLME_SendNetworkStatus( zclSampleLight_DstAddr.addr.shortAddr, NLME_GetShortAddr(), NWKSTAT_NONTREE_LINK_FAILURE, FALSE ); } if ( keys & HAL_KEY_SW_4 ) { giLightScreenMode = LIGHT_MAINMODE; if ( ( zclSampleLight_NwkState == DEV_ZB_COORD ) || ( zclSampleLight_NwkState == DEV_ROUTER ) ) { zAddrType_t tmpAddr; tmpAddr.addrMode = Addr16Bit; tmpAddr.addr.shortAddr = NLME_GetShortAddr(); // toggle permit join gPermitDuration = gPermitDuration ? 0 : 0xff; // Trust Center significance is always true ZDP_MgmtPermitJoinReq( &tmpAddr, gPermitDuration, TRUE, FALSE ); } } // Shift F5 does a Basic Reset (factory defaults) if ( shift && ( keys & HAL_KEY_SW_5 ) ) { zclSampleLight_BasicResetCB(); } else if ( keys & HAL_KEY_SW_5 ) { giLightScreenMode = giLightScreenMode ? LIGHT_MAINMODE : LIGHT_HELPMODE; }*/ // update the display, including the light zclSampleLight_LcdDisplayUpdate(); } /********************************************************************* * @fn zclSampleLight_LcdDisplayUpdate * * @brief Called to update the LCD display. * * @param none * * @return none */ void zclSampleLight_LcdDisplayUpdate( void ) { #ifdef LCD_SUPPORTED if ( giLightScreenMode == LIGHT_HELPMODE ) { zclSampleLight_LcdDisplayHelpMode(); } else { zclSampleLight_LcdDisplayMainMode(); } #endif zclReportCmd_t rptcmd; rptcmd.numAttr = 1; rptcmd.attrList[0].attrID = ATTRID_ON_OFF; rptcmd.attrList[0].dataType = ZCL_DATATYPE_BOOLEAN; rptcmd.attrList[0].attrData = (uint8*)&zclSampleLight_OnOff; // Set destination address to indirect zclSampleLight_DstAddr.addrMode = (afAddrMode_t)Addr16Bit; zclSampleLight_DstAddr.addr.shortAddr = 0; zclSampleLight_DstAddr.endPoint=1; zcl_SendReportCmd(SAMPLELIGHT_ENDPOINT,&zclSampleLight_DstAddr, ZCL_CLUSTER_ID_GEN_ON_OFF, &rptcmd, ZCL_FRAME_CLIENT_SERVER_DIR, false, 0 ); zclSampleLight_DisplayLight(); } #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) /********************************************************************* * @fn zclSampleLight_UpdateLampLevel * * @brief Update lamp level output with gamma compensation * * @param level * * @return none */ void zclSampleLight_UpdateLampLevel( uint8 level ) { uint16 gammaCorrectedLevel; // gamma correct the level gammaCorrectedLevel = (uint16) ( pow( ( (float)level / LEVEL_MAX ), (float)GAMMA_VALUE ) * (float)LEVEL_MAX); halTimer1SetChannelDuty(WHITE_LED, (uint16)(((uint32)gammaCorrectedLevel*PWM_FULL_DUTY_CYCLE)/LEVEL_MAX) ); } #endif /********************************************************************* * @fn zclSampleLight_DisplayLight * * @brief Displays current state of light on LED and also on main display if supported. * * @param none * * @return none */ static void zclSampleLight_DisplayLight( void ) { // set the LED1 based on light (on or off) if ( zclSampleLight_OnOff == LIGHT_ON & no == 0 ) { DATA_PIN = 0; forward = 0; backward = 1; /*for(int i=0; i= ATTR_LEVEL_MAX_LEVEL ) || ( zclSampleLight_LevelCurrentLevel == zclSampleLight_LevelOnLevel ) || ( ( zclSampleLight_LevelOnLevel == ATTR_LEVEL_ON_LEVEL_NO_EFFECT ) && ( zclSampleLight_LevelCurrentLevel == zclSampleLight_LevelLastLevel ) ) ) { HalLcdWriteString( (char *)sLightOn, HAL_LCD_LINE_2 ); } else // " LEVEL ###" { zclHA_uint8toa( zclSampleLight_LevelCurrentLevel, &sLightLevel[10] ); HalLcdWriteString( (char *)sLightLevel, HAL_LCD_LINE_2 ); } #else if ( zclSampleLight_OnOff ) { HalLcdWriteString( (char *)sLightOn, HAL_LCD_LINE_2 ); } else { HalLcdWriteString( (char *)sLightOff, HAL_LCD_LINE_2 ); } #endif // ZCL_LEVEL_CTRL } #endif // LCD_SUPPORTED } #ifdef LCD_SUPPORTED /********************************************************************* * @fn zclSampleLight_LcdDisplayMainMode * * @brief Called to display the main screen on the LCD. * * @param none * * @return none */ static void zclSampleLight_LcdDisplayMainMode( void ) { // display line 1 to indicate NWK status if ( zclSampleLight_NwkState == DEV_ZB_COORD ) { zclHA_LcdStatusLine1( ZCL_HA_STATUSLINE_ZC ); } else if ( zclSampleLight_NwkState == DEV_ROUTER ) { zclHA_LcdStatusLine1( ZCL_HA_STATUSLINE_ZR ); } else if ( zclSampleLight_NwkState == DEV_END_DEVICE ) { zclHA_LcdStatusLine1( ZCL_HA_STATUSLINE_ZED ); } // end of line 3 displays permit join status (*) if ( gPermitDuration ) { sSwHelp[15] = '*'; } else { sSwHelp[15] = ' '; } HalLcdWriteString( (char *)sSwHelp, HAL_LCD_LINE_3 ); } /********************************************************************* * @fn zclSampleLight_LcdDisplayHelpMode * * @brief Called to display the SW options on the LCD. * * @param none * * @return none */ static void zclSampleLight_LcdDisplayHelpMode( void ) { HalLcdWriteString( (char *)sSwLight, HAL_LCD_LINE_1 ); HalLcdWriteString( (char *)sSwEZMode, HAL_LCD_LINE_2 ); HalLcdWriteString( (char *)sSwHelp, HAL_LCD_LINE_3 ); } #endif // LCD_SUPPORTED /********************************************************************* * @fn zclSampleLight_ProcessIdentifyTimeChange * * @brief Called to process any change to the IdentifyTime attribute. * * @param none * * @return none */ static void zclSampleLight_ProcessIdentifyTimeChange( void ) { if ( zclSampleLight_IdentifyTime > 0 ) { osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_IDENTIFY_TIMEOUT_EVT, 1000 ); //HalLedBlink ( HAL_LED_4, 0xFF, HAL_LED_DEFAULT_DUTY_CYCLE, HAL_LED_DEFAULT_FLASH_TIME ); } else { #ifdef ZCL_EZMODE if ( zclSampleLight_IdentifyCommissionState & EZMODE_COMMISSION_OPERATIONAL ) { //HalLedSet ( HAL_LED_4, HAL_LED_MODE_ON ); } else { //HalLedSet ( HAL_LED_4, HAL_LED_MODE_OFF ); } #endif osal_stop_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_IDENTIFY_TIMEOUT_EVT ); } } /********************************************************************* * @fn zclSampleLight_BasicResetCB * * @brief Callback from the ZCL General Cluster Library * to set all the Basic Cluster attributes to default values. * * @param none * * @return none */ static void zclSampleLight_BasicResetCB( void ) { NLME_LeaveReq_t leaveReq; // Set every field to 0 osal_memset( &leaveReq, 0, sizeof( NLME_LeaveReq_t ) ); // This will enable the device to rejoin the network after reset. leaveReq.rejoin = TRUE; // Set the NV startup option to force a "new" join. zgWriteStartupOptions( ZG_STARTUP_SET, ZCD_STARTOPT_DEFAULT_NETWORK_STATE ); // Leave the network, and reset afterwards if ( NLME_LeaveReq( &leaveReq ) != ZSuccess ) { // Couldn't send out leave; prepare to reset anyway ZDApp_LeaveReset( FALSE ); } } /********************************************************************* * @fn zclSampleLight_IdentifyCB * * @brief Callback from the ZCL General Cluster Library when * it received an Identity Command for this application. * * @param srcAddr - source address and endpoint of the response message * @param identifyTime - the number of seconds to identify yourself * * @return none */ static void zclSampleLight_IdentifyCB( zclIdentify_t *pCmd ) { zclSampleLight_IdentifyTime = pCmd->identifyTime; zclSampleLight_ProcessIdentifyTimeChange(); } /********************************************************************* * @fn zclSampleLight_IdentifyQueryRspCB * * @brief Callback from the ZCL General Cluster Library when * it received an Identity Query Response Command for this application. * * @param srcAddr - requestor's address * @param timeout - number of seconds to identify yourself (valid for query response) * * @return none */ static void zclSampleLight_IdentifyQueryRspCB( zclIdentifyQueryRsp_t *pRsp ) { (void)pRsp; #ifdef ZCL_EZMODE { zclEZMode_ActionData_t data; data.pIdentifyQueryRsp = pRsp; zcl_EZModeAction ( EZMODE_ACTION_IDENTIFY_QUERY_RSP, &data ); } #endif } /********************************************************************* * @fn zclSampleLight_OnOffCB * * @brief Callback from the ZCL General Cluster Library when * it received an On/Off Command for this application. * * @param cmd - COMMAND_ON, COMMAND_OFF or COMMAND_TOGGLE * * @return none */ static void zclSampleLight_OnOffCB( uint8 cmd ) { afIncomingMSGPacket_t *pPtr = zcl_getRawAFMsg(); zclSampleLight_DstAddr.addr.shortAddr = pPtr->srcAddr.addr.shortAddr; // Turn on the light if ( cmd == COMMAND_ON ) { zclSampleLight_OnOff = LIGHT_ON; } // Turn off the light else if ( cmd == COMMAND_OFF ) { zclSampleLight_OnOff = LIGHT_OFF; } // Toggle the light else if ( cmd == COMMAND_TOGGLE ) { if ( zclSampleLight_OnOff == LIGHT_OFF ) { zclSampleLight_OnOff = LIGHT_ON; } else { zclSampleLight_OnOff = LIGHT_OFF; } } #if ZCL_LEVEL_CTRL zclSampleLight_DefaultMove( ); #endif // update the display zclSampleLight_LcdDisplayUpdate( ); } #ifdef ZCL_LEVEL_CTRL /********************************************************************* * @fn zclSampleLight_TimeRateHelper * * @brief Calculate time based on rate, and startup level state machine * * @param newLevel - new level for current level * * @return diff (directly), zclSampleLight_CurrentLevel32 and zclSampleLight_NewLevel, zclSampleLight_NewLevelUp */ static uint32 zclSampleLight_TimeRateHelper( uint8 newLevel ) { uint32 diff; uint32 newLevel32; // remember current and new level zclSampleLight_NewLevel = newLevel; zclSampleLight_CurrentLevel32 = (uint32)1000 * zclSampleLight_LevelCurrentLevel; // calculate diff newLevel32 = (uint32)1000 * newLevel; if ( zclSampleLight_LevelCurrentLevel > newLevel ) { diff = zclSampleLight_CurrentLevel32 - newLevel32; zclSampleLight_NewLevelUp = FALSE; // moving down } else { diff = newLevel32 - zclSampleLight_CurrentLevel32; zclSampleLight_NewLevelUp = TRUE; // moving up } return ( diff ); } /********************************************************************* * @fn zclSampleLight_MoveBasedOnRate * * @brief Calculate time based on rate, and startup level state machine * * @param newLevel - new level for current level * @param rate16 - fixed point rate (e.g. 16.123) * * @return none */ static void zclSampleLight_MoveBasedOnRate( uint8 newLevel, uint32 rate ) { uint32 diff; // determine how much time (in 10ths of seconds) based on the difference and rate zclSampleLight_Rate32 = rate; diff = zclSampleLight_TimeRateHelper( newLevel ); zclSampleLight_LevelRemainingTime = diff / rate; if ( !zclSampleLight_LevelRemainingTime ) { zclSampleLight_LevelRemainingTime = 1; } osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_LEVEL_CTRL_EVT, 100 ); } /********************************************************************* * @fn zclSampleLight_MoveBasedOnTime * * @brief Calculate rate based on time, and startup level state machine * * @param newLevel - new level for current level * @param time - in 10ths of seconds * * @return none */ static void zclSampleLight_MoveBasedOnTime( uint8 newLevel, uint16 time ) { uint16 diff; // determine rate (in units) based on difference and time diff = zclSampleLight_TimeRateHelper( newLevel ); zclSampleLight_LevelRemainingTime = zclSampleLight_GetTime( newLevel, time ); zclSampleLight_Rate32 = diff / time; osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_LEVEL_CTRL_EVT, 100 ); } /********************************************************************* * @fn zclSampleLight_GetTime * * @brief Determine amount of time that MoveXXX will take to complete. * * @param level = new level to move to * time = 0xffff=default, or 0x0000-n amount of time in tenths of seconds. * * @return none */ static uint16 zclSampleLight_GetTime( uint8 level, uint16 time ) { // there is a hiearchy of the amount of time to use for transistioning // check each one in turn. If none of defaults are set, then use fastest // time possible. if ( time == 0xFFFF ) { // use On or Off Transition Time if set (not 0xffff) if ( zclSampleLight_OnOff == LIGHT_ON ) { time = zclSampleLight_LevelOffTransitionTime; } else { time = zclSampleLight_LevelOnTransitionTime; } // else use OnOffTransitionTime if set (not 0xffff) if ( time == 0xFFFF ) { time = zclSampleLight_LevelOnOffTransitionTime; } // else as fast as possible if ( time == 0xFFFF ) { time = 1; } } if ( !time ) { time = 1; // as fast as possible } return ( time ); } /********************************************************************* * @fn zclSampleLight_DefaultMove * * @brief We were turned on/off. Use default time to move to on or off. * * @param zclSampleLight_OnOff - must be set prior to calling this function. * * @return none */ static void zclSampleLight_DefaultMove( void ) { uint8 newLevel; uint32 rate; // fixed point decimal (3 places, eg. 16.345) uint16 time; // if moving to on position, move to on level if ( zclSampleLight_OnOff ) { if ( zclSampleLight_LevelOnLevel == ATTR_LEVEL_ON_LEVEL_NO_EFFECT ) { // The last Level (before going OFF) should be used) newLevel = zclSampleLight_LevelLastLevel; } else { newLevel = zclSampleLight_LevelOnLevel; } time = zclSampleLight_LevelOnTransitionTime; } else { newLevel = ATTR_LEVEL_MIN_LEVEL; if ( zclSampleLight_LevelOnLevel == ATTR_LEVEL_ON_LEVEL_NO_EFFECT ) { // Save the current Level before going OFF to use it when the light turns ON // it should be back to this level zclSampleLight_LevelLastLevel = zclSampleLight_LevelCurrentLevel; } time = zclSampleLight_LevelOffTransitionTime; } // else use OnOffTransitionTime if set (not 0xffff) if ( time == 0xFFFF ) { time = zclSampleLight_LevelOnOffTransitionTime; } // else as fast as possible if ( time == 0xFFFF ) { time = 1; } // calculate rate based on time (int 10ths) for full transition (1-254) rate = 255000 / time; // units per tick, fixed point, 3 decimal places (e.g. 8500 = 8.5 units per tick) // start up state machine. zclSampleLight_WithOnOff = TRUE; zclSampleLight_MoveBasedOnRate( newLevel, rate ); } /********************************************************************* * @fn zclSampleLight_AdjustLightLevel * * @brief Called each 10th of a second while state machine running * * @param none * * @return none */ static void zclSampleLight_AdjustLightLevel( void ) { // one tick (10th of a second) less if ( zclSampleLight_LevelRemainingTime ) { --zclSampleLight_LevelRemainingTime; } // no time left, done if ( zclSampleLight_LevelRemainingTime == 0) { zclSampleLight_LevelCurrentLevel = zclSampleLight_NewLevel; } // still time left, keep increment/decrementing else { if ( zclSampleLight_NewLevelUp ) { zclSampleLight_CurrentLevel32 += zclSampleLight_Rate32; } else { zclSampleLight_CurrentLevel32 -= zclSampleLight_Rate32; } zclSampleLight_LevelCurrentLevel = (uint8)( zclSampleLight_CurrentLevel32 / 1000 ); } #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) zclSampleLight_UpdateLampLevel(zclSampleLight_LevelCurrentLevel); #endif // also affect on/off if ( zclSampleLight_WithOnOff ) { if ( zclSampleLight_LevelCurrentLevel > ATTR_LEVEL_MIN_LEVEL ) { zclSampleLight_OnOff = LIGHT_ON; #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) ENABLE_LAMP; #endif } else { zclSampleLight_OnOff = LIGHT_OFF; #if (defined HAL_BOARD_ZLIGHT) || (defined HAL_PWM) DISABLE_LAMP; #endif } } // display light level as we go zclSampleLight_DisplayLight( ); // keep ticking away if ( zclSampleLight_LevelRemainingTime ) { osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_LEVEL_CTRL_EVT, 100 ); } } /********************************************************************* * @fn zclSampleLight_LevelControlMoveToLevelCB * * @brief Callback from the ZCL General Cluster Library when * it received a LevelControlMoveToLevel Command for this application. * * @param pCmd - ZigBee command parameters * * @return none */ static void zclSampleLight_LevelControlMoveToLevelCB( zclLCMoveToLevel_t *pCmd ) { zclSampleLight_WithOnOff = pCmd->withOnOff; zclSampleLight_MoveBasedOnTime( pCmd->level, pCmd->transitionTime ); } /********************************************************************* * @fn zclSampleLight_LevelControlMoveCB * * @brief Callback from the ZCL General Cluster Library when * it received a LevelControlMove Command for this application. * * @param pCmd - ZigBee command parameters * * @return none */ static void zclSampleLight_LevelControlMoveCB( zclLCMove_t *pCmd ) { uint8 newLevel; uint32 rate; // convert rate from units per second to units per tick (10ths of seconds) // and move at that right up or down zclSampleLight_WithOnOff = pCmd->withOnOff; if ( pCmd->moveMode == LEVEL_MOVE_UP ) { newLevel = ATTR_LEVEL_MAX_LEVEL; // fully on } else { newLevel = ATTR_LEVEL_MIN_LEVEL; // fully off } rate = (uint32)100 * pCmd->rate; zclSampleLight_MoveBasedOnRate( newLevel, rate ); } /********************************************************************* * @fn zclSampleLight_LevelControlStepCB * * @brief Callback from the ZCL General Cluster Library when * it received an On/Off Command for this application. * * @param pCmd - ZigBee command parameters * * @return none */ static void zclSampleLight_LevelControlStepCB( zclLCStep_t *pCmd ) { uint8 newLevel; // determine new level, but don't exceed boundaries if ( pCmd->stepMode == LEVEL_MOVE_UP ) { if ( (uint16)zclSampleLight_LevelCurrentLevel + pCmd->amount > ATTR_LEVEL_MAX_LEVEL ) { newLevel = ATTR_LEVEL_MAX_LEVEL; } else { newLevel = zclSampleLight_LevelCurrentLevel + pCmd->amount; } } else { if ( pCmd->amount >= zclSampleLight_LevelCurrentLevel ) { newLevel = ATTR_LEVEL_MIN_LEVEL; } else { newLevel = zclSampleLight_LevelCurrentLevel - pCmd->amount; } } // move to the new level zclSampleLight_WithOnOff = pCmd->withOnOff; zclSampleLight_MoveBasedOnTime( newLevel, pCmd->transitionTime ); } /********************************************************************* * @fn zclSampleLight_LevelControlStopCB * * @brief Callback from the ZCL General Cluster Library when * it received an Level Control Stop Command for this application. * * @param pCmd - ZigBee command parameters * * @return none */ static void zclSampleLight_LevelControlStopCB( void ) { // stop immediately osal_stop_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_LEVEL_CTRL_EVT ); zclSampleLight_LevelRemainingTime = 0; } #endif /****************************************************************************** * * Functions for processing ZCL Foundation incoming Command/Response messages * *****************************************************************************/ /********************************************************************* * @fn zclSampleLight_ProcessIncomingMsg * * @brief Process ZCL Foundation incoming message * * @param pInMsg - pointer to the received message * * @return none */ static void zclSampleLight_ProcessIncomingMsg( zclIncomingMsg_t *pInMsg ) { switch ( pInMsg->zclHdr.commandID ) { #ifdef ZCL_READ case ZCL_CMD_READ_RSP: zclSampleLight_ProcessInReadRspCmd( pInMsg ); break; #endif #ifdef ZCL_WRITE case ZCL_CMD_WRITE_RSP: zclSampleLight_ProcessInWriteRspCmd( pInMsg ); break; #endif #ifdef ZCL_REPORT // Attribute Reporting implementation should be added here case ZCL_CMD_CONFIG_REPORT: // zclSampleLight_ProcessInConfigReportCmd( pInMsg ); break; case ZCL_CMD_CONFIG_REPORT_RSP: // zclSampleLight_ProcessInConfigReportRspCmd( pInMsg ); break; case ZCL_CMD_READ_REPORT_CFG: // zclSampleLight_ProcessInReadReportCfgCmd( pInMsg ); break; case ZCL_CMD_READ_REPORT_CFG_RSP: // zclSampleLight_ProcessInReadReportCfgRspCmd( pInMsg ); break; case ZCL_CMD_REPORT: // zclSampleLight_ProcessInReportCmd( pInMsg ); break; #endif case ZCL_CMD_DEFAULT_RSP: zclSampleLight_ProcessInDefaultRspCmd( pInMsg ); break; #ifdef ZCL_DISCOVER case ZCL_CMD_DISCOVER_CMDS_RECEIVED_RSP: zclSampleLight_ProcessInDiscCmdsRspCmd( pInMsg ); break; case ZCL_CMD_DISCOVER_CMDS_GEN_RSP: zclSampleLight_ProcessInDiscCmdsRspCmd( pInMsg ); break; case ZCL_CMD_DISCOVER_ATTRS_RSP: zclSampleLight_ProcessInDiscAttrsRspCmd( pInMsg ); break; case ZCL_CMD_DISCOVER_ATTRS_EXT_RSP: zclSampleLight_ProcessInDiscAttrsExtRspCmd( pInMsg ); break; #endif default: break; } if ( pInMsg->attrCmd ) osal_mem_free( pInMsg->attrCmd ); } #ifdef ZCL_READ /********************************************************************* * @fn zclSampleLight_ProcessInReadRspCmd * * @brief Process the "Profile" Read Response Command * * @param pInMsg - incoming message to process * * @return none */ static uint8 zclSampleLight_ProcessInReadRspCmd( zclIncomingMsg_t *pInMsg ) { zclReadRspCmd_t *readRspCmd; uint8 i; readRspCmd = (zclReadRspCmd_t *)pInMsg->attrCmd; for (i = 0; i < readRspCmd->numAttr; i++) { // Notify the originator of the results of the original read attributes // attempt and, for each successfull request, the value of the requested // attribute } return ( TRUE ); } #endif // ZCL_READ #ifdef ZCL_WRITE /********************************************************************* * @fn zclSampleLight_ProcessInWriteRspCmd * * @brief Process the "Profile" Write Response Command * * @param pInMsg - incoming message to process * * @return none */ static uint8 zclSampleLight_ProcessInWriteRspCmd( zclIncomingMsg_t *pInMsg ) { zclWriteRspCmd_t *writeRspCmd; uint8 i; writeRspCmd = (zclWriteRspCmd_t *)pInMsg->attrCmd; for ( i = 0; i < writeRspCmd->numAttr; i++ ) { // Notify the device of the results of the its original write attributes // command. } return ( TRUE ); } #endif // ZCL_WRITE /********************************************************************* * @fn zclSampleLight_ProcessInDefaultRspCmd * * @brief Process the "Profile" Default Response Command * * @param pInMsg - incoming message to process * * @return none */ static uint8 zclSampleLight_ProcessInDefaultRspCmd( zclIncomingMsg_t *pInMsg ) { // zclDefaultRspCmd_t *defaultRspCmd = (zclDefaultRspCmd_t *)pInMsg->attrCmd; // Device is notified of the Default Response command. (void)pInMsg; return ( TRUE ); } #ifdef ZCL_DISCOVER /********************************************************************* * @fn zclSampleLight_ProcessInDiscCmdsRspCmd * * @brief Process the Discover Commands Response Command * * @param pInMsg - incoming message to process * * @return none */ static uint8 zclSampleLight_ProcessInDiscCmdsRspCmd( zclIncomingMsg_t *pInMsg ) { zclDiscoverCmdsCmdRsp_t *discoverRspCmd; uint8 i; discoverRspCmd = (zclDiscoverCmdsCmdRsp_t *)pInMsg->attrCmd; for ( i = 0; i < discoverRspCmd->numCmd; i++ ) { // Device is notified of the result of its attribute discovery command. } return ( TRUE ); } /********************************************************************* * @fn zclSampleLight_ProcessInDiscAttrsRspCmd * * @brief Process the "Profile" Discover Attributes Response Command * * @param pInMsg - incoming message to process * * @return none */ static uint8 zclSampleLight_ProcessInDiscAttrsRspCmd( zclIncomingMsg_t *pInMsg ) { zclDiscoverAttrsRspCmd_t *discoverRspCmd; uint8 i; discoverRspCmd = (zclDiscoverAttrsRspCmd_t *)pInMsg->attrCmd; for ( i = 0; i < discoverRspCmd->numAttr; i++ ) { // Device is notified of the result of its attribute discovery command. } return ( TRUE ); } /********************************************************************* * @fn zclSampleLight_ProcessInDiscAttrsExtRspCmd * * @brief Process the "Profile" Discover Attributes Extended Response Command * * @param pInMsg - incoming message to process * * @return none */ static uint8 zclSampleLight_ProcessInDiscAttrsExtRspCmd( zclIncomingMsg_t *pInMsg ) { zclDiscoverAttrsExtRsp_t *discoverRspCmd; uint8 i; discoverRspCmd = (zclDiscoverAttrsExtRsp_t *)pInMsg->attrCmd; for ( i = 0; i < discoverRspCmd->numAttr; i++ ) { // Device is notified of the result of its attribute discovery command. } return ( TRUE ); } #endif // ZCL_DISCOVER #if ZCL_EZMODE /********************************************************************* * @fn zclSampleLight_ProcessZDOMsgs * * @brief Called when this node receives a ZDO/ZDP response. * * @param none * * @return status */ static void zclSampleLight_ProcessZDOMsgs( zdoIncomingMsg_t *pMsg ) { zclEZMode_ActionData_t data; ZDO_MatchDescRsp_t *pMatchDescRsp; // Let EZ-Mode know of the Simple Descriptor Response if ( pMsg->clusterID == Match_Desc_rsp ) { pMatchDescRsp = ZDO_ParseEPListRsp( pMsg ); data.pMatchDescRsp = pMatchDescRsp; zcl_EZModeAction( EZMODE_ACTION_MATCH_DESC_RSP, &data ); osal_mem_free( pMatchDescRsp ); } } /********************************************************************* * @fn zclSampleLight_EZModeCB * * @brief The Application is informed of events. This can be used to show on the UI what is * going on during EZ-Mode steering/finding/binding. * * @param state - an * * @return none */ static void zclSampleLight_EZModeCB( zlcEZMode_State_t state, zclEZMode_CBData_t *pData ) { #ifdef LCD_SUPPORTED char *pStr; uint8 err; #endif // time to go into identify mode if ( state == EZMODE_STATE_IDENTIFYING ) { #ifdef LCD_SUPPORTED HalLcdWriteString( "EZMode", HAL_LCD_LINE_2 ); #endif zclSampleLight_IdentifyTime = ( EZMODE_TIME / 1000 ); // convert to seconds zclSampleLight_ProcessIdentifyTimeChange(); } // autoclosing, show what happened (success, cancelled, etc...) if( state == EZMODE_STATE_AUTOCLOSE ) { #ifdef LCD_SUPPORTED pStr = NULL; err = pData->sAutoClose.err; if ( err == EZMODE_ERR_SUCCESS ) { pStr = "EZMode: Success"; } else if ( err == EZMODE_ERR_NOMATCH ) { pStr = "EZMode: NoMatch"; // not a match made in heaven } if ( pStr ) { if ( giLightScreenMode == LIGHT_MAINMODE ) { HalLcdWriteString ( pStr, HAL_LCD_LINE_2 ); } } #endif } // finished, either show DstAddr/EP, or nothing (depending on success or not) if( state == EZMODE_STATE_FINISH ) { // turn off identify mode zclSampleLight_IdentifyTime = 0; zclSampleLight_ProcessIdentifyTimeChange(); #ifdef LCD_SUPPORTED // if successful, inform user which nwkaddr/ep we bound to pStr = NULL; err = pData->sFinish.err; if( err == EZMODE_ERR_SUCCESS ) { // already stated on autoclose } else if ( err == EZMODE_ERR_CANCELLED ) { pStr = "EZMode: Cancel"; } else if ( err == EZMODE_ERR_BAD_PARAMETER ) { pStr = "EZMode: BadParm"; } else if ( err == EZMODE_ERR_TIMEDOUT ) { pStr = "EZMode: TimeOut"; } if ( pStr ) { if ( giLightScreenMode == LIGHT_MAINMODE ) { HalLcdWriteString ( pStr, HAL_LCD_LINE_2 ); } } #endif // show main UI screen 3 seconds after binding osal_start_timerEx( zclSampleLight_TaskID, SAMPLELIGHT_MAIN_SCREEN_EVT, 3000 ); } } #endif // ZCL_EZMODE /**************************************************************************** ****************************************************************************/