This is another sessin with the same device.

In the previous session, the device that joined did not make a "Device Announcement" after it received the Transport Link Key.

A good filter to start with is: frame.time_epoch >= 1593709799

The device makes a device announcement:
	17:10:00,156032	0x4ece	Broadcast	ZigBee ZDP	65	Device Announcement, Nwk Addr: 0x4ece, Ext Addr: Ember_00:11:61:86:52	3076

But it does not show up in the device list.

When the device reports some attributes that are also (partially) reported in the gateway report, they are reported to the application and associated with device "00:00:.....".
   

[2020-07-02T17:10:05]  Raw=17:00:53:22:08:22:12:0F:08:00:11:00:00:00:00:00:00:00:00:28:01:30:01:18:25:20:00
[2020-07-02T17:10:05] ===========> snsr_process_zone_status_change_ind: addr = 0,ep = 00000001,zonestatus = 00000025,extendedstatus = 00000000
[2020-07-02T17:10:05] attr_update_attribute_in_dev_table,IEEE=00:00:00:00:00:00:00:00 ep=01,clstr=0500
 vld=1, id=0002, tp=25, val=00000025
[2020-07-02T17:10:05] received from GATEWAY: len=12, cmd_id=21, subsystem=83
[2020-07-02T17:10:05]  Raw=0C:00:53:15:08:15:10:17:18:04:22:02:08:00:28:00
[2020-07-02T17:10:05] attr_process_read_attribute_response: Error: Status TIMEOUT - < type=0 >.
[2020-07-02T17:10:06] ###### EMIT commissioning_remaining((int)ds_network_status.permit_remaining_time) ######
[2020-07-02T17:10:06] received from GATEWAY: len=41, cmd_id=26, subsystem=83
[2020-07-02T17:10:06]  Raw=29:00:53:1A:08:1A:10:00:1A:0F:08:00:11:00:00:00:00:00:00:00:00:28:01:30:01:20:01:2A:07:08:20:10:20:1A:01:1C:2A:07:08:21:10:20:1A:01:96
[2020-07-02T17:10:06] attr_process_attribute_report_ind: Status SUCCESS.
[2020-07-02T17:10:06] addr=< type=0 ieeeaddr=00:00:00:00:00:00:00:00 endpointid=00000001 >, msg->n_attributerecordlist = 2
[2020-07-02T17:10:06] attr_id = -1280963515, , val=2000000020,attr_type = 1, len = -1246599224
[2020-07-02T17:10:06] attr_id = -1280963475, , val=2000000021,attr_type = 1, len = -1246599224
[2020-07-02T17:10:06] attr_update_attribute_in_dev_table,IEEE=00:00:00:00:00:00:00:00 ep=01,clstr=0001
 vld=1, id=0020, tp=32, val=78B5B21C
 vld=1, id=0021, tp=32, val=48B5B296