#! /bin/bash                                               
#
# script to start/stop zigbee gateway servers
#

export LINE="==================================================="

# NOTE: to turn on verbosity, set VERBOSE_GW_SCRIPT to something
# in the environment when starting this script

# for trap situation
killing_myself=0

# threshold that divides 'starting' from 'running' 
running_thresh_secs=5

# exit codes
ERROR_NO_TARGET=10
ERROR_BAD_TARGET=11

# this is used to do board-specific stuff that is not easily prarmaterized
BOARD_TYPE=unknown

VERBOSE=1
MERGE_OUTPUT=0

ZBEE_RESET_GPIO_LINE=

ZBEE_RESET_EXPLICIT_REVERSE=1
PROCESSOR_ZBEE_RESET_PIN=
ZBEE_SERIAL_PORT=/dev/ttymxc2
ignore_zbee_reset=0

if [ -n "$VERBOSE_GW_SCRIPT" ]; then
  if [ $VERBOSE_GW_SCRIPT -ge 1 ]; then
  	VERBOSE=$VERBOSE_GW_SCRIPT
  fi
fi

if [ "$MERGE_OUTPUT" = "" ]; then
	if [ $VERBOSE -ge 1 ]; then
		echo "defaulting output to merged, everything to console"
	fi
	MERGE_OUTPUT=1
fi

# UART baud rate settings
UART_BAUDRATE=115200 

# these are exit codes from network manager that we look for
# the network manager exit code determines how this script
# should behave when it exits, including how to call it when
# starting the servers up again

NWKMGR_SHUTDOWN_CODE=1
NWKMGR_SOFT_RESET_CODE=2
NWKMGR_HARD_RESET_CODE=3
NWKMGR_SLEEP_CODE=4
NWKMGR_WAKEUP_CODE=5
NWKMGR_OTHER_SERVER_DIED=666

# we redirect non netmgr server output to files
# so we can see what the hell is going on
NPI_OUT=/tmp/GW_SRVRS.out
ZLS_OUT=/tmp/GW_SRVRS.out
GWA_OUT=/tmp/GW_SRVRS.out
OTA_OUT=/tmp/GW_SRVRS.out
NWKMGR_OUT=/tmp/GW_SRVRS.out

/bin/rm -f $NPI_OUT $ZLS_OUT $GWA_OUT $OTA_OUT


# this is an optional flag passed to the network manager
# when this script re-starts it (it should be empty when
# started for the first time). This flag is set based on
# the exit code that network manager returns on exit.

NWKMGR_RESTART_FLAG=

# the following PIDs are recorded when the servers startup so 
# we can kill them later, but most importantly, get the exit
# code of the network manager. Strictly speaking the other
# PIDs aren't necessary since we do a killall based on the
# server name anyway

ZLSZNP_PID=0
GATEWAY_SERVER_PID=0
NETWORK_MGR_PID=0
NPI_PID=0
OTA_SERVER_PID=0
TRACKER_PID=0

# target is arm (eg, beaglebone), x86 (development machine),
# or unknown. As we get more target types we will have to
# use something more specific than a chip class as the target
# name!

TARGET=unknown

missing_files=0

check_exists()
{
	if [ ! -e $1 ]; then
		echo "file $1 $2 is missing"
		missing_files=$((missing_files + 1))
	fi
}

check_files()
{
	check_exists $NPI_NAME
	check_exists $NPI_CONFIG "(needed by $NPI_NAME)"
	check_exists $ZLSZNP_NAME
	check_exists $ZLSZNP_CONFIG "(needed by $ZLSZNP_NAME)"
	check_exists $GATEWAY_NAME
	check_exists $NWKMGR_NAME
	check_exists $OTA_SERVER_NAME

	if [ $missing_files -eq 0 ]; then
		return
	else
		echo "there are $missing_files missing files!"
		echo exiting $0
		exit 1
	fi
}

setup_for_arago()
{
	echo "running $0 on an ARM"
	export TARGET=arm

	export NPI_NAME=NPI_lnx_arago_server
	export NPI_CONFIG=NPI_Gateway.cfg
	export NPI_CMD="./$NPI_NAME $NPI_CONFIG"

	export ZLSZNP_NAME=ZLSZNP_arago
	export ZLSZNP_CONFIG=config.ini
	export ZLSZNP_CMD="./$ZLSZNP_NAME 127.0.0.1:2533 $ZLSZNP_CONFIG" 

	export GATEWAY_NAME=GATEWAY_SRVR_arago
	export GATEWAY_SERVER_CMD="./$GATEWAY_NAME 127.0.0.1:2536 127.0.0.1:2540"

	export NWKMGR_NAME=NWKMGR_SRVR_arago
	export NWKMGR_CMD="./$NWKMGR_NAME 127.0.0.1:2536"

	export OTA_SERVER_NAME=OTA_SRVR_arago
	export OTA_SERVER_CMD="./$OTA_SERVER_NAME 127.0.0.1:2536 127.0.0.1:2540"

	# busybox 'ps' doesn't take flags but seems equivalent to 'ps -e'
	export PS=ps

	export SOC_RESET_REQUIRED=1
}

setup_for_arm()
{
	echo "running $0 on an ARM"
	export TARGET=arm

	export NPI_NAME=NPI_lnx_arm_server

	export NPI_CONFIG=NPI_Gateway.cfg
	#export NPI_CMD="./$NPI_NAME $NPI_CONFIG -v 0x0000010E"
	export NPI_CMD="./$NPI_NAME $NPI_CONFIG -v 0xFFFFFFFF debugAll"
  # note: for less verbose output, remove '-v 0x0000010E' from the command above
  #       for more verbose output, replace 0x0000010E with 0xFFFFFFFF
  #       for even more verbose debug output, add 'debugAll' to the command above after 0xFFFFFFFF

	export ZLSZNP_NAME=ZLSZNP_arm
	export ZLSZNP_CONFIG=config.ini
	#export ZLSZNP_CMD="./$ZLSZNP_NAME 127.0.0.1:2533 $ZLSZNP_CONFIG -v 0x0000460E"
	export ZLSZNP_CMD="./$ZLSZNP_NAME 127.0.0.1:2533 $ZLSZNP_CONFIG -v 0xFFFFFFFF"
  # note: for less verbose output, remove '-v 0x0000460E' from the command above
  #       for more verbose output, replace 0x0000460E with 0xFFFFFFFF

	export GATEWAY_NAME=GATEWAY_SRVR_arm
	#export GATEWAY_SERVER_CMD="./$GATEWAY_NAME 127.0.0.1:2536 127.0.0.1:2540 -v 0x0000460E"
	export GATEWAY_SERVER_CMD="./$GATEWAY_NAME 127.0.0.1:2536 127.0.0.1:2540 -v 0xFFFFFFFF"
  # note: for less verbose output, remove '-v 0x0000460E' from the command above
  #       for more verbose output, replace 0x0000460E with 0xFFFFFFFF

	export NWKMGR_NAME=NWKMGR_SRVR_arm
	#export NWKMGR_CMD="./$NWKMGR_NAME 127.0.0.1:2536 -v 0x0000460E"
	export NWKMGR_CMD="./$NWKMGR_NAME 127.0.0.1:2536 -v 0xFFFFFFFF"
  # note: for less verbose output, remove '-v 0x0000460E' from the command above
  #       for more verbose output, replace 0x0000460E with 0xFFFFFFFF

	export OTA_SERVER_NAME=OTA_SRVR_arm
	#export OTA_SERVER_CMD="./$OTA_SERVER_NAME 127.0.0.1:2536 127.0.0.1:2540 -v 0x0000460E"
	export OTA_SERVER_CMD="./$OTA_SERVER_NAME 127.0.0.1:2536 127.0.0.1:2540 -v 0xFFFFFFFF"
  # note: for less verbose output, remove '-v 0x0000460E' from the command above
  #       for more verbose output, replace 0x0000460E with 0xFFFFFFFF

	# busybox 'ps' doesn't take flags but seems equivalent to 'ps -e'
	export PS=ps

	export SOC_RESET_REQUIRED=0
}

setup_for_x86()
{
	echo "running $0 on an x86"

	export TARGET=x86

	export NPI_NAME=NPI_lnx_x86_server
	export NPI_CONFIG=NPI_Gateway.cfg
	export NPI_CMD="./$NPI_NAME $NPI_CONFIG"
# -v 0x0000010E
# debugAll

	export ZLSZNP_NAME=ZLSZNP_x86
	export ZLSZNP_CONFIG=config.ini
	export ZLSZNP_CMD="./$ZLSZNP_NAME 127.0.0.1:2533 $ZLSZNP_CONFIG"
#-v 0x0000460E

	export GATEWAY_NAME=GATEWAY_SRVR_x86
	export GATEWAY_SERVER_CMD="./$GATEWAY_NAME 127.0.0.1:2536 127.0.0.1:2540"
#-v 0x0000460E

	export NWKMGR_NAME=NWKMGR_SRVR_x86
	export NWKMGR_CMD="./$NWKMGR_NAME 127.0.0.1:2536"
#-v 0x0000460E

	export OTA_SERVER_NAME=OTA_SRVR_x86
	export OTA_SERVER_CMD="./$OTA_SERVER_NAME 127.0.0.1:2536 127.0.0.1:2540"
#-v 0x0000460E

	export PS="ps -e"

	export SOC_RESET_REQUIRED=1
}

usage()
{
	echo -n "Usage: $0 [help "
	echo -n "| beaglebone | bbb "
	echo -n "| x86 ] "
	echo " "

	if [ "$1" != "" ]; then
		exit $1
	else
		exit 0
	fi
}

if [ $# -lt 1 ]; then

	if file `which ls` | grep -q 80386; then
		BOARD_TYPE=x86
	elif file `which ls` | grep -q x86; then
		BOARD_TYPE=x86
	else
		BOARD_TYPE=bbb
	fi
	echo Platform type selected automatically as $BOARD_TYPE.
	echo To override this selection, please stop this script, and then run it again, 
	echo specifying the desired platform type at the command line:
	echo "  $0 [help | bbb | x86 ]"
	echo

else

	export BOARD_TYPE=$1
fi

case "$BOARD_TYPE" in 

bbb | beaglebone)
	# beaglebone does some magic with the omap_mux
	# and as such an explicit reverse isn't needed
	ZBEE_RESET_EXPLICIT_REVERSE=0
	ZBEE_RESET_GPIO_LINE=77
	export ZBEE_SERIAL_PORT=/dev/ttymxc2
	setup_for_arm
	;;	
	
x86)
	export ZBEE_SERIAL_PORT=/dev/ttyACM0
	setup_for_x86
	;;	

help)
	usage
	;;

* )
	echo "I don't recognize target $BOARD_TYPE"
	usage $ERROR_BAD_TARGET
	;; 

esac



check_files


if [ $VERBOSE -ge 1 ]; then
	echo done processing arguments, board type $BOARD_TYPE, target $TARGET
	echo "NPI                 is '"$NPI_NAME"'"
	echo "Zstack linux server is '"$ZLSZNP_NAME"'"
	echo "gateway server      is '"$GATEWAY_NAME"'"
	echo "network manager     is '"$NWKMGR_NAME"'"
	echo "OTA server     	  is '"$OTA_SERVER_NAME"'"
fi

handle_znp_signal()
{
	#restore original signal handler
	LAST_STATUS=1
}

start_npi()
{

	if [ $VERBOSE -ge 1 ]; then
		echo $LINE
		echo "starting NPI, cmd '" $NPI_CMD "' on" `date`
	fi

	if [ $MERGE_OUTPUT -ge 1 ]; then 
		$NPI_CMD -p $$ -s $ZBEE_SERIAL_PORT&
	else
		$NPI_CMD -p $$ -s $ZBEE_SERIAL_PORT |& tee -a $NPI_OUT &
	fi
}

start_zlsznp()
{
	if [ $VERBOSE -ge 1 ]; then
		echo $LINE
		echo "starting ZLSZNP, cmd '" $ZLSZNP_CMD "' on" `date`
	fi

	if [ $MERGE_OUTPUT -ge 1 ]; then 
    		$ZLSZNP_CMD -p $$ & 
	else
    		$ZLSZNP_CMD -p $$ |& tee -a $ZLS_OUT &
	fi
}

start_gateway()
{
	if [ $VERBOSE -ge 1 ]; then
		echo $LINE
		echo "starting GATEWAY_SERVER, cmd '" $GATEWAY_SERVER_CMD "' on" `date`
	fi

	if [ $MERGE_OUTPUT -ge 1 ]; then 
    		$GATEWAY_SERVER_CMD -p $$ & 
	else
    		$GATEWAY_SERVER_CMD -p $$ |& tee -a $GWA_OUT &
	fi
}

start_netmgr()
{
	if [ $VERBOSE -ge 1 ]; then
		echo $LINE

		echo "starting NETWORK_MGR, cmd '" $NWKMGR_CMD $NWKMGR_RESTART_FLAG "' on" `date`
	fi
 
	if [ $MERGE_OUTPUT -ge 1 ]; then 
		$NWKMGR_CMD $NWKMGR_RESTART_FLAG -p $$ &
	else
		$NWKMGR_CMD $NWKMGR_RESTART_FLAG -p $$ |& tee -a $NWKMGR_OUT &
	fi
}


start_otaserver()
{
	if [ $VERBOSE -ge 1 ]; then
		echo $LINE
		echo "starting OTA_SERVER, cmd '"$OTA_SERVER_CMD "' on" `date`
	fi

	if [ $MERGE_OUTPUT -ge 1 ]; then 
    		$OTA_SERVER_CMD -p $$ & 
	else
    		$OTA_SERVER_CMD -p $$ |& tee -a $OTA_OUT &
	fi
}

start_tracker()
{
    # start a daemon (just a shell script) that sends us SIGUSR2
    # if anybody dies

    pids="$NPI_PID $ZLSZNP_PID $GATEWAY_SERVER_PID $OTA_SERVER_PID"

    # pass in our PID and a list of PIDs we care about
    echo starting tracker with our pid $0 and pid list $pids
    ./track_servers $$ "$pids" &

    export TRACKER_PID=$!
}

stop_tracker()
{
	if [ $TRACKER_PID != 0 ]; then
		kill -9 $TRACKER_PID
		wait $TRACKER_PID
		export TRACKER_PID=0
	fi
}

get_uptime()
{
	# note: this rounds down to nearest second
	export current_uptime=`cat /proc/uptime | awk -F"." '{print $1}'`
	export current_date="`date`"
}

start_all()                                                 
{                                                       
	echo "Starting the ZigBee gateway subsystem"

	export non_nwkmgr_died=0

	STARTUP_PHASE=1

	#save original signal handler
#	PREV_SIGUSR_TRAP=`trap -p SIGUSR1`
#	PREV_SIGUSR_TRAP=${PREV_SIGUSR_TRAP:9:${#PREV_SIGUSR_TRAP} - 18}  
	trap handle_znp_signal SIGUSR1 
	
	while [ $STARTUP_PHASE -lt 6 ]; do

		LAST_STATUS=0
	
		case $STARTUP_PHASE in
			1)
				#make sure no server is already running
				stop_all
                                                    
				#on some platforms it is more convinient not to reset the  SoC when trying to bring up the servers for the first time
				if [ $SOC_RESET_REQUIRED -ge 1 ]; then
					hw_reset_soc
				fi

				#a reset will be needed before we retry to being up the server after a bring-up failure
				SOC_RESET_REQUIRED=1
				
				start_npi
				SERVER_PID_VAR=NPI_PID
			;;
			2)
				start_zlsznp
				SERVER_PID_VAR=ZLSZNP_PID
			;;
			3)
				start_netmgr
				SERVER_PID_VAR=NETWORK_MGR_PID
			;;
			4)
				start_gateway
				SERVER_PID_VAR=GATEWAY_SERVER_PID
			;;
			5)
				start_otaserver
				SERVER_PID_VAR=OTA_SERVER_PID
			;;
		esac

		export LAST_PID=$!

		wait $LAST_PID

		if [ $LAST_STATUS -eq 0 ]; then
			echo Startup phase $STARTUP_PHASE failed
			STARTUP_PHASE=1
		else
			echo "Startup phase $STARTUP_PHASE completed successfully, server started ($SERVER_PID_VAR=$LAST_PID) on" `date`
			STARTUP_PHASE=$((STARTUP_PHASE + 1))
			eval $SERVER_PID_VAR=$LAST_PID
		fi
	done
	
#	trap $PREV_SIGUSR_TRAP SIGUSR1
	trap dump_status USR1 

	get_uptime
	export start_time=$current_uptime
	export start_date="$current_date"

	start_tracker

	echo $LINE
}                                                   

count_npi()
{
	export n_npi=`$PS | grep ${NPI_NAME:0:15} | grep -v grep | wc -l`
	if [ $VERBOSE -ge 2 ]; then
		echo n_npi is $n_npi
	fi
}

count_zls()
{
	export n_zls=`$PS | grep ${ZLSZNP_NAME:0:15} | grep -v grep | wc -l`
	if [ $VERBOSE -ge 2 ]; then
		echo n_zls is $n_zls
	fi
}

count_gtw()
{
	export n_gtw=`$PS | grep ${GATEWAY_NAME:0:15} | grep -v grep | wc -l`
	if [ $VERBOSE -ge 2 ]; then
		echo n_gtw is $n_gtw
	fi
}

count_nmg()
{
	export n_nmg=`$PS | grep ${NWKMGR_NAME:0:15} | grep -v grep | wc -l`
	if [ $VERBOSE -ge 2 ]; then
		echo n_nmg is $n_nmg
	fi
}

count_ota()
{
	export n_ota=`$PS | grep ${OTA_SERVER_NAME:0:15} | grep -v grep | wc -l`
	if [ $VERBOSE -ge 2 ]; then
		echo n_ota is $n_ota
	fi
}

count_offenders()
{

	count_npi
	count_zls
	count_gtw
	count_nmg
	count_ota

	export n_offenders=$(( $n_npi + $n_zls + $n_gtw + $n_nmg + $n_ota ))

	if [ $VERBOSE -ge 1 ]; then
		echo there are $n_npi NPI servers
		echo there are $n_zls ZLS servers
		echo there are $n_gtw GATEWAY servers
		echo there are $n_nmg NWKMGR servers
		echo there are $n_ota OTA servers
		echo "(total $n_offenders)"
	fi
}

make_sure_dead_dead_dead()
{
	if [ $VERBOSE -ge 1 ]; then
		echo making sure there are no lingering servers...
	fi

	count_offenders

	while [ $n_offenders -gt 0 ]; do

    		killall -s 9 $OTA_SERVER_NAME   2> /dev/null
    		killall -s 9 $GATEWAY_NAME	2> /dev/null
    		killall -s 9 $NWKMGR_NAME    	2> /dev/null
    		killall -s 9 $ZLSZNP_NAME    	2> /dev/null
    		killall -s 9 $NPI_NAME     	2> /dev/null

		count_offenders 

		if [ $n_offenders -gt 0 ]; then
			sleep 1
		fi

	done

	if [ $VERBOSE -ge 1 ]; then
		echo done
	fi

	sleep 1
}

stop_gateway()
{
	if [ $GATEWAY_SERVER_PID -ne 0 ]; then
    		killall $GATEWAY_NAME                  
		if [ $VERBOSE -ge 1 ]; then
			echo waiting for GATEWAY SERVER to exit
		fi

		wait $GATEWAY_SERVER_PID

		export GATEWAY_SERVER_PID=0

		# gawd I hate this sleep!
		sleep 5
	fi
}

stop_ota()
{
	if [ $OTA_SERVER_PID -ne 0 ]; then
		killall $OTA_SERVER_NAME                  
		if [ $VERBOSE -ge 1 ]; then
			echo waiting for OTA SERVER to exit
		fi

		wait $OTA_SERVER_PID
		export OTA_SERVER_PID=0
	fi
}

stop_zlsznp()
{
	if [ $ZLSZNP_PID -ne 0 ]; then
    		# kill zstack                                   
    		killall $ZLSZNP_NAME

		if [ $VERBOSE -ge 1 ]; then
			echo waiting for Zstack linux to exit
		fi

		wait $ZLSZNP_PID
		export ZLSZNP_PID=0
	fi
}

stop_npi()
{
	if [ $NPI_PID -ne 0 ]; then
    		# kill NPI                                  
    		killall $NPI_NAME        
		if [ $VERBOSE -ge 1 ]; then
			echo waiting for NPI to exit
		fi

		wait $NPI_PID
		export NPI_PID=0
	fi
}

stop_others()                                              
{                                                   
	stop_gateway
	stop_ota
	stop_zlsznp
	stop_npi                                                    
}                                                   

stop_nwkmgr()
{
	if [ $NETWORK_MGR_PID -ne 0 ]; then
		killall $NWKMGR_NAME
		wait $NETWORK_MGR_PID
		export NETWORK_MGR_PID=0
	fi
}

stop_all()
{
	stop_tracker
	stop_nwkmgr
	stop_others

    	# just to be completely anal...
	make_sure_dead_dead_dead
}

show_servers()
{
	echo here are the running servers:
	echo =============================
	$PS | grep $NPI_NAME | grep -v grep 
	$PS | grep $GATEWAY_NAME | grep -v grep 
	$PS | grep $ZLSZNP_NAME | grep -v grep 
	$PS | grep $NWKMGR_NAME | grep -v grep
	$PS | grep $OTA_SERVER_NAME | grep -v grep
	echo ======================================================
}

report()
{
	netpids=`$PS | grep zigbeenet.sh | grep -v grep | awk '{ print $1 }'`
	         $PS | grep zigbeenet.sh | grep -v grep | awk '{ print $1 }'

	echo zigbeennet.sh appears to have pid $netpids
	echo kill -$1 $netpids
	     kill -$1 $netpids
} 

dump_status()
{
	echo "I got a SIGUSR1 (asked to dump status)"
	show_servers > /tmp/hagw.servers

	status_stopped=USR2
	status_started=CONT
	status_running=USR1

	OLD_VERBOSE=$VERBOSE
	VERBOSE=2
	count_npi
	case $n_npi in
	0 )
		echo n_npi is 0, reporting stopped
		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;

	1)	# this is the normal case
		;;
	*)
		echo "there are $n_npi $NPI_NAME processes running!"
    		killall -9 $NPI_NAME        
		echo "not any more!"
  		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;
	esac

	count_zls
	case $n_zls in
	0 )
		echo n_zls is 0, reporting stopped
		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;

	1)	# this is the normal case
		;;
	*)
		echo "there are $n_zls $ZLSZNP_NAME processes running!"
    		killall -9 $ZLSZNP_NAME        
		echo "not any more!"
  		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;
	esac

	count_gtw
	case $n_gtw in
	0 )
		echo n_gtw is 0, reporting stopped
		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;

	1)	# this is the normal case
		;;
	*)
		echo "there are $n_zls $GATEWAY_NAME processes running!"
    		killall -9 $GATEWAY_NAME        
		echo "not any more!"
  		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;
	esac

	count_nmg
	case $n_nmg in
	0 )
		echo n_nmg is 0, reporting stopped
		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;

	1)	# this is the normal case
		;;
	*)
		echo "there are $n_nmg $NWKMGR_NAME processes running!"
    		killall -9 $NWKMGR_NAME        
		echo "not any more!"
  		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;
	esac

	count_ota
	case $n_ota in
	0 )
		echo n_ota is 0, reporting stopped
		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;

	1)	# this is the normal case
		;;
	*)
		echo "there are $n_zls $OTA_SERVER_NAME processes running!"
    		killall -9 $OTA_SERVER_NAME        
		echo "not any more!"
  		report $status_stopped
		VERBOSE=$OLD_VERBOSE
		return
		;;
	esac

	# if here, all expected servers are running, the
	# only question is how long
	
	echo "all servers are present (and no extras!)"
	get_uptime
	echo current_uptime is $current_uptime
	echo start_time is $start_time

	secs_running=$(( current_uptime - start_time ))
	echo servers have been running for $secs_running
	echo servers have been running since $start_date
	echo "running since $start_date ($secs_running secs)" > /tmp/tihagw.start

	if [ $secs_running -ge $running_thresh_secs ]; then
		echo reporting RUNNING since $start_date
		report $status_running
	else
		echo reporting STARTED at $start_date
		report $status_started
	fi
	echo exiting dump_status
}

clean_up()
{
	echo caught SIGTERM, killing all the servers and cleaning up

	# prevent myself from restarting stuff  when NWKMGR exits
	export killing_myself=1

	# kill everybody including network manager
	stop_all

	# now to kill myself
	echo "terminating zigbeeHAGW (pid $$)"
	kill -9 $$
	echo "am I still alive? that would be disconcerting..."
}

other_server_died()
{
	# track_servers sent us a SIGUSR2, indicating somebody
	# other than NWKMGR died

	export non_nwkmgr_died=1

	echo "caught SIGUSR2, a server other than NWKMGR died!"

	# allow myself to restart when NWKMGR exits
	export killing_myself=0

	# kill everybody besides network manager
	stop_others

	# now kill NWKMGR. this should cause us to fall out
	# of the 'wait'. because non_nwkmgr_died=1, we will
	# do a HW reset and restart the world with no special
	# flag passed to NWKMGR

	killall $NWKMGR_NAME
}

device_exported()
{
	if [ $# -ne 1 ]; then
		echo device_exported called without required argument
		exit 1
	fi

	GPIO_LINE=$1

	if [ -e  /sys/class/gpio/"gpio$GPIO_LINE" ]; then
		# echo device is exported
		return 1;
	else
		# echo device is not exported
		return 0;
	fi
}

hw_reset_soc()
{
	# before calling this function, make sure that the NPI server is not running.
	# if we reset the HW while NPI is running it can potentially
	# hold on to /dev/ttyXXX0 so that when we restart things, we
	# will get /dev/ttyXXX1 instead. 

	if [ $ignore_zbee_reset -eq 1 ]; then
		echo "skipping zigbee reset"
		return
	fi
	
	SCRIPTS_COUNT=0
	if [ -a ../tools/soc_reset_hold ]; then
		if [ -x ../tools/soc_reset_hold ]; then
			SCRIPTS_COUNT=$((SCRIPTS_COUNT + 1))
		else
			echo ../tools/soc_reset_hold exist but does not have execution permission
		fi
	fi
	if [ -a ../tools/soc_reset_release ]; then
		if [ -x ../tools/soc_reset_release ]; then
			SCRIPTS_COUNT=$((SCRIPTS_COUNT + 1))
		else
			echo ../tools/soc_reset_release exist but does not have execution permission
		fi
	fi
	if [ $SCRIPTS_COUNT -eq 2 ]; then
		echo Executing reset from external scripts
		#sh ../tools/soc_reset_hold
		#sh ../tools/soc_reset_release
	else
		case "$BOARD_TYPE" in

		bbb | beaglebone)

			echo "resetting ZigBee SoC"

			../tools/usbreset.bin
			while [ ! -e $ZBEE_SERIAL_PORT ]; do
				sleep 1
			done
			;;

		x86)
			echo ""
			echo "***************************************************************"
			echo ""
			if [ -e $ZBEE_SERIAL_PORT ]; then
				echo "Please unplug the ZigBee USB dongle ("$ZBEE_SERIAL_PORT") to continue..."
				while [ -e $ZBEE_SERIAL_PORT ]; do
					sleep 1
				done
			fi
			echo "Please wait..."
			sleep 2
			echo Please plug in the ZigBee USB dongle to continue...
			while [ ! -e $ZBEE_SERIAL_PORT ]; do
				sleep 1
			done
			echo "Please wait..."
			sleep 5
			;;	

		* )
			echo "I don't recognize target $BOARD_TYPE"
			usage $ERROR_BAD_TARGET
			;; 

		esac
	fi
}

# if we get a signal, kill all the servers and rm /tmp files
# and do other cleanup as needed
trap clean_up HUP INT TERM
trap other_server_died USR2 

# start all the servers in a reasonable order
start_all

while [ 1 ]                                         
do                                                  
	if [ $VERBOSE -ge 2 ]; then
		echo $LINE
		show_servers
	fi
	if [ $VERBOSE -ge 1 ]; then
	    echo waiting for netmgr to exit "(" pid $NETWORK_MGR_PID ") on" `date`
	fi

	wait $NETWORK_MGR_PID
	exit_code=$?

	# before I forget...
	NETWORK_MGR_PID=0

	if [ $exit_code -eq 127 ]; then
	    echo "oops! Network manager has already exited (!) on" `date`
	else
	    echo "NETWORK MANAGER exited with code $exit_code on" `date`
	fi
	
	if [ $killing_myself -eq 1 ]; then
		echo I am killing myself will not take further action
		break;
	fi


	# in all circumstances we stop all the daemons
	# NWKMGR should already be dead but call stop_all
	# just to make sure we get everybody

	stop_all

	# wipe the restart code clean until we know what we are doing
    	export NWKMGR_RESTART_FLAG=

	# if we are shutting down, that's all we do
	if [ $exit_code -eq $NWKMGR_SHUTDOWN_CODE ]; then 
		echo got SHUTDOWN from network manager, bailing out
		break
	fi

	# in all other cases we will restart the network manager
	# with a code that reflects what he gave us when exiting
	# we may also reset the hardware

	if [ $non_nwkmgr_died -eq 1 ]; then

		# if another network server died, we don't really
		# care how NWKMGR exited. We will stop everybody
		# and do a HW reset and then restart everybody
		echo "a server besides NWKMGR has exited!"
		echo "ignoring exit code $exit_code from netmgr"

		# both of these have already been done elsewhere
		# but let's be anal.
    		export NWKMGR_RESTART_FLAG=
		stop_all

		# make sure HW is ok, at least in theory...

		# note: hw_reset_soc should do any necessary waiting
		# so the device can be immediately used when it returns

		# now restart everybody
		start_all

		# and here we go again!
		continue
	fi

	case $exit_code in 

	$NWKMGR_SOFT_RESET_CODE )
    		export NWKMGR_RESTART_FLAG=--reset_soft
		start_all
		;;

	$NWKMGR_HARD_RESET_CODE )
		export NWKMGR_RESTART_FLAG=--reset_hard
		start_all
		;;

	$NWKMGR_SLEEP_CODE )
		# when sleeping we ONLY restart netmgr
    		export NWKMGR_RESTART_FLAG=--sleep
    		start_netmgr
		;; 

	$NWKMGR_WAKEUP_CODE)
    		export NWKMGR_RESTART_FLAG=--wakeup
		start_all
		;; 

	* )
		echo "unexpected exit code ($exit_code) from netmgr!"
    		export NWKMGR_RESTART_FLAG=
		start_all
		;;

	esac

done             

echo $0 exiting