CC1352P SimpleLink LaunchPad Settings & Resources
The CC1352P LaunchPad consists of a LaunchPad board with a CC1352P device.
Jumper Settings
- For any examples that use LEDs, make sure the LED’s jumper settings are closed.
Board resources used in driver examples:
The following table lists the Board names of the resources used by the driver examples, and their corresponding pins. Note that there may be other resources configured in the board files that are not used by any driver example. Only the example resources are listed in the table.
Board Resource | Pin |
---|---|
Board_ADC0 |
DIO23 |
Board_ADC1 |
DIO24 |
Board_ADCBUF0CHANNEL0 |
DIO23 |
Board_GPIO_BUTTON0 |
DIO15 |
Board_GPIO_BUTTON1 |
DIO14 |
Board_GPIO_LED0 |
DIO6 (Red - must be jumpered) |
Board_GPIO_LED1 |
DIO7 (Green - must be jumpered) |
Board_I2C_TMP |
DIO22 - SCL , DIO5 - SDA |
Board_PIN_LED0 |
DIO6 (Red - must be jumpered) |
Board_PIN_LED1 |
DIO7 (Green - must be jumpered) |
Board_PIN_LED2 |
DIO6 (Red - must be jumpered) |
Board_PIN_BUTTON0 |
DIO13 |
Board_PIN_BUTTON1 |
DIO14 |
Board_PWM0 |
DIO6 |
Board_PWM1 |
DIO7 |
Board_SD0 |
DIO8 - MISO , DIO9 - MOSI , DIO10 - CLK , DIO21 - CS |
Board_SPI0 |
DIO8 - MISO , DIO9 - MOSI , DIO10 - CLK |
Board_SPI_MASTER |
DIO8 - MISO , DIO9 - MOSI , DIO10 - CLK |
Board_SPI_SLAVE |
DIO8 - MISO , DIO9 - MOSI , DIO10 - CLK |
Board_SPI_MASTER_READY |
DIO15 |
Board_SPI_SLAVE_READY |
DIO21 |
Board_UART0 |
DIO12 - RX , DIO13 - TX |
BoosterPacks
The following examples require BoosterPacks.
Example | Booster Pack |
---|---|
display | BOOSTXL-SHARP128 LCD & SDCard BoosterPack |
i2ctmp007 | BOOSTXL-SENSORS Sensors BoosterPack |
portable | BOOSTXL-SENSORS Sensors BoosterPack |
sdraw | BOOSTXL-SHARP128 LCD & SDCard BoosterPack |
Display Sharp BoosterPack Modifications
Jumper wire the following on the back of the LaunchPad:
J1.5
toDIO19
microSD Card BoosterPack Modifications
Jumper wire the following on the back of the LaunchPad:
J1.8
toDIO19
Peripherals Used
The following list shows which CC1352P_2_LAUNCHXL peripherals are used by driver and kernel applications. Driver examples control which peripherals (and which ports) are used.
- TI-RTOS Kernel (SYS/BIOS)
- Uses the CC13xx’s RTC timer and that timer’s associated interrupts. The TI-RTOS Kernel manages the Interrupt Vector Table.
- TI-RTOS Drivers
- ADC: A CC13xx/CC26xx specific driver that uses the onboard ADC peripheral.
- Crypto: A CC13xx/CC26xx specific driver that uses the onboard AES Crypto processor.
- GPIO: The GPIO driver is used in various examples to drive
BOARD_GPIO_LED0
, and to monitor theBOARD_GPIO_BUTTON0
andBOARD_GPIO_BUTTON1
buttons. - I2C: The I2C driver is used to manage the
Board_I2C0
I2C instance. - NVS: The
Board_NVSINTERNAL
region uses on-chip flash memory. This NVS region is defined in the example application’s board file. - NVS SPI: The
Board_NVSEXTERNAL
region uses off-chip SPI flash memory. This NVS region is defined in the example application’s board file. - PIN: A CC13xx/CC26xx specific driver PIN driver that uses 2 output pins for the onboard
BOARD_PIN_LED0
andBOARD_PIN_LED1
and 2 input pins for buttonsBoard_PIN_BUTTON0
andBoard_PIN_BUTTON1
. - RF: The RF driver uses the on-chip radio module on CC13xx devices.
- SD: The SD driver is built on the GPIO and SPI drivers to communicate with an SD card via SPI.
Board_SD0
usesBoard_SPI0
to send data to-and-from the SD card. - SPI: The SPI driver uses SPI0 for
Board_SPI0
SPI instance. - UART: The UART driver uses UART0, which is attached to the onboard emulator to facilitate serial communications.
- Watchdog: The Watchdog driver example uses the Watchdog Timer WDT peripheral (
Board_WATCHDOG0
).