#include uint8_t t = 0; void setup() { Wire.begin(4); // join i2c bus with address #4 Wire.onReceive(receiveEvent); // register event Serial.begin(9600); // start serial for output Wire.onRequest(requestEvent); // register event } void loop() { } // function that executes whenever data is received from master // this function is registered as an event, see setup() void receiveEvent(int howMany) { while(1 < Wire.available()) // loop through all but the last { int c = Wire.read(); // receive byte as a character Serial.print((char)c); // print the character } int x = Wire.read(); // receive byte as an integer Serial.println((char)x); // print the integer } void requestEvent() { t++; if(t%10 >= 5) Wire.write("hello"); // respond with message of 6 bytes else Wire.write("world"); Serial.println(); Serial.println("requested!"); }