README
uartecho
Example Summary
Example that uses the UART driver to echo back to the console.
Peripherals Exercised
Board_GPIO_LED0- Indicates that the board was initialized withinmain()Board_UART0- Used to echo characters from host serial session
Resources & Jumper Settings
If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.
Example Usage
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection should have the following settings
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Run the example.
Board_GPIO_LED0turns ON to indicate driver initialization is complete.The target echoes back any character that is typed in the serial session.
If the serial session is started before the target completes initialization, the following is displayed:
Echoing characters:
Application Design Details
This example shows how to initialize the UART driver in blocking read and write mode with no data processing and echo characters back to a console.
A single thread,
echo, reads a character fromBoard_UART0and writes it back.Using the UART DMA Driver
The CC32XX platform has DMA support for the UART driver. The uartecho example can be built with either the UART driver with DMA support, or the non-DMA UART driver. The default configuration for this example is to use the non-DMA UART driver. Since only one character at a time is sent to the UART, this example is not an efficient use of the DMA, but it still serves to illustrate use of the UART DMA driver. To use the DMA version of the UART driver, build this example with the compile flag:
--define=TI_DRIVERS_UART_DMA=1
The
TI-RTOS:
- When building in Code Composer Studio, the kernel configuration project will be imported along with the example. The kernel configuration project is referenced by the example, so it will be built first. The “release” kernel configuration is the default project used. It has many debug features disabled. These feature include assert checking, logging and runtime stack checks. For a detailed difference between the “release” and “debug” kernel configurations and how to switch between them, please refer to the SimpleLink MCU SDK User’s Guide. The “release” and “debug” kernel configuration projects can be found under <SDK_INSTALL_DIR>/kernel/tirtos/builds/<BOARD>/(release|debug)/(ccs|gcc).
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.
IAR:
- When using any SensorTag(STK) Board, the XDS110 debugger must be selected with the 4-wire JTAG connection within your projects’ debugger configuration.