README

Example Summary

This example is the same as the “portable” example but instead of using POSIX APIs, it uses the native RTOS APIs. This example is still portable across devices (because of TI Drivers). This project requires less code/data space since there is no POSIX layer. This example is described in more detail in the SDK User’s Guide at <SDK_INSTALL_DIR>/docs/simplelink_mcu_sdk/Users_Guide.html.

Peripherals Exercised

Resources & Jumper Settings

If you’re using an IDE (such as CCS or IAR), please refer to Board.html in your project directory for resources used and board-specific jumper settings. Otherwise, you can find Board.html in the directory <SDK_INSTALL_DIR>/source/ti/boards/<BOARD>.

Example Usage

The connection should have the following settings

    Baud-rate:  115200
    Data bits:       8
    Stop bits:       1
    Parity:       None
    Flow Control: None

Application Design Details

TI-RTOS:

FreeRTOS:

Code Composer Studio:

SimpleLink Sensor and Actuator Plugin: