/* --COPYRIGHT--,BSD_EX * Copyright (c) 2017, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430FR60xx Demo - SDHS sampling at 8MSPS and DTC transfer results to RAM // // Description: Configure the SDHS for stand-alone use (register mode) at 8MSPS. // Use the DTC to transfer the results to an array in RAM named "results" (located // in LEA RAM at 0x5000). Convert array back to input voltage using: // V = (adc_code * (f_s/2))/(gain*7FF) + Bias // where,adc_code is the ADC result(16-Bit Signed Int),f_s = .755V(Full-scale voltage), // gain = 10^(0.1/20)) = approximately 1, Bias = .9V, 7FF = 2047 // // ***NOTE: On TS-Board, remove JP14, put SIG on inner pin and GND to outer pin. // Valid input range is 600mV - 1200mV, as configured.*** // MSP430FR6043 // --------------- // /|\| | // | | | // --|RST | // | P1.0|---> LED // | |-USSXTIN // | |-USSXTOUT // | CH0_IN|<--- input signal // // Gary Gao & Matt Calvo // Texas Instruments Inc. // February 2018 // Built with IAR Embedded Workbench V7.10 & Code Composer Studio V7.3 //****************************************************************************** #include #define OSCTYPE__CRYSTAL OSCTYPE_0 void HSPLL_init(void); #if defined(__TI_COMPILER_VERSION__) #pragma DATA_SECTION(results, ".leaRAM") #pragma RETAIN(results) int results[1024] = {0}; #elif defined(__IAR_SYSTEMS_ICC__) #pragma location=0x5000 __no_init int results[1024]; #pragma required = results #elif defined(__GNUC__) int results[1024] __attribute__ ((section (".leaRAM"), used)); #else #error Compiler not supported! #endif int main(void) { WDTCTL = WDTPW | WDTHOLD; // Stop WDT // Configure P1.0 as output for LED P1OUT &= ~BIT0; P1DIR |= BIT0; // Disable the GPIO power-on default high-impedance mode to activate // previously configured port settings PM5CTL0 &= ~LOCKLPM5; // Configure one FRAM waitstate as required by the device datasheet for MCLK // operation beyond 8MHz _before_ configuring the clock system. FRCTL0 = FRCTLPW | NWAITS_1; // Clock System Setup CSCTL0_H = CSKEY_H; // Unlock CS registers // Per Device Errata(CS12) set divider to 4 before changing frequency to // prevent out of spec operation from overshoot transient CSCTL3 = DIVA__4 | DIVS__4 | DIVM__4; // Set all corresponding clk sources to divide by 4 for errata(CS12) CSCTL1 = DCOFSEL_4 | DCORSEL; // Set DCO to 16MHz // Delay by ~10us to let DCO settle. 60 cycles = 20 cycles buffer + (10us / (1/4MHz)) __delay_cycles(60); CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // Set all dividers to 1 for 16MHz operation CSCTL3 = DIVA__1 | DIVS__1 | DIVM__1; // MCLK = SMCLK = 16MHz CSCTL0_H = 0; // Lock CS registers //Setup SAPH Bias Register Controlled SAPHKEY = KEY; SAPHBCTL &= ~ASQBSC; SAPHBCTL |= CPDA; SAPHICTL0 = 0; SAPHKEY = KEY+1; //Setup the SDHS with register mode SDHSCTL0 = TRGSRC_0 | AUTOSSDIS_1 | DFMSEL_0;// Software trigger,Left, 2s complement format SDHSCTL1 = OSR_0; // OSR = 10 (80MHz/10 = 8MSPS). CS must set MCLK >= 8MHz. SDHSCTL2 = 255; // SMPSZ = 255+1 samples SDHSCTL6 = 0x19; // PGA Gain 0.1 dB SDHSCTL7 = 0xC; // MODOPTI = 0xC (80MHz PLL output frequency) SDHSDTCDA = 0x800; // DTC transfer data to start of LEA RAM SDHSIMSC = ACQDONE; // Enable acquisition done interrupt (after 256 samples transferred) SDHSCTL3 = TRIGEN_1; // Enable trigger SDHSCTL4 = SDHSON; // Turn on SD and start conversion __delay_cycles(640); // Delay for PGA worst case 40us settling time HSPLL_init(); // Initialize the HSPLL and wait for it to lock // Configure TA2.1 for 1/sec to trigger the pulse generation and toggle LED TA2CCR0 = 9400; TA2CCR1 = 4700; TA2CCTL1 = OUTMOD_7 | CCIE; // Enable output signal to trigger PPG, enable Interrupt TA2CTL = TASSEL__ACLK | TACLR | MC__UP; // Timer sourced from ACLK (VLO), clear timer while(1) { __bis_SR_register(LPM0_bits | GIE); // Enter LPM0 w/interrupt __no_operation(); // For debug } } // Timer A2 interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = TIMER2_A1_VECTOR __interrupt void Timer2_A1_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(TIMER2_A1_VECTOR))) Timer2_A1_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(TA2IV, TAIV__TAIFG)) { case TAIV__NONE: break; // No interrupt case TAIV__TACCR1: SDHSCTL4&= ~SDHSON; SDHSCTL5 &= ~SSTART; SDHSCTL3 = 0; SDHSDTCDA = 0x800; SDHSCTL3 = TRIGEN_1; SDHSCTL4 = SDHSON; SDHSCTL5 |= SSTART; // Start conversion break; case TAIV__TAIFG: // overflow __no_operation(); break; default: break; } } // SDHS interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = SDHS_VECTOR __interrupt void SDHS_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(SDHS_VECTOR))) SDHS_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(SDHSIIDX, IIDX_6)) { case IIDX_0: break; // No interrupt case IIDX_1: __no_operation(); break; // OVF interrupt case IIDX_2: // ACQDONE interrupt P1OUT ^= BIT0; // Toggle LED to show new cyclelll __delay_cycles(1000); __no_operation(); // Put breakpoint here to view results break; case IIDX_3: break; // SSTRG interrupt case IIDX_4: break; // DTRDY interrupt case IIDX_5: break; // WINHI interrupt case IIDX_6: break; // WINLO interrupt default: break; } } void HSPLL_init(void) { // Configure USSXT Oscillator HSPLLUSSXTLCTL = OSCTYPE__CRYSTAL | USSXTEN; // Set up timer to wait in LPM for crystal stabilization time = 4096 clocks for crystal resonator. // For 8MHz XTAL, 4096 clocks = 512us. Using VLO = 9.4kHz, wait 5 timer clock cycles = 532us. TA4CCR0 = 5; TA4CCTL0 = CCIE; // Enable Interrupt TA4CTL = TASSEL__ACLK | TACLR | MC__UP; // Timer sourced from ACLK (VLO), clear timer __bis_SR_register(LPM3_bits | GIE); // Enter LPM3 w/interrupt __no_operation(); // For debug // Check if oscillator is stable while((HSPLLUSSXTLCTL & OSCSTATE) == 0); // Output oscillator on pin HSPLLUSSXTLCTL &= ~XTOUTOFF; // Init PLL // Use the PLLM setting to get 80MHz output from our 8MHz input // Equation: PLL output clock frequency x 2 = input clock frequency x (PLLM+1) // Input clock frequency = 8MHz // Desired PLL output clock frequency = 80MHz // PLLM = 19 HSPLLCTL = PLLM4 | PLLM1 | PLLM0 | PLLINFREQ; //PLLM = 19, PLL input frequency > 6MHz // Power up the UUPS to start the PLL UUPSCTL |= USSPWRUP; // Wait for UUPS to power up while((UUPSCTL & UPSTATE_3) != UPSTATE_3); // Wait for PLL to lock while(!(HSPLLCTL & PLL_LOCK)); } // Timer A4 interrupt service routine #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector = TIMER4_A0_VECTOR __interrupt void Timer4_A0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(TIMER4_A0_VECTOR))) Timer4_A0_ISR (void) #else #error Compiler not supported! #endif { // Stop the timer and wake from LPM TA4CTL = MC__STOP; __bic_SR_register_on_exit(LPM3_bits | GIE); __no_operation(); }