/*
 * flashctl_Nonmain_write.c
 *
 *  Created on: 28-Apr-2026
 *      Author: Lenovo
 */

#include "boot_config.h"

/* Base address of nonmain memory */
#define NONMAIN_BASE_ADDRESS                                      (0x41C00000U)

/* Base address of the BCR configuration structure in nonmain memory */
#define BCR_USER_CFG_BASE_ADDRESS                                 (0x41C00000U)

/* Base address of the BSL configuration structure in nonmain memory */
#define BSL_USER_CFG_BASE_ADDRESS                                 (0x41C00100U)

/* Size in bytes of the BSL and BCR configuration structures */
#define BCR_CONFIG_SIZE_BYTES                                             (96U)
#define BSL_CONFIG_SIZE_BYTES                                             (88U)

/* The calculated CRC based on the default configuration values */
#define BCR_CFG_DEFAULT_CRC                                          0x11c3a627  //(0x1879dac3)
#define BSL_CFG_DEFAULT_CRC                                         (0xf7df416)

/* Defines for CRC */
#define CRC_SEED                                                    (0xFFFFFFFF)

/* clang-format on */

/* Bootcode configuration */

/* clang-format on */

/* The default configuration of the BCR config struct */
BCR_Config gBCRConfig = {
    .bcrConfigID                   = 0x1,
    .debugAccess                   = BCR_CFG_DEBUG_ACCESS_EN,
    .swdpMode                      = BCR_CFG_SWDP_EN,
    .tifaMode                      = BCR_CFG_TIFA_EN,
    .bslPinInvokeEnable            = BCR_CFG_BSL_PIN_INVOKE_DIS,
    .passwordDebugLock             = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
        CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
    .fastBootMode                  = BCR_CFG_FAST_BOOT_DIS,
    .bootloaderMode                = BCR_CFG_BOOTLOADER_MODE_EN,
    .massEraseMode                 = BCR_CFG_MASS_ERASE_EN,
    .factoryResetMode              = BCR_CFG_FACTORY_RESET_EN,
    .passwordMassErase             = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
        CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
    .passwordFactoryReset          = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
        CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
    .staticWriteProtectionMainLow  = CFG_DEFAULT_VALUE,
    .staticWriteProtectionMainHigh = CFG_DEFAULT_VALUE,
    .staticWriteProtectionNonMain  = BCR_CFG_NON_MAIN_STATIC_PROT_DIS,
    .secureBootMode                = BCR_CFG_SECURE_BOOT_DIS,
    .userSecureAppStartAddr        = CFG_DEFAULT_VALUE,
    .userSecureAppLength           = CFG_DEFAULT_VALUE,
    .userSecureAppCrc              = CFG_DEFAULT_VALUE,
    .userCfgCRC                    = BCR_CFG_DEFAULT_CRC,
};

/* The default configuration of the BSL config struct */
BSL_Config gBSLConfig = {
    .configID                          = 0x1,
    .interfacePins.UART_RXD_pad_num    = DEF_UART_RXD_PAD,
    .interfacePins.UART_RXD_PF_mux_sel = DEF_UART_RXD_MUX,
    .interfacePins.UART_TXD_pad_num    = DEF_UART_TXD_PAD,
    .interfacePins.UART_TXD_PF_mux_sel = DEF_UART_TXD_MUX,
    .interfacePins.I2C_SDA_pad_num     = DEF_I2C_SDA_PAD,
    .interfacePins.I2C_SDA_PF_mux_sel  = DEF_I2C_SDA_MUX,
    .interfacePins.I2C_SCL_pad_num     = DEF_I2C_SCL_PAD,
    .interfacePins.I2C_SCL_PF_mux_sel  = DEF_I2C_SCL_MUX,
    .pin.pinData0                      = DEFAULT_BSL_PIN_INVOCATION_DATA0,
    .pin.pinData1                      = DEFAULT_BSL_PIN_INVOCATION_DATA1,
    .memoryRead                        = BSL_CFG_MEMORY_READOUT_DISABLE,
    .password   = {CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
        CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE,
        CFG_DEFAULT_VALUE, CFG_DEFAULT_VALUE},
    .pluginType = BSL_CFG_PLUGIN_TYPE_ANY,
    .flashPluginEnable  = BSL_CFG_PLUGIN_FLASH_NOT_EXIST,
    .pluginSramSize     = 0xFF,
    .pluginHook[0]      = CFG_DEFAULT_VALUE,
    .pluginHook[1]      = CFG_DEFAULT_VALUE,
    .pluginHook[2]      = CFG_DEFAULT_VALUE,
    .pluginHook[3]      = CFG_DEFAULT_VALUE,
    .BSLAlternateConfig = BSL_CFG_FLASH_BSL_NOT_EXIST,
    .reserved           = 0xFFFF,
    .BSLAlternateAddr   = CFG_DEFAULT_VALUE,
    .appRev             = (uint32_t *) CFG_DEFAULT_VALUE,
    .securityAlert      = BSL_CFG_SECURITY_IGNORE,
    .i2cSlaveAddress    = 0x48,
    .userCfgCRC         = BSL_CFG_DEFAULT_CRC,
};

uint32_t calcUserConfigCRC(uint8_t *dataPointer, uint32_t size)
{
    static uint32_t i;

    uint32_t calculatedCRC;

    DL_CRC_init(CRC, DL_CRC_32_POLYNOMIAL, DL_CRC_BIT_REVERSED,
        DL_CRC_INPUT_ENDIANESS_LITTLE_ENDIAN, DL_CRC_OUTPUT_BYTESWAP_DISABLED);

    /* Set the Seed value to reset the calculation */
    DL_CRC_setSeed32(CRC, CRC_SEED);

    for (i = (uint32_t) 0U; i < size; i++) {
        DL_CRC_feedData8(CRC, dataPointer[i]);
    }
    calculatedCRC = DL_CRC_getResult32(CRC);

    return calculatedCRC;
}

void SYSCFG_DL_CRC_init(void)
{
    DL_CRC_init(CRC, DL_CRC_32_POLYNOMIAL, DL_CRC_BIT_REVERSED,
        DL_CRC_INPUT_ENDIANESS_LITTLE_ENDIAN, DL_CRC_OUTPUT_BYTESWAP_DISABLED);

    DL_CRC_setSeed32(CRC, CRC_SEED);
}

void flashctl_NonMain_Write(void)
{
    DL_CRC_reset(CRC);
    DL_CRC_enablePower(CRC);
    delay_cycles(16);
    SYSCFG_DL_CRC_init();
    /*
     * Calculate the CRC for the BCR and BSL configuration structs
     * The CRC is 4 bytes in each struct, this should not be included in the calculation
     */
    gBCRConfig.userCfgCRC = calcUserConfigCRC((uint8_t *) &gBCRConfig,
        BCR_CONFIG_SIZE_BYTES - ((uint32_t) sizeof(gBCRConfig.userCfgCRC)));
    gBSLConfig.userCfgCRC = calcUserConfigCRC((uint8_t *) &gBSLConfig,
        BSL_CONFIG_SIZE_BYTES - ((uint32_t) sizeof(gBSLConfig.userCfgCRC)));

    /* Clear STATCMD register, unprotect NONMAIN, and then erase NONMAIN memory */
    DL_FlashCTL_executeClearStatus(FLASHCTL);
    DL_FlashCTL_unprotectSector(
        FLASHCTL, NONMAIN_BASE_ADDRESS, DL_FLASHCTL_REGION_SELECT_NONMAIN);
    DL_FlashCTL_eraseMemoryFromRAM(
        FLASHCTL, NONMAIN_BASE_ADDRESS, DL_FLASHCTL_COMMAND_SIZE_SECTOR);

    /*
     * Program the BCR config structure to NONMAIN memory.
     * The BCR config struct has a size of 96 bytes, and 4 bytes are
     * programmed at a time, resulting in 96 / 4 = 24 writes to Flash
     */
    DL_FlashCTL_programMemoryBlockingFromRAM64WithECCGenerated(FLASHCTL,
        BCR_USER_CFG_BASE_ADDRESS, (uint32_t *) &gBCRConfig,
        (BCR_CONFIG_SIZE_BYTES / 4), DL_FLASHCTL_REGION_SELECT_NONMAIN);

    /*
     * Program the BSL config structure to NONMAIN memory.
     * The BSL config struct has a size of 88 bytes, and 4 bytes are
     * programmed at a time, resulting in 88 / 4 = 22 writes to Flash
     */
    DL_FlashCTL_programMemoryBlockingFromRAM64WithECCGenerated(FLASHCTL,
        BSL_USER_CFG_BASE_ADDRESS, (uint32_t *) &gBSLConfig,
        (BSL_CONFIG_SIZE_BYTES / 4), DL_FLASHCTL_REGION_SELECT_NONMAIN);

}