/*
 * Copyright (c) 2023, Texas Instruments Incorporated - http://www.ti.com
 * All rights reserved.
 *
 * Redistribution and use in source and binary forms, with or without
 * modification, are permitted provided that the following conditions
 * are met:
 *
 * *  Redistributions of source code must retain the above copyright
 *    notice, this list of conditions and the following disclaimer.
 *
 * *  Redistributions in binary form must reproduce the above copyright
 *    notice, this list of conditions and the following disclaimer in the
 *    documentation and/or other materials provided with the distribution.
 *
 * *  Neither the name of Texas Instruments Incorporated nor the names of
 *    its contributors may be used to endorse or promote products derived
 *    from this software without specific prior written permission.
 *
 * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
 */

/*
 *  ============ ti_msp_dl_config.h =============
 *  Configured MSPM0 DriverLib module declarations
 *
 *  DO NOT EDIT - This file is generated for the MSPM0G350X
 *  by the SysConfig tool.
 */
#ifndef ti_msp_dl_config_h
#define ti_msp_dl_config_h

#define CONFIG_MSPM0G350X
#define CONFIG_MSPM0G3507

#if defined(__ti_version__) || defined(__TI_COMPILER_VERSION__)
#define SYSCONFIG_WEAK __attribute__((weak))
#elif defined(__IAR_SYSTEMS_ICC__)
#define SYSCONFIG_WEAK __weak
#elif defined(__GNUC__)
#define SYSCONFIG_WEAK __attribute__((weak))
#endif

#include <ti/devices/msp/msp.h>
#include <ti/driverlib/driverlib.h>
#include <ti/driverlib/m0p/dl_core.h>

#ifdef __cplusplus
extern "C" {
#endif

/*
 *  ======== SYSCFG_DL_init ========
 *  Perform all required MSP DL initialization
 *
 *  This function should be called once at a point before any use of
 *  MSP DL.
 */


/* clang-format off */

#define POWER_STARTUP_DELAY                                                (16)


#define GPIO_HFXT_PORT                                                     GPIOA
#define GPIO_HFXIN_PIN                                             DL_GPIO_PIN_5
#define GPIO_HFXIN_IOMUX                                         (IOMUX_PINCM10)
#define GPIO_HFXOUT_PIN                                            DL_GPIO_PIN_6
#define GPIO_HFXOUT_IOMUX                                        (IOMUX_PINCM11)
#define CPUCLK_FREQ                                                     40000000
/* Defines for SYSPLL_ERR_01 Workaround */
/* Represent 1.000 as 1000 */
#define FLOAT_TO_INT_SCALE                                               (1000U)
#define FCC_EXPECTED_RATIO                                                  1250
#define FCC_UPPER_BOUND                       (FCC_EXPECTED_RATIO * (1 + 0.003))
#define FCC_LOWER_BOUND                       (FCC_EXPECTED_RATIO * (1 - 0.003))

bool SYSCFG_DL_SYSCTL_SYSPLL_init(void);



/* Port definition for Pin Group GPIO_LEDS */
#define GPIO_LEDS_PORT                                                   (GPIOB)

/* Defines for USER_LED_1: GPIOB.22 with pinCMx 50 on package pin 21 */
#define GPIO_LEDS_USER_LED_1_PIN                                (DL_GPIO_PIN_22)
#define GPIO_LEDS_USER_LED_1_IOMUX                               (IOMUX_PINCM50)
/* Defines for USER_LED_2: GPIOB.26 with pinCMx 57 on package pin 28 */
#define GPIO_LEDS_USER_LED_2_PIN                                (DL_GPIO_PIN_26)
#define GPIO_LEDS_USER_LED_2_IOMUX                               (IOMUX_PINCM57)
/* Defines for USER_LED_3: GPIOB.27 with pinCMx 58 on package pin 29 */
#define GPIO_LEDS_USER_LED_3_PIN                                (DL_GPIO_PIN_27)
#define GPIO_LEDS_USER_LED_3_IOMUX                               (IOMUX_PINCM58)
/* Defines for USER_TEST_B16: GPIOB.16 with pinCMx 33 on package pin 4 */
#define GPIO_LEDS_USER_TEST_B16_PIN                             (DL_GPIO_PIN_16)
#define GPIO_LEDS_USER_TEST_B16_IOMUX                            (IOMUX_PINCM33)
/* Defines for USER_TEST_B0: GPIOB.0 with pinCMx 12 on package pin 47 */
#define GPIO_LEDS_USER_TEST_B0_PIN                               (DL_GPIO_PIN_0)
#define GPIO_LEDS_USER_TEST_B0_IOMUX                             (IOMUX_PINCM12)
/* Defines for USER_TEST_B6: GPIOB.6 with pinCMx 23 on package pin 58 */
#define GPIO_LEDS_USER_TEST_B6_PIN                               (DL_GPIO_PIN_6)
#define GPIO_LEDS_USER_TEST_B6_IOMUX                             (IOMUX_PINCM23)
/* Defines for USER_TEST_B7: GPIOB.7 with pinCMx 24 on package pin 59 */
#define GPIO_LEDS_USER_TEST_B7_PIN                               (DL_GPIO_PIN_7)
#define GPIO_LEDS_USER_TEST_B7_IOMUX                             (IOMUX_PINCM24)




/* Defines for MCAN0 */
#define MCAN0_INST                                                        CANFD0
#define GPIO_MCAN0_CAN_TX_PORT                                             GPIOA
#define GPIO_MCAN0_CAN_TX_PIN                                     DL_GPIO_PIN_12
#define GPIO_MCAN0_IOMUX_CAN_TX                                  (IOMUX_PINCM34)
#define GPIO_MCAN0_IOMUX_CAN_TX_FUNC               IOMUX_PINCM34_PF_CANFD0_CANTX
#define GPIO_MCAN0_CAN_RX_PORT                                             GPIOA
#define GPIO_MCAN0_CAN_RX_PIN                                     DL_GPIO_PIN_13
#define GPIO_MCAN0_IOMUX_CAN_RX                                  (IOMUX_PINCM35)
#define GPIO_MCAN0_IOMUX_CAN_RX_FUNC               IOMUX_PINCM35_PF_CANFD0_CANRX
#define MCAN0_INST_IRQHandler                                 CANFD0_IRQHandler
#define MCAN0_INST_INT_IRQN                                     CANFD0_INT_IRQn


/* Defines for MCAN0 MCAN RAM configuration */
#define MCAN0_INST_MCAN_STD_ID_FILT_START_ADDR     (0)
#define MCAN0_INST_MCAN_STD_ID_FILTER_NUM          (0)
#define MCAN0_INST_MCAN_EXT_ID_FILT_START_ADDR     (48)
#define MCAN0_INST_MCAN_EXT_ID_FILTER_NUM          (1)
#define MCAN0_INST_MCAN_TX_BUFF_START_ADDR         (148)
#define MCAN0_INST_MCAN_TX_BUFF_SIZE               (2)
#define MCAN0_INST_MCAN_FIFO_1_START_ADDR          (192)
#define MCAN0_INST_MCAN_FIFO_1_NUM                 (16)
#define MCAN0_INST_MCAN_TX_EVENT_START_ADDR        (164)
#define MCAN0_INST_MCAN_TX_EVENT_SIZE              (2)
#define MCAN0_INST_MCAN_EXT_ID_AND_MASK            (0x1FFFFFFFU)
#define MCAN0_INST_MCAN_RX_BUFF_START_ADDR         (208)
#define MCAN0_INST_MCAN_FIFO_0_START_ADDR          (172)
#define MCAN0_INST_MCAN_FIFO_0_NUM                 (0)

#define MCAN0_INST_MCAN_INTERRUPTS (DL_MCAN_INTERRUPT_ARA | \
						DL_MCAN_INTERRUPT_BEU | \
						DL_MCAN_INTERRUPT_BO | \
						DL_MCAN_INTERRUPT_DRX | \
						DL_MCAN_INTERRUPT_ELO | \
						DL_MCAN_INTERRUPT_EP | \
						DL_MCAN_INTERRUPT_EW | \
						DL_MCAN_INTERRUPT_MRAF | \
						DL_MCAN_INTERRUPT_PEA | \
						DL_MCAN_INTERRUPT_PED | \
						DL_MCAN_INTERRUPT_RF1F | \
						DL_MCAN_INTERRUPT_RF1L | \
						DL_MCAN_INTERRUPT_RF1N | \
						DL_MCAN_INTERRUPT_RF1W | \
						DL_MCAN_INTERRUPT_TC | \
						DL_MCAN_INTERRUPT_TOO | \
						DL_MCAN_INTERRUPT_TSW | \
						DL_MCAN_INTERRUPT_WDI)




/* clang-format on */

void SYSCFG_DL_init(void);
void SYSCFG_DL_initPower(void);
void SYSCFG_DL_GPIO_init(void);
void SYSCFG_DL_SYSCTL_init(void);

bool SYSCFG_DL_SYSCTL_SYSPLL_init(void);

void SYSCFG_DL_SYSTICK_init(void);
void SYSCFG_DL_MCAN0_init(void);

bool SYSCFG_DL_saveConfiguration(void);
bool SYSCFG_DL_restoreConfiguration(void);

#ifdef __cplusplus
}
#endif

#endif /* ti_msp_dl_config_h */