MSP430 DriverLib 1.60.02.01
Release Notes
Document Revision: 100713.1314
This is the MSP430 Peripheral Driver Library. This peripheral driver library's intent is to
allow
application development at an API level instead at the device register
level. Allowing developers to concentrate on their
applications
instead of the nuances of the particular MSP430 device they are using.
This document is divided into the following sections:
- MSP430ware Peripheral
Driver Library API
- MSP430ware
Peripheral
Driver Library User's Guides
- Manifest
- License
- Fixed issue with C++ bindings
- Fixed bug with USCI_A_UART recieveData, transmitData,
transmitBreak that used the wrong type of register access (16 instead
of 8)
- Fixed bug with USCI_B_I2C enableInterrupt, masterSingleReceive that used the wrong type of register access (16 instead of 8)
- Fixed include path in example projects to refer to driver library copy in workspace instead of from the installation
- Minor updates to inc/hw_memmap.h for each supported family
- Added C++ bindings to all driverlib peripherals
- Improved User's Guide Documentation
- Improved Release Notes Format
- Converted CCS examples to use CCS projectSpec
- In
all driverlib code examples, the source and header files are now copied
into the project and not linked (unlike previous driverlib releases)
- Examples generated from .projectspec file instead of .cproject/.project files
- Clear LPM5 bit for GPIO settings in all Wolverine examples
- Fixed Bug 4537- Set enable bit on ADC to 0 before turning ADC on or off in ADC12_B_enable and ADC12_B_disable
- Fixed Bug 4579- Changed comment in MPU_createThreeSegments() in MSP430FR5xx_6xx, MSP430FR57xx families
- Fixed Bug 4568 - Lock CS modules after unlocking in MSP430FR5xx_6xx, MSP430FR57xx families
- Removed
(E)USCI_A_UART_init() and (e)uart_baudrate.h/c files in all families.
Please use (E)USCI_A_UART_initAdvance() instead. The values
to be written into the clockPrescalar, firstModReg, secondModReg and
overSampling parameters of (E)USCI_A_UART_initAdvance() should be
pre-computed and passed into the initialization function.
http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430BaudRateConverter/index.html
helps pre-compute the necessary values.
- Removed busy bit checking for all FRAM peripherals
- Fixed Bug 4340 - (E)USCI_I2C timeout functions should use pre-decrement rather than post-decrement in while loop
- Fixed Bug 4591 - EUSCI_B_I2C_masterSendSingleByteWithTimeout() timeout incorrect
- Fixed
Bug 3856 - The following AES256 API for MSP430FR5xx_6xx are removed
AES256_decryptDataUsingEncryptionKey,
AES256_startDecryptDataUsingEncryptionKey,
AES256_generateFirstRoundKey,AES256_startGenerateFirstRoundKey. Two new
API are added - AES_setDecipherKey, AES_startSetDecipherKey
- Fixed Bug 4452 - Need FLASH apis that unlock info memory
- Added version.h to indicate driverlib version no.
- driverlib.h
file is now available in every supported device family. Including this one header
file in applications is sufficient for using any driverlib API call.
Including driverlib.h eliminates the need to include "inc/hw_memmap.h"
and every single "peripheral.h" the user would like to use.
- Driverlib code examples copy the driverlib source and header files instead of linking them
- Removed deprecated 5xx_6xx examples. All customers should be
using the new family based structure for driver library development.
Please refer to the family's user's guides for new APIs.
- EUSCI_SPI,
EUSCI_I2C, EUSCI_UART APIs are deprecated. Please use
EUSCI_A_SPI, EUSCI_B_SPI, EUSCI_B_I2C, EUSCI_A_UART APIs for EUSCI
operations.
- The deprecated EUSCI_SPI, EUSCI_I2C, EUSCI_UART APIs are removed for MSP430FR5xx_6xx family.
Revision History
1.60.00.46:
- Added C++ bindings to all driverlib peripherals
- Improved User's Guide Documentation
- Improved Release Notes Format
- Converted CCS examples to use CCS projectSpec
- In
all driverlib code examples, the source and header files are now copied
into the project and not linked (unlike previous driverlib releases)
- Examples generated from .projectspec file instead of .cproject/.project files
- Clear LPM5 bit for GPIO settings in all Wolverine examples
- Fixed Bug 4537- Set enable bit on ADC to 0 before turning ADC on or off in ADC12_B_enable and ADC12_B_disable
- Fixed Bug 4579- Changed comment in MPU_createThreeSegments() in MSP430FR5xx_6xx, MSP430FR57xx families
- Fixed Bug 4568 - Lock CS modules after unlocking in MSP430FR5xx_6xx, MSP430FR57xx families
- Removed
(E)USCI_A_UART_init() and (e)uart_baudrate.h/c files in all families.
Please use (E)USCI_A_UART_initAdvance() instead. The values
to be written into the clockPrescalar, firstModReg, secondModReg and
overSampling parameters of (E)USCI_A_UART_initAdvance() should be
pre-computed and passed into the initialization function.
http://software-dl.ti.com/msp430/msp430_public_sw/mcu/msp430/MSP430BaudRateConverter/index.html
helps pre-compute the necessary values.
- Removed busy bit checking for all FRAM peripherals
- Fixed Bug 4340 - (E)USCI_I2C timeout functions should use pre-decrement rather than post-decrement in while loop
- Fixed Bug 4591 - EUSCI_B_I2C_masterSendSingleByteWithTimeout() timeout incorrect
- Fixed
Bug 3856 - The following AES256 API for MSP430FR5xx_6xx are removed
AES256_decryptDataUsingEncryptionKey,
AES256_startDecryptDataUsingEncryptionKey,
AES256_generateFirstRoundKey,AES256_startGenerateFirstRoundKey. Two new
API are added - AES_setDecipherKey, AES_startSetDecipherKey
- Fixed Bug 4452 - Need FLASH apis that unlock info memory
- Added version.h to indicate driverlib version no.
- driverlib.h
file is now available in every supported device family. Including this one header
file in applications is sufficient for using any driverlib API call.
Including driverlib.h eliminates the need to include "inc/hw_memmap.h"
and every single "peripheral.h" the user would like to use.
- Driverlib code examples copy the driverlib source and header files instead of linking them
- Removed deprecated 5xx_6xx examples. All customers should be
using the new family based structure for driver library development.
Please refer to the family's user's guides for new APIs.
- EUSCI_SPI,
EUSCI_I2C, EUSCI_UART APIs are deprecated. Please use
EUSCI_A_SPI, EUSCI_B_SPI, EUSCI_B_I2C, EUSCI_A_UART APIs for EUSCI
operations.
- The deprecated EUSCI_SPI, EUSCI_I2C, EUSCI_UART APIs are removed for MSP430FR5xx_6xx family.
1.40.01.00:
- Changed some remaining UART APIs to use C99 types
- Fixed minor doxygen documentation for CS
- Fixed bug in GPIO_interruptEdgeSelect that caused it to fail to work with even ports (P2, P4, ..)
- Fixed bug in COMP_E that accidentally clears the previous settings in CECTL2
- Fixed bug in ADC12_B_memoryConfigure that did not allow enabling the window comparator
- The header files have been updated to be in sync with CCS5.5 Beta
- FRAM_configureWaitStateControl API in 5xx_6xx family now ignores the manualWaitState parameter
since this register bit is now changed to a reserved bit. The API
signature has not changed to maintain backward compatibility..
- FRAM_configureWaitStateControl
API in MSP430FR5xx_6xx family signature has changed to exclude
the manualWaitState parameter since this register bit is now
a reserved bit.
- PMM_lockLPM5() API is used in MSP430FR5xx_6xx
examples to disable the GPIO power-on default high-impedance mode to
activate previously configured port settings.
- Comp_E
examples in examples\driverlib\5xx_6xx\comp_e will fail to build due to a bug in the existing device header file for
versions of CCS less than CCS 5.3. To workaround this, please upgrade CCS or
replace the msp430fr5969.h from the CCS5.3 release in your CCS install.
- Comp_E
examples in examples\driverlib\5xx_6xx\comp_e will fail to build due to
a bug in the existing device header file for versions of IAR5.5. To
workaround this, please replace the msp430fr5969.h from
deprecated\msp430fr5xx_6xx_header_files\IAR from the in your IAR5.5
install.
1.40.00.00:
- Added TIMER_X_counterGet to get the current count of the timer
- Changed timer initialization functions to not start timer automatically
- Added documentation to create driverlib based projects from scratch
- Fixed byte order in AES encrypt/decrupt APIs
- Separated EUSCI_SPI to EUSCI_A_SPI and EUSCI_B_SPI
- Separated USCI_SPI to USCI_A_SPI and USCI_B_SPI
- Renamed EUCSI_UART to EUSCI_A_UART and USCI_UART to USCI_A_UART
- Renamed EUSCI_I2C to EUSCI_B_I2C and USCI_I2C to USCI_B_I2C
- Added API CRC_set8BitData and CRC_set16BitData
- Fixed minor doxygen documentation for ADC12_A
- Changed driverlib emptyProject to use ELF
- Comp_E
examples in examples\driverlib\5xx_6xx\comp_e will fail to build due to a bug in the existing device header file for
versions of CCS less than CCS 5.3. To workaround this, please upgrade CCS or
replace the msp430fr5969.h from the CCS5.3 release in your CCS install.
- Comp_E
examples in examples\driverlib\5xx_6xx\comp_e will fail to build due to
a bug in the existing device header file for versions of IAR5.5. To
workaround this, please replace the msp430fr5969.h from
deprecated\msp430fr5xx_6xx_header_files\IAR from the in your IAR5.5
install.
1.30.00.00:
- Added 4 wire EUSCI_SPI support
- Fixed typos in EUSCI examples
- Fixed comments in FRPMM
- Fixed parameters in UCS_clockSignalInit
- Added timeout functions to I2C and EUSCI_I2C peripheral drivers
- Fixed bug in GPIO_setDriveStrength API. Modified PxIES instead of PxDS
- Fixed comments in COMP_E examples
- Added support to ADC12_B to configure window comparator
- Comp_E
examples in examples\driverlib\5xx_6xx\comp_e will fail to build due to a bug in the existing device header file for
versions of CCS less than CCS 5.3. To workaround this, please upgrade CCS or
replace the msp430fr5969.h from the CCS5.3 release in your CCS install.
- Comp_E
examples in examples\driverlib\5xx_6xx\comp_e will fail to build due to
a bug in the existing device header file for versions of IAR5.5. To
workaround this, please replace the msp430fr5969.h from
deprecated\msp430fr5xx_6xx_header_files\IAR from the in your IAR5.5
install.
Generally DriverLib is
installed as part of MSP430ware. If you wish to update DriverLib
from the zip file, cd to MSP430ware_Installation_Directory and
unzip driverlib_x_xx_xx_xx.zip. The installation contains the driver
library core as well as peripheral examples and API documentation.
The MSP430 peripheral driver library contains the following components:
| deprecated | Header files that are not part of the standard CCS or IAR distribution |
| doc |
MSP430 Peripheral Driver Library
documentation |
| driverlib |
MSP430 Peripheral
Driver Library source code
|
| examples |
MSP430 Peripheral Driver Library examples |
| inc |
MSP430 Peripheral Driver Library deprecated include files |
Device Support
The following families of devices are support in this release of MSP430 Driver Library:
- MSP430F5xx_6xx
- MSP430FR57xx
- MSP430FR5xx_6xx
- 5xx_6xx
[Deprecated - Please do not use the contents of this folder for new
applications. This folder will be removed in the upcoming releases.]
This is the 1.60.02.01 release of MSP430 Peripheral Driver
Library. The following peripherals are supported in this
release:
- MSP430F5xx_6xx Devices
- ADC10_A
- ADC12_A
- AES
- BAK_BATT (Battery Backup System)
- COMP_B
- CRC
- DAC12_A
- DMA
- EUSCI_B_I2C
- EUSCI_A_SPI
- EUSCI_B_SPI
- EUSCI_A_UART
- FLASH
- SFR
- SYS
- GPIO
- LDOPWR
- MPY32
- PMAP
- PMM
- RAM Controller
- REF
- REF_A
- RTC_A
- RTC_B
- RTC_C
- SD24_B
- SFR
- SYS
- TEC
- TIMER_A
- TIMER_B
- TIMER_D
- TLV
- UCS
- USCI_B_I2C
- USCI_A_SPI
- USCI_B_SPI
- USCI_A_UART
- WDT_A
- MSP430FR57xx Devices
- ADC12_B
- AES256
- COMP_E
- CRC
- CS
- DMA
- EUSCI_B_I2C
- EUSCI_A_SPI
- EUSCI_B_SPI
- EUSCI_A_UART
- FRAM
- GPIO
- MPU
- MPY32
- PMM
- REF
- RTC_B
- SFR
- SYS
- TIMER_A
- TIMER_B
- TLV
- WDT_A
- MSP430FR5xx_6xx Devices
- ADC12_B
- AES256
- Comp_E
- CRC
- CS
- DMA
- EUSCI_B_I2C
- EUSCI_A_SPI
- EUSCI_B_SPI
- EUSCI_A_UART
- FRAM
- GPIO
- MPU
- MPY32
- PMM
- REF_A
- RTC_B
- SFR
- SYS
- TIMER_A
- TIMER_B
- TLV
- WDT_A
MSP4305xx_6xx devices
MSP430FR57xx devices
MSP430FR5xx_6xx devices
This release is a GA version.
Upgrade and Compatibility Information
N/A
The
examples may be built with either IAR or CCS. To build the examples navigate to
examples/<family>/<peripheral>/<ide> and double
click the .eww project files for IAR or import the .projectSpec file for CCS.
Current supported families are found in the Device Support section of the release notes.
Current supported peripherals are found in the Peripheral Support section of the release notes.
Known Issues
- Asserts in CCS work only when the project is optimized for size
This is build 1.60.02.01 of MSP430 driver library.
Additional Resources
For more information, visit www.ti.com.