MEMORY { /* BEGIN is used for the "boot to Flash" bootloader mode */ BEGIN : origin = 0x088000, length = 0x000002 BOOT_RSVD : origin = 0x000002, length = 0x0001AF /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x0001B1, length = 0x00024F RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ /* RAMD0 : origin = 0x00C000, length = 0x000800 */ /* RAMD1 : origin = 0x00C800, length = 0x000800 */ // This section is set for Ramfunc2 RAMD0D1 : origin = 0x00C000, length = 0x001000 /* ===== Ram sectors ===== */ /* RAMLS0 : origin = 0x008000, length = 0x000800 */ /* RAMLS1 : origin = 0x008800, length = 0x000800 */ /* RAMLS2 : origin = 0x009000, length = 0x000800 */ /* RAMLS3 : origin = 0x009800, length = 0x000800 */ /* RAMLS4 : origin = 0x00A000, length = 0x000800 */ /* RAMLS5 : origin = 0x00A800, length = 0x000800 */ /* RAMLS6 : origin = 0x00B000, length = 0x000800 */ // This section is set to CLA program RAMLS0LS6 : origin = 0x008000, length = 0x003800 // This section is set to CLA data RAMLS7 : origin = 0x00B800, length = 0x000800 /* RAMGS0 : origin = 0x00D000, length = 0x001000 */ /* RAMGS1 : origin = 0x00E000, length = 0x001000 */ /* RAMGS2 : origin = 0x00F000, length = 0x001000 */ CPU1RAMGS0GS1A : origin = 0x00D000, length = 0x001D00 CPU1RAMGS1BGS2 : origin = 0x00ED00, length = 0x001400 /* RAMGS3 : origin = 0x010000, length = 0x001000 */ /* RAMGS4 : origin = 0x011000, length = 0x001000 */ /* RAMGS5 : origin = 0x012000, length = 0x001000 */ /* RAMGS6 : origin = 0x013000, length = 0x001000 */ CPU1RAMGS3GS7A : origin = 0x010100, length = 0x004500 /* RAMGS7 : origin = 0x014000, length = 0x001000 */ /* RAMGS8 : origin = 0x015000, length = 0x001000 */ /* RAMGS9 : origin = 0x016000, length = 0x001000 */ CPU1RAMGS7BGS9 : origin = 0x014600, length = 0x002A00 /* RAMGS10 : origin = 0x017000, length = 0x001000 */ /* RAMGS11 : origin = 0x018000, length = 0x001000 */ /* RAMGS12 : origin = 0x019000, length = 0x001000 */ CPU2RAMGS10GS13A : origin = 0x017000, length = 0x003800 /* RAMGS13 : origin = 0x01A000, length = 0x001000 */ /* RAMGS14 : origin = 0x01B000, length = 0x001000 */ /* RAMGS15 : origin = 0x01C000, length = 0x000FF8 */ CPU2RAMGS13BGS15 : origin = 0x01A800, length = 0x0027F8 // RAMGS15_RSVD : origin = 0x01CFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ /* Flash sectors */ /* Start : Bootloader */ /* FLASH0 : origin = 0x080002, length = 0x001FFE on-chip Flash */ /* FLASH1 : origin = 0x082000, length = 0x002000 on-chip Flash */ /* FLASH2 : origin = 0x084000, length = 0x002000 on-chip Flash */ /* FLASH3 : origin = 0x086000, length = 0x002000 on-chip Flash */ /* End : Bootloader */ /* FLASH4 : origin = 0x088000, length = 0x008000 on-chip Flash */ /* FLASH5 : origin = 0x090000, length = 0x008000 on-chip Flash */ /* FLASH6 : origin = 0x098000, length = 0x008000 on-chip Flash */ /* FLASH7 : origin = 0x0A0000, length = 0x008000 on-chip Flash */ /* FLASH8 : origin = 0x0A8000, length = 0x008000 on-chip Flash */ /* FLASH9 : origin = 0x0B0000, length = 0x008000 on-chip Flash */ /* FLASH10 : origin = 0x0B8000, length = 0x002000 on-chip Flash */ /* FLASH11 : origin = 0x0BA000, length = 0x002000 on-chip Flash */ /* FLASH12 : origin = 0x0BC000, length = 0x002000 on-chip Flash */ /* FLASH13 : origin = 0x0BE000, length = 0x002000 on-chip Flash */ FLASHEN1 : origin = 0x088008, length = 0x037FB8 /* on-chip Flash */ /* Can not change this memory setting (Bootloader) */ FLASHN_APPINFO : origin = 0x0BFFC0, length = 0x000030 /* on-chip Flash */ // FLASH13_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ /* CPU1TOCPU2RAM : origin = 0x03A000, length = 0x000800 */ CPU1TOCPU2RAM1 : origin = 0x03A000, length = 0x000300 CPU1TOCPU2RAM2 : origin = 0x03A300, length = 0x000100 CPU1TOCPU2RAM3 : origin = 0x03A400, length = 0x000400 /* Reserved */ /* CPU2TOCPU1RAM : origin = 0x03B000, length = 0x000800 */ CPU2TOCPU1RAM1 : origin = 0x03B000, length = 0x000300 CPU2TOCPU1RAM2 : origin = 0x03B300, length = 0x000100 CPU2TOCPU1RAM3 : origin = 0x03B400, length = 0x000400 /* CMTOCPURAM : origin = 0x038000, length = 0x000800 */ CMTOCPU1RAM1 : origin = 0x038000, length = 0x000300 CMTOCPU1RAM2 : origin = 0x038300, length = 0x000500 /* Reserved */ /* CPUTOCMRAM : origin = 0x039000, length = 0x000800 */ CPU1TOCMRAM1 : origin = 0x039000, length = 0x000300 CPU1TOCMRAM2 : origin = 0x039300, length = 0x000500 /* Reserved */ CANA_MSG_RAM : origin = 0x049000, length = 0x000800 CANB_MSG_RAM : origin = 0x04B000, length = 0x000800 RESET : origin = 0x3FFFC0, length = 0x000002 } SECTIONS { codestart : > BEGIN, ALIGN(8) .text : > FLASHEN1, ALIGN(8) .cinit : > FLASHEN1, ALIGN(8) .switch : > FLASHEN1, ALIGN(8) .reset : > RESET, TYPE = DSECT /* not used, */ .stack : > RAMM0 /* There is stack size set in Properties->C2000 Linker->Basic Options-> -Stack */ #if defined(__TI_EABI__) .init_array : > FLASHEN1, ALIGN(8) .bss : > CPU1RAMGS3GS7A .data : > CPU1RAMGS3GS7A .sysmem : > RAMM0 /* Initalized sections go in Flash */ .const : > FLASHEN1, ALIGN(8) #else .pinit : > FLASHEN1, ALIGN(8) .ebss : > CPU1RAMGS3GS7A .esysmem : > RAMM0 /* Initalized sections go in Flash */ .econst : > FLASHEN1, ALIGN(8) #endif // EABI Format with no head "_" ramfuncs : LOAD = FLASHEN1, RUN = CPU1RAMGS7BGS9, LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), ALIGN(8) ramfuncs2 : LOAD = FLASHEN1, RUN = RAMD0D1, LOAD_START(Ramfuncs2LoadStart), LOAD_SIZE(Ramfuncs2LoadSize), LOAD_END(Ramfuncs2LoadEnd), RUN_START(Ramfuncs2RunStart), RUN_SIZE(Ramfuncs2RunSize), RUN_END(Ramfuncs2RunEnd), ALIGN(8) /* CLA specific sections */ Cla1Prog : LOAD = FLASHEN1, RUN = RAMLS0LS6, RUN_START(Cla1funcsRunStart), LOAD_START(Cla1funcsLoadStart), LOAD_SIZE(Cla1funcsLoadSize), ALIGN(8) CLADataLS0 : > RAMLS7 CLADataLS1 : > RAMLS7 #ifdef CLA_C /* CLA C compiler sections */ // // Must be allocated to memory the CLA has write access to // .scratchpad : > RAMLS7 .bss_cla : > RAMLS7 .const_cla : LOAD = FLASHEN1 RUN = RAMLS7, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), ALIGN(8) #endif //CLA_C /* AppInfo */ AppInfoFiles : > FLASHN_APPINFO, ALIGN(8) } /* //=========================================================================== // End of file. //=========================================================================== */