;// TI File $Revision: /main/1 $
;// Checkin $Date: December 1, 2004   11:11:32 $
;//###########################################################################
;//
;// FILE:  DSP28xxx_CodeStartBranch.asm	
;//
;// TITLE: Branch for redirecting code execution after boot. 
;//
;// For these examples, code_start is the first code that is executed after
;// exiting the boot ROM code. 
;//
;// The codestart section in the linker cmd file is used to physically place
;// this code at the correct memory location.  This section should be placed 
;// at the location the BOOT ROM will re-direct the code to.  For example, 
;// for boot to FLASH this code will be located at 0x3f7ff6. 
;//
;// From this code the watchdog will be disabled followed by calling the 
;// copy_section function to copy sections from flash to ram. 
;//
;// In addition, the example DSP28xxx projects are setup such that the codegen
;// entry point is also set to the code_start label.  This is done by linker 
;// option -e in the project build options.  When the debugger loads the code,
;// it will automatically set the PC to the "entry point" address indicated by
;// the -e linker option.  In this case the debugger is simply assigning the PC, 
;// it is not the same as a full reset of the device. 
;// 
;// The compiler may warn that the entry point for the project is other then
;//  _c_init00.  _c_init00 is the C environment setup and is run before 
;// main() is entered. The copy_sections code will re-direct the execution 
;// to _c_init00 and thus there is no worry and this warning can be ignored. 
;//
;//###########################################################################
;// $TI Release: DSP280x, DSP2801x Header Files V1.41 $
;// $Release Date: August 7th, 2006 $
;// Modified by: Tim Love
;// Modified Date: March 2008
;//###########################################################################


***********************************************************************

WD_DISABLE	.set	1		;set to 1 to disable WD, else set to 0
   .ref _c_int00
   ; .ref copy_sections
   .global code_start
   .ref _bootloader  ;;dsf
  ;  
***********************************************************************
* Function: codestart section
*
* Description: Branch to code starting point
***********************************************************************

    .sect "codestart"

code_start:
    .if WD_DISABLE == 1
        LB wd_disable       ;Branch to watchdog disable code
    .else
       ; LB copy_sections    ;Branch to copy_sections 
	   LB _bootloader
	 ;  LB _c_int00
    .endif

;end codestart section

***********************************************************************
* Function: wd_disable
*
* Description: Disables the watchdog timer
***********************************************************************
    .if WD_DISABLE == 1

    .sect "wddisable"
wd_disable:
    SETC OBJMODE        ;Set OBJMODE for 28x object code
    EALLOW              ;Enable EALLOW protected register access
    MOVZ DP, #7029h>>6  ;Set data page for WDCR register
    MOV @7029h, #0068h  ;Set WDDIS bit in WDCR to disable WD
    EDIS                ;Disable EALLOW protected register access
   ; LB copy_sections    ;Branch to copy_sections 
    LB _bootloader
;	LB _c_int00
    .endif

;end wd_disable

	.end
	
;//===========================================================================
;// End of file.
;//===========================================================================