-----[Print the board config pathname(s)]------------------------------------ /home/ganesh/.ti/ccs2002/0/1/BrdDat/testBoard.dat -----[Print the reset-command software log-file]----------------------------- This utility has selected a 560/2xx-class product. This utility will load the program 'libbh560v2u.out'. Loaded FPGA Image: /home/ganesh/ti/ccs2002/ccs/ccs_base/common/uscif/./././././dtc_top.jbc The library build date was 'Jan 21 2025'. The library build time was '18:27:29'. The library package version is '20.0.0.3344'. The library component version is '35.35.0.0'. The controller does not use a programmable FPGA. The controller has a version number of '6' (0x00000006). The controller has an insertion length of '0' (0x00000000). The cable+pod has a version number of '8' (0x00000008). The cable+pod has a capability number of '7423' (0x00001cff). This utility will attempt to reset the controller. This utility has successfully reset the controller. -----[Print the reset-command hardware log-file]----------------------------- The scan-path will be reset by toggling the JTAG TRST signal. The controller is the Nano-TBC VHDL. The link is a 560-class second-generation-560 cable. The software is configured for Nano-TBC VHDL features. The controller will be software reset via its registers. The controller has a logic ONE on its EMU[0] input pin. The controller has a logic ONE on its EMU[1] input pin. The controller will use falling-edge timing on output pins. The controller cannot control the timing on input pins. The scan-path link-delay has been set to exactly '2' (0x0002). The utility logic has not previously detected a power-loss. The utility logic is not currently detecting a power-loss. Loaded FPGA Image: /home/ganesh/ti/ccs2002/ccs/ccs_base/common/uscif/./././././dtc_top.jbc An error occurred while hard opening the controller. Segmentation fault (core dumped)