/*==================================================================================*/
/*	User specific Linker command file for running from FLASH						*/
/*==================================================================================*/


 _Cla1Prog_Start = _Cla1funcsRunStart;
-heap 0x400
-stack 0x400


MEMORY
{
/* Note that the memory allocation below does not create sections as necessary for
   the CLA on the F2803x.
*/


PAGE 0:
	RAML0	    : origin = 0x008000, length = 0x000800 /* on-chip RAM (L0-L1)*/
	RAML3	    : origin = 0x009000, length = 0x001000     /* data RAM (L3) */
	OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
	FLASHH      : origin = 0x3E8000, length = 0x002000     /* on-chip FLASH */
	FLASHG      : origin = 0x3EA000, length = 0x002000     /* on-chip FLASH */
	FLASHF      : origin = 0x3EC000, length = 0x002000     /* on-chip FLASH */
	FLASHE      : origin = 0x3EE000, length = 0x002000     /* on-chip FLASH */
	FLASHD      : origin = 0x3F0000, length = 0x002000     /* on-chip FLASH */
	FLASHC      : origin = 0x3F2000, length = 0x002000     /* on-chip FLASH */
	FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
	CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
	BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
	CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */

	FPUTABLES   : origin = 0x3FD860, length = 0x0006A0	  /* FPU Tables in Boot ROM */

	IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
	IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
	IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA     /* IQ Math Tables in Boot ROM */

	BOOTROM     : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
	RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
	VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */

PAGE 1 :
   BOOT_RSVD            : origin = 0x000002, length = 0x00004E     /* Part of M0, BOOT rom will use this for stack */
   RAMM0                : origin = 0x000050, length = 0x0003B0
   RAMM1                : origin = 0x000400, length = 0x000400
   dataRAM              : origin = 0x008C00, length = 0x000400
   //RAML2       : origin = 0x008C00, length = 0x000400     /* on-chip RAM block L2 */
   RAML4       : origin = 0x00A000, length = 0x002000     /* on-chip RAM block L4 */
   RAML5       : origin = 0x00C000, length = 0x002000     /* on-chip RAM block L5 */
   RAML6       : origin = 0x00E000, length = 0x002000     /* on-chip RAM block L6 */
   RAML7       : origin = 0x010000, length = 0x002000     /* on-chip RAM block L7 */
   RAML8       : origin = 0x012000, length = 0x002000     /* on-chip RAM block L8 */
   FLASHB      : origin = 0x3F0000, length = 0x004000     /* on-chip FLASH */


   CLA_CPU_MSGRAM      	: origin = 0x001480, length = 0x000080
   CPU_CLA_MSGRAM      	: origin = 0x001500, length = 0x000080


}


SECTIONS
{
   /* Allocate program areas: */
   .cinit            : > FLASHA,     PAGE = 0
   .pinit            : > FLASHA,     PAGE = 0
   .text             : > FLASHA,     PAGE = 0

   codestart         : > BEGIN       PAGE = 0

   ramfuncs          : LOAD = FLASHD,
                       RUN = RAML0,
                       LOAD_START(_RamfuncsLoadStart),
                       LOAD_END(_RamfuncsLoadEnd),
                       RUN_START(_RamfuncsRunStart),
                       LOAD_SIZE(_RamfuncsLoadSize),
                       PAGE = 0


   Cla1Prog         : LOAD = RAML3,
                      RUN = RAML3,
                      LOAD_START(_Cla1funcsLoadStart),
                      LOAD_END(_Cla1funcsLoadEnd),
                      RUN_START(_Cla1funcsRunStart),
                      LOAD_SIZE(_Cla1funcsLoadSize),
                      PAGE = 0


   csmpasswds        : > CSM_PWL     PAGE = 0
   csm_rsvd          : > CSM_RSVD    PAGE = 0

   /* Allocate uninitalized data sections: */
   .scratchpad       : > RAMM1,    PAGE = 1
   .stack            : > RAMM1,    PAGE = 1
   .ebss             : > RAML4,    PAGE = 1
   .bss_cla          : > RAML4,   PAGE = 1
   .esysmem          : > RAMM1,    PAGE = 1


   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst           : > FLASHA      PAGE = 0
   .switch           : > FLASHA      PAGE = 0

   /* Allocate IQ math areas: */
   IQmath            : > FLASHA      PAGE = 0                  /* Math Code */
   IQmathTables      : > IQTABLES     PAGE = 0, TYPE = NOLOAD   /* Math Tables In ROM */

   /* Allocate FPU math areas: */
   FPUmathTables       : > FPUTABLES,  PAGE = 0, TYPE = NOLOAD

   DMARAML5	           : > RAML5,      PAGE = 1
   DMARAML6	           : > RAML6,      PAGE = 1
   DMARAML7	           : > RAML7,      PAGE = 1
   DMARAML8	           : > RAML8,      PAGE = 1

   Cla1ToCpuMsgRAM   : > CLA_CPU_MSGRAM PAGE = 1
   CpuToCla1MsgRAM   : > CPU_CLA_MSGRAM PAGE = 1

   .reset            : > RESET,      PAGE = 0, TYPE = DSECT
   vectors           : > VECTORS     PAGE = 0, TYPE = DSECT


 /* Uncomment the section below if calling the IQNexp() or IQexp()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
   {

              IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)

   }
   */
   /* Uncomment the section below if calling the IQNasin() or IQasin()
      functions from the IQMath.lib library in order to utilize the
      relevant IQ Math table in Boot ROM (This saves space and Boot ROM
      is 1 wait-state). If this section is not uncommented, IQmathTables2
      will be loaded into other memory (SARAM, Flash, etc.) and will take
      up space, but 0 wait-state is possible.
   */
   /*
   IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
   {

              IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)

   }
   */

}


SECTIONS
{
.ebss             : >  RAML4,    PAGE = 1
.bss_cla          : >  RAML4,    PAGE = 1
}


SECTIONS
{
	Cla1DataRam1				   : > dataRAM				PAGE = 1
}