UART Module

The UART driver provides functions which can configure the data word length, baud rate, parity, and stop bits of the UART communication. It can also be used to enable or disable loopback mode, enable the FIFO enhancement, configure interrupts, and send and receive data. If FIFO enhancement is enabled, we must use the provided FIFO functions to configure and guarantee proper execution.

group uart_api

The UART module is used for UART configurations.

Defines

UART_INT_DMATX 0x20000U

DMA TX interrupt.

UART_INT_DMARX 0x10000U

DMA RX interrupt.

UART_INT_9BIT 0x1000U

9-bit address match interrupt

UART_INT_EOT 0x800U

Receive Interrupt Mask.

UART_INT_OE 0x400U

Overrun Error Interrupt Mask.

UART_INT_BE 0x200U

Break Error Interrupt Mask.

UART_INT_PE 0x100U

Parity Error Interrupt Mask.

UART_INT_FE 0x080U

Framing Error Interrupt Mask.

UART_INT_RT 0x040U

Receive Timeout Interrupt Mask.

UART_INT_TX 0x020U

Transmit Interrupt Mask.

UART_INT_RX 0x010U

Receive Interrupt Mask.

UART_CONFIG_WLEN_MASK 0x00000060UL

Mask for extracting wordlength.

UART_CONFIG_WLEN_8 0x00000060UL

8 bit data

UART_CONFIG_WLEN_7 0x00000040UL

7 bit data

UART_CONFIG_WLEN_6 0x00000020UL

6 bit data

UART_CONFIG_WLEN_5 0x00000000UL

5 bit data

UART_CONFIG_STOP_MASK 0x00000008UL

Mask for extracting stop bits.

UART_CONFIG_STOP_ONE 0x00000000UL

One stop bit.

UART_CONFIG_STOP_TWO 0x00000008UL

Two stop bits.

UART_CONFIG_PAR_MASK 0x00000086UL

Mask for extracting parity.

UART_CONFIG_PAR_NONE 0x00000000UL

No parity.

UART_CONFIG_PAR_EVEN 0x00000006UL

Even parity.

UART_CONFIG_PAR_ODD 0x00000002UL

Odd parity.

UART_CONFIG_PAR_ONE 0x00000082UL

Parity bit is one.

UART_CONFIG_PAR_ZERO 0x00000086UL

Parity bit is zero.

UART_FIFO_TX1_8 0x00000000UL

Transmit interrupt at 1/8 Full.

UART_FIFO_TX2_8 0x00000001UL

Transmit interrupt at 1/4 Full.

UART_FIFO_TX4_8 0x00000002UL

Transmit interrupt at 1/2 Full.

UART_FIFO_TX6_8 0x00000003UL

Transmit interrupt at 3/4 Full.

UART_FIFO_TX7_8 0x00000004UL

Transmit interrupt at 7/8 Full.

UART_FIFO_RX1_8 0x00000000UL

Receive interrupt at 1/8 Full.

UART_FIFO_RX2_8 0x00000008UL

Receive interrupt at 1/4 Full.

UART_FIFO_RX4_8 0x00000010UL

Receive interrupt at 1/2 Full.

UART_FIFO_RX6_8 0x00000018UL

Receive interrupt at 3/4 Full.

UART_FIFO_RX7_8 0x00000020UL

Receive interrupt at 7/8 Full.

UART_DMA_ERR_RXSTOP 0x00000004UL

Stop DMA receive if UART error.

UART_DMA_TX 0x00000002UL

Enable DMA for transmit.

UART_DMA_RX 0x00000001UL

Enable DMA for receive.

UART_RXERROR_OVERRUN 0x00000008UL
UART_RXERROR_BREAK 0x00000004UL
UART_RXERROR_PARITY 0x00000002UL
UART_RXERROR_FRAMING 0x00000001UL
UART_TXINT_MODE_FIFO 0x00000000UL

trigger based on tx FIFOlevel

UART_TXINT_MODE_EOT 0x00000010UL

trigger when transmitter idle

UART_CLK_DIVIDER 8U
UART_CLK_FREQ DEVICE_SYSCLK_FREQ

CPU SYSCLK frequency.

UART_RSR_ALL_M (UART_RSR_BE | UART_RSR_FE | UART_RSR_OE | UART_RSR_PE)
UART_CLK_IRLPBAUD16 1843200U
UART_RAW_INT false

raw interrupt

UART_MASKED_INT true

masked interrupt

UART_SIR_LOWPOWER_DISABLE false

raw interrupt

UART_SIR_LOWPOWER_ENABLE true

masked interrupt

Typedefs

typedef bool Uart_IntType
typedef bool Uart_SirLPMode

Functions

void UART_setParityMode(uint32_t base, uint32_t parity)

Sets the type of parity.

This function configures the type of parity to use for transmitting and expect when receiving. The

parity parameter must be one of UART_CONFIG_PAR_NONE, UART_CONFIG_PAR_EVEN, UART_CONFIG_PAR_ODD, UART_CONFIG_PAR_ONE, or UART_CONFIG_PAR_ZERO. The last two parameters allow direct control of the parity bit; it is always either one or zero based on the mode.
Parameters
  • base: is the base address of the UART port.

  • parity: specifies the type of parity to use.

Return

None.

uint32_t UART_getParityMode(uint32_t base)

Gets the type of parity currently being used.

This function gets the type of parity used for transmitting data and expected when receiving data.

Parameters
  • base: is the base address of the UART port.

Return

Returns the current parity settings, specified as one of UART_CONFIG_PAR_NONE, UART_CONFIG_PAR_EVEN, UART_CONFIG_PAR_ODD, UART_CONFIG_PAR_ONE, or UART_CONFIG_PAR_ZERO.

void UART_setFIFOLevel(uint32_t base, uint32_t txLevel, uint32_t rxLevel)

Sets the FIFO level at which interrupts are generated.

This function configures the FIFO level at which transmit and receive interrupts are generated.

Parameters
  • base: is the base address of the UART port.

  • txLevel: is the transmit FIFO interrupt level, specified as one of UART_FIFO_TX1_8, UART_FIFO_TX2_8, UART_FIFO_TX4_8, UART_FIFO_TX6_8, or UART_FIFO_TX7_8.

  • rxLevel: is the receive FIFO interrupt level, specified as one of UART_FIFO_RX1_8, UART_FIFO_RX2_8, UART_FIFO_RX4_8, UART_FIFO_RX6_8, or UART_FIFO_RX7_8.

Return

None.

void UART_getFIFOLevel(uint32_t base, uint32_t *txLevel, uint32_t *rxLevel)

Gets the FIFO level at which interrupts are generated.

This function gets the FIFO level at which transmit and receive interrupts are generated.

Parameters
  • base: is the base address of the UART port.

  • txLevel: is a pointer to storage for the transmit FIFO level, returned as one of UART_FIFO_TX1_8, UART_FIFO_TX2_8, UART_FIFO_TX4_8, UART_FIFO_TX6_8, or UART_FIFO_TX7_8.

  • rxLevel: is a pointer to storage for the receive FIFO level, returned as one of UART_FIFO_RX1_8, UART_FIFO_RX2_8, UART_FIFO_RX4_8, UART_FIFO_RX6_8, or UART_FIFO_RX7_8.

Return

None.

void UART_enableModule(uint32_t base)

Enables transmitting and receiving.

This function enables the UART and its transmit and receive FIFOs.

Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_disableModule(uint32_t base)

Disables transmitting and receiving.

This function disables the UART, waits for the end of transmission of the current character, and flushes the transmit FIFO.

Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_enableFIFO(uint32_t base)

Enables the transmit and receive FIFOs.

This functions enables the transmit and receive FIFOs in the UART.

Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_disableFIFO(uint32_t base)

Disables the transmit and receive FIFOs.

This function disables the transmit and receive FIFOs in the UART.

Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_enableModuleNonFIFO(uint32_t base)

Enables transmitting and receiving without FIFO.

This function enables the UART.

Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_disableModuleNonFIFO(uint32_t base)

Disables transmitting and receiving without FIFO.

This function disables the UART, waits for the end of transmission of the current character.

Parameters
  • base: is the base address of the UART port.

Return

None.

bool UART_isFIFOEnabled(uint32_t base)

Determines if the transmit and receive FIFOs are enabled

This function returns a flag indicating whether or not the transmit and receive FIFOs are enabled.

Parameters
  • base: is the base address of the UART port.

Return

Returns true if FIFOs are enabled or false if FIFOs are not enabled.

void UART_enableSIR(uint32_t base, Uart_SirLPMode bLowPower)

Enables SIR (IrDA) mode on the specified UART.

This function enables SIR (IrDA) mode on the UART. If the

bLowPower flag is set, then SIR low power mode will be selected as well. This function only has an effect if the UART has not been enabled by a call to UART_enableModule(). The call UART_enableSIR() must be made before a call to UART_setConfig() because the UART_setConfig() function calls the UART_enableModule() function. Another option is to call UART_disableModule() followed by UART_enableSIR() and then enable the UART by calling UART_enableModule().
Parameters
  • base: is the base address of the UART port.

  • bLowPower: indicates if SIR Low Power Mode is to be used. This parameter is of type UART_SirLPMode.

Note

The IrDA SIR physical layer specifies a minimum 10-ms delay between transmission and reception which needs to be provided.

Return

None.

void UART_disableSIR(uint32_t base)

Disables SIR (IrDA) mode on the specified UART.

This function disables SIR(IrDA) mode on the UART. This function only has an effect if the UART has not been enabled by a call to

UART_enableModule(). The call UART_enableSIR() must be made before a call to UART_setConfig() because the UART_setConfig() function calls the UART_enableModule() function. Another option is to call UART_disableModule() followed by UART_enableSIR() and then enable the UART by calling UART_enableModule().
Parameters
  • base: is the base address of the UART port.

Note

The IrDA SIR physical layer specifies a minimum 10-ms delay between transmission and reception which needs to be provided.

Return

None.

void UART_setTxIntMode(uint32_t base, uint32_t mode)

Sets the operating mode for the UART transmit interrupt.

This function allows the mode of the UART transmit interrupt to be set. By default, the transmit interrupt is asserted when the FIFO level falls past a threshold set via a call to

UART_setFIFOLevel(). Alternatively, if this function is called with mode set to UART_TXINT_MODE_EOT, the transmit interrupt is asserted once the transmitter is completely idle - the transmit FIFO is empty and all bits, including any stop bits, have cleared the transmitter.
Parameters
  • base: is the base address of the UART port.

  • mode: is the operating mode for the transmit interrupt. It may be UART_TXINT_MODE_EOT to trigger interrupts when the transmitter is idle or UART_TXINT_MODE_FIFO to trigger based on the current transmit FIFO level.

Return

None.

uint32_t UART_getTxIntMode(uint32_t base)

Returns the current operating mode for the UART transmit interrupt.

This function returns the current operating mode for the UART transmit interrupt. The return value is

UART_TXINT_MODE_EOT if the transmit interrupt is currently configured to be asserted once the transmitter is completely idle - the transmit FIFO is empty and all bits, including any stop bits, have cleared the transmitter. The return value is UART_TXINT_MODE_FIFO if the interrupt is configured to be asserted based on the level of the transmit FIFO.
Parameters
  • base: is the base address of the UART port.

Return

Returns UART_TXINT_MODE_FIFO or UART_TXINT_MODE_EOT.

bool UART_isDataAvailable(uint32_t base)

Determines if there are any characters in the receive FIFO.

This function returns a flag indicating whether or not there is data available in the receive FIFO.

Parameters
  • base: is the base address of the UART port.

Return

Returns true if there is data in the receive FIFO or false if there is no data in the receive FIFO.

bool UART_isSpaceAvailable(uint32_t base)

Determines if there is any space in the transmit FIFO.

This function returns a flag indicating whether or not there is space available in the transmit FIFO.

Parameters
  • base: is the base address of the UART port.

Return

Returns true if there is space available in the transmit FIFO or false if there is no space available in the transmit FIFO.

int32_t UART_readCharNonBlocking(uint32_t base)

Receives a character from the specified port.

This function gets a character from the receive FIFO for the specified port.

Parameters
  • base: is the base address of the UART port.

Return

Returns the character read from the specified port, cast as a int32_t. A -1 is returned if there are no characters present in the receive FIFO. The UART_isDataAvailable() function should be called before attempting to call this function.

int32_t UART_readChar(uint32_t base)

Waits for a character from the specified port.

This function gets a character from the receive FIFO for the specified port. If there are no characters available, this function waits until a character is received before returning.

Parameters
  • base: is the base address of the UART port.

Return

Returns the character read from the specified port, cast as a int32_t.

void UART_writeChar(uint32_t base, uint8_t data)

Waits to send a character from the specified port.

This function sends the character

data to the transmit FIFO for the specified port. If there is no space available in the transmit FIFO, this function waits until there is space available before returning.
Parameters
  • base: is the base address of the UART port.

  • data: is the character to be transmitted.

Return

None.

void UART_setBreakConfig(uint32_t base, bool breakState)

Causes a BREAK to be sent.

Calling this function with

bBreakState set to true asserts a break condition on the UART. Calling this function with bBreakState set to false removes the break condition. For proper transmission of a break command, the break must be asserted for at least two complete frames.
Parameters
  • base: is the base address of the UART port.

  • breakState: controls the output level.

Return

None.

bool UART_isBusy(uint32_t base)

Determines whether the UART transmitter is busy or not.

This function allows the caller to determine whether all transmitted bytes have cleared the transmitter hardware. If

false is returned, the transmit FIFO is empty and all bits of the last transmitted character, including all stop bits, have left the hardware shift register.
Parameters
  • base: is the base address of the UART port.

Return

Returns true if the UART is transmitting or false if all transmissions are complete.

void UART_registerInterrupt(uint32_t interruptNum, void (*pfnHandler)(void))

Registers an interrupt handler for a UART interrupt.

This function does the actual registering of the interrupt handler. This function enables the global interrupt in the interrupt controller; specific UART interrupts must be enabled via

UART_enableInterrupt(). It is the interrupt handler’s responsibility to clear the interrupt source.
Parameters
  • interruptNum: specifies the interrupt in question.

  • pfnHandler: is a pointer to the function to be called when the UART interrupt occurs.

See

Interrupt_register() for important information about registering interrupt handlers.

Return

None.

void UART_unregisterInterrupt(uint32_t interruptNum)

Unregisters an interrupt handler for a UART interrupt.

This function does the actual unregistering of the interrupt handler. It clears the handler to be called when a UART interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.

Parameters
  • interruptNum: specifies the interrupt in question.

See

Interrupt_unregister() for important information about registering interrupt handlers.

Return

None.

void UART_clearGlobalInterruptFlag(uint32_t base)

Clears UART global interrupt flag.

This function clears the indicated UART global interrupt flag register.

Parameters
  • base: is the base address of the UART port.

Return

None.

bool UART_getGlobalInterruptFlagStatus(uint32_t base)

Returns the status of UART global interrupt flag.

This function returns the status of UART global interrupt flag register.

Parameters
  • base: is the base address of the UART port.

Return

Returns the status of UART global interrupt flag register.

void UART_enableInterrupt(uint32_t base, uint32_t intFlags)

Enables individual UART interrupt sources.

This function enables the indicated UART interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt disabled sources have no effect on the processor.

Parameters
  • base: is the base address of the UART port.

  • intFlags: is the bit mask of the interrupt sources to be enabled.

The intFlags parameter is the logical OR of any of the following:

  • UART_INT_DMATX - Transmit DMA interrupt

  • UART_INT_DMARX - Receive DMA interrupt

  • UART_INT_9BIT - 9-bit Address Match interrupt

  • UART_INT_EOT - End of Transmission interrupt

  • UART_INT_OE - Overrun Error interrupt

  • UART_INT_BE - Break Error interrupt

  • UART_INT_PE - Parity Error interrupt

  • UART_INT_FE - Framing Error interrupt

  • UART_INT_RT - Receive Timeout interrupt

  • UART_INT_TX - Transmit interrupt

  • UART_INT_RX - Receive interrupt

Return

None.

void UART_disableInterrupt(uint32_t base, uint32_t intFlags)

Disables individual UART interrupt sources.

This function disables the indicated UART interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt disabled sources have no effect on the processor.

Parameters
  • base: is the base address of the UART port.

  • intFlags: is the bit mask of the interrupt sources to be disabled.

The intFlags parameter has the same definition as the intFlags parameter to UART_enableInterrupt().

Return

None.

uint32_t UART_getInterruptStatus(uint32_t base, Uart_IntType masked)

Gets the current interrupt status.

This function returns the interrupt status for the specified UART. Either the raw interrupt status or the status of interrupts that are allowed to reflect to the processor can be returned.

Parameters
  • base: is the base address of the UART port.

  • masked: of type Uart_IntType is UART_RAW_INT if the raw interrupt status is requested and UART_MASKED_INT if the masked interrupt status is requested.

Return

Returns the current interrupt status, enumerated as a bit field of values described in UART_enableInterrupt().

void UART_clearInterruptStatus(uint32_t base, uint32_t intFlags)

Clears UART interrupt sources.

The specified UART interrupt sources are cleared, so that they no longer assert. This function must be called in the interrupt handler to keep the interrupt from being triggered again immediately upon exit.

Parameters
  • base: is the base address of the UART port.

  • intFlags: is a bit mask of the interrupt sources to be cleared.

The intFlags parameter has the same definition as the intFlags parameter to UART_enableInterrupt().

Return

None.

void UART_enableDMA(uint32_t base, uint32_t dmaFlags)

Enable UART uDMA operation.

The specified UART uDMA features are enabled. The UART can be configured to use uDMA for transmit or receive and to disable receive if an error occurs. The

dmaFlags parameter is the logical OR of any of the following values:
Parameters
  • base: is the base address of the UART port.

  • dmaFlags: is a bit mask of the uDMA features to enable.

  • UART_DMA_RX - enable uDMA for receive

  • UART_DMA_TX - enable uDMA for transmit

  • UART_DMA_ERR_RXSTOP - disable uDMA receive on UART error

Note

The uDMA controller must also be set up before DMA can be used with the UART.

Return

None.

void UART_disableDMA(uint32_t base, uint32_t dmaFlags)

Disable UART uDMA operation.

This function is used to disable UART uDMA features that were enabled by

UART_enableDMA(). The specified UART uDMA features are disabled. The dmaFlags parameter is the logical OR of any of the following values:
Parameters
  • base: is the base address of the UART port.

  • dmaFlags: is a bit mask of the uDMA features to disable.

  • UART_DMA_RX - disable uDMA for receive

  • UART_DMA_TX - disable uDMA for transmit

  • UART_DMA_ERR_RXSTOP - do not disable uDMA receive on UART error

Return

None.

uint32_t UART_getRxError(uint32_t base)

Gets current receiver errors.

This function returns the current state of each of the 4 receiver error sources. The returned errors are equivalent to the four error bits returned via the previous call to

UART_readChar() or UART_readCharNonBlocking() with the exception that the overrun error is set immediately when the overrun occurs rather than when a character is next read.
Parameters
  • base: is the base address of the UART port.

Return

Returns a logical OR combination of the receiver error flags, UART_RXERROR_FRAMING, UART_RXERROR_PARITY, UART_RXERROR_BREAK and UART_RXERROR_OVERRUN.

void UART_clearRxError(uint32_t base)

Clears all reported receiver errors.

This function is used to clear all receiver error conditions reported via

UART_getRxError(). If using the overrun, framing error, parity error or break interrupts, this function must be called after clearing the interrupt to ensure that later errors of the same type trigger another interrupt.
Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_enable9Bit(uint32_t base)

Enables 9-bit mode on the specified UART.

This function enables the 9-bit operational mode of the UART.

Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_disable9Bit(uint32_t base)

Disables 9-bit mode on the specified UART.

This function disables the 9-bit operational mode of the UART.

Parameters
  • base: is the base address of the UART port.

Return

None.

void UART_set9BitAddress(uint32_t base, uint8_t addr, uint8_t mask)

Sets the device address(es) for 9-bit mode.

This function configures the device address or range of device addresses that respond to requests on the 9-bit UART port. The received address is masked with the mask and then compared against the given address, allowing either a single address (if

mask is 0xff) or a set of addresses to be matched.
Parameters
  • base: is the base address of the UART port.

  • addr: is the device address.

  • mask: is the device address mask.

Return

None.

void UART_setIrDALPDivisor(uint32_t base, uint32_t uartClk)

Sets the SIR (IrDA) Low Power Divisor.

This function configures the SIR (IrDA) Low power divisor. This function is used only if the SIR ( IrDA ) is to be used in Low Power mode which is indicated as part of the

UART_enableSIR().
Parameters
  • base: is the base address of the UART port.

  • uartClk: is the rate of the clock supplied to the UART module. It should be provided as UART_CLK_FREQ using the updated clk rate.

Return

None.

void UART_enableLoopback(uint32_t base)

Enables internal loopback mode for an UART port.

This function configures an UART port in internal loopback mode to help with diagnostics and debug.In this mode, the UART Tx path is fed through the UARTRx path. This allows data to be transferred between the TX and RX of the same UART port, without having to go through I/O’s.UART_writeChar() &

UART_writeCharNonBlocking() can be used along with this function.
Parameters
  • base: is the base address of the UART module.

Return

None.

void UART_disableLoopback(uint32_t base)

Disables internal loopback mode for an UART port.

This function disables internal loopback mode in an UART port. In this mode, the UARTTx path is not fed through the UARTRx path. This prevents data to be transferred between the TX and RX of the same UART port, without having to go through I/O’s.

Parameters
  • base: is the base address of the UART module.

Return

None.

void UART_send9BitAddress(uint32_t base, uint8_t addr)

Sends an address character from the specified port when operating in 9-bit mode.

This function waits until all data has been sent from the specified port and then sends the given address as an address byte. It then waits until the address byte has been transmitted before returning.

Parameters
  • base: is the base address of the UART port.

  • addr: is the address to be transmitted.

Return

None.

void UART_stop9BitDataMode(uint32_t base, uint32_t lcrh)

Exits the 9-bit data transmission mode for the specified port.

This function waits until all data has been sent from the specified port and then restores the settings for the normal transmission mode.

Parameters
  • base: is the base address of the UART port.

  • lcrh: is the address/data setting needed to restore the normal transmission mode after the full 9-bit data transmission.

Return

None.

uint32_t UART_configure9BitDataMode(uint32_t base)

Configures the specified port to operate in 9-bit data mode.

This function waits until all data has been sent from the specified port and then configures to send 9-bit data.

Parameters
  • base: is the base address of the UART port.

Note

The 9-bit data is sent after the UART_send9BitAddress() is complete. The data transmission is left to the user to handle outside this API. This can be done using UART_writeChar() or UART_writeCharNonBlocking().

Return

Returns the address/data setting needed to restore the normal transmission mode after the full 9-bit data transmission.

void UART_setConfig(uint32_t base, uint32_t uartClk, uint32_t baud, uint32_t config)

Sets the configuration of a UART.

This function configures the UART for operation in the specified data format. The baud rate is provided in the

baud parameter and the data format in the config parameter.
Parameters
  • base: is the base address of the UART port.

  • uartClk: is the rate of the clock supplied to the UART module. It should be provided as UART_CLK_FREQ using the updated clk rate

  • baud: is the desired baud rate.

  • config: is the data format for the port (number of data bits, number of stop bits, and parity).

The config parameter is the logical OR of three values: the number of data bits, the number of stop bits, and the parity. UART_CONFIG_WLEN_8, UART_CONFIG_WLEN_7, UART_CONFIG_WLEN_6, and UART_CONFIG_WLEN_5 select from eight to five data bits per byte (respectively). UART_CONFIG_STOP_ONE and UART_CONFIG_STOP_TWO select one or two stop bits (respectively). UART_CONFIG_PAR_NONE UART_CONFIG_PAR_EVEN, UART_CONFIG_PAR_ODD, UART_CONFIG_PAR_ONE, and UART_CONFIG_PAR_ZERO select the parity mode (no parity bit, even parity bit, odd parity bit, parity bit always one, and parity bit always zero, respectively).

Return

None.

void UART_getConfig(uint32_t base, uint32_t uartClk, uint32_t *baud, uint32_t *config)

Gets the current configuration of a UART.

This function determines the baud rate and data format for the UART, given an explicitly provided peripheral clock. The returned baud rate is the actual baud rate; it may not be the exact baud rate requested or an `

official’ baud rate. The data format returned in config is enumerated the same as the config parameter of UART_setConfig().
Parameters
  • base: is the base address of the UART port.

  • uartClk: is the rate of the clock supplied to the UART module. It should be provided as UART_CLK_FREQ using the updated clk rate

  • baud: is the desired baud rate.

  • baud: is a pointer to storage for the baud rate.

  • config: is a pointer to storage for the data format.

Return

None.

bool UART_writeCharNonBlocking(uint32_t base, uint8_t data)

Sends a character to the specified port.

This function writes the character

data to the transmit FIFO for the specified port. This function does not block, so if there is no space available, then a false is returned and the application must retry the function later.
Parameters
  • base: is the base address of the UART port.

  • data: is the character to be transmitted.

Return

Returns true if the character was successfully placed in the transmit FIFO or false if there was no space available in the transmit FIFO.

The code for this module is contained in driverlib/uart.c, with driverlib/uart.h containing the API declarations for use by applications.