MEMCFG Module

The MemCfg module provides an API to configure the device’s Memory Control Module. The functions that are provided fall into three main categories: RAM section configuration, access violation status and interrupts, and memory error status an interrupts. The RAM section configuration functions can initialize RAM, configure access protection settings, and configure section ownership. The access violation and memory error categories contain functions that can return violation and error status and address information as well as configure interrupts that can be generated as a result of these issues.

group memcfg_api

Defines

MEMCFG_SECT_TYPE_MASK 0xFF000000U
MEMCFG_SECT_TYPE_D 0x00000000U
MEMCFG_SECT_TYPE_LS 0x01000000U
MEMCFG_SECT_TYPE_GS 0x02000000U
MEMCFG_SECT_TYPE_MSG 0x03000000U
MEMCFG_SECT_NUM_MASK 0x00FFFFFFU
MEMCFG_XACCPROTX_M ((uint32_t)MEMCFG_GSXACCPROT0_FETCHPROT_GS0

| \

(uint32_t)

MEMCFG_GSXACCPROT0_CPUWRPROT_GS0

| \

(uint32_t)

MEMCFG_GSXACCPROT0_DMAWRPROT_GS0)
MEMCFG_XTEST_M MEMCFG_DXTEST_TEST_M0_M
MEMCFG_NMVIOL_MASK 0x0000FFFFU
MEMCFG_MVIOL_MASK 0x000F0000U
MEMCFG_MVIOL_SHIFT 16U
MEMCFG_SECT_M0 0x00000001U

M0 RAM.

MEMCFG_SECT_M1 0x00000002U

M1 RAM.

MEMCFG_SECT_D0 0x00000004U

D0 RAM.

MEMCFG_SECT_D1 0x00000008U

D1 RAM.

MEMCFG_SECT_DX_ALL 0x0000000FU

All M and D RAM.

MEMCFG_SECT_LS0 0x01000001U

LS0 RAM.

MEMCFG_SECT_LS1 0x01000002U

LS1 RAM.

MEMCFG_SECT_LS2 0x01000004U

LS2 RAM.

MEMCFG_SECT_LS3 0x01000008U

LS3 RAM.

MEMCFG_SECT_LS4 0x01000010U

LS4 RAM.

MEMCFG_SECT_LS5 0x01000020U

LS5 RAM.

MEMCFG_SECT_LSX_ALL 0x0100003FU

All LS RAM.

MEMCFG_SECT_GS0 0x02000001U

GS0 RAM.

MEMCFG_SECT_GS1 0x02000002U

GS1 RAM.

MEMCFG_SECT_GS2 0x02000004U

GS2 RAM.

MEMCFG_SECT_GS3 0x02000008U

GS3 RAM.

MEMCFG_SECT_GS4 0x02000010U

GS4 RAM.

MEMCFG_SECT_GS5 0x02000020U

GS5 RAM.

MEMCFG_SECT_GS6 0x02000040U

GS6 RAM.

MEMCFG_SECT_GS7 0x02000080U

GS7 RAM.

MEMCFG_SECT_GS8 0x02000100U

GS8 RAM.

MEMCFG_SECT_GS9 0x02000200U

GS9 RAM.

MEMCFG_SECT_GS10 0x02000400U

GS10 RAM.

MEMCFG_SECT_GS11 0x02000800U

GS11 RAM.

MEMCFG_SECT_GS12 0x02001000U

GS12 RAM.

MEMCFG_SECT_GS13 0x02002000U

GS13 RAM.

MEMCFG_SECT_GS14 0x02004000U

GS14 RAM.

MEMCFG_SECT_GS15 0x02008000U

GS15 RAM.

MEMCFG_SECT_GSX_ALL 0x0200FFFFU

All GS RAM.

MEMCFG_SECT_MSGCPUTOCLA1 0x03000002U

CPU-to-CLA1 message RAM.

MEMCFG_SECT_MSGCLA1TOCPU 0x03000004U

CLA1-to-CPU message RAM.

MEMCFG_SECT_MSGX_ALL 0x03000006U

All message RAM.

MEMCFG_SECT_ALL 0xFFFFFFFFU

All configurable RAM.

MEMCFG_PROT_ALLOWCPUFETCH 0x00000000U

CPU fetch allowed.

MEMCFG_PROT_BLOCKCPUFETCH 0x00000001U

CPU fetch blocked.

MEMCFG_PROT_ALLOWCPUWRITE 0x00000000U

CPU write allowed.

MEMCFG_PROT_BLOCKCPUWRITE 0x00000002U

CPU write blocked.

MEMCFG_PROT_ALLOWDMAWRITE 0x00000000U

DMA write allowed (GSxRAM)

MEMCFG_PROT_BLOCKDMAWRITE 0x00000004U

DMA write blocked (GSxRAM)

MEMCFG_NMVIOL_CPUREAD 0x00000001U

Non-master CPU read access.

MEMCFG_NMVIOL_CPUWRITE 0x00000002U

Non-master CPU write access.

MEMCFG_NMVIOL_CPUFETCH 0x00000004U

Non-master CPU fetch access.

MEMCFG_NMVIOL_DMAWRITE 0x00000008U

Non-master DMA write access.

MEMCFG_NMVIOL_CLA1READ 0x00000010U

Non-master CLA1 read access.

MEMCFG_NMVIOL_CLA1WRITE 0x00000020U

Non-master CLA1 write access.

MEMCFG_NMVIOL_CLA1FETCH 0x00000040U

Non-master CLA1 fetch access.

MEMCFG_MVIOL_CPUFETCH 0x00010000U

Master CPU fetch access.

MEMCFG_MVIOL_CPUWRITE 0x00020000U

Master CPU write access.

MEMCFG_MVIOL_DMAWRITE 0x00040000U

Master DMA write access.

MEMCFG_CERR_CPUREAD 0x0001U

Correctable CPU read error.

MEMCFG_CERR_DMAREAD 0x0002U

Correctable DMA read error.

MEMCFG_CERR_CLA1READ 0x0004U

Correctable CLA1 read error.

MEMCFG_UCERR_CPUREAD 0x0001U

Uncorrectable CPU read error.

MEMCFG_UCERR_DMAREAD 0x0002U

Uncorrectable DMA read error.

MEMCFG_UCERR_CLA1READ 0x0004U

Uncorrectable CLA1 read error.

Enums

enum MemCfg_CLAMemoryType

Values that can be passed to MemCfg_setCLAMemType() as the claMemType parameter.

Values:

enumerator MEMCFG_CLA_MEM_DATA

Section is CLA data memory.

enumerator MEMCFG_CLA_MEM_PROGRAM

Section is CLA program memory.

enum MemCfg_LSRAMMasterSel

Values that can be passed to MemCfg_setLSRAMMasterSel() as the masterSel parameter.

Values:

enumerator MEMCFG_LSRAMMASTER_CPU_ONLY

CPU is the master of the section.

enumerator MEMCFG_LSRAMMASTER_CPU_CLA1

CPU and CLA1 share this section.

enum MemCfg_TestMode

Values that can be passed to MemCfg_setTestMode() as the testMode parameter.

Values:

enumerator MEMCFG_TEST_FUNCTIONAL = 0

Functional mode. Test mode is disabled.

enumerator MEMCFG_TEST_WRITE_DATA = 1

Writes allowed to data only.

enumerator MEMCFG_TEST_WRITE_ECC = 2

Writes allowed to ECC only (for DxRAM/MxRAM)

enumerator MEMCFG_TEST_WRITE_PARITY = 2

Writes allowed to parity only (for LSxRAM, GSxRAM, and MSGxRAM)

Functions

void MemCfg_setCLAMemType(uint32_t ramSections, MemCfg_CLAMemoryType claMemType)

Sets the CLA memory type of the specified RAM section.

This function sets the CLA memory type configuration of the RAM section. If the

claMemType parameter is MEMCFG_CLA_MEM_DATA, the RAM section will be configured as CLA data memory. If MEMCFG_CLA_MEM_PROGRAM, the RAM section will be configured as CLA program memory.
Parameters
  • ramSections: is the logical OR of the sections to be configured.

  • claMemType: indicates data memory or program memory.

The ramSections parameter is an OR of the following indicators: MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx.

Note

This API only applies to LSx RAM and has no effect if the CLA isn’t master of the memory section.

See

MemCfg_setLSRAMMasterSel()

Return

None.

void MemCfg_enableViolationInterrupt(uint32_t intFlags)

Enables individual RAM access violation interrupt sources.

Return

None.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be enabled. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-master CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-master CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-master CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-master DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-master CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-master CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-master CLA1 fetch access

    • MEMCFG_MVIOL_CPUFETCH - Master CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Master CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Master DMA write access This function enables the indicated RAM access violation interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

void MemCfg_disableViolationInterrupt(uint32_t intFlags)

Disables individual RAM access violation interrupt sources.

This function disables the indicated RAM access violation interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be disabled. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-master CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-master CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-master CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-master DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-master CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-master CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-master CLA1 fetch access

    • MEMCFG_MVIOL_CPUFETCH - Master CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Master CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Master DMA write access

Note

Note that only non-master violations may generate interrupts.

Return

None.

uint32_t MemCfg_getViolationInterruptStatus(void)

Gets the current RAM access violation status.

This function returns the RAM access violation status. This function will return flags for both master and non-master access violations although only the non-master flags have the ability to cause the generation of an interrupt.

Return

Returns the current violation status, enumerated as a bit field of the values:

  • MEMCFG_NMVIOL_CPUREAD - Non-master CPU read access

  • MEMCFG_NMVIOL_CPUWRITE - Non-master CPU write access

  • MEMCFG_NMVIOL_CPUFETCH - Non-master CPU fetch access

  • MEMCFG_NMVIOL_DMAWRITE - Non-master DMA write access

  • MEMCFG_NMVIOL_CLA1READ - Non-master CLA1 read access

  • MEMCFG_NMVIOL_CLA1WRITE - Non-master CLA1 write access

  • MEMCFG_NMVIOL_CLA1FETCH - Non-master CLA1 fetch access

  • MEMCFG_MVIOL_CPUFETCH - Master CPU fetch access

  • MEMCFG_MVIOL_CPUWRITE - Master CPU write access

  • MEMCFG_MVIOL_DMAWRITE - Master DMA write access

void MemCfg_forceViolationInterrupt(uint32_t intFlags)

Sets the RAM access violation status.

This function sets the RAM access violation status. This function will set flags for both master and non-master access violations, and an interrupt will be generated if it is enabled.

Parameters
  • intFlags: is a bit mask of the access violation flags to be set. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-master CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-master CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-master CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-master DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-master CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-master CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-master CLA1 fetch access

    • MEMCFG_MVIOL_CPUFETCH - Master CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Master CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Master DMA write access

Return

None.

void MemCfg_clearViolationInterruptStatus(uint32_t intFlags)

Clears RAM access violation flags.

Return

None.

Parameters
  • intFlags: is a bit mask of the access violation flags to be cleared. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-master CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-master CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-master CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-master DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-master CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-master CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-master CLA1 fetch access

    • MEMCFG_MVIOL_CPUFETCH - Master CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Master CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Master DMA write access

void MemCfg_setCorrErrorThreshold(uint32_t threshold)

Sets the correctable error threshold value.

This value sets the error-count threshold at which a correctable error interrupt is generated. That is when the error count register reaches the value specified by the

threshold parameter, an interrupt is generated if it is enabled.
Parameters
  • threshold: is the correctable error threshold.

Return

None.

uint32_t MemCfg_getCorrErrorCount(void)

Gets the correctable error count.

Return

Returns the number of correctable error have occurred.

void MemCfg_enableCorrErrorInterrupt(uint32_t intFlags)

Enables individual RAM correctable error interrupt sources.

This function enables the indicated RAM correctable error interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be enabled. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

void MemCfg_disableCorrErrorInterrupt(uint32_t intFlags)

Disables individual RAM correctable error interrupt sources.

This function disables the indicated RAM correctable error interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be disabled. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

uint32_t MemCfg_getCorrErrorInterruptStatus(void)

Gets the current RAM correctable error interrupt status.

Return

Returns the current error interrupt status. Will return a value of MEMCFG_CERR_CPUREAD if an interrupt has been generated. If not, the function will return 0.

void MemCfg_forceCorrErrorInterrupt(uint32_t intFlags)

Sets the RAM correctable error interrupt status.

This function sets the correctable error interrupt flag.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be set. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

void MemCfg_clearCorrErrorInterruptStatus(uint32_t intFlags)

Clears the RAM correctable error interrupt status.

This function clears the correctable error interrupt flag.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be cleared. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

uint32_t MemCfg_getCorrErrorStatus(void)

Gets the current correctable RAM error status.

Return

Returns the current error status, enumerated as a bit field of MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ

uint32_t MemCfg_getUncorrErrorStatus(void)

Gets the current uncorrectable RAM error status.

Return

Returns the current error status, enumerated as a bit field of MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ, or MEMCFG_UCERR_ECATMEMREAD.

void MemCfg_forceCorrErrorStatus(uint32_t stsFlags)

Sets the specified correctable RAM error status flag.

This function sets the specified correctable RAM error status flag.

Parameters
  • stsFlags: is a bit mask of the error sources. This parameter can be any of the following values: MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ

Return

None.

void MemCfg_forceUncorrErrorStatus(uint32_t stsFlags)

Sets the specified uncorrectable RAM error status flag.

This function sets the specified uncorrectable RAM error status flag.

Parameters
  • stsFlags: is a bit mask of the error sources. This parameter can be any of the following values: MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ, or MEMCFG_UCERR_ECATMEMREAD.

Return

None.

void MemCfg_clearCorrErrorStatus(uint32_t stsFlags)

Clears correctable RAM error flags.

This function clears the specified correctable RAM error flags.

Parameters
  • stsFlags: is a bit mask of the status flags to be cleared. This parameter can be any of the following : MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ

Return

None.

void MemCfg_clearUncorrErrorStatus(uint32_t stsFlags)

Clears uncorrectable RAM error flags.

This function clears the specified uncorrectable RAM error flags.

Parameters
  • stsFlags: is a bit mask of the status flags to be cleared. This parameter can be any of the following : MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ, or MEMCFG_UCERR_ECATMEMREAD.

Return

None.

void MemCfg_enableROMWaitState(void)

Enables ROM wait state.

This function enables the ROM wait state. This mean CPU accesses to ROM are 1-wait.

Return

None.

void MemCfg_disableROMWaitState(void)

Disables ROM wait state.

This function enables the ROM wait state. This mean CPU accesses to ROM are 0-wait.

Return

None.

void MemCfg_enableROMPrefetch(void)

Enables ROM prefetch.

This function enables the ROM prefetch for both secure ROM and boot ROM.

Return

None.

void MemCfg_disableROMPrefetch(void)

Disables ROM prefetch.

This function enables the ROM prefetch for both secure ROM and boot ROM.

Return

None.

void MemCfg_lockConfig(uint32_t memSections)

Locks the writes to the configuration of specified memory sections.

This function locks writes to the access protection and master select configuration of a memory section.That means calling

MemCfg_setProtection() or MemCfg_setLSRAMMasterSel() for a locked memory section will have no effect until MemCfg_unlockConfig() is called.
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_D0 and MEMCFG_SECT_D1 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_unlockConfig(uint32_t memSections)

Unlocks the writes to the configuration of a memory section.

This function unlocks writes to the access protection and master select configuration of a memory section that has been locked using

MemCfg_lockConfig().
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_D0 and MEMCFG_SECT_D1 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_commitConfig(uint32_t memSections)

Permanently locks writes to the configuration of a memory section.

This function permanently locks writes to the access protection and master select configuration of a memory section. That means calling

MemCfg_setProtection() or MemCfg_setLSRAMMasterSel() for a locked memory section will have no effect. To lock the configuration in a nonpermanent way, use MemCfg_lockConfig().
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_D0 and MEMCFG_SECT_D1 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_setProtection(uint32_t memSection, uint32_t protectMode)

Sets the access protection mode of a single memory section.

This function sets the access protection mode of a specified memory section. The mode is passed into the

protectMode parameter as the logical OR of the following values:
  • MEMCFG_PROT_ALLOWCPUFETCH or MEMCFG_PROT_BLOCKCPUFETCH - CPU fetch

  • MEMCFG_PROT_ALLOWCPUWRITE or MEMCFG_PROT_BLOCKCPUWRITE - CPU write

  • MEMCFG_PROT_ALLOWDMAWRITE or MEMCFG_PROT_BLOCKDMAWRITE - DMA write

Parameters
  • memSection: is the memory section to be configured.

  • protectMode: is the logical OR of the settings to be applied.

The memSection parameter is one of the following indicators:

  • MEMCFG_SECT_D0 or MEMCFG_SECT_D1

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx

This function will have no effect if the associated registers have been locked by MemCfg_lockConfig() or MemCfg_commitConfig() or if the memory is configured as CLA program memory.

Return

None.

void MemCfg_setLSRAMMasterSel(uint32_t ramSection, MemCfg_LSRAMMasterSel masterSel)

Sets the master of the specified LSxRAM section.

This function sets the master select configuration of the LSxRAM section.If the

masterSel parameter is MEMCFG_LSRAMMASTER_CPU_ONLY, the LSxRAM section passed into the ramSection parameter will be dedicated to the CPU. If MEMCFG_LSRAMMASTER_CPU_CLA1, the memory section will be shared between the CPU and the CLA.
Parameters
  • ramSection: is the LSxRAM section to be configured.

  • masterSel: is the sharing selection.

The ramSection parameter should be a value from MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx.

This function will have no effect if the associated registers have been locked by MemCfg_lockConfig() or MemCfg_commitConfig().

Note

This API only applies to LSxRAM.

Return

None.

void MemCfg_setTestMode(uint32_t memSection, MemCfg_TestMode testMode)

Sets the test mode of the specified memory section.

This function sets the test mode configuration of the RAM section. The

testMode parameter can take one of the following values:
  • MEMCFG_TEST_FUNCTIONAL

  • MEMCFG_TEST_WRITE_DATA

  • MEMCFG_TEST_WRITE_ECC

  • MEMCFG_TEST_WRITE_PARITY

Parameters
  • memSection: is the memory section to be configured.

  • testMode: is the test mode selected.

The memSection parameter is one of the following indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1

  • MEMCFG_SECT_D0, MEMCFG_SECT_D1

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx

  • MEMCFG_SECT_MSGCPUTOCPU, MEMCFG_SECT_MSGCPUTOCLA1, or MEMCFG_SECT_MSGCLA1TOCPU

Return

None.

void MemCfg_initSections(uint32_t ramSections)

Starts the initialization the specified RAM sections.

This function starts the initialization of the specified RAM sections. Use

MemCfg_getInitStatus() to check if the initialization is done.
Parameters
  • ramSections: is the logical OR of the sections to be initialized.

The ramSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1, MEMCFG_SECT_D0, MEMCFG_SECT_D1, or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx, or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx, or MEMCFG_SECT_GSX_ALL

  • MEMCFG_SECT_MSGCPUTOCPU, MEMCFG_SECT_MSGCPUTOCLA1, or MEMCFG_SECT_MSGCLA1TOCPU

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

bool MemCfg_getInitStatus(uint32_t ramSections)

Get the status of initialized RAM sections.

This function gets the initialization status of the RAM sections specified by the

ramSections parameter.
Parameters
  • ramSections: is the logical OR of the sections to be checked.

The ramSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1, MEMCFG_SECT_D0, MEMCFG_SECT_D1, or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx, or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx, or MEMCFG_SECT_GSX_ALL

  • MEMCFG_SECT_MSGCPUTOCPU, MEMCFG_SECT_MSGCPUTOCLA1, or MEMCFG_SECT_MSGCLA1TOCPU

  • OR use MEMCFG_SECT_ALL to get status of all possible sections.

Note

Use MemCfg_initSections() to start the initialization.

Return

Returns true if all the sections specified by ramSections have been initialized and false if not.

uint32_t MemCfg_getViolationAddress(uint32_t intFlag)

Get the violation address associated with a intFlag.

Return

Returns the violation address associated with the intFlag.

Parameters
  • intFlag: is the type of access violation as indicated by ONE of these values:

    • MEMCFG_NMVIOL_CPUREAD - Non-master CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-master CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-master CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-master DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-master CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-master CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-master CLA1 fetch access

    • MEMCFG_MVIOL_CPUFETCH - Master CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Master CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Master DMA write access

uint32_t MemCfg_getCorrErrorAddress(uint32_t stsFlag)

Get the correctable error address associated with a stsFlag.

Return

Returns the error address associated with the stsFlag.

Parameters
  • stsFlag: is the type of error to which the returned address will correspond. Can currently take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

uint32_t MemCfg_getUncorrErrorAddress(uint32_t stsFlag)

Get the uncorrectable error address associated with a stsFlag.

Return

Returns the error address associated with the stsFlag.

Parameters
  • stsFlag: is the type of error to which the returned address will correspond. It may be passed one of these values: MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, or MEMCFG_UCERR_CLA1READ values

Many of the functions provided by this API to configure RAM sections’ settings will take a RAM section identifier or an OR of several identifiers as a parameter. These are #defines with names in the format MEMCFG_SECT_X. Take care to read the function description to learn which functions can operate on multiple sections of the same type at a time and which ones can only configure one section at a time. A quick way to check this is to see if the parameter says e ramSection or the plural e ramSections. Some functions may also be able to take a MEMCFG_SECT_ALL value to indicate that all RAM sections should be operated on at the same time. Again, read the function’s detailed description to be sure.

The code for this module is contained in driverlib/memcfg.c, with driverlib/memcfg.h containing the API declarations for use by applications.