SYSCTL Module

System Control (SysCtl) determines the overall operation of the device. The API provides functions to configure the clocking of the device, the set of peripherals that are enabled, the windowed watchdog, the NMI watchdog, and low-power modes. It also provides functions to handle and obtain information about resets and missing clock detection failures.

group sysctl_api

Defines

SYSCTL_WD_CHKBITS 0x0028U
SYSCTL_WD_ENRSTKEY 0x0055U
SYSCTL_WD_RSTKEY 0x00AAU
SYSCTL_PERIPH_REG_M 0x001FU
SYSCTL_PERIPH_REG_S 0x0000U
SYSCTL_PERIPH_BIT_M 0x1F00U
SYSCTL_PERIPH_BIT_S 0x0008U
SYSCTL_REG_KEY 0xA5A50000U
SYSCTL_PLL_KEY 0XCAFE0000U
SYSCTL_TYPE_LOCK_S 0xFU
SYSCTL_LPM_IDLE 0x0000U
SYSCTL_LPM_STANDBY 0x0001U
SYSCTL_LPM_HALT 0x0002U
SYSCTL_LPM_HIB 0x0003U
SYSCTL_DEFAULT_OSC_FREQ 10000000U
SYSCTL_SYNCSELECT_SYNCIN_M SYSCTL_SYNCSELECT_EPWM4SYNCIN_M
SYSCTL_BOOT_ROM_STATUS 0x002CU
SYSCTL_BOOT_ROM_POR 0x8000U
SYSCTL_BOOT_ROM_XRS 0x4000U
Device_cal ((void (*)(void))((uintptr_t)0x070282))
SYSCTL_SYSDIV_M 0x00001F80U
SYSCTL_SYSDIV_S 7U
SYSCTL_SYSDIV(x) ((((x) / 2U) << SYSCTL_SYSDIV_S) & SYSCTL_SYSDIV_M)

Macro to format system clock divider value. x must be 1 or even values up to 126.

SYSCTL_IMULT_M 0x0000007FU
SYSCTL_IMULT_S 0U
SYSCTL_IMULT(x) (((x) << SYSCTL_IMULT_S) & SYSCTL_IMULT_M)

Macro to format integer multiplier value. x is a number from 1 to 127.

SYSCTL_FMULT_M 0x00006000U
SYSCTL_FMULT_S 13U
SYSCTL_FMULT_NONE 0x00000000U

No fractional multiplier.

SYSCTL_FMULT_0 0x00000000U

No fractional multiplier.

SYSCTL_FMULT_1_4 0x00002000U

Fractional multiplier of 0.25.

SYSCTL_FMULT_1_2 0x00004000U

Fractional multiplier of 0.50.

SYSCTL_FMULT_3_4 0x00006000U

Fractional multiplier of 0.75.

SYSCTL_OSCSRC_M 0x00030000U
SYSCTL_OSCSRC_S 16U
SYSCTL_OSCSRC_OSC2 0x00000000U

Internal oscillator INTOSC2.

SYSCTL_OSCSRC_XTAL 0x00010000U

External oscillator (XTAL) in crystal mode.

SYSCTL_OSCSRC_OSC1 0x00020000U

Internal oscillator INTOSC1.

SYSCTL_PLL_ENABLE 0x80000000U

Enable PLL.

SYSCTL_PLL_DISABLE 0x00000000U

Disable PLL.

SYSCTL_AUXPLL_DIV_1 0x00000000U

Auxiliary PLL divide by 1.

SYSCTL_AUXPLL_DIV_2 0x00000080U

Auxiliary PLL divide by 2.

SYSCTL_AUXPLL_DIV_4 0x00000100U

Auxiliary PLL divide by 4.

SYSCTL_AUXPLL_DIV_8 0x00000180U

Auxiliary PLL divide by 8.

SYSCTL_AUXPLL_IMULT(x) SYSCTL_IMULT((x))

Macro to format integer multiplier value. x is a number from 1 to 127.

SYSCTL_AUXPLL_FMULT_NONE 0x00000000U

No fractional multiplier.

SYSCTL_AUXPLL_FMULT_0 0x00000000U

No fractional multiplier.

SYSCTL_AUXPLL_FMULT_1_4 0x00002000U

Fractional multiplier - 0.25.

SYSCTL_AUXPLL_FMULT_1_2 0x00004000U

Fractional multiplier - 0.50.

SYSCTL_AUXPLL_FMULT_3_4 0x00006000U

Fractional multiplier - 0.75.

SYSCTL_AUXPLL_OSCSRC_OSC2 0x00000000U

Internal oscillator INTOSC2 as auxiliary clock input.

SYSCTL_AUXPLL_OSCSRC_XTAL 0x00010000U

External oscillator (XTAL) as auxiliary clock input.

SYSCTL_AUXPLL_OSCSRC_AUXCLKIN 0x00020000U

AUXCLKIN (from GPIO) as auxiliary clock input.

SYSCTL_AUXPLL_ENABLE 0x80000000U

Enable AUXPLL.

SYSCTL_AUXPLL_DISABLE 0x00000000U

Disable AUXPLL.

SYSCTL_SEC_MASTER_CLA 0x0U

Configure CLA as the secondary master.

SYSCTL_SEC_MASTER_DMA 0x1U

Configure DMA as the secondary master.

SYSCTL_NMI_NMIINT 0x1U

NMI Interrupt Flag.

SYSCTL_NMI_CLOCKFAIL 0x2U

Clock Fail Interrupt Flag.

SYSCTL_NMI_RAMUNCERR 0x4U

RAM Uncorrectable Error NMI Flag.

SYSCTL_NMI_FLUNCERR 0x8U

Flash Uncorrectable Error NMI Flag.

SYSCTL_NMI_CPU1HWBISTERR 0x10U

HW BIST Error NMI Flag.

SYSCTL_NMI_CLBNMI 0x100U

Configurable Logic Block NMI Flag.

SYSCTL_CAUSE_POR 0x00000001U

Power-on reset.

SYSCTL_CAUSE_XRS 0x00000002U

External reset pin.

SYSCTL_CAUSE_WDRS 0x00000004U

Watchdog reset.

SYSCTL_CAUSE_NMIWDRS 0x00000008U

NMI watchdog reset.

SYSCTL_CAUSE_SCCRESET 0x00000100U

SCCRESETn by DCSM.

SYSCTL_ADCSOC_SRC_PWM1SOCA 0x1U

ePWM1 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM2SOCA 0x2U

ePWM2 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM3SOCA 0x4U

ePWM3 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM4SOCA 0x8U

ePWM4 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM5SOCA 0x10U

ePWM5 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM6SOCA 0x20U

ePWM6 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM7SOCA 0x40U

ePWM7 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM8SOCA 0x80U

ePWM8 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM9SOCA 0x100U

ePWM9 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM10SOCA 0x200U

ePWM10 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM11SOCA 0x400U

ePWM11 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM12SOCA 0x800U

ePWM12 SOCA for ADCSOCAO

SYSCTL_ADCSOC_SRC_PWM1SOCB 0x10000U

ePWM1 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM2SOCB 0x20000U

ePWM2 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM3SOCB 0x40000U

ePWM3 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM4SOCB 0x80000U

ePWM4 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM5SOCB 0x100000U

ePWM5 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM6SOCB 0x200000U

ePWM6 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM7SOCB 0x400000U

ePWM7 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM8SOCB 0x800000U

ePWM8 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM9SOCB 0x1000000U

ePWM9 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM10SOCB 0x2000000U

ePWM10 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM11SOCB 0x4000000U

ePWM11 SOCB for ADCSOCBO

SYSCTL_ADCSOC_SRC_PWM12SOCB 0x8000000U

ePWM12 SOCB for ADCSOCBO

Enums

enum SysCtl_PeripheralPCLOCKCR

The following are values that can be passed to SysCtl_enablePeripheral() and SysCtl_disablePeripheral() as the peripheral parameter.

Values:

enumerator SYSCTL_PERIPH_CLK_CLA1 = 0x0000

CLA1 clock.

enumerator SYSCTL_PERIPH_CLK_DMA = 0x0200

DMA clock.

enumerator SYSCTL_PERIPH_CLK_TIMER0 = 0x0300

CPUTIMER0 clock.

enumerator SYSCTL_PERIPH_CLK_TIMER1 = 0x0400

CPUTIMER1 clock.

enumerator SYSCTL_PERIPH_CLK_TIMER2 = 0x0500

CPUTIMER2 clock.

enumerator SYSCTL_PERIPH_CLK_HRPWM = 0x1000

HRPWM clock.

enumerator SYSCTL_PERIPH_CLK_TBCLKSYNC = 0x1200

TBCLKSYNC clock.

enumerator SYSCTL_PERIPH_CLK_EMIF1 = 0x0001

EMIF1 clock.

enumerator SYSCTL_PERIPH_CLK_EMIF2 = 0x0101

EMIF2 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM1 = 0x0002

EPWM1 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM2 = 0x0102

EPWM2 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM3 = 0x0202

EPWM3 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM4 = 0x0302

EPWM4 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM5 = 0x0402

EPWM5 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM6 = 0x0502

EPWM6 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM7 = 0x0602

EPWM7 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM8 = 0x0702

EPWM8 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM9 = 0x0802

EPWM9 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM10 = 0x0902

EPWM10 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM11 = 0x0A02

EPWM11 clock.

enumerator SYSCTL_PERIPH_CLK_EPWM12 = 0x0B02

EPWM12 clock.

enumerator SYSCTL_PERIPH_CLK_ECAP1 = 0x0003

ECAP1 clock.

enumerator SYSCTL_PERIPH_CLK_ECAP2 = 0x0103

ECAP2 clock.

enumerator SYSCTL_PERIPH_CLK_ECAP3 = 0x0203

ECAP3 clock.

enumerator SYSCTL_PERIPH_CLK_ECAP4 = 0x0303

ECAP4 clock.

enumerator SYSCTL_PERIPH_CLK_ECAP5 = 0x0403

ECAP5 clock.

enumerator SYSCTL_PERIPH_CLK_ECAP6 = 0x0503

ECAP6 clock.

enumerator SYSCTL_PERIPH_CLK_EQEP1 = 0x0004

EQEP1 clock.

enumerator SYSCTL_PERIPH_CLK_EQEP2 = 0x0104

EQEP2 clock.

enumerator SYSCTL_PERIPH_CLK_EQEP3 = 0x0204

EQEP3 clock.

enumerator SYSCTL_PERIPH_CLK_SD1 = 0x0006

SD1 clock.

enumerator SYSCTL_PERIPH_CLK_SD2 = 0x0106

SD2 clock.

enumerator SYSCTL_PERIPH_CLK_SCIA = 0x0007

SCI_A clock.

enumerator SYSCTL_PERIPH_CLK_SCIB = 0x0107

SCI_B clock.

enumerator SYSCTL_PERIPH_CLK_SCIC = 0x0207

SCI_C clock.

enumerator SYSCTL_PERIPH_CLK_SCID = 0x0307

SCI_D clock.

enumerator SYSCTL_PERIPH_CLK_SPIA = 0x0008

SPI_A clock.

enumerator SYSCTL_PERIPH_CLK_SPIB = 0x0108

SPI_B clock.

enumerator SYSCTL_PERIPH_CLK_SPIC = 0x0208

SPI_C clock.

enumerator SYSCTL_PERIPH_CLK_I2CA = 0x0009

I2C_A clock.

enumerator SYSCTL_PERIPH_CLK_I2CB = 0x0109

I2C_B clock.

enumerator SYSCTL_PERIPH_CLK_CANA = 0x000A

CAN_A clock.

enumerator SYSCTL_PERIPH_CLK_CANB = 0x010A

CAN_B clock.

enumerator SYSCTL_PERIPH_CLK_MCBSPA = 0x000B

MCBSP_A clock.

enumerator SYSCTL_PERIPH_CLK_MCBSPB = 0x010B

MCBSP_B clock.

enumerator SYSCTL_PERIPH_CLK_USBA = 0x100B

USB_A clock.

enumerator SYSCTL_PERIPH_CLK_UPPA = 0x000C

UPP_A clock.

enumerator SYSCTL_PERIPH_CLK_ADCA = 0x000D

ADC_A clock.

enumerator SYSCTL_PERIPH_CLK_ADCB = 0x010D

ADC_B clock.

enumerator SYSCTL_PERIPH_CLK_ADCC = 0x020D

ADC_C clock.

enumerator SYSCTL_PERIPH_CLK_ADCD = 0x030D

ADC_D clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS1 = 0x000E

CMPSS1 clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS2 = 0x010E

CMPSS2 clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS3 = 0x020E

CMPSS3 clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS4 = 0x030E

CMPSS4 clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS5 = 0x040E

CMPSS5 clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS6 = 0x050E

CMPSS6 clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS7 = 0x060E

CMPSS7 clock.

enumerator SYSCTL_PERIPH_CLK_CMPSS8 = 0x070E

CMPSS8 clock.

enumerator SYSCTL_PERIPH_CLK_DACA = 0x1010

DAC_A clock.

enumerator SYSCTL_PERIPH_CLK_DACB = 0x1110

DAC_B clock.

enumerator SYSCTL_PERIPH_CLK_DACC = 0x1210

DAC_C clock.

enum SysCtl_PeripheralSOFTPRES

The following are values that can be passed to SysCtl_resetPeripheral() as the peripheral parameter.

Values:

enumerator SYSCTL_PERIPH_RES_CPU1CLA1 = 0x0000

Reset CPU1_CLA1 clock.

enumerator SYSCTL_PERIPH_RES_EMIF1 = 0x0001

Reset EMIF1 clock.

enumerator SYSCTL_PERIPH_RES_EMIF2 = 0x0101

Reset EMIF2 clock.

enumerator SYSCTL_PERIPH_RES_EPWM1 = 0x0002

Reset EPWM1 clock.

enumerator SYSCTL_PERIPH_RES_EPWM2 = 0x0102

Reset EPWM2 clock.

enumerator SYSCTL_PERIPH_RES_EPWM3 = 0x0202

Reset EPWM3 clock.

enumerator SYSCTL_PERIPH_RES_EPWM4 = 0x0302

Reset EPWM4 clock.

enumerator SYSCTL_PERIPH_RES_EPWM5 = 0x0402

Reset EPWM5 clock.

enumerator SYSCTL_PERIPH_RES_EPWM6 = 0x0502

Reset EPWM6 clock.

enumerator SYSCTL_PERIPH_RES_EPWM7 = 0x0602

Reset EPWM7 clock.

enumerator SYSCTL_PERIPH_RES_EPWM8 = 0x0702

Reset EPWM8 clock.

enumerator SYSCTL_PERIPH_RES_EPWM9 = 0x0802

Reset EPWM9 clock.

enumerator SYSCTL_PERIPH_RES_EPWM10 = 0x0902

Reset EPWM10 clock.

enumerator SYSCTL_PERIPH_RES_EPWM11 = 0x0A02

Reset EPWM11 clock.

enumerator SYSCTL_PERIPH_RES_EPWM12 = 0x0B02

Reset EPWM12 clock.

enumerator SYSCTL_PERIPH_RES_ECAP1 = 0x0003

Reset ECAP1 clock.

enumerator SYSCTL_PERIPH_RES_ECAP2 = 0x0103

Reset ECAP2 clock.

enumerator SYSCTL_PERIPH_RES_ECAP3 = 0x0203

Reset ECAP3 clock.

enumerator SYSCTL_PERIPH_RES_ECAP4 = 0x0303

Reset ECAP4 clock.

enumerator SYSCTL_PERIPH_RES_ECAP5 = 0x0403

Reset ECAP5 clock.

enumerator SYSCTL_PERIPH_RES_ECAP6 = 0x0503

Reset ECAP6 clock.

enumerator SYSCTL_PERIPH_RES_EQEP1 = 0x0004

Reset EQEP1 clock.

enumerator SYSCTL_PERIPH_RES_EQEP2 = 0x0104

Reset EQEP2 clock.

enumerator SYSCTL_PERIPH_RES_EQEP3 = 0x0204

Reset EQEP3 clock.

enumerator SYSCTL_PERIPH_RES_SD1 = 0x0006

Reset SD1 clock.

enumerator SYSCTL_PERIPH_RES_SD2 = 0x0106

Reset SD2 clock.

enumerator SYSCTL_PERIPH_RES_SCIA = 0x0007

Reset SCI_A clock.

enumerator SYSCTL_PERIPH_RES_SCIB = 0x0107

Reset SCI_B clock.

enumerator SYSCTL_PERIPH_RES_SCIC = 0x0207

Reset SCI_C clock.

enumerator SYSCTL_PERIPH_RES_SCID = 0x0307

Reset SCI_D clock.

enumerator SYSCTL_PERIPH_RES_SPIA = 0x0008

Reset SPI_A clock.

enumerator SYSCTL_PERIPH_RES_SPIB = 0x0108

Reset SPI_B clock.

enumerator SYSCTL_PERIPH_RES_SPIC = 0x0208

Reset SPI_C clock.

enumerator SYSCTL_PERIPH_RES_I2CA = 0x0009

Reset I2C_A clock.

enumerator SYSCTL_PERIPH_RES_I2CB = 0x0109

Reset I2C_B clock.

enumerator SYSCTL_PERIPH_RES_MCBSPA = 0x000B

Reset MCBSP_A clock.

enumerator SYSCTL_PERIPH_RES_MCBSPB = 0x010B

Reset MCBSP_B clock.

enumerator SYSCTL_PERIPH_RES_USBA = 0x100B

Reset USB_A clock.

enumerator SYSCTL_PERIPH_RES_ADCA = 0x000D

Reset ADC_A clock.

enumerator SYSCTL_PERIPH_RES_ADCB = 0x010D

Reset ADC_B clock.

enumerator SYSCTL_PERIPH_RES_ADCC = 0x020D

Reset ADC_C clock.

enumerator SYSCTL_PERIPH_RES_ADCD = 0x030D

Reset ADC_D clock.

enumerator SYSCTL_PERIPH_RES_CMPSS1 = 0x000E

Reset CMPSS1 clock.

enumerator SYSCTL_PERIPH_RES_CMPSS2 = 0x010E

Reset CMPSS2 clock.

enumerator SYSCTL_PERIPH_RES_CMPSS3 = 0x020E

Reset CMPSS3 clock.

enumerator SYSCTL_PERIPH_RES_CMPSS4 = 0x030E

Reset CMPSS4 clock.

enumerator SYSCTL_PERIPH_RES_CMPSS5 = 0x040E

Reset CMPSS5 clock.

enumerator SYSCTL_PERIPH_RES_CMPSS6 = 0x050E

Reset CMPSS6 clock.

enumerator SYSCTL_PERIPH_RES_CMPSS7 = 0x060E

Reset CMPSS7 clock.

enumerator SYSCTL_PERIPH_RES_CMPSS8 = 0x070E

Reset CMPSS8 clock.

enumerator SYSCTL_PERIPH_RES_DACA = 0x1010

Reset DAC_A clock.

enumerator SYSCTL_PERIPH_RES_DACB = 0x1110

Reset DAC_B clock.

enumerator SYSCTL_PERIPH_RES_DACC = 0x1210

Reset DAC_C clock.

enum SysCtl_WDPrescaler

The following are values that can be passed to SysCtl_setWatchdogPrescaler() as the prescaler parameter.

Values:

enumerator SYSCTL_WD_PRESCALE_1 = 1

WDCLK = PREDIVCLK / 1.

enumerator SYSCTL_WD_PRESCALE_2 = 2

WDCLK = PREDIVCLK / 2.

enumerator SYSCTL_WD_PRESCALE_4 = 3

WDCLK = PREDIVCLK / 4.

enumerator SYSCTL_WD_PRESCALE_8 = 4

WDCLK = PREDIVCLK / 8.

enumerator SYSCTL_WD_PRESCALE_16 = 5

WDCLK = PREDIVCLK / 16.

enumerator SYSCTL_WD_PRESCALE_32 = 6

WDCLK = PREDIVCLK / 32.

enumerator SYSCTL_WD_PRESCALE_64 = 7

WDCLK = PREDIVCLK / 64.

enum SysCtl_WDMode

The following are values that can be passed to SysCtl_setWatchdogMode() as the prescaler parameter.

Values:

enumerator SYSCTL_WD_MODE_RESET

Watchdog can generate a reset signal.

enumerator SYSCTL_WD_MODE_INTERRUPT

Watchdog can generate an interrupt signal; reset signal is disabled.

enum SysCtl_LSPCLKPrescaler

The following are values that can be passed to SysCtl_setLowSpeedClock() as the prescaler parameter.

Values:

enumerator SYSCTL_LSPCLK_PRESCALE_1 = 0

LSPCLK = SYSCLK / 1.

enumerator SYSCTL_LSPCLK_PRESCALE_2 = 1

LSPCLK = SYSCLK / 2.

enumerator SYSCTL_LSPCLK_PRESCALE_4 = 2

LSPCLK = SYSCLK / 4 (default)

enumerator SYSCTL_LSPCLK_PRESCALE_6 = 3

LSPCLK = SYSCLK / 6.

enumerator SYSCTL_LSPCLK_PRESCALE_8 = 4

LSPCLK = SYSCLK / 8.

enumerator SYSCTL_LSPCLK_PRESCALE_10 = 5

LSPCLK = SYSCLK / 10.

enumerator SYSCTL_LSPCLK_PRESCALE_12 = 6

LSPCLK = SYSCLK / 12.

enumerator SYSCTL_LSPCLK_PRESCALE_14 = 7

LSPCLK = SYSCLK / 14.

enum SysCtl_EPWMCLKDivider

The following are values that can be passed to SysCtl_setEPWMClockDivider() as the divider parameter.

Values:

enumerator SYSCTL_EPWMCLK_DIV_1

EPWMCLK = PLLSYSCLK / 1.

enumerator SYSCTL_EPWMCLK_DIV_2

EPWMCLK = PLLSYSCLK / 2.

enum SysCtl_EMIF1CLKDivider

The following are values that can be passed to SysCtl_setEMIF1ClockDivider() as the divider parameter.

Values:

enumerator SYSCTL_EMIF1CLK_DIV_1

EMIF1CLK = PLLSYSCLK / 1.

enumerator SYSCTL_EMIF1CLK_DIV_2

EMIF1CLK = PLLSYSCLK / 2.

enum SysCtl_EMIF2CLKDivider

The following are values that can be passed to SysCtl_setEMIF2ClockDivider() as the divider parameter.

Values:

enumerator SYSCTL_EMIF2CLK_DIV_1

EMIF2CLK = PLLSYSCLK / 1.

enumerator SYSCTL_EMIF2CLK_DIV_2

EMIF2CLK = PLLSYSCLK / 2.

enum SysCtl_ClockOut

The following are values that can be passed to SysCtl_selectClockOutSource() as the source parameter.

Values:

enumerator SYSCTL_CLOCKOUT_PLLSYS = 0U

PLL System Clock post SYSCLKDIV.

enumerator SYSCTL_CLOCKOUT_PLLRAW = 1U

PLL Raw Clock.

enumerator SYSCTL_CLOCKOUT_SYSCLK = 2U

CPU System Clock.

enumerator SYSCTL_CLOCKOUT_INTOSC1 = 5U

Internal Oscillator 1.

enumerator SYSCTL_CLOCKOUT_INTOSC2 = 6U

Internal Oscillator 2.

enumerator SYSCTL_CLOCKOUT_XTALOSC = 7U

External Oscillator.

enum SysCtl_SyncInput

The following values define the syncInput parameter for SysCtl_setSyncInputConfig().

Values:

enumerator SYSCTL_SYNC_IN_EPWM4 = 0

Sync input to EPWM4.

enumerator SYSCTL_SYNC_IN_EPWM7 = 3

Sync input to EPWM7.

enumerator SYSCTL_SYNC_IN_EPWM10 = 6

Sync input to EPWM10.

enumerator SYSCTL_SYNC_IN_ECAP1 = 9

Sync input to ECAP1.

enumerator SYSCTL_SYNC_IN_ECAP4 = 12

Sync input to ECAP4.

enum SysCtl_SyncInputSource

The following values define the syncSrc parameter for SysCtl_setSyncInputConfig(). Note that some of these are only valid for certain values of syncInput. See device technical reference manual for info on time-base counter synchronization for details.

Values:

enumerator SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT = 0

EPWM1SYNCOUT.

enumerator SYSCTL_SYNC_IN_SRC_EPWM4SYNCOUT = 1

EPWM4SYNCOUT.

enumerator SYSCTL_SYNC_IN_SRC_EPWM7SYNCOUT = 2

EPWM7SYNCOUT.

enumerator SYSCTL_SYNC_IN_SRC_EPWM10SYNCOUT = 3

EPWM10SYNCOUT.

enumerator SYSCTL_SYNC_IN_SRC_ECAP1SYNCOUT = 4

ECAP1SYNCOUT.

enumerator SYSCTL_SYNC_IN_SRC_EXTSYNCIN1 = 5

EXTSYNCIN1Valid for all values of syncInput.

enumerator SYSCTL_SYNC_IN_SRC_EXTSYNCIN2 = 6

EXTSYNCIN2Valid for all values of syncInput.

enum SysCtl_SyncOutputSource

The following values define the syncSrc parameter for SysCtl_setSyncOutputConfig().

Values:

enumerator SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT

EPWM1SYNCOUT –> EXTSYNCOUT.

enumerator SYSCTL_SYNC_OUT_SRC_EPWM4SYNCOUT

EPWM4SYNCOUT –> EXTSYNCOUT.

enumerator SYSCTL_SYNC_OUT_SRC_EPWM7SYNCOUT

EPWM7SYNCOUT –> EXTSYNCOUT.

enumerator SYSCTL_SYNC_OUT_SRC_EPWM10SYNCOUT

EPWM10SYNCOUT –> EXTSYNCOUT.

enum SysCtl_DeviceParametric

The following values define the parametric parameter for SysCtl_getDeviceParametric().

Values:

enumerator SYSCTL_DEVICE_QUAL

Device Qualification Status.

enumerator SYSCTL_DEVICE_PINCOUNT

Device Pin Count.

enumerator SYSCTL_DEVICE_INSTASPIN

Device InstaSPIN Feature Set.

enumerator SYSCTL_DEVICE_FLASH

Device Flash size (KB)

enumerator SYSCTL_DEVICE_PARTID

Device Part ID Format Revision.

enumerator SYSCTL_DEVICE_FAMILY

Device Family.

enumerator SYSCTL_DEVICE_PARTNO

Device Part Number.

enumerator SYSCTL_DEVICE_CLASSID

Device Class ID.

enum SysCtl_XClkDivider

The following are values that can be passed to SysCtl_setXClk() as divider parameter.

Values:

enumerator SYSCTL_XCLKOUT_DIV_1 = 0

XCLKOUT = XCLKOUT / 1.

enumerator SYSCTL_XCLKOUT_DIV_2 = 1

XCLKOUT = XCLKOUT / 2.

enumerator SYSCTL_XCLKOUT_DIV_4 = 2

XCLKOUT = XCLKOUT / 4.

enumerator SYSCTL_XCLKOUT_DIV_8 = 3

XCLKOUT = XCLKOUT / 8.

enum SysCtl_AuxPLLClkDivider

The following are values that can be passed to SysCtl_setAuxPLLClk() as divider parameter.

Values:

enumerator SYSCTL_AUXPLLCLK_DIV_1

AUXPLL clock = AUXPLL clock / 1.

enumerator SYSCTL_AUXPLLCLK_DIV_2

AUXPLL clock = AUXPLL clock / 2.

enumerator SYSCTL_AUXPLLCLK_DIV_4

AUXPLL clock = AUXPLL clock / 4.

enumerator SYSCTL_AUXPLLCLK_DIV_8

AUXPLL clock = AUXPLL clock / 8.

enumerator SYSCTL_AUXPLLCLK_DIV_3

AUXPLL clock = AUXPLL clock / 3.

enumerator SYSCTL_AUXPLLCLK_DIV_5

AUXPLL clock = AUXPLL clock / 5.

enumerator SYSCTL_AUXPLLCLK_DIV_6

AUXPLL clock = AUXPLL clock / 6.

enumerator SYSCTL_AUXPLLCLK_DIV_7

AUXPLL clock = AUXPLL clock / 7.

enum SysCtl_Cputimer2ClkDivider

The following are values that can be passed to SysCtl_setCputimer2Clk() as divider parameter.

Values:

enumerator SYSCTL_TMR2CLKPRESCALE_1

Cputimer2 clock = Cputimer2 clock / 1.

enumerator SYSCTL_TMR2CLKPRESCALE_2

Cputimer2 clock = Cputimer2 clock / 2.

enumerator SYSCTL_TMR2CLKPRESCALE_4

Cputimer2 clock = Cputimer2 clock / 4.

enumerator SYSCTL_TMR2CLKPRESCALE_8

Cputimer2 clock = Cputimer2 clock / 8.

enumerator SYSCTL_TMR2CLKPRESCALE_16

Cputimer2 clock = Cputimer2 clock / 16.

enum SysCtl_Cputimer2ClkSource

The following are values that can be passed to SysCtl_setCputimer2Clk() as source parameter.

Values:

enumerator SYSCTL_TMR2CLKSRCSEL_SYSCLK = 0U

System Clock.

enumerator SYSCTL_TMR2CLKSRCSEL_INTOSC1 = 1U

Internal Oscillator 1.

enumerator SYSCTL_TMR2CLKSRCSEL_INTOSC2 = 2U

Internal Oscillator 2.

enumerator SYSCTL_TMR2CLKSRCSEL_XTAL = 3U

Crystal oscillator.

enumerator SYSCTL_TMR2CLKSRCSEL_AUXPLLCLK = 6U

Aux PLL CLock.

Functions

void SysCtl_deviceCal(void)

Wrapper function for Device_cal function

Return

None.

Parameters
  • None: This is a wrapper function for the Device_cal function available in the OTP memory. The function saves and restores the core registers which are being used by the Device_cal function

void SysCtl_resetPeripheral(SysCtl_PeripheralSOFTPRES peripheral)

Resets a peripheral

This function uses the SOFTPRESx registers to reset a specified peripheral. Module registers will be returned to their reset states.

Parameters
  • peripheral: is the peripheral to reset.

Note

This includes registers containing trim values.The peripheral software reset needed by CPU2 can be communicated to CPU1 via IPC for all shared peripherals.

Return

None.

void SysCtl_enablePeripheral(SysCtl_PeripheralPCLOCKCR peripheral)

Enables a peripheral.

Peripherals are enabled with this function. At power-up, all peripherals are disabled; they must be enabled in order to operate or respond to register reads/writes.

Parameters
  • peripheral: is the peripheral to enable.

Note

Note that there should be atleast 5 cycles delay between enabling the peripheral clock and accessing the peripheral registers. The delay should be added by the user if the peripheral is accessed immediately after this function call. Use asm(” RPT #5 || NOP”); to add 5 cycle delay post this function call.

Return

None.

void SysCtl_disablePeripheral(SysCtl_PeripheralPCLOCKCR peripheral)

Disables a peripheral.

Peripherals are disabled with this function. Once disabled, they will not operate or respond to register reads/writes.

Parameters
  • peripheral: is the peripheral to disable.

Return

None.

void SysCtl_resetDevice(void)

Resets the device.

This function performs a watchdog reset of the device.

Return

This function does not return.

uint32_t SysCtl_getResetCause(void)

Gets the reason for a reset.

This function will return the reason(s) for a reset. Since the reset reasons are sticky until either cleared by software or an external reset, multiple reset reasons may be returned if multiple resets have occurred. The reset reason will be a logical OR of

  • SYSCTL_CAUSE_POR - Power-on reset

  • SYSCTL_CAUSE_XRS - External reset pin

  • SYSCTL_CAUSE_WDRS - Watchdog reset

  • SYSCTL_CAUSE_NMIWDRS - NMI watchdog reset

  • SYSCTL_CAUSE_SCCRESET - SCCRESETn reset from DCSM

Note

If you re-purpose the reserved boot ROM RAM, the POR and XRS reset statuses won’t be accurate.

Return

Returns the reason(s) for a reset.

void SysCtl_clearResetCause(uint32_t rstCauses)

Clears reset reasons.

This function clears the specified sticky reset reasons. Once cleared, another reset for the same reason can be detected, and a reset for a different reason can be distinguished (instead of having two reset causes set). If the reset reason is used by an application, all reset causes should be cleared after they are retrieved with

SysCtl_getResetCause().
Parameters
  • rstCauses: are the reset causes to be cleared; must be a logical OR of SYSCTL_CAUSE_POR, SYSCTL_CAUSE_XRS, SYSCTL_CAUSE_WDRS, SYSCTL_CAUSE_NMIWDRS, and/or SYSCTL_CAUSE_SCCRESET.

Note

Some reset causes are cleared by the boot ROM.

Return

None.

void SysCtl_setLowSpeedClock(SysCtl_LSPCLKPrescaler prescaler)

Sets the low speed peripheral clock rate prescaler.

This function configures the clock rate of the low speed peripherals. The

prescaler parameter is the value by which the SYSCLK rate is divided to get the LSPCLK rate. For example, a prescaler of SYSCTL_LSPCLK_PRESCALE_4 will result in a LSPCLK rate that is a quarter of the SYSCLK rate.
Parameters
  • prescaler: is the LSPCLK rate relative to SYSCLK

Return

None.

void SysCtl_setEPWMClockDivider(SysCtl_EPWMCLKDivider divider)

Sets the ePWM clock divider.

This function configures the clock rate of the EPWMCLK. The

divider parameter is the value by which the SYSCLK rate is divided to get the EPWMCLK rate. For example, SYSCTL_EPWMCLK_DIV_2 will select an EPWMCLK rate that is half the PLLSYSCLK rate.
Parameters
  • divider: is the value by which PLLSYSCLK is divided

Return

None.

void SysCtl_setEMIF1ClockDivider(SysCtl_EMIF1CLKDivider divider)

Sets the EMIF1 clock divider.

This function configures the clock rate of the EMIF1CLK. The

divider parameter is the value by which the SYSCLK rate is divided to get the EMIF1CLK rate. For example, SYSCTL_EMIF1CLK_DIV_2 will select an EMIF1CLK rate that is half the PLLSYSCLK (or CPU1.SYSCLK on a dual core device) rate.
Parameters
  • divider: is the value by which PLLSYSCLK (or CPU1.SYSCLK on a dual core device) is divided

Return

None.

void SysCtl_setEMIF2ClockDivider(SysCtl_EMIF2CLKDivider divider)

Sets the EMIF2 clock divider.

This function configures the clock rate of the EMIF2CLK. The

divider parameter is the value by which the SYSCLK rate is divided to get the EMIF2CLK rate. For example, SYSCTL_EMIF2CLK_DIV_2 will select an EMIF2CLK rate that is half the PLLSYSCLK (or CPU1.SYSCLK on a dual core device) rate.
Parameters
  • divider: is the value by which PLLSYSCLK (or CPU1.SYSCLK on a dual core device) is divided

Return

None.

void SysCtl_selectClockOutSource(SysCtl_ClockOut source)

Selects a clock source to mux to an external GPIO pin (XCLKOUT).

This function configures the specified clock source to be muxed to an external clock out (XCLKOUT) GPIO pin. The

source parameter may take a value of one of the following values:
  • SYSCTL_CLOCKOUT_PLLSYS

  • SYSCTL_CLOCKOUT_PLLRAW

  • SYSCTL_CLOCKOUT_SYSCLK

  • SYSCTL_CLOCKOUT_INTOSC1

  • SYSCTL_CLOCKOUT_INTOSC2

  • SYSCTL_CLOCKOUT_XTALOSC

Parameters
  • source: is the internal clock source to be configured.

Return

None.

uint16_t SysCtl_getExternalOscCounterValue(void)

Gets the external oscillator counter value.

This function returns the X1 clock counter value. When the return value reaches 0x3FF, it freezes. Before switching from INTOSC2 to an external oscillator (XTAL), an application should call this function to make sure the counter is saturated.

Return

Returns the value of the 10-bit X1 clock counter.

void SysCtl_turnOnOsc(uint32_t oscSource)

Turns on the specified oscillator sources.

This function turns on the oscillator specified by the

oscSource parameter which may take a value of SYSCTL_OSCSRC_XTAL or SYSCTL_OSCSRC_OSC2.
Parameters
  • oscSource: is the oscillator source to be configured.

Note

SYSCTL_OSCSRC_OSC1 is not a valid value for oscSource.

Return

None.

void SysCtl_turnOffOsc(uint32_t oscSource)

Turns off the specified oscillator sources.

This function turns off the oscillator specified by the

oscSource parameter which may take a value of SYSCTL_OSCSRC_XTAL or SYSCTL_OSCSRC_OSC2.
Parameters
  • oscSource: is the oscillator source to be configured.

Note

SYSCTL_OSCSRC_OSC1 is not a valid value for oscSource.

Return

None.

void SysCtl_enterIdleMode(void)

Enters IDLE mode.

This function puts the device into IDLE mode. The CPU clock is gated while all peripheral clocks are left running. Any enabled interrupt will wake the CPU up from IDLE mode.

Return

None.

void SysCtl_enterStandbyMode(void)

Enters STANDBY mode.

This function puts the device into STANDBY mode. This will gate both the CPU clock and any peripheral clocks derived from SYSCLK. The watchdog is left active, and an NMI or an optional watchdog interrupt will wake the CPU subsystem from STANDBY mode.

GPIOs may be configured to wake the CPU subsystem. See SysCtl_enableLPMWakeupPin().

The CPU will receive an interrupt (WAKEINT) on wakeup.

Return

None.

void SysCtl_enterHaltMode(void)

Enters HALT mode.

This function puts the device into HALT mode. This will gate almost all systems and clocks and allows for the power-down of oscillators and analog blocks. The watchdog may be left clocked to produce a reset. See SysCtl_enableWatchdogInHalt() to enable this. GPIOs should be configured to wake the CPU subsystem. See SysCtl_enableLPMWakeupPin().

The CPU will receive an interrupt (WAKEINT) on wakeup.

Return

None.

void SysCtl_enterHibernateMode(void)

Enters Hibernate mode.

This function puts the device into Hibernate mode. Hibernate (HIB) is a global low-power mode that gates the supply voltages to most of the system. This mode affects both CPU subsystems. HIB is essentially a controlled power-down with remote wakeup capability, and can be used to save power during long periods of inactivity.

To wake the device from HIB mode:

  1. Assert the dedicated GPIOHIBWAKE pin (GPIO41) low to enable the power-up of the device clock sources.

  2. Assert GPIOHIBWAKE pin high again. This triggers the power-up of the rest of the device.

Return

None.

void SysCtl_enableLPMWakeupPin(uint32_t pin)

Enables a pin to wake up the device from the following mode(s):

  • STANDBY

  • HALT

This function connects a pin to the LPM circuit, allowing an event on the pin to wake up the device when when it is in following mode(s):

  • STANDBY

  • HALT

Parameters
  • pin: is the identifying number of the pin.

The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as pin. Only GPIOs 0 through 63 are capable of being connected to the LPM circuit.

Return

None.

void SysCtl_disableLPMWakeupPin(uint32_t pin)

Disables a pin to wake up the device from the following mode(s):

  • STANDBY

  • HALT

This function disconnects a pin to the LPM circuit, disallowing an event on the pin to wake up the device when when it is in following mode(s):

  • STANDBY

  • HALT

Parameters
  • pin: is the identifying number of the pin.

The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as pin. Only GPIOs 0 through 63 are valid.

Return

None.

void SysCtl_setStandbyQualificationPeriod(uint16_t cycles)

Sets the number of cycles to qualify an input on waking from STANDBY mode.

This function sets the number of OSCCLK clock cycles used to qualify the selected inputs when waking from STANDBY mode. The

cycles parameter should be passed a cycle count between 2 and 65 cycles inclusive.
Parameters
  • cycles: is the number of OSCCLK cycles.

Return

None.

void SysCtl_enableWatchdogStandbyWakeup(void)

Enable the device to wake from STANDBY mode upon a watchdog interrupt.

Note

In order to use this option, you must configure the watchdog to generate an interrupt using SysCtl_setWatchdogMode().

Return

None.

void SysCtl_disableWatchdogStandbyWakeup(void)

Disable the device from waking from STANDBY mode upon a watchdog interrupt.

Return

None.

void SysCtl_enableWatchdogInHalt(void)

Enable the watchdog to run while in HALT mode.

This function configures the watchdog to continue to run while in HALT mode. Additionally, INTOSC1 and INTOSC2 are not powered down when the system enters HALT mode. By default the watchdog is gated when the system enters HALT.

Return

None.

void SysCtl_disableWatchdogInHalt(void)

Disable the watchdog from running while in HALT mode.

This function gates the watchdog when the system enters HALT mode. INTOSC1 and INTOSC2 will be powered down. This is the default behavior of the device.

Return

None.

void SysCtl_setWatchdogMode(SysCtl_WDMode mode)

Configures whether the watchdog generates a reset or an interrupt signal.

This function configures the action taken when the watchdog counter reaches its maximum value. When the

mode parameter is SYSCTL_WD_MODE_INTERRUPT, the watchdog is enabled to generate a watchdog interrupt signal and disables the generation of a reset signal. This will allow the watchdog module to wake up the device from IDLE or STANDBY if desired (see SysCtl_enableWatchdogStandbyWakeup()).
Parameters
  • mode: is a flag to select the watchdog mode.

When the mode parameter is SYSCTL_WD_MODE_RESET, the watchdog will be put into reset mode and generation of a watchdog interrupt signal will be disabled. This is how the watchdog is configured by default.

Note

Check the status of the watchdog interrupt using SysCtl_isWatchdogInterruptActive() before calling this function. If the interrupt is still active, switching from interrupt mode to reset mode will immediately reset the device.

Return

None.

bool SysCtl_isWatchdogInterruptActive(void)

Gets the status of the watchdog interrupt signal.

This function returns the status of the watchdog interrupt signal. If the interrupt is active, this function will return true. If false, the interrupt is NOT active.

Note

Make sure to call this function to ensure that the interrupt is not active before making any changes to the configuration of the watchdog to prevent any unexpected behavior. For instance, switching from interrupt mode to reset mode while the interrupt is active will immediately reset the device.

Return

true if the interrupt is active and false if it is not.

void SysCtl_disableWatchdog(void)

Disables the watchdog.

This function disables the watchdog timer. Note that the watchdog timer is enabled on reset.

Return

None.

void SysCtl_enableWatchdog(void)

Enables the watchdog.

This function enables the watchdog timer. Note that the watchdog timer is enabled on reset.

Return

None.

void SysCtl_serviceWatchdog(void)

Services the watchdog.

This function resets the watchdog.

Return

None.

void SysCtl_enableWatchdogReset(void)

Writes the first key to enter the watchdog reset.

This function writes the first key to enter the watchdog reset.

Return

None.

void SysCtl_resetWatchdog(void)

Writes the second key to reset the watchdog.

This function writes the second key to reset the watchdog.

Return

None.

void SysCtl_setWatchdogPrescaler(SysCtl_WDPrescaler prescaler)

Sets up watchdog clock (WDCLK) prescaler.

This function sets up the watchdog clock (WDCLK) prescaler. The

prescaler parameter divides INTOSC1 down to WDCLK.
Parameters
  • prescaler: is the value that configures the watchdog clock relative to the value from the pre-divider.

Return

None.

uint16_t SysCtl_getWatchdogCounterValue(void)

Gets the watchdog counter value.

Return

Returns the current value of the 8-bit watchdog counter. If this count value overflows, a watchdog output pulse is generated.

bool SysCtl_getWatchdogResetStatus(void)

Gets the watchdog reset status.

This function returns the watchdog reset status. If this function returns true, that indicates that a watchdog reset generated the last reset condition. Otherwise, it was an external device or power-up reset condition.

Return

Returns true if the watchdog generated the last reset condition.

void SysCtl_clearWatchdogResetStatus(void)

Clears the watchdog reset status.

This function clears the watchdog reset status. To check if it was set first, see SysCtl_getWatchdogResetStatus().

Return

None.

void SysCtl_setWatchdogWindowValue(uint16_t value)

Set the minimum threshold value for windowed watchdog

This function sets the minimum threshold value used to define the lower limit of the windowed watchdog functionality.

Parameters
  • value: is the value to set the window threshold

Return

None.

void SysCtl_clearWatchdogOverride(void)

Clears the watchdog override.

This function clears the watchdog override and locks the watchdog timer module to remain in its prior state which could be either enable /disable. The watchdog timer will remain in this state until the next system reset.

Return

None.

void SysCtl_enableNMIGlobalInterrupt(void)

Enable the NMI Global interrupt bit

Note: This bit should be set after the device security related initialization is complete.

Return

None.

bool SysCtl_getNMIStatus(void)

Read NMI interrupts.

Read the current state of NMI interrupt.

Return

true if NMI interrupt is triggered, false if not.

uint16_t SysCtl_getNMIFlagStatus(void)

Read NMI Flags.

Read the current state of individual NMI interrupts

Return

Value of NMIFLG register. These defines are provided to decode the value:

  • SYSCTL_NMI_NMIINT - NMI Interrupt Flag

  • SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag

  • SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag

  • SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag

  • SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag

  • SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag

bool SysCtl_isNMIFlagSet(uint32_t nmiFlags)

Check if the individual NMI interrupts are set.

Check if interrupt flags corresponding to the passed in bit mask are asserted.

Parameters
  • nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:

    • SYSCTL_NMI_NMIINT - NMI Interrupt Flag

    • SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag

    • SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag

    • SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag

    • SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag

    • SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag

Return

true if any of the NMI asked for in the parameter bit mask is set. false if none of the NMI requested in the parameter bit mask are set.

void SysCtl_clearNMIStatus(uint32_t nmiFlags)

Function to clear individual NMI interrupts.

Clear NMI interrupt flags that correspond with the passed in bit mask.

Parameters
  • nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:

    • SYSCTL_NMI_NMIINT - NMI Interrupt Flag

    • SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag

    • SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag

    • SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag

    • SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag

    • SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag

Note: The NMI Interrupt flag is always cleared by default and therefore doesn’t have to be included in the bit mask.

Return

None.

void SysCtl_clearAllNMIFlags(void)

Clear all the NMI Flags that are currently set.

Return

None.

void SysCtl_forceNMIFlags(uint32_t nmiFlags)

Function to force individual NMI interrupt fail flags

Return

None.

Parameters
  • nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:

    • SYSCTL_NMI_NMIINT - NMI Interrupt Flag

    • SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag

    • SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag

    • SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag

    • SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag

    • SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag

uint16_t SysCtl_getNMIWatchdogCounter(void)

Gets the NMI watchdog counter value.

Note: The counter is clocked at the SYSCLKOUT rate.

Return

Returns the NMI watchdog counter register’s current value.

void SysCtl_setNMIWatchdogPeriod(uint16_t wdPeriod)

Sets the NMI watchdog period value.

This function writes to the NMI watchdog period register that holds the value to which the NMI watchdog counter is compared. When the two registers match, a reset is generated. By default, the period is 0xFFFF.

Parameters
  • wdPeriod: is the 16-bit value at which a reset is generated.

Note

If a value smaller than the current counter value is passed into the wdPeriod parameter, a NMIRSn will be forced.

Return

None.

uint16_t SysCtl_getNMIWatchdogPeriod(void)

Gets the NMI watchdog period value.

Return

Returns the NMI watchdog period register’s current value.

uint32_t SysCtl_getNMIShadowFlagStatus(void)

Read NMI Shadow Flags.

Read the current state of individual NMI interrupts

Return

Value of NMISHDFLG register. These defines are provided to decode the value:

  • SYSCTL_NMI_NMIINT - NMI Interrupt Flag

  • SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag

  • SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag

  • SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag

  • SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag

  • SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag

bool SysCtl_isNMIShadowFlagSet(uint32_t nmiFlags)

Check if the individual NMI shadow flags are set.

Check if interrupt flags corresponding to the passed in bit mask are asserted.

Parameters
  • nmiFlags: Bit mask of the NMI interrupts that user wants to clear. The bit format of this parameter is same as of the NMIFLG register. These defines are provided:

    • SYSCTL_NMI_NMIINT - NMI Interrupt Flag

    • SYSCTL_NMI_CLOCKFAIL - Clock Fail Interrupt Flag

    • SYSCTL_NMI_RAMUNCERR - RAM Uncorrectable Error NMI Flag

    • SYSCTL_NMI_FLUNCERR - Flash Uncorrectable Error NMI Flag

    • SYSCTL_NMI_CPU1HWBISTERR - HW BIST Error NMI Flag

    • SYSCTL_NMI_CLBNMI - Configurable Logic Block NMI Flag

Return

true if any of the NMI asked for in the parameter bit mask is set. false if none of the NMI requested in the parameter bit mask are set.

void SysCtl_enableMCD(void)

Enable the missing clock detection (MCD) Logic

Return

None.

void SysCtl_disableMCD(void)

Disable the missing clock detection (MCD) Logic

Return

None.

bool SysCtl_isMCDClockFailureDetected(void)

Get the missing clock detection Failure Status

Note

A failure means the oscillator clock is missing

Return

Returns true if a failure is detected or false if a failure isn’t detected

void SysCtl_resetMCD(void)

Reset the missing clock detection logic after clock failure

Return

None.

void SysCtl_connectMCDClockSource(void)

Re-connect missing clock detection clock source to stop simulating clock failure

Return

None.

void SysCtl_disconnectMCDClockSource(void)

Disconnect missing clock detection clock source to simulate clock failure. This is for testing the MCD functionality.

Return

None.

void SysCtl_setSyncInputConfig(SysCtl_SyncInput syncInput, SysCtl_SyncInputSource syncSrc)

Configures the sync input source for the ePWM and eCAP signals.

This function configures the sync input source for the ePWM and eCAP modules. The

syncInput parameter is the sync input being configured. It should be passed a value of SYSCTL_SYNC_IN_XXXX, where XXXX is the ePWM or eCAP instance the sync signal is entering.
Parameters
  • syncInput: is the sync input being configured

  • syncSrc: is sync input source selection.

The syncSrc parameter is the sync signal selected as the source of the sync input. It should be passed a value of SYSCTL_SYNC_IN_SRC_XXXX, XXXX is a sync signal coming from an ePWM, eCAP or external sync output. where For example, a syncInput value of SYSCTL_SYNC_IN_ECAP1 and a syncSrc value of SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT will make the EPWM1SYNCOUT signal drive eCAP1’s SYNCIN signal.

Note that some syncSrc values are only valid for certain values of syncInput. See device technical reference manual for details on time-base counter synchronization.

Return

None.

void SysCtl_setSyncOutputConfig(SysCtl_SyncOutputSource syncSrc)

Configures the sync output source.

This function configures the sync output source from the ePWM modules. The

syncSrc parameter is a value SYSCTL_SYNC_OUT_SRC_XXXX, where XXXX is a sync signal coming from an ePWM such as SYSCTL_SYNC_OUT_SRC_EPWM1SYNCOUT
Parameters
  • syncSrc: is sync output source selection.

Return

None.

void SysCtl_enableExtADCSOCSource(uint32_t adcsocSrc)

Enables ePWM SOC signals to drive an external (off-chip) ADCSOC signal.

This function configures which ePWM SOC signals are enabled as a source for either ADCSOCAO or ADCSOCBO. The

adcsocSrc parameter takes a logical OR of SYSCTL_ADCSOC_SRC_PWMxSOCA/B values that correspond to different signals.
Parameters
  • adcsocSrc: is a bit field of the selected signals to be enabled

Return

None.

void SysCtl_disableExtADCSOCSource(uint32_t adcsocSrc)

Disables ePWM SOC signals from driving an external ADCSOC signal.

This function configures which ePWM SOC signals are disabled as a source for either ADCSOCAO or ADCSOCBO. The

adcsocSrc parameter takes a logical OR of SYSCTL_ADCSOC_SRC_PWMxSOCA/B values that correspond to different signals.
Parameters
  • adcsocSrc: is a bit field of the selected signals to be disabled

Return

None.

void SysCtl_lockExtADCSOCSelect(void)

Locks the SOC Select of the Trig X-BAR.

This function locks the external ADC SOC select of the Trig X-BAR.

Return

None.

void SysCtl_selectSecMaster(uint16_t periFrame1Config, uint16_t periFrame2Config)

Configures whether the dual ported bridge is connected with DMA or CLA as the secondary master.

One of the following values can be passed as parameter.

SYSCTL_SEC_MASTER_CLA SYSCTL_SEC_MASTER_DMA
Parameters
  • periFrame1Config: indicates whether CLA or DMA is configured as secondary master on peripheral frame 1.

  • periFrame2Config: indicates whether CLA or DMA is configured as secondary master on peripheral frame 2.

Return

None.

void SysCtl_lockSyncSelect(void)

Locks the Sync Select of the Trig X-BAR.

This function locks Sync Input and Output Select of the Trig X-BAR.

Return

None.

uint32_t SysCtl_getDeviceRevision(void)

Get the Device Silicon Revision ID

This function returns the silicon revision ID for the device.

Note

This API is applicable only for the CPU1 subsystem.

Return

Returns the silicon revision ID value.

uint16_t SysCtl_getEfuseError(void)

Gets the error status of the Efuse

The function provides both the Efuse Autoload & the Efuse Self Test Error Status.

Note

This API is applicable only for the CPU1 subsystem.

Return

Fuse Error status.

void SysCtl_setXClk(SysCtl_XClkDivider divider)

Sets up XCLK divider.

This function sets up the XCLK divider. There is only one divider that scales INTOSC1 to XCLK.

Parameters
  • divider: is the value that configures the divider.

The divider parameter can have one enumerated value from SysCtl_XClkDivider

Return

None.

void SysCtl_setPLLSysClk(uint16_t divider)

Sets up PLLSYSCLK divider.

This function sets up the PLLSYSCLK divider. There is only one divider that scales PLLSYSCLK to generate the system clock.

Parameters
  • divider: is the value that configures the divider.

The divider parameter can have one value from the set below: 0x0 = /1 0x1 = /2 0x2 = /4 (default on reset) 0x3 = /6 0x4 = /8 …… 0x3F =/126

Return

None.

Note

Please make sure to check if the PLL is locked and valid using the SysCtl_isPLLValid() before setting the divider.

void SysCtl_setAuxPLLClk(SysCtl_AuxPLLClkDivider divider)

Sets up AUXPLLCLK divider.

This function sets up the AUXPLLCLK divider. There is only one divider that scales AUXPLLCLK to generate the system clock.

Parameters
  • divider: is the value that configures the divider.

The divider parameter can have one enumerated value from SysCtl_AuxPLLClkDivider

Return

None.

Note

Please make sure to check if the PLL is locked and valid using the SysCtl_isPLLValid() before setting the divider.

void SysCtl_setCputimer2Clk(SysCtl_Cputimer2ClkDivider divider, SysCtl_Cputimer2ClkSource source)

Sets up CPU Timer 2 CLK source & divider.

This function sets up the CPU Timer 2 CLK divider based on the source that is selected. There is only one divider that scales the “source” to CPU Timer 2 CLK.

Parameters
  • divider: is the value that configures the divider.

  • source: is the source for the clock divider

The divider parameter can have one enumerated value from SysCtl_Cputimer2ClkDivider The source parameter can have one enumerated value from SysCtl_Cputimer2ClkSource

Return

None.

uint32_t SysCtl_getPIEVErrAddr(void)

Gets the PIE Vector Fetch Error Handler Routine Address.

The function indicates the address of the PIE Vector Fetch Error handler routine.

Return

Error Handler Address.

Note

Its the responsibility of user to initialize this register. If this register is not initialized, a default error handler at address 0x3fffbe will get executed.

uint32_t SysCtl_isPresentUSBPHY(void)

Check if the Internal PHY is present or not for the USB module

Provides the USB module Internal PHY presence

Note

This API is applicable only for the CPU1 subsystem.

Return

true if Internal USB PHY Module is present false if Internal USB PHY Module is not present

void SysCtl_delay(uint32_t count)

Delays for a fixed number of cycles.

This function generates a constant length delay using assembly code. The loop takes 5 cycles per iteration plus 9 cycles of overhead.

Parameters
  • count: is the number of delay loop iterations to perform.

Note

If count is equal to zero, the loop will underflow and run for a very long time.

Note

Refer to the macro DEVICE_DELAY_US(x) in device.h which can be used to insert a delay in microseconds.

Return

None.

uint32_t SysCtl_getClock(uint32_t clockInHz)

Calculates the system clock frequency (SYSCLK).

This function determines the frequency of the system clock based on the frequency of the oscillator clock source (from

clockInHz) and the PLL and clock divider configuration registers.
Parameters
  • clockInHz: is the frequency of the oscillator clock source (OSCCLK).

Return

Returns the system clock frequency. If a missing clock is detected, the function will return the INTOSC1 frequency. This needs to be corrected and cleared (see SysCtl_resetMCD()) before trying to call this function again.

uint32_t SysCtl_getAuxClock(uint32_t clockInHz)

Calculates the system auxiliary clock frequency (AUXPLLCLK).

This function determines the frequency of the auxiliary clock based on the frequency of the oscillator clock source (from

clockInHz) and the AUXPLL and clock divider configuration registers.
Parameters
  • clockInHz: is the frequency of the oscillator clock source (AUXOSCCLK).

Return

Returns the auxiliary clock frequency.

bool SysCtl_setClock(uint32_t config)

Configures the clocking of the device.

This function configures the clocking of the device. The input crystal frequency, oscillator to be used, use of the PLL, and the system clock divider are all configured with this function.

Parameters
  • config: is the required configuration of the device clocking.

The config parameter is the OR of several different values, many of which are grouped into sets where only one can be chosen.

  • The system clock divider is chosen with the macro SYSCTL_SYSDIV(x) where x is either 1 or an even value up to 126.

  • The use of the PLL is chosen with either SYSCTL_PLL_ENABLE or SYSCTL_PLL_DISABLE.

  • The integer multiplier is chosen SYSCTL_IMULT(x) where x is a value from 1 to 127.

  • The fractional multiplier is chosen with either SYSCTL_FMULT_0, SYSCTL_FMULT_1_4, SYSCTL_FMULT_1_2, or SYSCTL_FMULT_3_4.

  • The oscillator source chosen with SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, or SYSCTL_OSCSRC_OSC1.

This function uses the watchdog as a monitor for the PLL. The user watchdog settings will be modified and restored upon completion. Make sure that the WDOVERRIDE bit isn’t set before calling this function. Re-lock attempt is carried out if either SLIP condition occurs or SYSCLK to input clock ratio is off by 10%.

This function uses the following resources to support PLL initialization:

  • Watchdog

  • CPU Timer 1

  • CPU Timer 2

Note

See your device errata for more details about locking the PLL.

Return

Returns false if a missing clock error is detected. This needs to be cleared (see SysCtl_resetMCD()) before trying to call this function again. Otherwise, returns true.

void SysCtl_selectXTAL(void)

Configures the external oscillator for the clocking of the device.

This function configures the external oscillator (XTAL) to be used for the clocking of the device in crystal mode. It follows the procedure to turn on the oscillator, wait for it to power up, and select it as the source of the system clock.

Please note that this function blocks while it waits for the XTAL to power up. If the XTAL does not manage to power up properly, the function will loop for a long time. It is recommended that you modify this function to add an appropriate timeout and error-handling procedure.

Return

None.

void SysCtl_selectOscSource(uint32_t oscSource)

Selects the oscillator to be used for the clocking of the device.

This function configures the oscillator to be used in the clocking of the device. The

oscSource parameter may take a value of SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, or SYSCTL_OSCSRC_OSC1.
Parameters
  • oscSource: is the oscillator source to be configured.

See

SysCtl_turnOnOsc()

Return

None.

void SysCtl_selectOscSourceAuxPLL(uint32_t oscSource)

Selects the oscillator to be used for the AUXPLL.

This function configures the oscillator to be used in the clocking of the AUXPLL. The

oscSource parameter may take a value of SYSCTL_OSCSRC_OSC2, SYSCTL_OSCSRC_XTAL, or SYSCTL_OSCSRC_OSC1.
Parameters
  • oscSource: is the oscillator source to be configured.

See

SysCtl_turnOnOsc()

Return

None.

uint32_t SysCtl_getLowSpeedClock(uint32_t clockInHz)

Calculates the low-speed peripheral clock frequency (LSPCLK).

This function determines the frequency of the low-speed peripheral clock based on the frequency of the oscillator clock source (from

clockInHz) and the PLL and clock divider configuration registers.
Parameters
  • clockInHz: is the frequency of the oscillator clock source (OSCCLK).

Return

Returns the low-speed peripheral clock frequency.

uint16_t SysCtl_getDeviceParametric(SysCtl_DeviceParametric parametric)

Get the device part parametric value

This function gets the device part parametric value.

Parameters
  • parametric: is the requested device parametric value

The parametric parameter can have one the following enumerated values:

  • SYSCTL_DEVICE_QUAL - Device Qualification Status

  • SYSCTL_DEVICE_PINCOUNT - Device Pin Count

  • SYSCTL_DEVICE_INSTASPIN - Device InstaSPIN Feature Set

  • SYSCTL_DEVICE_FLASH - Device Flash size (KB)

  • SYSCTL_DEVICE_PARTID - Device Part ID Format Revision

  • SYSCTL_DEVICE_FAMILY - Device Family

  • SYSCTL_DEVICE_PARTNO - Device Part Number

  • SYSCTL_DEVICE_CLASSID - Device Class ID

Note

This API is applicable only for the CPU1 subsystem.

Return

Returns the specified parametric value.

void SysCtl_setAuxClock(uint32_t config)

Configures the auxiliary PLL for clocking USB.

This function configures the clock source for auxiliary PLL, the integer multiplier, fractional multiplier and divider.

Parameters
  • config: is the required configuration of the device clocking.

The config parameter is the OR of several different values, many of which are grouped into sets where only one can be chosen.

  • The system clock divider is chosen with one of the following macros: SYSCTL_AUXPLL_DIV_1, SYSCTL_AUXPLL_DIV_2, SYSCTL_AUXPLL_DIV_4, SYSCTL_AUXPLL_DIV_8

  • The use of the PLL is chosen with either SYSCTL_AUXPLL_ENABLE or SYSCTL_AUXPLL_DISABLE.

  • The integer multiplier is chosen with SYSCTL_AUXPLL_IMULT(x) where x is a value from 1 to 127.

  • The oscillator source chosen with one of SYSCTL_AUXPLL_OSCSRC_OSC2, SYSCTL_AUXPLL_OSCSRC_XTAL, SYSCTL_AUXPLL_OSCSRC_AUXCLKIN,

Note

This function uses CPU Timer 2 to monitor a successful lock of the AUXPLL. For this function to properly detect the PLL startup SYSCLK >= 2*AUXPLLCLK after the AUXPLL is selected as the clocking source. User configuration of CPU Timer 2 will be backed up and restored.

Note

See your device errata for more details about locking the PLL.

Return

None.

Many of the functions provided by the SysCtl API are related to device clocking. The most important of these functions is SysCtl_setClock() which will configure which oscillator is to be used, configure the PLL, and configure the system clock divider. SysCtl_getClock() is a complementary function to this one that will, given the frequency of the oscillator source used, read back the configuration of the PLL and clock divider and calculate the system clock frequency. A similar pair of functions is provided for the low-speed peripheral clock, SysCtl_setLowSpeedClock() and SysCtl_getLowSpeedClock().

The ability to enable (turn on the module clock), disable (gate off the module clock), and perform a software reset on most of the peripherals on a device is provided by SysCtl_enablePeripheral(), SysCtl_disablePeripheral(), and SysCtl_resetPeripheral() respectively.

The device’s windowed watchdog is enabled and disabled by SysCtl_enableWatchdog() and SysCtl_disableWatchdog() respectively. The watchdog can be serviced by SysCtl_serviceWatchdog(). Several functions are also provided to configure the watchdog’s clock and windowed functionality.

This section will give further details of these functions and each of the others used for the configuration of SysCtl.

The code for this module is contained in driverlib/sysctl.c, with driverlib/sysctl.h containing the API declarations for use by applications.