Version¶
The version driver provides a function which can be used to check the version number of the driverlib.lib that is in use.
-
group
version_api Defines
-
VERSION_NUMBER4001000U¶ Version number to be returned by Version_getLibVersion()
Functions
-
uint32_t
Version_getLibVersion(void)¶ Returns the driverlib version number
This function can be used to check the version number of the driverlib.lib that is in use. The version number will take the format x.xx.xx.xx, so for example, if the function returns 2100200, the driverlib version being used is 2.10.02.00.
- Return
Returns an integer value indicating the driverlib version.
-
The code for this module is contained in driverlib/version.c, with driverlib/version.h containing the API declarations for use by applications.