/******************************************************************************/
/* This file was taken from STLport <www.stlport.org> and modified by         */
/* Texas Instruments.                                                         */
/******************************************************************************/

/*
 * Copyright (c) 1998
 * Silicon Graphics Computer Systems, Inc.
 *
 * Copyright (c) 1999
 * Boris Fomitchev
 *
 * Copyright (c) 2014-2014 Texas Instruments Incorporated
 *
 * This material is provided "as is", with absolutely no warranty expressed
 * or implied. Any use is at your own risk.
 *
 * Permission to use or copy this software for any purpose is hereby granted
 * without fee, provided the above notices are retained on all copies.
 * Permission to modify the code and to distribute modified code is granted,
 * provided the above notices are retained, and a notice that the code was
 * modified is included with the above copyright notice.
 *
 */

#ifndef _STLP_BITSET

// This implementation of bitset<> has a second template parameter,
// _WordT, which defaults to unsigned long.  *YOU SHOULD NOT USE
// THIS FEATURE*.  It is experimental, and it may be removed in
// future releases.

// A bitset of size N, using words of type _WordT, will have
// N % (sizeof(_WordT) * CHAR_BIT) unused bits.  (They are the high-
// order bits in the highest word.)  It is a class invariant
// of class bitset<> that those unused bits are always zero.

// Most of the actual code isn't contained in bitset<> itself, but in the
// base class _Base_bitset.  The base class works with whole words, not with
// individual bits.  This allows us to specialize _Base_bitset for the
// important special case where the bitset is only a single word.

// The C++ standard does not define the precise semantics of operator[].
// In this implementation the const version of operator[] is equivalent
// to test(), except that it does no range checking.  The non-const version
// returns a reference to a bit, again without doing any range checking.

#ifndef _STLP_OUTERMOST_HEADER_ID
#  define _STLP_OUTERMOST_HEADER_ID 0x2
#  include <s__prolog.h>
#  define _STLP_BITSET
#endif

#if (_STLP_OUTERMOST_HEADER_ID == 0x2)
#  ifndef _STLP_INTERNAL_BITSET
#    include <s__bitset.h>
#  endif
#endif

#if (_STLP_OUTERMOST_HEADER_ID != 0x2) || defined (_STLP_IMPORT_VENDOR_STD)
#  if defined (_STLP_HAS_INCLUDE_NEXT)
#    include_next <bitset>
#  else
#    include _STLP_NATIVE_HEADER(bitset)
#  endif
#endif

#if (_STLP_OUTERMOST_HEADER_ID == 0x2 )
#  include <s__epilog.h>
#  undef _STLP_OUTERMOST_HEADER_ID
#endif

#endif /* _STLP_BITSET */

// Local Variables:
// mode:C++
// End: