/******************************************************************************/
/* This file was taken from STLport <www.stlport.org> and modified by         */
/* Texas Instruments.                                                         */
/******************************************************************************/

/*
 * Copyright (c) 1999
 * Silicon Graphics Computer Systems, Inc.
 *
 * Copyright (c) 1999
 * Boris Fomitchev
 *
 * Copyright (c) 2014-2014 Texas Instruments Incorporated
 *
 * This material is provided "as is", with absolutely no warranty expressed
 * or implied. Any use is at your own risk.
 *
 * Permission to use or copy this software for any purpose is hereby granted
 * without fee, provided the above notices are retained on all copies.
 * Permission to modify the code and to distribute modified code is granted,
 * provided the above notices are retained, and a notice that the code was
 * modified is included with the above copyright notice.
 *
 */

#ifndef _STLP_IOSTREAM

#ifndef _STLP_OUTERMOST_HEADER_ID
#  define _STLP_OUTERMOST_HEADER_ID 0x1037
#  include <s__prolog.h>
#  define _STLP_IOSTREAM
#endif

#if (_STLP_OUTERMOST_HEADER_ID == 0x1037) && \
   !(defined (_STLP_NO_IOSTREAMS) && defined (_STLP_IMPORT_VENDOR_STD))
#  include <s__ioserr.h>

#  ifdef _STLP_REDIRECT_STDSTREAMS
// for ofstream redirection
#    ifndef _STLP_INTERNAL_FSTREAM_H
#      include <s__fstream.h>
#    endif
#  endif

#  ifndef _STLP_INTERNAL_IOSFWD
#    include <s__iosfwd.h>
#  endif

#  ifndef _STLP_INTERNAL_ISTREAM
#    include <s__istream.h>
#  endif

_STLP_BEGIN_NAMESPACE

#if defined (__TI_COMPILER_VERSION__)
/* Workaround since we don't support ensuring library globals are initialized first.
 * This declaration ensures that any inclusion of this header will force cout/cin/cerr
 * to initialize. */
static ios_base::Init _ios_initer;
#endif

#  ifndef _STLP_USE_NAMESPACES
// in case of SGI iostreams, we have to rename our streams not to clash with those
// provided in native lib
#    define cin _STLP_cin
#    define cout _STLP_cout
#    define cerr _STLP_cerr
#    define clog _STLP_clog
#  endif

// Note: cin and wcin are both associated with stdio.  The C standard
// (Amendment 1, section 4.6.2.1) says that it is an error to mix
// wide- and narrow-oriented I/O on the same stream.  This implies
// that it is an error to use both cin and wcin in the same C++
// program; the same applies to cout and wcout, and cerr/clog and
// wcerr/wclog.

_DATA_ACCESS extern _STLP_DECLSPEC istream cin;

#  ifdef _STLP_REDIRECT_STDSTREAMS
_DATA_ACCESS extern _STLP_DECLSPEC ofstream cout;
_DATA_ACCESS extern _STLP_DECLSPEC ofstream cerr;
_DATA_ACCESS extern _STLP_DECLSPEC ofstream clog;
#  else
_DATA_ACCESS extern _STLP_DECLSPEC ostream cout;
_DATA_ACCESS extern _STLP_DECLSPEC ostream cerr;
_DATA_ACCESS extern _STLP_DECLSPEC ostream clog;
#  endif

#  ifndef _STLP_NO_WCHAR_T
_DATA_ACCESS extern _STLP_DECLSPEC wistream wcin;
_DATA_ACCESS extern _STLP_DECLSPEC wostream wcout;
_DATA_ACCESS extern _STLP_DECLSPEC wostream wcerr;
_DATA_ACCESS extern _STLP_DECLSPEC wostream wclog;
#  endif

_STLP_END_NAMESPACE

#endif

#if (_STLP_OUTERMOST_HEADER_ID != 0x1037) || defined (_STLP_IMPORT_VENDOR_STD)
#  if defined (_STLP_HAS_INCLUDE_NEXT)
#    include_next <iostream>
#  else
#    include _STLP_NATIVE_HEADER(iostream)
#  endif
#endif

#if (_STLP_OUTERMOST_HEADER_ID == 0x1037)
#  include <s__epilog.h>
#  undef _STLP_OUTERMOST_HEADER_ID
#endif

#endif /* _STLP_IOSTREAM */

// Local Variables:
// mode:C++
// End: