DCSM Module

The DCSM driver accesses the DCSM COMMON registers. In order to configure the Dual Code Security Module, the user must program the Linkpointer in DCSM OTP as well as the security configuration registers of the Zone Select Blocks in DCSM OTP. The DCSM driver provides functions which secure and unsecure each zone and return the ownership, security status, EXEONLY status of specific RAM modules or Flash sectors. Included are two functions which can claim and release the Flash pump to operate on a specific zone.

group dcsm_api

Defines

DCSM_O_Z1_CSMPSWD0 0x00U

Z1 CSMPSWD0 offset.

DCSM_O_Z1_CSMPSWD1 0x02U

Z1 CSMPSWD1 offset.

DCSM_O_Z1_CSMPSWD2 0x04U

Z1 CSMPSWD2 offset.

DCSM_O_Z1_CSMPSWD3 0x06U

Z1 CSMPSWD3 offset.

DCSM_O_Z2_CSMPSWD0 0x00U

Z2 CSMPSWD0 offset.

DCSM_O_Z2_CSMPSWD1 0x02U

Z2 CSMPSWD1 offset.

DCSM_O_Z2_CSMPSWD2 0x04U

Z2 CSMPSWD2 offset.

DCSM_O_Z2_CSMPSWD3 0x06U

Z2 CSMPSWD3 offset.

FLSEM_KEY 0xA5U

Zone semaphore key.

DCSM_FORCE_SECERR_KEY 0x5A5AU
DCSM_ALLZERO 0x08U

CSM Passwords all zeros.

DCSM_ALLONE 0x10U

CSM Passwords all ones.

DCSM_UNSECURE 0x20U

Zone is secure/unsecure.

DCSM_ARMED 0x40U

CSM is armed.

DCSM_EXEONLYSECTR_M 0x0000FFFFU
DCSM_EXEONLYSECTR_S 16U
DCSM_ZX_CR_S 16U
DCSM_Z1_EXEONLYRAM1R_CPU2 31U
DCSM_Z2_EXEONLYRAM1R_CPU2 31U
DCSM_Z1_OTPSECLOCK_JTAGLOCK_M 0x1U
DCSM_Z1_OTPSECLOCK_JTAGLOCK_S 0U
DCSM_OTPSECLOCK_INVALID 0xFFFFU

Enums

enum DCSM_MemoryStatus

Values to distinguish the status of RAM or FLASH sectors. These values describe which zone the memory location belongs too. These values can be returned from DCSM_getRAMZone(), DCSM_getFlashSectorZone().

Values:

enumerator DCSM_MEMORY_INACCESSIBLE

Inaccessible.

enumerator DCSM_MEMORY_ZONE1

Zone 1.

enumerator DCSM_MEMORY_ZONE2

Zone 2.

enumerator DCSM_MEMORY_FULL_ACCESS

Full access.

enum DCSM_SemaphoreZone

Values to pass to DCSM_claimZoneSemaphore(). These values are used to describe the zone that can write to Flash Wrapper registers.

Values:

enumerator DCSM_FLSEM_ZONE1 = 0x01U

Flash semaphore Zone 1.

enumerator DCSM_FLSEM_ZONE2 = 0x02U

Flash semaphore Zone 2.

enum DCSM_SecurityStatus

Values to distinguish the security status of the zones. These values can be returned from DCSM_getZone1CSMSecurityStatus(), DCSM_getZone2CSMSecurityStatus().

Values:

enumerator DCSM_STATUS_SECURE

Secure.

enumerator DCSM_STATUS_UNSECURE

Unsecure.

enumerator DCSM_STATUS_LOCKED

Locked.

enumerator DCSM_STATUS_BLOCKED

Blocked.

enum DCSM_EXEOnlyStatus

Values to decribe the EXEONLY Status. These values are returned from to DCSM_getZone1RAMEXEStatus(), DCSM_getZone2RAMEXEStatus(), DCSM_getZone1FlashEXEStatus(), DCSM_getZone2FlashEXEStatus().

Values:

enumerator DCSM_PROTECTED

Protected.

enumerator DCSM_UNPROTECTED

Unprotected.

enumerator DCSM_INCORRECT_ZONE

Incorrect Zone.

enum DCSM_RAMModule

Values to distinguish RAM Module. These values can be passed to DCSM_getZone1RAMEXEStatus() DCSM_getZone2RAMEXEStatus(), DCSM_getRAMZone().

Values:

enumerator DCSM_RAMLS0

RAMLS0.

enumerator DCSM_RAMLS1

RAMLS1.

enumerator DCSM_RAMLS2

RAMLS2.

enumerator DCSM_RAMLS3

RAMLS3.

enumerator DCSM_RAMLS4

RAMLS4.

enumerator DCSM_RAMLS5

RAMLS5.

enumerator DCSM_RAMLS6

RAMLS6.

enumerator DCSM_RAMLS7

RAMLS7.

enumerator DCSM_RAMLS8

RAMLS8.

enumerator DCSM_RAMLS9

RAMLS9.

enumerator DCSM_RAMD0

RAMD0.

enumerator DCSM_RAMD1

RAMD1.

enumerator DCSM_RAMD2

RAMD2.

enumerator DCSM_RAMD3

RAMD3.

enumerator DCSM_RAMD4

RAMD4.

enumerator DCSM_RAMD5

RAMD5.

enumerator DCSM_C28_RAM_END
enumerator DCSM_RAM1_CPU1_CPU2

CPU1 to CPU2 Message RAM 1.

enumerator DCSM_RAM2_CPU1_CPU2

CPU1 to CPU2 Message RAM 2.

enumerator DCSM_RAM1_CPU2_CPU1

CPU2 to CPU1 Message RAM 1.

enumerator DCSM_RAM2_CPU2_CPU1

CPU2 to CPU1 Message RAM 2.

enum DCSM_Sector

Values to distinguish Flash Sector. These values can be passed to DCSM_getZone1FlashEXEStatus() DCSM_getZone2FlashEXEStatus(), DCSM_getFlashSectorZone().

Values:

enumerator DCSM_BANK0_SECTOR_0

Bank 0 - Sector 0.

enumerator DCSM_BANK0_SECTOR_1

Bank 0 - Sector 1.

enumerator DCSM_BANK0_SECTOR_2

Bank 0 - Sector 2.

enumerator DCSM_BANK0_SECTOR_3

Bank 0 - Sector 3.

enumerator DCSM_BANK0_SECTOR_31_4

Bank 0 - Sector 31-4.

enumerator DCSM_BANK0_SECTOR_63_32

Bank 0 - Sector 63-32.

enumerator DCSM_BANK0_SECTOR_95_64

Bank 0 - Sector 95-64.

enumerator DCSM_BANK0_SECTOR_127_96

Bank 0 - Sector 127-96.

enumerator DCSM_BANK1_SECTOR_0

Bank 1 - Sector 0.

enumerator DCSM_BANK1_SECTOR_1

Bank 1 - Sector 1.

enumerator DCSM_BANK1_SECTOR_2

Bank 1 - Sector 2.

enumerator DCSM_BANK1_SECTOR_3

Bank 1 - Sector 3.

enumerator DCSM_BANK1_SECTOR_31_4

Bank 1 - Sector 31-4.

enumerator DCSM_BANK1_SECTOR_63_32

Bank 1 - Sector 63-32.

enumerator DCSM_BANK1_SECTOR_95_64

Bank 1 - Sector 95-64.

enumerator DCSM_BANK1_SECTOR_127_96

Bank 1 - Sector 127-96.

enumerator DCSM_BANK2_SECTOR_0

Bank 2 - Sector 0.

enumerator DCSM_BANK2_SECTOR_1

Bank 2 - Sector 1.

enumerator DCSM_BANK2_SECTOR_2

Bank 2 - Sector 2.

enumerator DCSM_BANK2_SECTOR_3

Bank 2 - Sector 3.

enumerator DCSM_BANK2_SECTOR_31_4

Bank 2 - Sector 31-4.

enumerator DCSM_BANK2_SECTOR_63_32

Bank 2 - Sector 63-32.

enumerator DCSM_BANK2_SECTOR_95_64

Bank 2 - Sector 95-64.

enumerator DCSM_BANK2_SECTOR_127_96

Bank 2 - Sector 127-96.

enumerator DCSM_BANK3_SECTOR_0

Bank 3 - Sector 0.

enumerator DCSM_BANK3_SECTOR_1

Bank 3 - Sector 1.

enumerator DCSM_BANK3_SECTOR_2

Bank 3 - Sector 2.

enumerator DCSM_BANK3_SECTOR_3

Bank 3 - Sector 3.

enumerator DCSM_BANK3_SECTOR_31_4

Bank 3 - Sector 31-4.

enumerator DCSM_BANK3_SECTOR_63_32

Bank 3 - Sector 63-32.

enumerator DCSM_BANK3_SECTOR_95_64

Bank 3 - Sector 95-64.

enumerator DCSM_BANK3_SECTOR_127_96

Bank 3 - Sector 127-96.

enumerator DCSM_BANK4_SECTOR_0

Bank 4 - Sector 0.

enumerator DCSM_BANK4_SECTOR_1

Bank 4 - Sector 1.

enumerator DCSM_BANK4_SECTOR_2

Bank 4 - Sector 2.

enumerator DCSM_BANK4_SECTOR_3

Bank 4 - Sector 3.

enumerator DCSM_BANK4_SECTOR_31_4

Bank 4 - Sector 31-4.

enumerator DCSM_BANK4_SECTOR_63_32

Bank 4 - Sector 63-32.

enumerator DCSM_BANK4_SECTOR_95_64

Bank 4 - Sector 95-64.

enumerator DCSM_BANK4_SECTOR_127_96

Bank 4 - Sector 127-96.

enum DCSM_CPUSel

The following are values that can be passed to DCSM_getRAMZone(), DCSM_getZone2FlashEXEStatus() ,DCSM_getZone1FlashEXEStatus() & DCSM_getFlashSectorZone() as cpuInst parameter.

Values:

enumerator DCSM_CPUSEL_CPU1 = 0x0U

To access CPU1 Memory.

enumerator DCSM_CPUSEL_CPU2 = 0x2U

To access CPU2 Memory.

enum DCSM_OTPLock

The following are values that can be passed to DCSM_getZone1OTPSecureLockStatus() & DCSM_getZone2OTPSecureLockStatus() as lockType parameter.

Values:

enumerator DCSM_OTPSECLOCK_JTAG = 0x0U

JTAG Lock Status.

enumerator DCSM_OTPSECLOCK_PSWDLOCK = 0x1U

Zone Password Lock.

enumerator DCSM_OTPSECLOCK_CRCLOCK = 0x2U

Zone CRC Lock.

enum DCSM_PERSem

The following are values that can be passed to DCSM_forcePerSemStatus() & DCSM_getPerSemStatus() as grabType parameter.

Values:

enumerator DCSM_GRABWD = 0U

Grab Watchdog configuration.

enumerator DCSM_GRABNMIWD = 2U

Grab NMIWD configuration.

enumerator DCSM_GRABTIMER1 = 4U

Grab TIMER1 configuration.

enumerator DCSM_GRABCLKCTL = 6U

Grab Clock configuration.

enumerator DCSM_GRABRSTCTL = 8U

Grab Reset configuration.

Functions

void DCSM_secureZone1(void)

Secures zone 1 by setting the FORCESEC bit of Z1_CR register

This function resets the state of the zone. If the zone is unlocked, it will lock(secure) the zone and also reset all the bits in the Control Register.

Return

None.

void DCSM_secureZone2(void)

Secures zone 2 by setting the FORCESEC bit of Z2_CR register

This function resets the state of the zone. If the zone is unlocked, it will lock(secure) the zone and also reset all the bits in the Control Register.

Return

None.

DCSM_SecurityStatus DCSM_getZone1CSMSecurityStatus(void)

Returns the CSM security status of zone 1

This function returns the security status of zone 1 CSM

Return

Returns security status as an enumerated type DCSM_SecurityStatus.

DCSM_SecurityStatus DCSM_getZone2CSMSecurityStatus(void)

Returns the CSM security status of zone 2

This function returns the security status of zone 2 CSM

Return

Returns security status as an enumerated type DCSM_SecurityStatus.

uint16_t DCSM_getZone1ControlStatus(void)

Returns the Control Status of zone 1

This function returns the Control Status of zone 1 CSM

Return

Returns the contents of the Control Register which can be used with provided defines.

uint16_t DCSM_getZone2ControlStatus(void)

Returns the Control Status of zone 2

This function returns the Control Status of zone 2 CSM

Return

Returns the contents of the Control Register which can be used with the provided defines.

DCSM_MemoryStatus DCSM_getRAMZone(DCSM_RAMModule module)

Returns the security zone a RAM section belongs to

This function returns the security zone a RAM section belongs to.

Note

DCSM_CPUSEL_CPU1 can only be used with C28x RAMs (in DCSM_RAMModule)

Parameters
  • module: is the RAM module value. Valid values are type DCSM_RAMModule C28x RAMs :

    • DCSM_RAMLS0

    • DCSM_RAMLS1

    • DCSM_RAMLS2

    • DCSM_RAMLS3

    • DCSM_RAMLS4

    • DCSM_RAMLS5

    • DCSM_RAMLS6

    • DCSM_RAMLS7

    • DCSM_RAMLS8

    • DCSM_RAMLS9

    • DCSM_RAMD0

    • DCSM_RAMD1

    • DCSM_RAMD2

    • DCSM_RAMD3

    • DCSM_RAMD4

    • DCSM_RAMD5

    • DCSM_RAM1_CPU1_CPU2

    • DCSM_RAM2_CPU1_CPU2

    • DCSM_RAM1_CPU2_CPU1

    • DCSM_RAM2_CPU2_CPU1

Return

Returns DCSM_MEMORY_INACCESSIBLE if the section is inaccessible, DCSM_MEMORY_ZONE1 if the section belongs to zone 1, DCSM_MEMORY_ZONE2 if the section belongs to zone 2 and DCSM_MEMORY_FULL_ACCESS if the section doesn’t belong to any zone (or if the section is unsecure).

DCSM_MemoryStatus DCSM_getFlashSectorZone(DCSM_Sector sector)

Returns the security zone a flash sector belongs to

This function returns the security zone a flash sector belongs to.

Parameters
  • sector: is the flash sector value. Use DCSM_Sector type.

Return

Returns DCSM_MEMORY_INACCESSIBLE if the section is inaccessible , DCSM_MEMORY_ZONE1 if the section belongs to zone 1, DCSM_MEMORY_ZONE2 if the section belongs to zone 2 and DCSM_MEMORY_FULL_ACCESS if the section doesn’t belong to any zone (or if the section is unsecure)..

uint32_t DCSM_getZone1LinkPointerError(void)

Read Zone 1 Link Pointer Error

A non-zero value indicates an error on the bit position that is set to 1.

Return

Returns the value of the Zone 1 Link Pointer error.

uint32_t DCSM_getZone2LinkPointerError(void)

Read Zone 2 Link Pointer Error

A non-zero value indicates an error on the bit position that is set to 1.

Return

Returns the value of the Zone 2 Link Pointer error.

bool DCSM_getFlashErrorStatus(void)

Get the status of the security configuration load from USER-OTP or sector error status

Return

Returns 0 if no error in loading security information from USER-OTP, 1 if an error has occurred in the load from USER-OTP.

void DCSM_clearFlashErrorStatus(void)

Clear the Flash Error Status bit

Write a ‘1’ to the clear bit to clear the sector error status bit.

Return

None.

void DCSM_forceFlashErrorStatus(void)

Set the force Flash Error Status bit

Write a ‘1’ to force bit to set the sector error status bit.

Return

None.

uint32_t DCSM_getZone1OTPSecureLockStatus(DCSM_OTPLock lockType)

Returns the OTP secure Lock status of zone 1

The

lockType parameter can have one of the following values of the DCSM_CPUSel type:
  • DCSM_OTPSECLOCK_JTAG - JTAG Lock Status

  • DCSM_OTPSECLOCK_CRCLOCK - Zone CRC Lock

  • DCSM_OTPSECLOCK_PSWDLOCK - Zone Password Lock

Parameters
  • lockType: is the OTP secure Lock feature type .

This function takes in a valid OTP secure Lock feature type and returns the status of zone 1 lock feature

For Zone Password Lock : 1111 - CSM Pwd locations in the OTP are not protected and can be read from the debugger as well as code running from anywhere. Other Value : CSM Pwd locations in the OTP are protected and can’t be read without unlocking CSM of that zone.

Return

Returns security lock status can be: For JTAG lock : 0 - JTAG is not locked , 1 - JTAG is locked

For Zone CRC Lock : 1111 : VCU has ability to calculate CRC on secure memories. Other Value : VCU doesn’t have the ability to calculate CRC on secure memories.

uint32_t DCSM_getZone2OTPSecureLockStatus(DCSM_OTPLock lockType)

Returns the OTP secure Lock status of zone 2

The

lockType parameter can have one of the following values of the DCSM_CPUSel type:
  • DCSM_OTPSECLOCK_CRCLOCK - Zone CRC Lock

  • DCSM_OTPSECLOCK_PSWDLOCK - Zone Password Lock

Parameters
  • lockType: is the OTP secure Lock feature type .

This function takes in a valid OTP secure Lock feature type and returns the status of zone 2 lock feature

For Zone Password Lock : 1111 - CSM Pwd locations in the OTP are not protected and can be read from the debugger as well as code running from anywhere. Other Value : CSM Pwd locations in the OTP are protected and can’t be read without unlocking CSM of that zone.

Return

Returns security lock status can be:

For Zone CRC Lock : 1111 : VCU has ability to calculate CRC on secure memories. Other Value : VCU doesn’t have the ability to calculate CRC on secure memories.

uint16_t DCSM_getFlashDenyCodeStatus(void)

Returns the status of Deny Code register

This function returns the status of Deny Code register

Return

Returns the Status of Deny Code register which can be used with the provided defines.

uint32_t DCSM_getDeviceUIDLow(void)

Get the device UID_UNIQUE value bits 31 to 0

This function returns the device UID_UNIQUE value bits 31 to 0.

Return

Returns the device UID_UNIQUE value low.

uint32_t DCSM_getDeviceUIDHigh(void)

Get the device UID_UNIQUE value bits 63 to 32

This function returns the device UID_UNIQUE value bits 63 to 32.

Return

Returns the device UID_UNIQUE value high.

uint32_t DCSM_getDevicePartID(void)

Get the device PARTIDH value

This function returns the device PARTIDH value

Return

Returns the device PARTIDH value

uint32_t DCSM_getPerSemStatus(DCSM_PERSem grabType)

Get the Flash wrapper semaphore register value

This function returns the Flash wrapper register value

Return

Returns the Flash wrapper semaphore register value

void DCSM_forcePerSemStatus(DCSM_PERSem grabType, uint16_t value)

Force the Flash wrapper semaphore register value

This function writes into the Flash wrapper register field

Return

None.

void DCSM_unlockZone1CSM(const DCSM_CSMPasswordKey *const psCMDKey)

Unlocks Zone 1 CSM.

This function unlocks the CSM password. It first reads the four password locations in the User OTP. If any of the password values is different from 0xFFFFFFFF, it unlocks the device by writing the provided passwords into CSM Key registers

Parameters
  • psCMDKey: is a pointer to the DCSM_CSMPasswordKey struct that has the CSM password for zone 1.

Return

None.

Note

This function should not be called in an actual application, should only be used for once to program the OTP memory. Ensure flash data cache is disabled before calling this function(Flash_disableCache).

void DCSM_unlockZone2CSM(const DCSM_CSMPasswordKey *const psCMDKey)

Unlocks Zone 2 CSM.

This function unlocks the CSM password. It first reads the four password locations in the User OTP. If any of the password values is different from 0xFFFFFFFF, it unlocks the device by writing the provided passwords into CSM Key registers

Parameters
  • psCMDKey: is a pointer to the CSMPSWDKEY that has the CSM password for zone 2.

Return

None.

Note

This function should not be called in an actual application, should only be used for once to program the OTP memory. Ensure flash data cache is disabled before calling this function(Flash_disableCache).

void DCSM_writeZone1CSM(const DCSM_CSMPasswordKey *const psCMDKey)

Write Zone 1 CSM.

Password match flow is essentially a sequence of dummy reads from password locations (PWL) followed by writes to CSMKEY registers. This function helps writing the provided passwords into the CSM Key registers. The

DCSM_readZone1CSMPwd() should be called by CPU1 before calling this API.
Parameters
  • psCMDKey: is a pointer to the CSMPSWDKEY that has the CSM password for zone 1.

Return

None.

void DCSM_writeZone2CSM(const DCSM_CSMPasswordKey *const psCMDKey)

Write Zone 2 CSM.

Password match flow is essentially a sequence of dummy reads from password locations (PWL) followed by writes to CSMKEY registers. This function helps writing the provided passwords into the CSM Key registers. The

DCSM_readZone2CSMPwd() should be called by CPU1 before calling this API.
Parameters
  • psCMDKey: is a pointer to the CSMPSWDKEY that has the CSM password for zone 2.

Return

None.

DCSM_EXEOnlyStatus DCSM_getZone1FlashEXEStatus(DCSM_Sector sector)

Returns the EXE-ONLY status of zone 1 for a flash sector

This function takes in a valid sector value and returns the status of EXE ONLY security protection for the sector.

Parameters
  • sector: is the flash sector value. Use DCSM_Sector type.

Return

Returns DCSM_PROTECTED if the sector is EXE-ONLY protected, DCSM_UNPROTECTED if the sector is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if sector does not belong to this zone.

DCSM_EXEOnlyStatus DCSM_getZone1RAMEXEStatus(DCSM_RAMModule module)

Returns the EXE-ONLY status of zone 1 for a RAM module

This function takes in a valid module value and returns the status of EXE ONLY security protection for that module.

Parameters
  • module: is the RAM module value. Valid values are type DCSM_RAMModule C28x RAMs :

    • DCSM_RAMLS0

    • DCSM_RAMLS1

    • DCSM_RAMLS2

    • DCSM_RAMLS3

    • DCSM_RAMLS4

    • DCSM_RAMLS5

    • DCSM_RAMLS6

    • DCSM_RAMLS7

    • DCSM_RAMLS8

    • DCSM_RAMLS9

    • DCSM_RAMD0

    • DCSM_RAMD1

    • DCSM_RAMD2

    • DCSM_RAMD3

    • DCSM_RAMD4

    • DCSM_RAMD5

    • DCSM_RAM1_CPU1_CPU2

    • DCSM_RAM2_CPU1_CPU2

    • DCSM_RAM1_CPU2_CPU1

    • DCSM_RAM2_CPU2_CPU1

Return

Returns DCSM_PROTECTED if the module is EXE-ONLY protected, DCSM_UNPROTECTED if the module is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if module does not belong to this zone.

DCSM_EXEOnlyStatus DCSM_getZone2FlashEXEStatus(DCSM_Sector sector)

Returns the EXE-ONLY status of zone 2 for a flash sector

This function takes in a valid sector value and returns the status of EXE ONLY security protection for the sector.

Parameters
  • sector: is the flash sector value. Use DCSM_Sector type.

Return

Returns DCSM_PROTECTED if the sector is EXE-ONLY protected, DCSM_UNPROTECTED if the sector is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if sector does not belong to this zone.

DCSM_EXEOnlyStatus DCSM_getZone2RAMEXEStatus(DCSM_RAMModule module)

Returns the EXE-ONLY status of zone 2 for a RAM module

This function takes in a valid module value and returns the status of EXE ONLY security protection for that module.

Parameters
  • module: is the RAM module value. Valid values are type DCSM_RAMModule C28x RAMs :

    • DCSM_RAMLS0

    • DCSM_RAMLS1

    • DCSM_RAMLS2

    • DCSM_RAMLS3

    • DCSM_RAMLS4

    • DCSM_RAMLS5

    • DCSM_RAMLS6

    • DCSM_RAMLS7

    • DCSM_RAMLS8

    • DCSM_RAMLS9

    • DCSM_RAMD0

    • DCSM_RAMD1

    • DCSM_RAMD2

    • DCSM_RAMD3

    • DCSM_RAMD4

    • DCSM_RAMD5

    • DCSM_RAM1_CPU1_CPU2

    • DCSM_RAM2_CPU1_CPU2

    • DCSM_RAM1_CPU2_CPU1

    • DCSM_RAM2_CPU2_CPU1

Return

Returns DCSM_PROTECTED if the module is EXE-ONLY protected, DCSM_UNPROTECTED if the module is not EXE-ONLY protected, DCSM_INCORRECT_ZONE if module does not belong to this zone.

bool DCSM_claimZoneSemaphore(DCSM_SemaphoreZone zone)

Claims the zone semaphore which allows access to the Flash Wrapper register for that zone.

Return

Returns true for a successful semaphore capture, false if it was unable to capture the semaphore.

Parameters
  • zone: is the zone which is trying to claim the semaphore which allows access to the Flash Wrapper registers.

bool DCSM_releaseZoneSemaphore(void)

Releases the zone semaphore.

Return

Returns true if it was successful in releasing the zone semaphore and false if it was unsuccessful in releasing the zone semaphore.

Note

If the calling function is not in the right zone to be able to access this register, it will return a false.

void DCSM_readZone1CSMPwd(void)

Perform dummy reads on the 128-bit Zone 1 CSM password.

This function reads the four password locations in the User OTP needed to be done as part of the Password Match Flow before writes to the CSMKEY registers. This would need to be done before a DCSM_writeZone1CSM().

Return

None.

Note

This API to be called from CPU1.

void DCSM_readZone2CSMPwd(void)

Perform dummy reads on the 128-bit Zone 2 CSM password.

This function reads the four password locations in the User OTP needed to be done as part of the Password Match Flow before writes to the CSMKEY registers. This would need to be done before a DCSM_writeZone2CSM().

Return

None.

Note

This API to be called from CPU1.

struct DCSM_CSMPasswordKey
#include <dcsm.h>

Data structures to hold password keys.

The code for this module is contained in driverlib/dcsm.c, with driverlib/dcsm.h containing the API declarations for use by applications.