Interrupt Module¶
The Interrupt API provides a set of functions for dealing with the Peripheral Interrupt Expansion (PIE) Controller as well as CPU-level interrupt configuration. Functions are provided to initialize interrupt-related registers, enable and disable interrupts, and register interrupt handlers.
Interrupt API functions rely on an interrupt number defined to specify which interrupt is being configured. These interrupt numbers are found in inc/hw_ints.h and are in the format INT_X. For example, INT_EPWM2_TZ would be used to specify the trip zone interrupt for EPWM2 wherever a function has an e interruptNumber parameter.
-
group
interrupt_api Defines
-
PIEVECTTABLE_BASEPIEVECTTABLEMAIN_BASE¶
-
INTERRUPT_CPU_INT10x1U¶ CPU Interrupt Number 1.
-
INTERRUPT_CPU_INT20x2U¶ CPU Interrupt Number 2.
-
INTERRUPT_CPU_INT30x4U¶ CPU Interrupt Number 3.
-
INTERRUPT_CPU_INT40x8U¶ CPU Interrupt Number 4.
-
INTERRUPT_CPU_INT50x10U¶ CPU Interrupt Number 5.
-
INTERRUPT_CPU_INT60x20U¶ CPU Interrupt Number 6.
-
INTERRUPT_CPU_INT70x40U¶ CPU Interrupt Number 7.
-
INTERRUPT_CPU_INT80x80U¶ CPU Interrupt Number 8.
-
INTERRUPT_CPU_INT90x100U¶ CPU Interrupt Number 9.
-
INTERRUPT_CPU_INT100x200U¶ CPU Interrupt Number 10.
-
INTERRUPT_CPU_INT110x400U¶ CPU Interrupt Number 11.
-
INTERRUPT_CPU_INT120x800U¶ CPU Interrupt Number 12.
-
INTERRUPT_CPU_INT130x1000U¶ CPU Interrupt Number 13.
-
INTERRUPT_CPU_INT140x2000U¶ CPU Interrupt Number 14.
-
INTERRUPT_CPU_DLOGINT0x4000U¶ CPU Data Log Interrupt.
-
INTERRUPT_CPU_RTOSINT0x8000U¶ CPU RTOS Interrupt.
-
INTERRUPT_ACK_GROUP10x1U¶ Acknowledge PIE Interrupt Group 1.
-
INTERRUPT_ACK_GROUP20x2U¶ Acknowledge PIE Interrupt Group 2.
-
INTERRUPT_ACK_GROUP30x4U¶ Acknowledge PIE Interrupt Group 3.
-
INTERRUPT_ACK_GROUP40x8U¶ Acknowledge PIE Interrupt Group 4.
-
INTERRUPT_ACK_GROUP50x10U¶ Acknowledge PIE Interrupt Group 5.
-
INTERRUPT_ACK_GROUP60x20U¶ Acknowledge PIE Interrupt Group 6.
-
INTERRUPT_ACK_GROUP70x40U¶ Acknowledge PIE Interrupt Group 7.
-
INTERRUPT_ACK_GROUP80x80U¶ Acknowledge PIE Interrupt Group 8.
-
INTERRUPT_ACK_GROUP90x100U¶ Acknowledge PIE Interrupt Group 9.
-
INTERRUPT_ACK_GROUP100x200U¶ Acknowledge PIE Interrupt Group 10.
-
INTERRUPT_ACK_GROUP110x400U¶ Acknowledge PIE Interrupt Group 11.
-
INTERRUPT_ACK_GROUP120x800U¶ Acknowledge PIE Interrupt Group 12.
Functions
-
void
Interrupt_defaultHandler(void)¶ The default interrupt handler.
- Return
None.
-
void
Interrupt_illegalOperationHandler(void)¶ The default illegal instruction trap interrupt handler.
- Return
None.
-
void
Interrupt_nmiHandler(void)¶ The default non-maskable interrupt handler.
- Return
None.
-
bool
Interrupt_enableGlobal(void)¶ Allows the CPU to process interrupts.
This function clears the global interrupt mask bit (INTM) in the CPU, allowing the processor to respond to interrupts.
- Return
Returns true if interrupts were disabled when the function was called or false if they were initially enabled.
-
bool
Interrupt_disableGlobal(void)¶ Stops the CPU from processing interrupts.
This function sets the global interrupt mask bit (INTM) in the CPU, preventing the processor from receiving maskable interrupts.
- Return
Returns true if interrupts were already disabled when the function was called or false if they were initially enabled.
-
void
Interrupt_register(uint32_t interruptNumber, void (*handler)(void))¶ Registers a function to be called when an interrupt occurs.
This function is used to specify the handler function to be called when the given interrupt is asserted to the processor. When the interrupt occurs, if it is enabled (via
Interrupt_enable()), the handler function will be called in interrupt context. Since the handler function can preempt other code, care must be taken to protect memory or peripherals that are accessed by the handler and other non-handler code.- Parameters
interruptNumber: specifies the interrupt in question.handler: is a pointer to the function to be called.
The available interruptNumber values are supplied in
inc/hw_ints.h.- Note
This function assumes that the PIE has been enabled. See Interrupt_initModule().
- Return
None.
-
void
Interrupt_unregister(uint32_t interruptNumber)¶ Unregisters the function to be called when an interrupt occurs.
This function is used to indicate that a default handler
Interrupt_defaultHandler() should be called when the given interrupt is asserted to the processor. Call Interrupt_disable() to disable the interrupt before calling this function.- Parameters
interruptNumber: specifies the interrupt in question.
The available interruptNumber values are supplied in
inc/hw_ints.h.- See
Interrupt_register() for important information about registering interrupt handlers.
- Return
None.
-
void
Interrupt_enableInCPU(uint16_t cpuInterrupt)¶ Enables CPU interrupt channels
This function enables the specified interrupts in the CPU. The
cpuInterrupt parameter is a logical OR of the values INTERRUPT_CPU_INTx where x is the interrupt number between 1 and 14, INTERRUPT_CPU_DLOGINT, and INTERRUPT_CPU_RTOSINT.- Parameters
cpuInterrupt: specifies the CPU interrupts to be enabled.
- Note
Note that interrupts 1-12 correspond to the PIE groups with those same numbers.
- Return
None.
-
void
Interrupt_disableInCPU(uint16_t cpuInterrupt)¶ Disables CPU interrupt channels
This function disables the specified interrupts in the CPU. The
cpuInterrupt parameter is a logical OR of the values INTERRUPT_CPU_INTx where x is the interrupt number between 1 and 14, INTERRUPT_CPU_DLOGINT, and INTERRUPT_CPU_RTOSINT.- Parameters
cpuInterrupt: specifies the CPU interrupts to be disabled.
- Note
Note that interrupts 1-12 correspond to the PIE groups with those same numbers.
- Return
None.
-
void
Interrupt_clearACKGroup(uint16_t group)¶ Acknowledges PIE Interrupt Group
The specified interrupt group is acknowledged and clears any interrupt flag within that respective group.
- Parameters
group: specifies the interrupt group to be acknowledged.
The group parameter must be a logical OR of the following: INTERRUPT_ACK_GROUP1, INTERRUPT_ACK_GROUP2, INTERRUPT_ACK_GROUP3 INTERRUPT_ACK_GROUP4, INTERRUPT_ACK_GROUP5, INTERRUPT_ACK_GROUP6 INTERRUPT_ACK_GROUP7, INTERRUPT_ACK_GROUP8, INTERRUPT_ACK_GROUP9 INTERRUPT_ACK_GROUP10, INTERRUPT_ACK_GROUP11, INTERRUPT_ACK_GROUP12.
- Return
None.
-
void
Interrupt_enablePIE(void)¶ Enables the PIE block.
This function enables the vector fetching for the peripheral interrupts by enabling the PIE block.
- Return
None.
-
void
Interrupt_disablePIE(void)¶ Disables the PIE block.
This function disables the vector fetching for the peripheral interrupts by disabling the PIE block. PIEACK, PIEIFR, and PIEIER registers can be accessed even when the PIE block is disabled.
- Return
None.
-
void
Interrupt_initModule(void)¶ Initializes the PIE control registers by setting them to a known state.
This function initializes the PIE control registers. After globally disabling interrupts and enabling the PIE, it clears all of the PIE interrupt enable bits and interrupt flags.
- Return
None.
-
void
Interrupt_initVectorTable(void)¶ Initializes the PIE vector table by setting all vectors to a default handler function.
- Return
None.
-
void
Interrupt_enable(uint32_t interruptNumber)¶ Enables an interrupt.
The specified interrupt is enabled in the interrupt controller. Other enables for the interrupt (such as at the peripheral level) are unaffected by this function.
- Parameters
interruptNumber: specifies the interrupt to be enabled.
The available interruptNumber values are supplied in
inc/hw_ints.h.- Return
None.
-
void
Interrupt_disable(uint32_t interruptNumber)¶ Disables an interrupt.
The specified interrupt is disabled in the interrupt controller. Other enables for the interrupt (such as at the peripheral level) are unaffected by this function.
- Parameters
interruptNumber: specifies the interrupt to be disabled.
The available interruptNumber values are supplied in
inc/hw_ints.h.- Return
None.
-
uint16_t
__disable_interrupts(void)¶
-
uint16_t
__enable_interrupts(void)¶
-
The Interrupt API provides two functions to initialize the module, Interrupt_initModule() and Interrupt_initVectorTable(). The former puts the PIE registers and the interrupt-related registers in the CPU into a known state. It clears all flags, disables interrupts at all levels, and enables vector fetching from the PIE. The latter initializes the PIE Vector Table to a set of default handlers–Interrupt_nmiHandler() for non-maskable interrupts, Interrupt_illegalOperationHandler() for an ITRAP interrupt, and Interrupt_defaultHandler() for all others. These defaults are intended to help with debugging. They should be modified or replaced more appropriate ISRs by the user.
Each interrupt source can be individually enabled and disabled via Interrupt_enable() and Interrupt_disable(). These affect the interrupt both on the PIE and on the CPU’s IER register. The processor interrupt can be enabled and disabled via Interrupt_enableMaster() and Interrupt_disableMaster(); this does not affect the individual interrupt enable states. Masking of the processor interrupt can be utilized as a simple critical section (only NMI will interrupt the processor while the processor interrupt is disabled), though this will have adverse effects on the interrupt response time.
When an interrupt occurs, in order for further interrupts on its PIE group to be received, Interrupt_clearACKGroup() must be called. This is typically done at the end of the ISR.
The code for this module is contained in driverlib/interrupt.c, with driverlib/interrupt.h containing the API declarations for use by applications.