MEMCFG Module

The MemCfg module provides an API to configure the device’s Memory Control Module. The functions that are provided fall into three main categories: RAM section configuration, access violation status and interrupts, and memory error status an interrupts. The RAM section configuration functions can initialize RAM, configure access protection settings, and configure section ownership. The access violation and memory error categories contain functions that can return violation and error status and address information as well as configure interrupts that can be generated as a result of these issues.

group memcfg_api

Defines

MEMCFG_SECT_TYPE_MASK 0xFF000000U
MEMCFG_SECT_TYPE_D 0x00000000U
MEMCFG_SECT_TYPE_LS 0x01000000U
MEMCFG_SECT_TYPE_GS 0x02000000U
MEMCFG_SECT_TYPE_MSG 0x03000000U
MEMCFG_SECT_TYPE_ROM 0x04000000U
MEMCFG_SECT_TYPE_PERIMEM 0x05000000U
MEMCFG_SECT_NUM_MASK 0x00FFFFFFU
MEMCFG_XACCPROTX_M ((uint32_t)MEMCFG_GSXACCPROT0_FETCHPROT_GS0

| \

(uint32_t)

MEMCFG_GSXACCPROT0_CPUWRPROT_GS0

| \

(uint32_t)

MEMCFG_GSXACCPROT0_DMAWRPROT_GS0)
MEMCFG_XTEST_M MEMCFG_DXTEST_TEST_M0_M
MEMCFG_NMVIOL_MASK 0x0000FFFFU
MEMCFG_MVIOL_MASK 0x000F0000U
MEMCFG_MVIOL_SHIFT 16U
MEMCFG_TESTLOCK_KEY 0xA5A50000U
MEMCFG_SECT_M0 0x00000001U

M0 RAM.

MEMCFG_SECT_M1 0x00000002U

M1 RAM.

MEMCFG_SECT_D0 0x00000004U

D0 RAM.

MEMCFG_SECT_D1 0x00000008U

D1 RAM.

MEMCFG_SECT_D2 0x00000010U

D2 RAM.

MEMCFG_SECT_D3 0x00000020U

D3 RAM.

MEMCFG_SECT_D4 0x00000040U

D4 RAM.

MEMCFG_SECT_D5 0x00000080U

D5 RAM.

MEMCFG_SECT_DX_ALL 0x000000FFU

All M and D RAM.

MEMCFG_SECT_PIEVECT 0x00000100U

PIEVECT RAM.

MEMCFG_SECT_LS0 0x01000001U

LS0 RAM.

MEMCFG_SECT_LS1 0x01000002U

LS1 RAM.

MEMCFG_SECT_LS2 0x01000004U

LS2 RAM.

MEMCFG_SECT_LS3 0x01000008U

LS3 RAM.

MEMCFG_SECT_LS4 0x01000010U

LS4 RAM.

MEMCFG_SECT_LS5 0x01000020U

LS5 RAM.

MEMCFG_SECT_LS6 0x01000040U

LS6 RAM.

MEMCFG_SECT_LS7 0x01000080U

LS7 RAM.

MEMCFG_SECT_LS8 0x01000100U

LS8 RAM.

MEMCFG_SECT_LS9 0x01000200U

LS9 RAM.

MEMCFG_SECT_LSX_ALL 0x010003FFU

All LS RAM.

MEMCFG_SECT_GS0 0x02000001U

GS0 RAM.

MEMCFG_SECT_GS1 0x02000002U

GS1 RAM.

MEMCFG_SECT_GS2 0x02000004U

GS2 RAM.

MEMCFG_SECT_GS3 0x02000008U

GS3 RAM.

MEMCFG_SECT_GS4 0x02000010U

GS4 RAM.

MEMCFG_SECT_GSX_ALL 0x0200001FU

All GS RAM.

MEMCFG_SECT_MSGCPUTOCPU0 0x03000001U

CPU-to-CPU message RAM0.

MEMCFG_SECT_MSGCPUTOCLA1 0x03000002U

CPU-to-CLA1 message RAM.

MEMCFG_SECT_MSGCLA1TOCPU 0x03000004U

CLA1-to-CPU message RAM.

MEMCFG_SECT_MSGCLA1TODMA 0x03000020U

CLA1-to-DMA message RAM.

MEMCFG_SECT_MSGDMATOCLA1 0x03000040U

DMA-to-CLA1 message RAM.

MEMCFG_SECT_MSGCPUTOCPU1 0x03000080U

CPU-to-CPU message RAM1.

MEMCFG_SECT_MSGX_ALL 0x030000E7U

All message RAM.

MEMCFG_SECT_ROMBOOT 0x04000001U

BOOT ROM.

MEMCFG_SECT_ROMSECURE 0x04000002U

Secure ROM.

MEMCFG_SECT_ROMCLADATA 0x04000004U

CLA Data ROM.

MEMCFG_SECT_ROM_ALL 0x04000007U

All ROMs.

MEMCFG_SECT_PERIMEM_ETHERCAT 0x05000020U

Ethercat memory.

MEMCFG_SECT_PERIMEM_ALL 0x05000020U

All peripheral memories.

MEMCFG_SECT_ALL 0xFFFFFFFFU

All configurable RAM.

MEMCFG_PROT_ALLOWCPUFETCH 0x00000000U

CPU fetch allowed.

MEMCFG_PROT_BLOCKCPUFETCH 0x00000001U

CPU fetch blocked.

MEMCFG_PROT_ALLOWCPUWRITE 0x00000000U

CPU write allowed.

MEMCFG_PROT_BLOCKCPUWRITE 0x00000002U

CPU write blocked.

MEMCFG_PROT_ALLOWDMAWRITE 0x00000000U

DMA write allowed (GSxRAM)

MEMCFG_PROT_BLOCKDMAWRITE 0x00000004U

DMA write blocked (GSxRAM)

MEMCFG_NMVIOL_CPUREAD 0x00000001U

Non-controller CPU read access.

MEMCFG_NMVIOL_CPUWRITE 0x00000002U

Non-controller CPU write access.

MEMCFG_NMVIOL_CPUFETCH 0x00000004U

Non-controller CPU fetch access.

MEMCFG_NMVIOL_DMAWRITE 0x00000008U

Non-controller DMA write access.

MEMCFG_NMVIOL_CLA1READ 0x00000010U

Non-controller CLA1 read access.

MEMCFG_NMVIOL_CLA1WRITE 0x00000020U

Non-controller CLA1 write access.

MEMCFG_NMVIOL_CLA1FETCH 0x00000040U

Non-controller CLA1 fetch access.

MEMCFG_NMVIOL_DMAREAD 0x00000400U

Non-controller DMA read access.

MEMCFG_MVIOL_CPUFETCH 0x00010000U

Controller CPU fetch access.

MEMCFG_MVIOL_CPUWRITE 0x00020000U

Controller CPU write access.

MEMCFG_MVIOL_DMAWRITE 0x00040000U

Controller DMA write access.

MEMCFG_CERR_CPUREAD 0x0001U

Correctable CPU read error.

MEMCFG_CERR_DMAREAD 0x0002U

Correctable DMA read error.

MEMCFG_CERR_CLA1READ 0x0004U

Correctable CLA1 read error.

MEMCFG_UCERR_CPUREAD 0x0001U

Uncorrectable CPU read error.

MEMCFG_UCERR_DMAREAD 0x0002U

Uncorrectable DMA read error.

MEMCFG_UCERR_CLA1READ 0x0004U

Uncorrectable CLA1 read error.

MEMCFG_UCERR_ECATMEMREAD 0x0010U

Uncorrectable ECAT RAM read error.

MEMCFG_DIAGERR_UNCORR 0x00000002U

Uncorr error in diag/test mode.

MEMCFG_DIAGERR_CORR 0x00000001U

Corr error in diag/test mode.

Enums

enum MemCfg_CLAMemoryType

Values that can be passed to MemCfg_setCLAMemType() as the claMemType parameter.

Values:

enumerator MEMCFG_CLA_MEM_DATA

Section is CLA data memory.

enumerator MEMCFG_CLA_MEM_PROGRAM

Section is CLA program memory.

enum MemCfg_LSRAMControllerSel

Values that can be passed to MemCfg_setLSRAMControllerSel() as the controllerSel parameter.

Values:

enumerator MEMCFG_LSRAMCONTROLLER_CPU_ONLY

CPU is the owner of the section.

enumerator MEMCFG_LSRAMCONTROLLER_CPU_CLA1

CPU and CLA1 share this section.

enum MemCfg_GSRAMControllerSel

Values that can be passed to MemCfg_setGSRAMControllerSel() as the controllerSel parameter.

Values:

enumerator MEMCFG_GSRAMCONTROLLER_CPU1

CPU1 is controller of the section.

enumerator MEMCFG_GSRAMCONTROLLER_CPU2

CPU2 is controller of the section.

enum MemCfg_TestMode

Values that can be passed to MemCfg_setTestMode() as the testMode parameter.

Values:

enumerator MEMCFG_TEST_FUNCTIONAL = 0

Functional mode. Test mode is disabled.

enumerator MEMCFG_TEST_WRITE_DATA = 1

Writes allowed to data only.

enumerator MEMCFG_TEST_WRITE_ECC = 2

Writes allowed to ECC only (for DxRAM/MxRAM )

enumerator MEMCFG_TEST_WRITE_PARITY = 2

Writes allowed to Parity only (for LSxRAM, GSxRAM, and MSGxRAM)

enumerator MEMCFG_TEST_FUNC_DIAG = 3

Diagnostic mode, similar to functional mode but NMI is not generated.

Functions

void MemCfg_setCLAMemType(uint32_t ramSections, MemCfg_CLAMemoryType claMemType)

Sets the CLA memory type of the specified RAM section.

This function sets the CLA memory type configuration of the RAM section. If the

claMemType parameter is MEMCFG_CLA_MEM_DATA, the RAM section will be configured as CLA data memory. If MEMCFG_CLA_MEM_PROGRAM, the RAM section will be configured as CLA program memory.
Parameters
  • ramSections: is the logical OR of the sections to be configured.

  • claMemType: indicates data memory or program memory.

The ramSections parameter is an OR of the following indicators: MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx.

Note

This API only applies to LSx RAM and has no effect if the CLA isn’t controller of the memory section.

See

MemCfg_setLSRAControllerSel()

Return

None.

void MemCfg_enableViolationInterrupt(uint32_t intFlags)

Enables individual RAM access violation interrupt sources.

Return

None.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be enabled. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access

    • MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access

    • MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Controller CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Controller DMA write access This function enables the indicated RAM access violation interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

void MemCfg_disableViolationInterrupt(uint32_t intFlags)

Disables individual RAM access violation interrupt sources.

This function disables the indicated RAM access violation interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be disabled. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access

    • MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access

    • MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Controller CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Controller DMA write access

Note

Note that only non-controller violations may generate interrupts.

Return

None.

uint32_t MemCfg_getViolationInterruptStatus(void)

Gets the current RAM access violation status.

This function returns the RAM access violation status. This function will return flags for both controller and non-controller access violations although only the non-controller flags have the ability to cause the generation of an interrupt.

Return

Returns the current violation status, enumerated as a bit field of the values:

  • MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access

  • MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access

  • MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access

  • MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access

  • MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access

  • MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access

  • MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access

  • MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access

  • MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access

  • MEMCFG_MVIOL_CPUWRITE - Controller CPU write access

  • MEMCFG_MVIOL_DMAWRITE - Controller DMA write access

void MemCfg_forceViolationInterrupt(uint32_t intFlags)

Sets the RAM access violation status.

This function sets the RAM access violation status. This function will set flags for both controller and non-controller access violations, and an interrupt will be generated if it is enabled.

Parameters
  • intFlags: is a bit mask of the access violation flags to be set. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access

    • MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access

    • MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Controller CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Controller DMA write access

Return

None.

void MemCfg_clearViolationInterruptStatus(uint32_t intFlags)

Clears RAM access violation flags.

Return

None.

Parameters
  • intFlags: is a bit mask of the access violation flags to be cleared. Can be a logical OR any of the following values:

    • MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access

    • MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access

    • MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Controller CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Controller DMA write access

void MemCfg_setCorrErrorThreshold(uint32_t threshold)

Sets the correctable error threshold value.

This value sets the error-count threshold at which a correctable error interrupt is generated. That is when the error count register reaches the value specified by the

threshold parameter, an interrupt is generated if it is enabled.
Parameters
  • threshold: is the correctable error threshold.

Return

None.

uint32_t MemCfg_getCorrErrorCount(void)

Gets the correctable error count.

Return

Returns the number of correctable error have occurred.

void MemCfg_enableCorrErrorInterrupt(uint32_t intFlags)

Enables individual RAM correctable error interrupt sources.

This function enables the indicated RAM correctable error interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be enabled. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

void MemCfg_disableCorrErrorInterrupt(uint32_t intFlags)

Disables individual RAM correctable error interrupt sources.

This function disables the indicated RAM correctable error interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be disabled. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

uint32_t MemCfg_getCorrErrorInterruptStatus(void)

Gets the current RAM correctable error interrupt status.

Return

Returns the current error interrupt status. Will return a value of MEMCFG_CERR_CPUREAD if an interrupt has been generated. If not, the function will return 0.

void MemCfg_forceCorrErrorInterrupt(uint32_t intFlags)

Sets the RAM correctable error interrupt status.

This function sets the correctable error interrupt flag.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be set. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

void MemCfg_clearCorrErrorInterruptStatus(uint32_t intFlags)

Clears the RAM correctable error interrupt status.

This function clears the correctable error interrupt flag.

Parameters
  • intFlags: is a bit mask of the interrupt sources to be cleared. Can take the value MEMCFG_CERR_CPUREAD only. Other values are reserved.

Note

Note that only correctable errors may generate interrupts.

Return

None.

uint32_t MemCfg_getCorrErrorStatus(void)

Gets the current correctable RAM error status.

Return

Returns the current error status, enumerated as a bit field of MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ

uint32_t MemCfg_getUncorrErrorStatus(void)

Gets the current uncorrectable RAM error status.

Return

Returns the current error status, enumerated as a bit field of MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ, or MEMCFG_UCERR_ECATMEMREAD.

void MemCfg_forceCorrErrorStatus(uint32_t stsFlags)

Sets the specified correctable RAM error status flag.

This function sets the specified correctable RAM error status flag.

Parameters
  • stsFlags: is a bit mask of the error sources. This parameter can be any of the following values: MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ

Return

None.

void MemCfg_forceUncorrErrorStatus(uint32_t stsFlags)

Sets the specified uncorrectable RAM error status flag.

This function sets the specified uncorrectable RAM error status flag.

Parameters
  • stsFlags: is a bit mask of the error sources. This parameter can be any of the following values: MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ, or MEMCFG_UCERR_ECATMEMREAD.

Return

None.

void MemCfg_clearCorrErrorStatus(uint32_t stsFlags)

Clears correctable RAM error flags.

This function clears the specified correctable RAM error flags.

Parameters
  • stsFlags: is a bit mask of the status flags to be cleared. This parameter can be any of the following : MEMCFG_CERR_CPUREAD, MEMCFG_CERR_DMAREAD, or MEMCFG_CERR_CLA1READ

Return

None.

void MemCfg_clearUncorrErrorStatus(uint32_t stsFlags)

Clears uncorrectable RAM error flags.

This function clears the specified uncorrectable RAM error flags.

Parameters
  • stsFlags: is a bit mask of the status flags to be cleared. This parameter can be any of the following : MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ, or MEMCFG_UCERR_ECATMEMREAD.

Return

None.

uint32_t MemCfg_getDiagErrorStatus(void)

Gets the diagnostics corr/uncorr memory error status in test mode.

Return

Returns the diagnostics error status in test mode. It can return following values: MEMCFG_DIAGERR_UNCORR, and/or MEMCFG_DIAGERR_CORR.

void MemCfg_clearDiagErrorStatus(uint32_t stsFlags)

Clears the diagnostics corr/uncorr memory error status.

This function clears the specified diagnostics corr/uncorr RAM/ROM memory error flags in test mode. The param

stsFlags can be any of the following values: MEMCFG_DIAGERR_UNCORR, and/or MEMCFG_DIAGERR_CORR.
Parameters
  • stsFlags: is a bit mask of the status flags to be cleared.

Return

None.

uint32_t MemCfg_getDiagErrorAddress(void)

Gets address location of diagnostics corr/uncorr memory read/write error.

Return

Return address location of diagnostics corr/uncorr memory error error in test mode.

void MemCfg_enableROMWaitState(void)

Enables ROM wait state.

This function enables the ROM wait state. This mean CPU accesses to ROM are 1-wait.

Return

None.

void MemCfg_disableROMWaitState(void)

Disables ROM wait state.

This function enables the ROM wait state. This mean CPU accesses to ROM are 0-wait.

Return

None.

void MemCfg_lockConfig(uint32_t memSections)

Locks the writes to the configuration of specified memory sections.

This function locks writes to the access protection and controller select configuration of a memory section.That means calling

MemCfg_setProtection() or MemCfg_setLSRAMControllerSel() for a locked memory section will have no effect until MemCfg_unlockConfig() is called.
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0 and MEMCFG_SECT_M1 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_D0 through MEMCFG_SECT_D5 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL

  • MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU1, or use MEMCFG_SECT_MSGX_ALL to configure all possible message RAM sections.

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_unlockConfig(uint32_t memSections)

Unlocks the writes to the configuration of a memory section.

This function unlocks writes to the access protection and controller select configuration of a memory section that has been locked using

MemCfg_lockConfig().
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0 and MEMCFG_SECT_M1 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_D0 through MEMCFG_SECT_D5 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL

  • MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU1, or use MEMCFG_SECT_MSGX_ALL to configure all possible message RAM sections.

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_commitConfig(uint32_t memSections)

Permanently locks writes to the configuration of a memory section.

This function permanently locks writes to the access protection and controller select configuration of a memory section. That means calling

MemCfg_setProtection() or MemCfg_setLSRAMControllerSel() for a locked memory section will have no effect. To lock the configuration in a nonpermanent way, use MemCfg_lockConfig().
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0 and MEMCFG_SECT_M1 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_D0 through MEMCFG_SECT_D5 or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or MEMCFG_SECT_GSX_ALL

  • MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU1, or use MEMCFG_SECT_MSGX_ALL to configure all possible message RAM sections.

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_setProtection(uint32_t memSection, uint32_t protectMode)

Sets the access protection mode of a single memory section.

This function sets the access protection mode of a specified memory section. The mode is passed into the

protectMode parameter as the logical OR of the following values:
  • MEMCFG_PROT_ALLOWCPUFETCH or MEMCFG_PROT_BLOCKCPUFETCH - CPU fetch

  • MEMCFG_PROT_ALLOWCPUWRITE or MEMCFG_PROT_BLOCKCPUWRITE - CPU write

  • MEMCFG_PROT_ALLOWDMAWRITE or MEMCFG_PROT_BLOCKDMAWRITE - DMA write

Parameters
  • memSection: is the memory section to be configured.

  • protectMode: is the logical OR of the settings to be applied.

The memSection parameter is one of the following indicators:

  • MEMCFG_SECT_M0 or MEMCFG_SECT_M1

  • MEMCFG_SECT_D0 through MEMCFG_SECT_Dx

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx

  • MEMCFG_SECT_MSGCPUTOCPU0 or MEMCFG_SECT_MSGCPUTOCPU1

This function will have no effect if the associated registers have been locked by MemCfg_lockConfig() or MemCfg_commitConfig() or if the memory is configured as CLA program memory.

Return

None.

void MemCfg_setLSRAMControllerSel(uint32_t ramSection, MemCfg_LSRAMControllerSel controllerSel)

Sets the controller of the specified LSxRAM section.

This function sets the controller select configuration of the LSxRAM section. If the

controllerSel parameter is MEMCFG_LSRAMCONTROLLER_CPU_ONLY, the LSxRAM section passed into the ramSection parameter will be dedicated to the CPU. If MEMCFG_LSRAMCONTROLLER_CPU_CLA1, the memory section will be shared between the CPU and the CLA.
Parameters
  • ramSection: is the LSxRAM section to be configured.

  • controllerSel: is the sharing selection.

The ramSection parameter should be a value from MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx.

This function will have no effect if the associated registers have been locked by MemCfg_lockConfig() or MemCfg_commitConfig().

Note

This API only applies to LSxRAM.

Return

None.

void MemCfg_setGSRAMControllerSel(uint32_t ramSections, MemCfg_GSRAMControllerSel controllerSel)

Sets the controller of the specified GSxRAM section.

This function sets the controller select configuration of the GSxRAM section.If the

controllerSel parameter is MEMCFG_GSRAMCONTROLLER_CPU1, the GSRAM sections passed into the ramSections parameter will be dedicated to CPU1. If MEMCFG_GSRAMCONTROLLER_CPU2, the memory section will be dedicated to CPU2.
Parameters
  • ramSections: is the logical OR of the sections to be configured.

  • controllerSel: is the sharing selection.

The ramSections parameter should be a logical OR of values from MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx.

This function will have no effect if the associated registers have been locked by MemCfg_lockConfig() or MemCfg_commitConfig().

Note

This API only applies to GSxRAM.

Return

None.

void MemCfg_lockTestConfig(uint32_t memSections)

Locks the writes to the test mode configuration of specified memory sections.

This function locks writes to the test mode configuration of a RAM section. That means calling

MemCfg_setTestMode() for a locked RAM section will have no effect until MemCfg_unlockTestConfig() is called.
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1, MEMCFG_SECT_D0, MEMCFG_SECT_D1 or use MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or use MEMCFG_SECT_LSX_ALL to configure all possible LSRAM sections.

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or use MEMCFG_SECT_GSX_ALL to configure all possible GSRAM sections.

  • MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCPU1, , or use MEMCFG_SECT_MSGX_ALL

  • MEMCFG_SECT_ROMBOOT, MEMCFG_SECT_ROMSECURE, MEMCFG_SECT_ROMCLADATA or MEMCFG_SECT_ROM_ALL to configure all possible ROM sections.

  • MEMCFG_SECT_PERIMEM_ETHERCAT or MEMCFG_SECT_PERIMEM_ALL to configure all possible peal memories.ripher

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_unlockTestConfig(uint32_t memSections)

Unlocks the writes to the test mode configuration of specified memory sections.

This function unlocks writes to the test mode configuration of a RAM section that has been locked using

MemCfg_lockTestConfig().
Parameters
  • memSections: is the logical OR of the sections to be configured.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1, MEMCFG_SECT_D0, MEMCFG_SECT_D1 or use MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx or use MEMCFG_SECT_LSX_ALL to configure all possible LSRAM sections.

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx or use MEMCFG_SECT_GSX_ALL to configure all possible GSRAM sections.

  • MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCPU1, , or use MEMCFG_SECT_MSGX_ALL

  • MEMCFG_SECT_ROMBOOT, MEMCFG_SECT_ROMSECURE, MEMCFG_SECT_ROMCLADATA or MEMCFG_SECT_ROM_ALL to configure all possible ROM sections.

  • MEMCFG_SECT_PERIMEM_ETHERCAT or MEMCFG_SECT_PERIMEM_ALL to configure all possible peripheral memories.

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

void MemCfg_setTestMode(uint32_t memSection, MemCfg_TestMode testMode)

Sets the test mode of the specified memory section.

This function sets the test mode configuration of the RAM section. The

testMode parameter can take one of the following values:
  • MEMCFG_TEST_FUNCTIONAL

  • MEMCFG_TEST_WRITE_DATA

  • MEMCFG_TEST_WRITE_ECC

  • MEMCFG_TEST_WRITE_PARITY

  • MEMCFG_TEST_FUNC_DIAG

Parameters
  • memSection: is the memory section to be configured.

  • testMode: is the test mode selected.

The memSection parameter is one of the following indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1

  • MEMCFG_SECT_D0, MEMCFG_SECT_D1

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx

  • MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCPU1,

  • MEMCFG_SECT_ROMBOOT, MEMCFG_SECT_ROMSECURE, MEMCFG_SECT_ROMCLADATA

  • MEMCFG_SECT_PERIMEM_ETHERCAT

Return

None.

void MemCfg_initSections(uint32_t ramSections)

Starts the initialization the specified RAM sections.

This function starts the initialization of the specified RAM sections. Use

MemCfg_getInitStatus() to check if the initialization is done.
Parameters
  • ramSections: is the logical OR of the sections to be initialized.

The ramSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1, MEMCFG_SECT_D0, MEMCFG_SECT_D1, or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx, or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx, or MEMCFG_SECT_GSX_ALL

  • MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCPU1, or MEMCFG_SECT_MSGX_ALL

  • OR use MEMCFG_SECT_ALL to configure all possible sections.

Return

None.

bool MemCfg_getInitStatus(uint32_t ramSections)

Get the status of initialized RAM sections.

This function gets the initialization status of the RAM sections specified by the

ramSections parameter.
Parameters
  • ramSections: is the logical OR of the sections to be checked.

The ramSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_M0, MEMCFG_SECT_M1, MEMCFG_SECT_D0, MEMCFG_SECT_D1, or MEMCFG_SECT_DX_ALL

  • MEMCFG_SECT_LS0 through MEMCFG_SECT_LSx, or MEMCFG_SECT_LSX_ALL

  • MEMCFG_SECT_GS0 through MEMCFG_SECT_GSx, or MEMCFG_SECT_GSX_ALL

  • MEMCFG_SECT_MSGCPUTOCLA1, MEMCFG_SECT_MSGCLA1TOCPU, MEMCFG_SECT_MSGCLA1TODMA, MEMCFG_SECT_MSGDMATOCLA1, MEMCFG_SECT_MSGCPUTOCPU0, MEMCFG_SECT_MSGCPUTOCPU1, or MEMCFG_SECT_MSGX_ALL

  • OR use MEMCFG_SECT_ALL to get status of all possible sections.

Note

Use MemCfg_initSections() to start the initialization.

Return

Returns true if all the sections specified by ramSections have been initialized and false if not.

uint32_t MemCfg_getViolationAddress(uint32_t intFlag)

Get the violation address associated with a intFlag.

Return

Returns the violation address associated with the intFlag.

Parameters
  • intFlag: is the type of access violation as indicated by ONE of these values:

    • MEMCFG_NMVIOL_CPUREAD - Non-controller CPU read access

    • MEMCFG_NMVIOL_CPUWRITE - Non-controller CPU write access

    • MEMCFG_NMVIOL_CPUFETCH - Non-controller CPU fetch access

    • MEMCFG_NMVIOL_DMAWRITE - Non-controller DMA write access

    • MEMCFG_NMVIOL_CLA1READ - Non-controller CLA1 read access

    • MEMCFG_NMVIOL_CLA1WRITE - Non-controller CLA1 write access

    • MEMCFG_NMVIOL_CLA1FETCH - Non-controller CLA1 fetch access

    • MEMCFG_NMVIOL_DMAREAD - Non-controller DMA read access

    • MEMCFG_MVIOL_CPUFETCH - Controller CPU fetch access

    • MEMCFG_MVIOL_CPUWRITE - Controller CPU write access

    • MEMCFG_MVIOL_DMAWRITE - Controller DMA write access

uint32_t MemCfg_getCorrErrorAddress(uint32_t stsFlag)

Get the correctable error address associated with a stsFlag.

Return

Returns the error address associated with the stsFlag.

Parameters
  • stsFlag: is the type of error to which the returned address will correspond. It can take following values: MEMCFG_CERR_CPUREAD, MEMCFG_CERR_CLA1READ, MEMCFG_CERR_DMAREAD.

uint32_t MemCfg_getUncorrErrorAddress(uint32_t stsFlag)

Get the uncorrectable error address associated with a stsFlag.

Return

Returns the error address associated with the stsFlag.

Parameters
  • stsFlag: is the type of error to which the returned address will correspond. It may be passed one of these values: MEMCFG_UCERR_CPUREAD, MEMCFG_UCERR_DMAREAD, MEMCFG_UCERR_CLA1READ, or MEMCFG_UCERR_ECATMEMREAD values.

void MemCfg_forceMemError(uint32_t memSections)

Forces parity error in the selected memory.

This function forces the parity error in the memories specified by the

memSections parameter.
Parameters
  • memSections: is the logical OR of the sections to be tested.

The memSections parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_ROMBOOT, MEMCFG_SECT_ROMSECURE , MEMCFG_SECT_ROMCLADATA, MEMCFG_SECT_ROM_ALL.

  • MEMCFG_SECT_PERIMEM_ETHERCAT, or MEMCFG_SECT_PERIMEM_ALL

  • OR use MEMCFG_SECT_ALL to force parity error in all possible memory sections.

Return

None.

void MemCfg_enablePeriMemTestMode(uint32_t memSections)

Enables test mode for selected peripheral memories.

This function enables test mode for selected peripheral memories specified by the

memTypes parameter.
Parameters
  • memSections: is the logical OR of the type of peripheral memories to be tested.

The memTypes parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_PERIMEM_ETHERCAT, or MEMCFG_SECT_PERIMEM_ALL

Return

None.

void MemCfg_disablePeriMemTestMode(uint32_t memSections)

Disables the test mode for selected peripheral memories.

This function disables test mode for selected peripheral memories specified by the

memSections parameter.
Parameters
  • memSections: is the logical OR of the type of peripheral memories to be tested.

The memTypes parameter is an OR of one of the following sets of indicators:

  • MEMCFG_SECT_PERIMEM_ETHERCAT, or MEMCFG_SECT_PERIMEM_ALL

Return

None.

Many of the functions provided by this API to configure RAM sections’ settings will take a RAM section identifier or an OR of several identifiers as a parameter. These are #defines with names in the format MEMCFG_SECT_X. Take care to read the function description to learn which functions can operate on multiple sections of the same type at a time and which ones can only configure one section at a time. A quick way to check this is to see if the parameter says e ramSection or the plural e ramSections. Some functions may also be able to take a MEMCFG_SECT_ALL value to indicate that all RAM sections should be operated on at the same time. Again, read the function’s detailed description to be sure.

The code for this module is contained in driverlib/memcfg.c, with driverlib/memcfg.h containing the API declarations for use by applications.