This Folder contains the following files:

1. Lighting_DCDC.exe this is the executable GUI to be used with the DCDC LED Lighting Kit.
2. Lighting_DCDC-FlashImage.out is the flash image of the code pre flashed into the control card shipped with the kit.
4. Lighting_DDCDC-F2803x-SCI.a00 is image of the program flashed onto the controlCARD that can be loaded in using the SCI boot loader.
3. QSG-Lighting_DCDC.pdf is the guide that explains the kit's contents and how the GUI can be used.

The XDS100 drivers referenced in the quickstart guide can also be found in C:\TI\controlSUITE\libs\utilities