V3.1 of the SDFlash serial algos supports the following devices, and uses the listed Flash API algorithms:

 TMS320F2801    with Flash API V3.02
 TMS320F2801-60 with Flash API V3.02
 TMS320F2802    with Flash API V3.02
 TMS320F2802-60 with Flash API V3.02
 TMS320F2806    with Flash API V3.02
 TMS320F2808    with Flash API V3.02
 TMS320F2809    with Flash API V3.02
 TMS320F2810    with Flash API V2.10  
 TMS320F2811    with Flash API V2.10  
 TMS320F2812    with Flash API V2.10
 TMS320F28015   with Flash API V1.00
 TMS320F28016   with Flash API V1.00
 TMS320F28044   with Flash API V1.00

By default, the SDFlash algos will be installed in
the sdf28xx_v3_1_serial directory under:
c:\CCStudio_v3.3\specdig\sdflash\myprojects\

Please refer to the SDFlash_Serial_RefGuide_v3_1.pdf 
in the myprojects\sdf28xx_v3_1 directory