V3.3 of the SDFlash serial algos supports the following devices, and uses the listed Flash API algorithms:

 TMS320F2801	with Flash API V3.02
 TMS320F2801-60	with Flash API V3.02
 TMS320F2802	with Flash API V3.02
 TMS320F2802-60	with Flash API V3.02
 TMS320F2806	with Flash API V3.02
 TMS320F2808	with Flash API V3.02
 TMS320F2809	with Flash API V3.02
 TMS320F2810	with Flash API V2.10  
 TMS320F2811	with Flash API V2.10  
 TMS320F2812	with Flash API V2.10
 TMS320F28015	with Flash API V1.00
 TMS320F28016	with Flash API V1.00
 TMS320F28044	with Flash API V1.00
 TMS320F28335	with Flash API V2.10
 TMS320F28334	with Flash API V2.10
 TMS320F28332	with Flash API V2.10
 TMS320F28235	with Flash API V2.10 
 TMS320F28234	with Flash API V2.10
 TMS320F28232	with Flash API V2.10

By default, the SDFlash algos will be installed in
the sdf28xx_v3_3_serial directory under:
c:\CCStudio_v3.3\specdig\sdflash\myprojects\

Please refer to the SDFlash_Serial_RefGuide_v3_3.pdf 
in the myprojects\sdf28xx_v3_3 directory