=== Build (Elapsed: 1:02 min) ===
    ### Starting build procedure for: PID_CLA_built
    ### Generating code and artifacts to 'Model specific' folder structure
    ### Generating code into build folder: D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw
    The model PID_CLA_built is configured to simulate flush-to-zero (FTZ) behavior, but is using normal mode simulation. To observe FTZ behavior, simulate the model using an accelerated mode.
    Warning:Parameter precision loss occurred for 'Value' of 'PID_CLA_built/CLA_model/PID Controller1/UI_REG3/Constant1'. The parameter's value cannot be represented exactly using the run-time data type. A small quantization error has occurred. To disable this warning or error, in the Configuration Parameters > Diagnostics > Data Validity pane, set the 'Detect precision loss' option in the Parameters group to 'none'.
    Warning:Parameter precision loss occurred for 'Value' of 'PID_CLA_built/CLA_model/PID Controller1/prop_gain'. The parameter's value cannot be represented exactly using the run-time data type. A small quantization error has occurred. To disable this warning or error, in the Configuration Parameters > Diagnostics > Data Validity pane, set the 'Detect precision loss' option in the Parameters group to 'none'.
    Warning:Parameter precision loss occurred for 'Value' of 'PID_CLA_built/CLA_model/PID Controller1/UI_REG3/Constant'. The parameter's value cannot be represented exactly using the run-time data type. A small quantization error has occurred. To disable this warning or error, in the Configuration Parameters > Diagnostics > Data Validity pane, set the 'Detect precision loss' option in the Parameters group to 'none'.
    ### Invoking Target Language Compiler on PID_CLA_built.rtw
    ### Using System Target File: D:\Matlab2020a\rtw\c\ert\ert.tlc
    ### Loading TLC function libraries
    ### Generating TLC interface API for custom data
    ### Initial pass through model to cache user defined code
    .
    ### Caching model source code
        ### Writing header file PID_CLA_built_types.h
        ### Writing header file PID_CLA_built.h
        ### Writing source file PID_CLA_built.c
        ### Writing header file rtwtypes.h
        ### Writing header file rt_nonfinite.h
    .
        ### Writing source file rt_nonfinite.c
        ### Writing header file rtGetInf.h
        ### Writing source file rtGetInf.c
        ### Writing header file rtGetNaN.h
        ### Writing source file rtGetNaN.c
        ### Writing header file PID_CLA_built_private.h
    .
        ### Writing header file cla_header.h
        ### Writing source file PID_CLA_built_data.c
        ### Writing header file rtmodel.h
        ### Writing source file ert_main.c
    ### TLC code generation complete.
    ### Evaluating PostCodeGenCommand specified in the model
    ### Creating CCS Project at : D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw\CCS_Project
    ### CCS project created successfully Open project in Code Composer Studio.
    ### Using toolchain: Texas Instruments Code Composer Studio (C2000)
    ### Creating 'D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw\PID_CLA_built.mk' ...
    ### Building 'PID_CLA_built': "D:\Matlab2020a\bin\win64\gmake"  -B -f PID_CLA_built.mk all
    ### Build procedure for PID_CLA_built aborted due to an error.
    Error:
    D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw>cd . 
    
    D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw>if "" == "" ("D:\Matlab2020a\bin\win64\gmake"  -B -f PID_CLA_built.mk all )  else ("D:\Matlab2020a\bin\win64\gmake"  -B -f PID_CLA_built.mk  ) 
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="MW_c28xx_board.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/MW_c28xx_board.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="MW_c28xx_adc.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/MW_c28xx_adc.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="MW_c28xx_csl.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/MW_c28xx_csl.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="PID_CLA_built.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/PID_CLA_built.c"
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/PID_CLA_built.c", line 224: warning: conversion from pointer to smaller integer
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="PID_CLA_built_data.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/PID_CLA_built_data.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="rtGetInf.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/rtGetInf.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="rtGetNaN.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/rtGetNaN.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="rt_nonfinite.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/rt_nonfinite.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="c2837xDBoard_Realtime_Support.obj" "C:/ProgramData/MATLAB/SupportPackages/R2020a/toolbox/target/supportpackages/tic2000/src/c2837xDBoard_Realtime_Support.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_CpuTimers.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_CpuTimers.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_DefaultISR.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_DefaultISR.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_GlobalVariableDefs.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_headers/source/F2837xD_GlobalVariableDefs.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_PieCtrl.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_PieCtrl.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_PieVect.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_PieVect.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_SysCtrl.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_SysCtrl.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" -s -v28 -ml --float_support=fpu32 --output_file="F2837xD_usDelay.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_usDelay.asm"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" -s -v28 -ml --float_support=fpu32 --output_file="F2837xD_CodeStartBranch.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_CodeStartBranch.asm"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_Dma.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_Dma.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_Adc.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_Adc.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_Gpio.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_Gpio.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_Ipc_Driver_Lite.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_Ipc_Driver_Lite.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="F2837xD_Emif.obj" "C:/ti/controlSUITE/device_support/F2837xD/v190/F2837xD_common/source/F2837xD_Emif.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="profiler_Support.obj" "C:/ProgramData/MATLAB/SupportPackages/R2020a/toolbox/target/supportpackages/tic2000/src/profiler_Support.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="MW_c28xGPIO.obj" "C:/ProgramData/MATLAB/SupportPackages/R2020a/toolbox/target/supportpackages/tic2000/src/MW_c28xGPIO.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="c2837xDSchedulerTimer0.obj" "C:/ProgramData/MATLAB/SupportPackages/R2020a/toolbox/target/supportpackages/tic2000/src/c2837xDSchedulerTimer0.c"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/bin/cl2000" --compile_only --large_memory_model --silicon_version=28 --define="LARGE_MODEL" -i"/~SupportFiles/DSP280x_headers" -i"/~SupportFiles/DSP280x_headers/include" -i"C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include" -DCLA_BLOCK_INCLUDED --cla_support=cla1 -v28 --float_support=fpu32 -ml -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 --tmu_support=tmu0 --fp_mode=relaxed -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTID01EQ=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -D__MW_TARGET_USE_HARDWARE_RESOURCES_H__ -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DCLASSIC_INTERFACE=0 -DALLOCATIONFCN=0 -DTERMFCN=1 -DONESTEPFCN=1 -DMAT_FILE=0 -DMULTI_INSTANCE_CODE=0 -DINTEGER_CODE=0 -DMT=1  -DTID01EQ=0 -DDAEMON_MODE=1 -DXCP_CUSTOM_PLATFORM -DMW_PIL_SCIFIFOLEN=16 -DF2837X_REG_FORMAT -DMW_F2837XD -DSTACK_SIZE=1024 -DRT -DF28379D -DCPU1 -DBOOT_FROM_FLASH=1 -DMODEL=PID_CLA_built -DNUMST=3 -DNCSTATES=0 -DHAVESTDIO -DMODEL_HAS_DYNAMICALLY_LOADED_SFCNS=0 -ID:/maaatlab/New_folder_1 -ID:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw -ID:/Matlab2020a/extern/include -ID:/Matlab2020a/simulink/include -ID:/Matlab2020a/rtw/c/src -ID:/Matlab2020a/rtw/c/src/ext_mode/common -ID:/Matlab2020a/rtw/c/ert -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/inc -ID:/Matlab2020a/toolbox/shared/can/src/scanutil -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/SUPPOR~1/tic2000/src -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~4/include -IC:/ti/CONTRO~1/DEVICE~1/F2837xD/v190/F2837X~1 -ID:/Matlab2020a/toolbox/rtw/targets/common/can/blocks/tlc_c -IC:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/toolbox/target/shared/EXTERN~1/include -IC:/ti/CONTRO~1/libs/math/CLAmath/V4_00_~1/include --output_file="cla_task.obj" "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla"
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include/stdbool.h", line 36: warning: incompatible redefinition of macro "false" (declared at line 22 of "D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw\rtwtypes.h")
    "C:/PROGRA~3/MATLAB/SUPPOR~1/R2020a/3P778C~1.INS/TIC200~1.INS/TI-CGT~1.LTS/include/stdbool.h", line 37: warning: incompatible redefinition of macro "true" (declared at line 26 of "D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw\rtwtypes.h")
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla", line 26: error: identifier "PID_CLA_built_DW" is undefined
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla", line 31: warning: function "floor" declared implicitly
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla", line 32: warning: function "rtIsNaN" declared implicitly
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla", line 32: warning: function "rtIsInf" declared implicitly
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla", line 35: warning: function "fmod" declared implicitly
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla", line 42: warning: function "__IQmpy" declared implicitly
    "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla", line 42: error: identifier "PID_CLA_built_ConstB" is undefined
    2 errors detected in the compilation of "D:/maaatlab/New_folder_1/PID_CLA_built_ert_rtw/cla_task.cla".
    
    >> Compilation failure
    gmake: *** [cla_task.obj] Error 1
    
    D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw>echo The make command returned an error of 2 
    The make command returned an error of 2
    
    D:\maaatlab\New_folder_1\PID_CLA_built_ert_rtw>exit 1 
    
    Error(s) encountered while building "PID_CLA_built":
    ### Failed to generate all binary outputs.