Code Interface Report for TwoPhaseForStuck

Table of Contents

Entry-Point Functions

Function: TwoPhaseForStuck_initialize

Prototype void TwoPhaseForStuck_initialize(void)
Description Initialization entry point of generated code
Timing Must be called exactly once
Arguments None
Return value None
Header file TwoPhaseForStuck.h

Function: TwoPhaseForStuck_step

Prototype void TwoPhaseForStuck_step(void)
Description Output entry point of generated code
Timing Must be called periodically, every 1.25e-06 seconds
Arguments None
Return value None
Header file TwoPhaseForStuck.h

Function: TwoPhaseForStuck_terminate

Prototype void TwoPhaseForStuck_terminate(void)
Description Termination entry point of generated code
Timing Must be called exactly once
Arguments None
Return value None
Header file TwoPhaseForStuck.h

Inports

No Inports in model.

Outports

No Outports in model.

Interface Parameters

[-]
Parameter Source Code Identifier Data Type Dimension
<Root>/DuryCycle TwoPhaseForStuck_P.DuryCycle_Value real_T 1
<Root>/TMPRRD TwoPhaseForStuck_P.TMPRRD_Gain real_T 1
<Root>/Phase_2 TwoPhaseForStuck_P.Phase_2_Value real_T 1

Data Stores

No data stores in the model; note that this report lists only data stores with non-auto storage class and global data stores