Code Interface Report for m3_core

Table of Contents

Entry Point Functions

Function: m3_core_initialize

Prototype void m3_core_initialize(void)
Description Initialization entry point of generated code
Timing Must be called exactly once
Arguments None
Return value None
Header file m3_core.h

Function: m3_core_step0

Prototype void m3_core_step0(void)
Description Output entry point of generated code
Timing Must be called periodically, every 0.05 seconds
Arguments None
Return value None
Header file m3_core.h

Function: m3_core_step1

Prototype void m3_core_step1(void)
Description Output entry point of generated code
Timing Must be called periodically, every 0.1 seconds
Arguments None
Return value None
Header file m3_core.h

Function: m3_core_step2

Prototype void m3_core_step2(void)
Description Output entry point of generated code
Timing Must be called periodically, every 0.25 seconds
Arguments None
Return value None
Header file m3_core.h

Function: m3_core_terminate

Prototype void m3_core_terminate(void)
Description Termination entry point of generated code
Timing Must be called exactly once
Arguments None
Return value None
Header file m3_core.h

Inports

No Inports in model.

Outports

No Outports in model.

Interface Parameters

[-]
Parameter Source Code Identifier Data Type Dimension
<S1>/Pulse Generator m3_core_P.PulseGenerator_Amp real_T 1
<S1>/Pulse Generator m3_core_P.PulseGenerator_Period real_T 1
<S1>/Pulse Generator m3_core_P.PulseGenerator_Duty real_T 1
<S1>/Pulse Generator m3_core_P.PulseGenerator_PhaseDelay real_T 1
<Root>/Constant m3_core_P.Constant_Value uint16_T [1 8]

Data Stores

No data stores in the model; note that this report lists only data stores with non-auto storage class and global data stores