| Build Log |
|
| Command Lines |
Creating temporary file "c:\Simma\USB_Bulk_Stress_Test\Release\RSP00000328523940.rsp" with contents [ /GL /I "../lmusbdll" /D "_UNICODE" /D "UNICODE" /FD /EHsc /MD /Fo"Release\\" /Fd"Release\vc90.pdb" /W3 /c /Wp64 /Zi /TC .\usb_bulk_example.c ] Creating command line "cl.exe @c:\Simma\USB_Bulk_Stress_Test\Release\RSP00000328523940.rsp /nologo /errorReport:prompt" |
| Output Window |
Compiling... cl : Command line warning D9035 : option 'Wp64' has been deprecated and will be removed in a future release usb_bulk_example.c .\usb_bulk_example.c(58) : fatal error C1083: Cannot open include file: 'lmusbdll.h': No such file or directory |
| Results |
Build log was saved at "file://c:\Simma\USB_Bulk_Stress_Test\Release\BuildLog.htm" usb_bulk_example - 1 error(s), 1 warning(s) |