Migration Report - usb_bulk_example

Overview

ProjectPathErrorsWarningsMessages
usb_bulk_exampleusb_bulk_example.vcproj092
Solutionusb_bulk_example.sln013

Solution and projects

usb_bulk_example

Message
usb_bulk_example.vcproj: VCWebServiceProxyGeneratorTool is no longer supported. The tool has been removed from your project settings.
usb_bulk_example.vcproj: Attribute 'Detect64BitPortabilityProblems' of 'VCCLCompilerTool' is not supported in this version and has been removed during conversion.
usb_bulk_example.vcproj: Attribute 'Detect64BitPortabilityProblems' of 'VCCLCompilerTool' is not supported in this version and has been removed during conversion.
usb_bulk_example.vcproj: All user macros reported below for configuration 'Debug|Win32' are used before their definition, which can cause undesirable build results; this is not supported in this release. You can resolve this by changing the inclusion order of the consuming property sheets and making sure they come after the property sheets defining the user macros.
usb_bulk_example.vcproj: MSB4211: C:\Program Files (x86)\MSBuild\12.0\bin\Microsoft.Common.CurrentVersion.targets (86,5); The property "TargetPlatformIdentifier" is being set to a value for the first time, but it was already consumed at "C:\Program Files (x86)\MSBuild\Microsoft.Cpp\v4.0\V120\Microsoft.Cpp.Common.props (103,5)".
usb_bulk_example.vcproj: MSB4211: C:\Program Files (x86)\MSBuild\12.0\bin\Microsoft.Common.CurrentVersion.targets (87,5); The property "TargetPlatformVersion" is being set to a value for the first time, but it was already consumed at "C:\Program Files (x86)\MSBuild\Microsoft.Cpp\v4.0\V120\Microsoft.Cpp.Common.props (103,5)".
usb_bulk_example.vcproj: All user macros reported below for configuration 'Release|Win32' are used before their definition, which can cause undesirable build results; this is not supported in this release. You can resolve this by changing the inclusion order of the consuming property sheets and making sure they come after the property sheets defining the user macros.
usb_bulk_example.vcproj: MSB4211: C:\Program Files (x86)\MSBuild\12.0\bin\Microsoft.Common.CurrentVersion.targets (86,5); The property "TargetPlatformIdentifier" is being set to a value for the first time, but it was already consumed at "C:\Program Files (x86)\MSBuild\Microsoft.Cpp\v4.0\V120\Microsoft.Cpp.Common.props (103,5)".
usb_bulk_example.vcproj: MSB4211: C:\Program Files (x86)\MSBuild\12.0\bin\Microsoft.Common.CurrentVersion.targets (87,5); The property "TargetPlatformVersion" is being set to a value for the first time, but it was already consumed at "C:\Program Files (x86)\MSBuild\Microsoft.Cpp\v4.0\V120\Microsoft.Cpp.Common.props (103,5)".
Show 2 additional messages
usb_bulk_example.vcproj: Converting project file 'C:\cs30_controlsuite_submodules\cs30_f2837x\F28X7x_common\tools\USB_Bulk_Stress_Test\usb_bulk_example.vcproj'.
usb_bulk_example.vcproj: Done converting to new project file 'C:\cs30_controlsuite_submodules\cs30_f2837x\F28X7x_common\tools\USB_Bulk_Stress_Test\usb_bulk_example.vcxproj'.
Hide 2 additional messages

Solution

Message
usb_bulk_example.sln: Visual Studio needs to make non-functional changes to this project in order to enable the project to open in Visual Studio 2013, Visual Studio 2012, and Visual Studio 2010 SP1 without impacting project behavior.
Show 3 additional messages
usb_bulk_example.sln: File successfully backed up as C:\cs30_controlsuite_submodules\cs30_f2837x\F28X7x_common\tools\USB_Bulk_Stress_Test\Backup\usb_bulk_example.sln
usb_bulk_example.v12.suo: File successfully backed up as C:\cs30_controlsuite_submodules\cs30_f2837x\F28X7x_common\tools\USB_Bulk_Stress_Test\Backup\usb_bulk_example.v12.suo
usb_bulk_example.sln: Solution migrated successfully
Hide 3 additional messages