################################################################################
# Automatically-generated file. Do not edit!
################################################################################

EMPTY := 
SPACE := $(EMPTY) $(EMPTY)

ORDERED_OBJS += \
$(GEN_CMDS_QUOTED) \
"D:/tic2000/myprojects/can/Debug/DSP28_Xintf.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_XIntrupt.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_SysCtrl.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_PieVect.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_PieCtrl.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_Mcbsp.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_Gpio.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_GlobalVariableDefs.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_ECan.obj" \
"D:/tic2000/myprojects/can/Debug/DSP28_DefaultIsr.obj" \
"D:/tic2000/myprojects/can/Debug/CAN_TEST.obj" \
-l"rts2800_ml.lib" \
"E:/workspace/dec2812/03.Example Program/01. DSP/can/SRAM.cmd" \

-include ../makefile.init

RM := DEL /F

# All of the sources participating in the build are defined here
-include sources.mk
-include subdir.mk
-include objects.mk

ifneq ($(MAKECMDGOALS),clean)
ifneq ($(strip $(S62_DEPS)),)
-include $(S62_DEPS)
endif
ifneq ($(strip $(ASM_DEPS)),)
-include $(ASM_DEPS)
endif
ifneq ($(strip $(C55_DEPS)),)
-include $(C55_DEPS)
endif
ifneq ($(strip $(S_UPPER_DEPS)),)
-include $(S_UPPER_DEPS)
endif
ifneq ($(strip $(C++_DEPS)),)
-include $(C++_DEPS)
endif
ifneq ($(strip $(S_DEPS)),)
-include $(S_DEPS)
endif
ifneq ($(strip $(CC_DEPS)),)
-include $(CC_DEPS)
endif
ifneq ($(strip $(C64_DEPS)),)
-include $(C64_DEPS)
endif
ifneq ($(strip $(CPP_DEPS)),)
-include $(CPP_DEPS)
endif
ifneq ($(strip $(S64_DEPS)),)
-include $(S64_DEPS)
endif
ifneq ($(strip $(CXX_DEPS)),)
-include $(CXX_DEPS)
endif
ifneq ($(strip $(C67_DEPS)),)
-include $(C67_DEPS)
endif
ifneq ($(strip $(S67_DEPS)),)
-include $(S67_DEPS)
endif
ifneq ($(strip $(S43_DEPS)),)
-include $(S43_DEPS)
endif
ifneq ($(strip $(C62_DEPS)),)
-include $(C62_DEPS)
endif
ifneq ($(strip $(C43_DEPS)),)
-include $(C43_DEPS)
endif
ifneq ($(strip $(C??_DEPS)),)
-include $(C??_DEPS)
endif
ifneq ($(strip $(ASM_UPPER_DEPS)),)
-include $(ASM_UPPER_DEPS)
endif
ifneq ($(strip $(OPT_DEPS)),)
-include $(OPT_DEPS)
endif
ifneq ($(strip $(S??_DEPS)),)
-include $(S??_DEPS)
endif
ifneq ($(strip $(S55_DEPS)),)
-include $(S55_DEPS)
endif
ifneq ($(strip $(C_DEPS)),)
-include $(C_DEPS)
endif
ifneq ($(strip $(SA_DEPS)),)
-include $(SA_DEPS)
endif
ifneq ($(strip $(C_UPPER_DEPS)),)
-include $(C_UPPER_DEPS)
endif
endif

-include ../makefile.defs

# Add inputs and outputs from these tool invocations to the build variables 

# All Target
all: E:/workspace/dec2812/03.Example\ Program/01.\ DSP/can/Debug/CAN.out

# Tool invocations
E:/workspace/dec2812/03.Example\ Program/01.\ DSP/can/Debug/CAN.out: $(GEN_CMDS) $(CMD_SRCS) $(OBJS)
	@echo 'Building target: $@'
	@echo 'Invoking: Linker'
	$(shell echo --silicon_version=28 > ccsLinker.opt)
	$(shell echo -g >> ccsLinker.opt)
	$(shell echo --define="_DEBUG" --define="LARGE_MODEL" >> ccsLinker.opt)
	$(shell echo --quiet >> ccsLinker.opt)
	$(shell echo --diag_warning=225 >> ccsLinker.opt)
	$(shell echo --large_memory_model >> ccsLinker.opt)
	$(shell echo --obj_directory="D:/tic2000/myprojects/can/Debug" >> ccsLinker.opt)
	$(shell echo -z >> ccsLinker.opt)
	$(shell echo -m"CAN.map" >> ccsLinker.opt)
	$(shell echo --warn_sections >> ccsLinker.opt)
	$(shell echo -i"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c2000/lib" -i"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c2000/include" -i"E:/workspace/dec2812/03.Example Program/01. DSP/can/CAN" -i"E:/workspace/dec2812/03.Example Program/01. DSP/can" >> ccsLinker.opt)
	$(shell echo --reread_libs >> ccsLinker.opt)
	$(shell echo --rom_model >> ccsLinker.opt)
	$(shell type ccsObjs.opt >> ccsLinker.opt)
	"C:/Program Files/Texas Instruments/ccsv4/tools/compiler/c2000/bin/cl2000" -@ccsLinker.opt -o "E:/workspace/dec2812/03.Example Program/01. DSP/can/Debug/CAN.out"
	@echo 'Finished building target: $@'
	@echo ' '

# Other Targets
clean:
	-$(RM) $(C2000_EXECUTABLE_OUTPUTS__QTD) "E:\workspace\dec2812\03.Example Program\01. DSP\can\Debug\CAN.out"
	-$(RM) "D:\tic2000\myprojects\can\Debug\CAN_TEST.obj" "D:\tic2000\myprojects\can\Debug\DSP28_DefaultIsr.obj" "D:\tic2000\myprojects\can\Debug\DSP28_ECan.obj" "D:\tic2000\myprojects\can\Debug\DSP28_GlobalVariableDefs.obj" "D:\tic2000\myprojects\can\Debug\DSP28_Gpio.obj" "D:\tic2000\myprojects\can\Debug\DSP28_Mcbsp.obj" "D:\tic2000\myprojects\can\Debug\DSP28_PieCtrl.obj" "D:\tic2000\myprojects\can\Debug\DSP28_PieVect.obj" "D:\tic2000\myprojects\can\Debug\DSP28_SysCtrl.obj" "D:\tic2000\myprojects\can\Debug\DSP28_XIntrupt.obj" "D:\tic2000\myprojects\can\Debug\DSP28_Xintf.obj" 
	-$(RM) ".\CAN_TEST.pp" ".\DSP28_DefaultIsr.pp" ".\DSP28_ECan.pp" ".\DSP28_GlobalVariableDefs.pp" ".\DSP28_Gpio.pp" ".\DSP28_Mcbsp.pp" ".\DSP28_PieCtrl.pp" ".\DSP28_PieVect.pp" ".\DSP28_SysCtrl.pp" ".\DSP28_XIntrupt.pp" ".\DSP28_Xintf.pp" 
	-@echo ' '

.PHONY: all clean dependents
.SECONDARY:

-include ../makefile.targets