//############################################################################# // // FILE: device.c // // TITLE: Device setup for examples. // //############################################################################# /* * Copyright (c) 2020 Texas Instruments Incorporated - http://www.ti.com * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ //############################################################################# // // Included Files // #include "device.h" #include "board.h" #include "clocktree.h" #include "driverlib.h" #include "inc/hw_ipc.h" #ifdef CMDTOOL #include "device_cmd.h" #endif #ifdef __cplusplus using std::memcpy; #endif //***************************************************************************** // // Function to initialize the device. Primarily initializes system control to a // known state by disabling the watchdog, setting up the SYSCLKOUT frequency, // and enabling the clocks to the peripherals. // //***************************************************************************** void Device_init(void) { // // Disable the watchdog // SysCtl_disableWatchdog(); #ifdef CMDTOOL CMD_init(); #endif #ifdef _FLASH #ifndef CMDTOOL // // Copy time critical code and flash setup code to RAM. This includes the // following functions: InitFlash(); // // The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart symbols // are created by the linker. Refer to the device .cmd file. // memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize); #endif // // Call Flash Initialization to setup flash waitstates. This function must // reside in RAM. // Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, DEVICE_FLASH_WAITSTATES); #endif #ifdef CPU1 // // Configure Analog Trim in case of untrimmed or TMX sample // if((SysCtl_getDeviceParametric(SYSCTL_DEVICE_QUAL) == 0x0U) && (HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_ANAREFTRIMA) == 0x0U)) { Device_configureTMXAnalogTrim(); } // // Set up PLL control and clock dividers // SysCtl_setClock(DEVICE_SETCLOCK_CFG); SysCtl_setLowSpeedClock(DEVICE_LSPCLK_CFG); // // These asserts will check that the #defines for the clock rates in // device.h match the actual rates that have been configured. If they do // not match, check that the calculations of DEVICE_SYSCLK_FREQ and // DEVICE_LSPCLK_FREQ are accurate. Some examples will not perform as // expected if these are not correct. // // // From ClockTree Configurations // SysCtl_selectOscSourceAuxPLL(SYSCTL_OSCSRC_XTAL); CAN_selectClockSource(CANA_BASE, CAN_CLOCK_SOURCE_SYS); CAN_selectClockSource(CANB_BASE, CAN_CLOCK_SOURCE_SYS); SysCtl_setEPWMClockDivider(SYSCTL_EPWMCLK_DIV_2); SysCtl_setEMIF1ClockDivider(SYSCTL_EMIF1CLK_DIV_1); ASSERT(SysCtl_getClock(DEVICE_OSCSRC_FREQ) == DEVICE_SYSCLK_FREQ); ASSERT(SysCtl_getLowSpeedClock(DEVICE_OSCSRC_FREQ) == DEVICE_LSPCLK_FREQ); #ifndef _FLASH // // Call Device_cal function when run using debugger // This function is called as part of the Boot code. The function is called // in the Device_init function since during debug time resets, the boot code // will not be executed and the gel script will reinitialize all the // registers and the calibrated values will be lost. // Sysctl_deviceCal is a wrapper function for Device_Cal // SysCtl_deviceCal(); #endif #endif } //***************************************************************************** // // Function to turn on all peripherals, enabling reads and writes to the // peripherals' registers. // // Note that to reduce power, unused peripherals should be disabled. // //***************************************************************************** void Device_enableAllPeripherals(void) { SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CLA1); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DMA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TIMER0); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TIMER1); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TIMER2); #ifdef CPU1 SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_HRPWM); #endif #ifdef CPU1 SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EMIF1); #endif #ifdef CPU1 SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EMIF2); #endif SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM1); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM2); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM3); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM4); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM5); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM6); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM7); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM8); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM9); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM10); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM11); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EPWM12); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP1); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP2); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP3); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP4); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP5); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ECAP6); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EQEP1); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EQEP2); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_EQEP3); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SD1); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SD2); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIB); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCIC); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SCID); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPIA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPIB); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_SPIC); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_I2CA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_I2CB); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CANA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CANB); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_MCBSPA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_MCBSPB); #ifdef CPU1 SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_USBA); #endif #ifdef CPU1 SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_UPPA); #endif SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCB); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCC); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCD); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS1); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS2); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS3); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS4); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS5); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS6); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS7); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CMPSS8); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DACA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DACB); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_DACC); } //***************************************************************************** // // Function to disable pin locks and enable pullups on GPIOs. // //***************************************************************************** void Device_initGPIO(void) { // // Disable pin locks. // GPIO_unlockPortConfig(GPIO_PORT_A, 0xFFFFFFFF); GPIO_unlockPortConfig(GPIO_PORT_B, 0xFFFFFFFF); GPIO_unlockPortConfig(GPIO_PORT_C, 0xFFFFFFFF); GPIO_unlockPortConfig(GPIO_PORT_D, 0xFFFFFFFF); GPIO_unlockPortConfig(GPIO_PORT_E, 0xFFFFFFFF); GPIO_unlockPortConfig(GPIO_PORT_F, 0xFFFFFFFF); // // Enable GPIO Pullups // Device_enableUnbondedGPIOPullups(); } //***************************************************************************** // // Function to enable pullups for the unbonded GPIOs on the 100PZ package: // GPIOs Grp Bits // 0-1 A 1:0 // 5-9 A 9:5 // 22-40 A 31:22 // B 8:0 // 44-57 B 25:12 // 67-68 C 4:3 // 74-77 C 13:10 // 79-83 C 19:15 // 93-168 C 31:29 // D 31:0 // E 31:0 // F 8:0 // //***************************************************************************** void Device_enableUnbondedGPIOPullupsFor100Pin(void) { EALLOW; HWREG(GPIOCTRL_BASE + GPIO_O_GPAPUD) = ~0xFFC003E3U; HWREG(GPIOCTRL_BASE + GPIO_O_GPBPUD) = ~0x03FFF1FFU; HWREG(GPIOCTRL_BASE + GPIO_O_GPCPUD) = ~0xE10FBC18U; HWREG(GPIOCTRL_BASE + GPIO_O_GPDPUD) = ~0xFFFFFFF7U; HWREG(GPIOCTRL_BASE + GPIO_O_GPEPUD) = ~0xFFFFFFFFU; HWREG(GPIOCTRL_BASE + GPIO_O_GPFPUD) = ~0x000001FFU; EDIS; } //***************************************************************************** // // Function to enable pullups for the unbonded GPIOs on the 176PTP package: // GPIOs Grp Bits // 95-132 C 31 // D 31:0 // E 4:0 // 134-168 E 31:6 // F 8:0 // //***************************************************************************** void Device_enableUnbondedGPIOPullupsFor176Pin(void) { EALLOW; HWREG(GPIOCTRL_BASE + GPIO_O_GPCPUD) = ~0x80000000U; HWREG(GPIOCTRL_BASE + GPIO_O_GPDPUD) = ~0xFFFFFFF7U; HWREG(GPIOCTRL_BASE + GPIO_O_GPEPUD) = ~0xFFFFFFDFU; HWREG(GPIOCTRL_BASE + GPIO_O_GPFPUD) = ~0x000001FFU; EDIS; } //***************************************************************************** // // Function to enable pullups for the unbonded GPIOs on the 100PZ or // 176PTP package. // //***************************************************************************** void Device_enableUnbondedGPIOPullups(void) { // // bits 8-10 have pin count // uint16_t pinCount = ((HWREG(DEVCFG_BASE + SYSCTL_O_PARTIDL) & (uint32_t)SYSCTL_PARTIDL_PIN_COUNT_M) >> SYSCTL_PARTIDL_PIN_COUNT_S); /* * 5 = 100 pin * 6 = 176 pin * 7 = 337 pin */ if(pinCount == 5) { Device_enableUnbondedGPIOPullupsFor100Pin(); } else if(pinCount == 6) { Device_enableUnbondedGPIOPullupsFor176Pin(); } else { // // Do nothing - this is 337 pin package // } } #ifdef CPU1 //***************************************************************************** // // Function to implement Analog trim of TMX devices // //***************************************************************************** void Device_configureTMXAnalogTrim(void) { // // Enable ADC clock // SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCA); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCB); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCC); SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_ADCD); // // Configure ADC reference trim for TMX devices // EALLOW; HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_ANAREFTRIMA) = 0x7BDDU; HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_ANAREFTRIMB) = 0x7BDDU; HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_ANAREFTRIMC) = 0x7BDDU; HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_ANAREFTRIMD) = 0x7BDDU; // // Configure ADC offset trim. The user should generate the trim values // by following the instructions in the "ADC Zero Offset Calibration" // section in device TRM. The below lines needs to be uncommented and // updated with the correct trim values. // // HWREGH(ADCA_BASE + ADC_O_OFFTRIM) = 0x0U; // HWREGH(ADCB_BASE + ADC_O_OFFTRIM) = 0x0U; // HWREGH(ADCC_BASE + ADC_O_OFFTRIM) = 0x0U; // HWREGH(ADCD_BASE + ADC_O_OFFTRIM) = 0x0U; // // Configure internal oscillator trim. If the internal oscillator trim // contains all zeros, the user can adjust the lowest 10 bits of the // oscillator trim register between 1 (minimum) and 1023 (maximum) // while observing the system clock on the XCLOCKOUT pin. The below // lines needs to be uncommented and updated with the correct trim values. // // if(HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_INTOSC1TRIM) == 0x0U) // { // HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_INTOSC1TRIM) = 0x0U; // } // if( HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_INTOSC2TRIM) = 0x0U) // { // HWREGH(ANALOGSUBSYS_BASE + ASYSCTL_O_INTOSC2TRIM) = 0x0U; // } EDIS; // // Disable ADC clock // SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_ADCA); SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_ADCB); SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_ADCC); SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_ADCD); } //***************************************************************************** //! Executes a CPU02 control system bootloader. //! //! \param bootMode specifies which CPU02 control system boot mode to execute. //! //! This function will allow the CPU01 controller system to boot the CPU02 control //! system via the following modes: Boot to RAM, Boot to Flash, Boot via SPI, //! SCI, I2C, or parallel I/O. This function blocks and waits until the //! control system boot ROM is configured and ready to receive CPU01 to CPU02 //! IPC INT0 interrupts. It then blocks and waits until IPC INT0 and //! IPC FLAG31 are available in the CPU02 boot ROM prior to sending the //! command to execute the selected bootloader. //! //! The \e bootMode parameter accepts one of the following values: //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_PARALLEL //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_SCI //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_SPI //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_I2C //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_CAN //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_RAM //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH //! //! \return 0 (success) if command is sent, or 1 (failure) if boot mode is //! invalid and command was not sent. // //***************************************************************************** uint16_t Device_bootCPU2(uint32_t bootMode) { uint32_t bootStatus; uint16_t pin; uint16_t returnStatus = STATUS_PASS; // // If CPU2 has already booted, return a fail to let the application // know that something is out of the ordinary. // bootStatus = HWREG(IPC_BASE + IPC_O_BOOTSTS) & 0x0000000FU; if(bootStatus == C2_BOOTROM_BOOTSTS_C2TOC1_BOOT_CMD_ACK) { // // Check if MSB is set as well // bootStatus = ((uint32_t)(HWREG(IPC_BASE + IPC_O_BOOTSTS) & 0x80000000U)) >> 31U; if(bootStatus != 0) { returnStatus = STATUS_FAIL; return returnStatus; } } // // Wait until CPU02 control system boot ROM is ready to receive // CPU01 to CPU02 INT1 interrupts. // do { bootStatus = HWREG(IPC_BASE + IPC_O_BOOTSTS) & C2_BOOTROM_BOOTSTS_SYSTEM_READY; } while ((bootStatus != C2_BOOTROM_BOOTSTS_SYSTEM_READY)); // // Loop until CPU02 control system IPC flags 1 and 32 are available // while (((HWREG(IPC_BASE + IPC_O_FLG) & IPC_FLG_IPC0) != 0U) || ((HWREG(IPC_BASE + IPC_O_FLG) & IPC_FLG_IPC31) != 0U)) { } if (bootMode >= C1C2_BROM_BOOTMODE_BOOT_COMMAND_MAX_SUPPORT_VALUE) { returnStatus = STATUS_FAIL; } else { // // Based on boot mode, enable pull-ups on peripheral pins and // give GPIO pin control to CPU02 control system. // switch (bootMode) { case C1C2_BROM_BOOTMODE_BOOT_FROM_SCI: // //SCIA connected to CPU02 // SysCtl_selectCPUForPeripheral(SYSCTL_CPUSEL5_SCI, 1, SYSCTL_CPUSEL_CPU2); // //Allows CPU02 bootrom to take control of clock //configuration registers // EALLOW; HWREG(CLKCFG_BASE + SYSCTL_O_CLKSEM) = 0xA5A50000U; HWREG(CLKCFG_BASE + SYSCTL_O_LOSPCP) = 0x0002U; EDIS; GPIO_setDirectionMode(29, GPIO_DIR_MODE_OUT); GPIO_setQualificationMode(29, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_29_SCITXDA); GPIO_setControllerCore(29, GPIO_CORE_CPU2); GPIO_setDirectionMode(28, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(28, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_28_SCIRXDA); GPIO_setControllerCore(28, GPIO_CORE_CPU2); break; case C1C2_BROM_BOOTMODE_BOOT_FROM_SPI: // //SPI-A connected to CPU02 // SysCtl_selectCPUForPeripheral(SYSCTL_CPUSEL6_SPI, 1, SYSCTL_CPUSEL_CPU2); // //Allows CPU02 bootrom to take control of clock configuration // registers // EALLOW; HWREG(CLKCFG_BASE + SYSCTL_O_CLKSEM) = 0xA5A50000U; EDIS; GPIO_setDirectionMode(16, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(16, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_16_SPISIMOA); GPIO_setControllerCore(16, GPIO_CORE_CPU2); GPIO_setDirectionMode(17, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(17, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_17_SPISOMIA); GPIO_setControllerCore(17, GPIO_CORE_CPU2); GPIO_setDirectionMode(18, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(18, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_18_SPICLKA); GPIO_setControllerCore(18, GPIO_CORE_CPU2); GPIO_setDirectionMode(19, GPIO_DIR_MODE_OUT); GPIO_setQualificationMode(19, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_19_GPIO19); GPIO_setControllerCore(19, GPIO_CORE_CPU2); break; case C1C2_BROM_BOOTMODE_BOOT_FROM_I2C: // //I2CA connected to CPU02 // SysCtl_selectCPUForPeripheral(SYSCTL_CPUSEL7_I2C, 1, SYSCTL_CPUSEL_CPU2); // //Allows CPU2 bootrom to take control of clock //configuration registers // EALLOW; HWREG(CLKCFG_BASE + SYSCTL_O_CLKSEM) = 0xA5A50000U; HWREG(CLKCFG_BASE + SYSCTL_O_LOSPCP) = 0x0002U; EDIS; GPIO_setDirectionMode(32, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(32, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_32_SDAA); GPIO_setControllerCore(32, GPIO_CORE_CPU2); GPIO_setDirectionMode(33, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(33, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_33_SCLA); GPIO_setControllerCore(33, GPIO_CORE_CPU2); break; case C1C2_BROM_BOOTMODE_BOOT_FROM_PARALLEL: for(pin=58;pin<=65;pin++) { GPIO_setDirectionMode(pin, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(pin, GPIO_QUAL_ASYNC); GPIO_setControllerCore(pin, GPIO_CORE_CPU2); } GPIO_setDirectionMode(69, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(69, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_69_GPIO69); GPIO_setControllerCore(69, GPIO_CORE_CPU2); GPIO_setDirectionMode(70, GPIO_DIR_MODE_IN); GPIO_setQualificationMode(70, GPIO_QUAL_ASYNC); GPIO_setPinConfig(GPIO_70_GPIO70); GPIO_setControllerCore(70, GPIO_CORE_CPU2); break; case C1C2_BROM_BOOTMODE_BOOT_FROM_CAN: // //Set up the GPIO mux to bring out CANATX on GPIO71 //and CANARX on GPIO70 // GPIO_unlockPortConfig(GPIO_PORT_C, 0xFFFFFFFFU); GPIO_setControllerCore(71, GPIO_CORE_CPU2); GPIO_setPinConfig(GPIO_71_CANTXA); GPIO_setQualificationMode(71, GPIO_QUAL_ASYNC); GPIO_setControllerCore(70, GPIO_CORE_CPU2); GPIO_setPinConfig(GPIO_70_CANRXA); GPIO_setQualificationMode(70, GPIO_QUAL_ASYNC); GPIO_lockPortConfig(GPIO_PORT_C, 0xFFFFFFFFU); // // Set CANA Bit-Clock Source Select = SYSCLK and enable CAN // EALLOW; HWREG(CLKCFG_BASE + SYSCTL_O_CLKSRCCTL2) &= SYSCTL_CLKSRCCTL2_CANABCLKSEL_M; EDIS; SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_CANA); break; } // //CPU01 to CPU02 IPC Boot Mode Register // HWREG(IPC_BASE + IPC_O_BOOTMODE) = bootMode; // // CPU01 To CPU02 IPC Command Register // HWREG(IPC_BASE + IPC_O_SENDCOM) = BROM_IPC_EXECUTE_BOOTMODE_CMD; // // CPU01 to CPU02 IPC flag register // HWREG(IPC_BASE + IPC_O_SET) = 0x80000001U; } return returnStatus; } #endif //***************************************************************************** // // Error handling function to be called when an ASSERT is violated // //***************************************************************************** void __error__(const char *filename, uint32_t line) { // // An ASSERT condition was evaluated as false. You can use the filename and // line parameters to determine what went wrong. // ESTOP0; }