//############################################################################# // // FILE: device.h // // TITLE: Device setup for examples. // //############################################################################# // // Copyright (C) 2014-2022 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# #ifndef __DEVICE_H__ #define __DEVICE_H__ // // Included Files // #include "driverlib.h" #include "clocktree.h" #if (!defined(CPU1) && !defined(CPU2)) #error "You must define CPU1 or CPU2 in your project properties. Otherwise, \ the offsets in your header files will be inaccurate." #endif #if (defined(CPU1) && defined(CPU2)) #error "You have defined both CPU1 and CPU2 in your project properties. Only \ a single CPU should be defined." #endif //***************************************************************************** // // Macro to call SysCtl_delay() to achieve a delay in microseconds. The macro // will convert the desired delay in microseconds to the count value expected // by the function. \b x is the number of microseconds to delay. // //***************************************************************************** #define DEVICE_DELAY_US(x) SysCtl_delay(((((long double)(x)) / (1000000.0L / \ (long double)DEVICE_SYSCLK_FREQ)) - 9.0L) / 5.0L) //***************************************************************************** // // The macros that can be used as parameter to the function Device_bootCPU2 // #define C1C2_BROM_BOOTMODE_BOOT_FROM_PARALLEL 0x00000000U #define C1C2_BROM_BOOTMODE_BOOT_FROM_SCI 0x00000001U #define C1C2_BROM_BOOTMODE_BOOT_FROM_SPI 0x00000004U #define C1C2_BROM_BOOTMODE_BOOT_FROM_I2C 0x00000005U #define C1C2_BROM_BOOTMODE_BOOT_FROM_CAN 0x00000007U #define C1C2_BROM_BOOTMODE_BOOT_FROM_RAM 0x0000000AU #define C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH 0x0000000BU // // Other macros that are needed for the Device_bootCPU2 function // #define BROM_IPC_EXECUTE_BOOTMODE_CMD 0x00000013U #define C1C2_BROM_BOOTMODE_BOOT_COMMAND_MAX_SUPPORT_VALUE 0x0000000CU #define C2_BOOTROM_BOOTSTS_C2TOC1_IGNORE 0x00000000U #define C2_BOOTROM_BOOTSTS_SYSTEM_START_BOOT 0x00000001U #define C2_BOOTROM_BOOTSTS_SYSTEM_READY 0x00000002U #define C2_BOOTROM_BOOTSTS_C2TOC1_BOOT_CMD_ACK 0x00000003U #define C2_BOOTROM_BOOTSTS_C2TOC1_BOOT_CMD_NAK_STATUS_NOT_SUPPORTED 0x00000004U #define C2_BOOTROM_BOOTSTS_C2TOC1_BOOT_CMD_NAK_STATUS_BUSY_WITH_BOOT 0x00000005U // // Macros used as return value by the Device_bootCPU2 Function // #define STATUS_FAIL 0x0001 #define STATUS_PASS 0x0000 //***************************************************************************** // // Defines, Globals, and Header Includes related to Flash Support // //***************************************************************************** #ifdef _FLASH #include #ifndef CMDTOOL extern uint16_t RamfuncsLoadStart; extern uint16_t RamfuncsLoadEnd; extern uint16_t RamfuncsLoadSize; extern uint16_t RamfuncsRunStart; extern uint16_t RamfuncsRunEnd; extern uint16_t RamfuncsRunSize; #endif #define DEVICE_FLASH_WAITSTATES 3 #endif //***************************************************************************** // // Function Prototypes // //***************************************************************************** //***************************************************************************** // //! \addtogroup device_api //! @{ // //***************************************************************************** //***************************************************************************** // //! Function to initialize the device. Primarily initializes system //! control to a known state by disabling the watchdog, setting up the //! SYSCLKOUT frequency, and enabling the clocks to the peripherals. //! //! \param None. //! \return None. // //***************************************************************************** extern void Device_init(void); //***************************************************************************** //! //! //! @brief Function to turn on all peripherals, enabling reads and writes to the //! peripherals' registers. //! //! Note that to reduce power, unused peripherals should be disabled. //! //! @param None //! @return None // //***************************************************************************** extern void Device_enableAllPeripherals(void); //***************************************************************************** //! //! //! @brief Function to disable pin locks on GPIOs. //! //! @param None //! @return None // //***************************************************************************** extern void Device_initGPIO(void); //***************************************************************************** //! //! @brief Function to enable pullups for the unbonded GPIOs on the 176PTP package: //! GPIOs Grp Bits //! 95-132 C 31 //! D 31:0 //! E 4:0 //! 134-168 E 31:6 //! F 8:0 //! //! @param None //! @return None // //***************************************************************************** extern void Device_enableUnbondedGPIOPullupsFor176Pin(void); //***************************************************************************** //! //! @brief Function to enable pullups for the unbonded GPIOs on the 100PZ package: //! GPIOs Grp Bits //! 0-1 A 1:0 //! 5-9 A 9:5 //! 22-40 A 31:22 //! B 8:0 //! 44-57 B 25:12 //! 67-68 C 4:3 //! 74-77 C 13:10 //! 79-83 C 19:15 //! 93-168 C 31:29 //! D 31:0 //! E 31:0 //! F 8:0 //! @param None //! @return None // // //***************************************************************************** extern void Device_enableUnbondedGPIOPullupsFor100Pin(void); //***************************************************************************** //! //! @brief Function to enable pullups for the unbonded GPIOs on the //! 176PTP package. //! //! @param None //! @return None // //***************************************************************************** extern void Device_enableUnbondedGPIOPullups(void); #ifdef CPU1 //***************************************************************************** //! //! @brief Function to implement Analog trim of TMX devices //! //! @param None //! @return None // //***************************************************************************** extern void Device_configureTMXAnalogTrim(void); //***************************************************************************** //! @brief Executes a CPU02 control system bootloader. //! //! \param bootMode specifies which CPU02 control system boot mode to execute. //! //! This function will allow the CPU01 master system to boot the CPU02 control //! system via the following modes: Boot to RAM, Boot to Flash, Boot via SPI, //! SCI, I2C, or parallel I/O. This function blocks and waits until the //! control system boot ROM is configured and ready to receive CPU01 to CPU02 //! IPC INT0 interrupts. It then blocks and waits until IPC INT0 and //! IPC FLAG31 are available in the CPU02 boot ROM prior to sending the //! command to execute the selected bootloader. //! //! The \e bootMode parameter accepts one of the following values: //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_PARALLEL //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_SCI //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_SPI //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_I2C //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_CAN //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_RAM //! - \b C1C2_BROM_BOOTMODE_BOOT_FROM_FLASH //! //! \return 0 (success) if command is sent, or 1 (failure) if boot mode is //! invalid and command was not sent. // //***************************************************************************** extern uint16_t Device_bootCPU2(uint32_t ulBootMode); #endif //***************************************************************************** //! //! @brief Error handling function to be called when an ASSERT is violated //! //! @param *filename File name in which the error has occurred //! @param line Line number within the file //! @return None // //***************************************************************************** extern void __error__(const char *filename, uint32_t line); // // #endif // __DEVICE_H__