C29xx_CPU1: Warning: Target CPU may be stuck in a persistent fault state C29xx_CPU1: Before doing any flash operations using the flash plugin: C29xx_CPU1: (a)Please select which bank mode will be used for CPU operation - Bank Mode 0, Bank Mode 1, Bank Mode 2, Bank Mode 3. C29xx_CPU1: (b)Please select the flash banks that the user would like the flash plugin to erase in the flash plugin GUI.  C29xx_CPU1: When loading data to SECCFG memory region within your .out file, you can select the option to C29xx_CPU1: 'Allow NonMain Flash erase before loading data to Flash memory'. C29xx_CPU1: WARNING - Erasing SECCFG will erase programmable OTP, please proceed with caution (device may get locked). C29xx_CPU1: Enable NonMain sector erase ONLY if necessary.  C29xx_CPU1: When programming the NonMain BANKMGMT Settings to set the Bank Mode, check that the Flash Bank Mode Select C29xx_CPU1: in the User Config Settings matches the set mode before resuming operations.  C29xx_CPU1: After programming the BANKMGMT, the device MUST BE RESET THROUGH XRSn to enable the new configuration.  C29xx_CPU1: Note: When loading Multi-Core Flash Examples, ensure that the device is in the correct Bank Mode prior to programming. C29xx_CPU1: Bank Mode 2 and Bank Mode 3 can be used for Multi-Core Flash programming. C29xx_CPU1: Resetting the target... C29xx_CPU1: Resetting the target completed... C29xx_CPU1: Configured PLL for 200MHz C29xx_CPU1: Error writing the init algorithm. Flash algorithm returned error code. Operation cancelled. C29xx_CPU1: File Loader: Memory write failed: Unknown error C29xx_CPU1: GEL: File: D:\0_Project\odu_rd_1_0\PDCP\output\PDCP.out: Load failed. File: D:\0_Project\odu_rd_1_0\PDCP\output\PDCP.out: Load failed.C29xx_CPU1: Resetting the target... C29xx_CPU1: Resetting the target completed... C29xx_CPU1: Configured PLL for 200MHz C29xx_CPU1: Error occurred during flash operation: Timed out waiting for target to halt while executing wr_pll.alg C29xx_CPU1: Error writing the PLL values (Flash algorithm timed out). Operation cancelled. C29xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click on the RESUME button in CCS debug window) before erasing/loading the Flash.  If that does not help to perform a successful Flash erase/load, check the Reset cause (RESC) register, NMI status flag (NMI_STS) register and the Boot-ROM status register for further debug. C29xx_CPU1: File Loader: Memory write failed: Unknown error C29xx_CPU1: GEL: File: D:\0_Project\odu_rd_1_0\PDCP\output\PDCP.out: Load failed. File: D:\0_Project\odu_rd_1_0\PDCP\output\PDCP.out: Load failed.C29xx_CPU1: Resetting the target... C29xx_CPU1: Resetting the target completed... C29xx_CPU1: Configured PLL for 200MHz C29xx_CPU1: Error writing the init algorithm. Flash algorithm returned error code. Operation cancelled. C29xx_CPU1: File Loader: Memory write failed: Unknown error C29xx_CPU1: GEL: File: D:\0_Project\odu_rd_1_0\PDCP\output\PDCP.out: Load failed. File: D:\0_Project\odu_rd_1_0\PDCP\output\PDCP.out: Load failed.