//----------------------------------------------------------------------------------
//  FILE:           endat.c
//
//  Description:    Contains all the initialization, data declarations and setup
//                  for EnDat encoder interface. This file serves are a template for
//                  using PM_endat22 Library to interface and incorporates all the encoder
//                  and library specific initializations and other important aspects of usage.
//
//  Version:        1.0
//
//  Target:         TMS320F28377D,
//
//----------------------------------------------------------------------------------
//  Copyright Texas Instruments 占� 2004-2015
//----------------------------------------------------------------------------------
//  Revision History:
//----------------------------------------------------------------------------------
//  Date      | Description / Status
//----------------------------------------------------------------------------------
// Nov 2015  - Example project for PM EnDat22 Library Usage
//----------------------------------------------------------------------------------

#include "F28x_Project.h"     // Device Headerfile and Examples Include File
#include "endat.h"
uint16_t endat22CRCtable[SIZEOF_ENDAT_CRCTABLE];    // Declare CRC table for EnDat CRC calculations

ENDAT_DATA_STRUCT endat22Data;      //PM EnDat22 data structure

uint16_t crc5_result;   //variable for calculated crc result checking
uint16_t retval1;       //used for function return val storage and checks


// Function to initialize EnDat operation
void EnDat_Init(void) {

    EALLOW;
//Enable clocks to PWM1/2/3/4
    CpuSysRegs.PCLKCR2.bit.EPWM1 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM2 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM3 = 1;
    CpuSysRegs.PCLKCR2.bit.EPWM4 = 1;
    EDIS;

//Configure EPWM4 to drive default values on GPIO6 and GPIO7
    EPWM4_Config();

// Generate table for EnDat Polynomial defied as POLY1
    PM_endat22_generateCRCTable(NBITS_POLY1, POLY1, endat22CRCtable);
//GPIO configuration for ENDat operation
    Endat_setup_GPIO();
//XBAR configuration for ENDat operation
    Endat_config_XBAR();

    endat22Data.spi = &SpibRegs;
    PM_endat22_setupPeriph();

    EALLOW;
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
    PieVectTable.SPIB_RX_INT = &spiRxFifoIsr;
    PieCtrlRegs.PIECTRL.bit.ENPIE = 1;   // Enable the PIE block
    PieCtrlRegs.PIEIER6.bit.INTx3 = 1;     // Enable PIE Group 6, INT 9
    IER |= 0x20;                            // Enable CPU INT6
    EINT;
    EDIS;

    // Power up EnDat 5v supply through GPIO32
    GpioDataRegs.GPBDAT.bit.GPIO32 = 1;
    DELAY_US(10000L);   //Delay 10us
    //EncCLK high for 100ms
    EALLOW;
    GpioCtrlRegs.GPADIR.bit.GPIO6 = 1;  //set as GPIO output
    GpioDataRegs.GPASET.bit.GPIO6 = 1; //set GPIO output to be high once GPIO6 is turned to be a GPIO
    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 0;
    DELAY_US(100000L);
    //EncCLK low for ~200ns (>125ns)
    GpioDataRegs.GPADAT.bit.GPIO6 = 0;
    //EncCLK high for 425ms (>381ms)
    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1;
    DELAY_US(425000L);

    //Ensure that EncData is now low
    if (GpioDataRegs.GPADAT.bit.GPIO24 == 1) {
            ESTOP0;
    }

    PM_endat22_setFreq(ENDAT_INIT_FREQ_DIVIDER);


//Encoder Receive Reset - Command ERR
    // 전송할 SPI 및 기타 모듈 설정
    // 모든 트랜잭션은 이 명령어로 시작해야 함
    // Endat 전송을 위한 주변 장치를 설정하지만 실제로 전송이나 활동 수행 X
    // 인코더로 전송할 데이터를 포함하여 sdata 배열을 채움
    // Val - 비정상 : 0, 정상 : 1
    // 0xAA, 0x2222 : 의미없는 값
    // 클럭 상승 - 물론 이미 상승인 상태여서 변화가 있는 건 아니다
    // 이 함수 호출 시 endat22Data.dataReady을 0으로 설정
    retval1 = PM_endat22_setupCommand (ENCODER_RECEIVE_RESET, 0xAA, 0x2222, 0); //data1=any; data2=any
    // 호출할 EnDat 전송 시작

    // 이후 인코더로부터 데이터를 수신할 때 SPI 인터럽트 서비스 루틴에 의해 설정되어야 함
    // 클럭 하강
    PM_endat22_startOperation();

//    // test
//    SpibRegs.SPITXBUF = 0xAAAA;

    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_RECEIVE_RESET, 0);
    DELAY_US(1000000L);     //Delay 1s

    retval1 = PM_endat22_setupCommand (ENCODER_RECEIVE_RESET, 0xAA, 0x2222, 0); //data1=any; data2=any
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_RECEIVE_RESET, 0);

    DELAY_US(2000L);

//Select memory area to read out encoder manufacturer parameters.
//MRS Code A1 - Select Parameters of Encoder Manufacturer
     retval1 = PM_endat22_setupCommand (SELECTION_OF_MEMORY_AREA, 0xA1, 0x5555, 0);  //data1=MRS; data2=any
     PM_endat22_startOperation();
     while (endat22Data.dataReady != 1) {}
     //CHECK CRC!
     retval1 = PM_endat22_receiveData(SELECTION_OF_MEMORY_AREA, 0);
     crc5_result =  PM_endat22_getCrcNorm(endat22Data.address, endat22Data.data, endat22CRCtable);
     if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
             ESTOP0;
     }

     DELAY_US(200L);    //Delay 200us

//Request Encoder to send the number of clock pulses needed to shift out Encoder Position Values
//Reading Address 0xD Returns no.of clock pulses needed to shift out position data
     retval1 = PM_endat22_setupCommand (ENCODER_SEND_PARAMETER, 0xD, 0xAAAA, 0);    //data1=address; data2=any
     PM_endat22_startOperation();
     while (endat22Data.dataReady != 1) {}
     //CHECK CRC!
     retval1 = PM_endat22_receiveData(ENCODER_SEND_PARAMETER, 0);
     crc5_result =  PM_endat22_getCrcNorm(endat22Data.address, endat22Data.data, endat22CRCtable);

     if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
             ESTOP0;
     }

// No.of clocks for position data needs to be set before attempting any position data access
     endat22Data.position_clocks = endat22Data.data & 0xFF;

     DELAY_US(200L);
}

void Endat_setup_GPIO(void) {

    EALLOW;
    // CLB = Confiugrable Logic Block
    // 사용자 정의 가능한 하드웨어 로직 블록
    // FPGA처럼 쓸 수 있는 마이크로컨트롤러 내부 하드웨어 회로
    // FSM = Finite State Machine - 정해진 순서대로 신호를 만듦

    GpioCtrlRegs.GPAMUX1.bit.GPIO6 = 1; // Configure GPIO6 as EnDat Clk master
    GpioCtrlRegs.GPAMUX1.bit.GPIO7 = 1; // Configure GPIO7 as SPI Clk slave

    GpioCtrlRegs.GPAGMUX2.bit.GPIO24 = 1;
    GpioCtrlRegs.GPAGMUX2.bit.GPIO25 = 1;
    GpioCtrlRegs.GPAGMUX2.bit.GPIO26 = 1;
    GpioCtrlRegs.GPAGMUX2.bit.GPIO27 = 1;

    GpioCtrlRegs.GPAMUX2.bit.GPIO24 = 2; // Configure GPIO24 as SPISIMOB
    GpioCtrlRegs.GPAMUX2.bit.GPIO25 = 2; // Configure GPIO25 as SPISOMIB
    GpioCtrlRegs.GPAMUX2.bit.GPIO26 = 2; // Configure GPIO26 as SPICLKB
    GpioCtrlRegs.GPAMUX2.bit.GPIO27 = 2; // Configure GPIO27 as SPISTEB

    GpioCtrlRegs.GPAQSEL2.bit.GPIO24 = 3; // Asynch input GPIO24 (SPISIMOB)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO25 = 3; // Asynch input GPIO25 (SPISOMIB)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO26 = 3; // Asynch input GPIO26 (SPICLKB)
    GpioCtrlRegs.GPAQSEL2.bit.GPIO27 = 3; // Asynch input GPIO27 (SPISTEB)

    GpioCtrlRegs.GPBMUX1.bit.GPIO34 = 1; // Configure GPIO34 as EnDat TxEN

    GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1; // Configure GPIO32 as EnDat Pwr Ctl

    EDIS;
}

void Endat_config_XBAR(void)
{
    EALLOW;

//Choose SPISIMO GPIO as InputXbar Input1 - SPISIMO (B) on GPIO24 in this case
    InputXbarRegs.INPUT1SELECT = 24;    // GPTRIP XBAR TRIP1 -> GPIO24
    EDIS;
}

//Template for performing delay compensation
//This function should only be called while operating at low frequencies (~200KHz) only.
void EnDat_initDelayComp(void) {
    uint16_t delay1, delay2;

//Transmit Send position values command to the encoder
//Delay is internally measured during this command operation
    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES, 0, 0, 0);
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES, 0);

    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT21, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);
    if (!CheckCRC(crc5_result,endat22Data.data_crc))
    {
            ESTOP0;
    }
     DELAY_US(200L);    //Delay 200us
//Delay is internally measured during the above operation
//Read the measured delay and store in a variable - n * 2 * SYSCLKs
    delay1 = PM_endat22_getDelayCompVal();

//Redo the same procedure again
    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES, 0, 0, 0);
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES, 0);

    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT21, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
         ESTOP0;
     }
     DELAY_US(200L);    //Delay 200us

 //Delay is internally measured during the above operation
 //Read the measured delay and store in a variable - n * 2 * SYSCLKs
     delay2 = PM_endat22_getDelayCompVal();

//Average value of the measured delays has to be updated into endat22Data.delay_comp
// for delay compensation to take effect
    endat22Data.delay_comp = (delay1+delay2) >> 1;
}


void error(void) {
    asm("     ESTOP0");
    //Test failed!! Stop!
    for (;;);
}

interrupt void spiRxFifoIsr(void)
{
    uint16_t i;
    for (i=0;i<=endat22Data.fifo_level;i++){endat22Data.rdata[i]= endat22Data.spi->SPIRXBUF;}
    endat22Data.spi->SPIFFRX.bit.RXFFOVFCLR=1;  // Clear Overflow flag
    endat22Data.spi->SPIFFRX.bit.RXFFINTCLR=1;  // Clear Interrupt flag
    PieCtrlRegs.PIEACK.all|=0x20;       // Issue PIE ack
    endat22Data.dataReady=1;
}


void EPWM4_Config(void) {
// Set the PWMA and B high as default values of ENDAT clk.
    EALLOW;
    EPwm4Regs.TZCTL.bit.TZA = 1;
    EPwm4Regs.TZCTL.bit.TZB = 1;
    EPwm4Regs.TZFRC.bit.OST = 1;
    EDIS;
}

uint16_t CheckCRC (uint16_t expectcrc5, uint16_t receivecrc5) {
    if (expectcrc5 == receivecrc5) {
        return 1;
    }
    else {
        return 0;
    }
}



void endat22_setupAddlData(void)
{
// EnDat22 Command reading position values and performing selection of memory area
// 0xA1 MRS code for selection of encoder manufacturer parameters
// Additional data enabled at this time is 0

    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES_AND_SELECTION_OF_THE_MEMORY_AREA, 0xA1, 0, 0);
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES_AND_SELECTION_OF_THE_MEMORY_AREA, 0);

    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT22, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
     ESTOP0;
     }

     DELAY_US(200L);    //Delay 200us

// EnDat22 Command reading position values and sending a parameter to encoder
// Send 0xD parameter address - will select no. of clock pulses to shift out position value
// Additional data enabled at this time is 0

    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES_AND_SEND_PARAMETER, 0xD, 0, 0);
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES_AND_SEND_PARAMETER, 0);

    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT22, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
     ESTOP0;
     }

     DELAY_US(200L);    //Delay 200us

// Enable Additional data 1 - to read out no. of  clock pulses to shift out position value
// MRS code 0x45    - Acknowledge memory content LSB

    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES_AND_SELECTION_OF_THE_MEMORY_AREA, 0x45, 0, 0);
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES_AND_SELECTION_OF_THE_MEMORY_AREA, 0);

    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT22, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
     ESTOP0;
     }

     DELAY_US(200L);    //Delay 200us

 // Enable Additional data 2 - to read out Operating status and error sources
 // MRS code 0x59   - operating status on additional data 2
 // Additional data enabled before this command is 1, after this command 2
    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES_AND_SELECTION_OF_THE_MEMORY_AREA, 0x59, 0, 1);
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES_AND_SELECTION_OF_THE_MEMORY_AREA, 1);

    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT22, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
     ESTOP0;
     }

     DELAY_US(2000L);   //Delay 200us

}

void endat22_readPositionWithAddlData(void)
{
// Read out position value with 2 additional data previously enabled
// Additional data enabled at this time is 2
    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES_WITH_ADDITIONAL_DATA, 0, 0, 2);
    PM_endat22_startOperation();
    for (int i = 0; i < 100000; i++)
    {
        if (endat22Data.dataReady == 1)
        {
            break;
        }
    }

    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES_WITH_ADDITIONAL_DATA, 2);

// CRC check for Position Data
    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT22, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.data_crc))
     {
     //ESTOP0;
     }

// CRC check for Additional Data 1
    crc5_result =  PM_endat22_getCrcNorm((endat22Data.additional_data1 >> 16), endat22Data.additional_data1, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.additional_data1_crc))
     {
     //ESTOP0;
     }

// CRC check for Additional Data 2
    crc5_result =  PM_endat22_getCrcNorm((endat22Data.additional_data2 >> 16), endat22Data.additional_data2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.additional_data2_crc))
     {
     //ESTOP0;
     }
     DELAY_US(200L);    //Delay 200us
}

void endat21_readPosition(void)
{
// Read position value in EnDat21 mode - no additional data
    retval1 = PM_endat22_setupCommand (ENCODER_SEND_POSITION_VALUES, 0, 0, 0);
    PM_endat22_startOperation();
    while (endat22Data.dataReady != 1) {}
    retval1 = PM_endat22_receiveData(ENCODER_SEND_POSITION_VALUES, 0);

// CRC check for Position Data
    crc5_result =  PM_endat22_getCrcPos(endat22Data.position_clocks, ENDAT21, endat22Data.position_lo,
                    endat22Data.position_hi, endat22Data.error1, endat22Data.error2, endat22CRCtable);

    if (!CheckCRC(crc5_result,endat22Data.data_crc))
    {
        endat22Data.position_hi = 0;
        endat22Data.position_lo = 0;
        ESTOP0;
    }
    DELAY_US(200L);    //Delay 200us
}
//***************************************************************************
// End of file
// **************************************************************************

void Endat_Setup(void)
{
    //A template for running all the EnDat21 commands
    //This is optional in real applications.
    //Function defined in endat_commands.c
    endat21_runCommandSet();

    if (ENCODER_TYPE == 22)
    {
    //A template for running all the EnDat22 commands
    //This is optional in real applications.
    //Function defined in endat_commands.c
        endat22_runCommandSet();
    }

    //Enables 2 additional datas in endat22 operation
    //This is also optional in real applications. Function defined in endat.c
    endat22_setupAddlData();

    //Peforms cable propagation delay calculation.
    //This is required for long cable lengths and higher EnDat Clock frequencies
    //Function defined in endat.c
    EnDat_initDelayComp();

    //Switch to high frequency - 8.3MHz (=200/4*ENDAT_RUNTIME_FREQ_DIVIDER)
    //PM_endat22_setFreq(ENDAT_RUNTIME_FREQ_DIVIDER);
    PM_endat22_setFreq(200);
    DELAY_US(800L);     //Delay 800us
}
//***************************************************************************
// End of file
// **************************************************************************