|
MotorWare f2806x Driver API Documentation
|
Contains the various functions related to the analog-to-digital converter (ADC) object. More...
#include "sw/drivers/adc/src/32b/f28x/f2806x/adc.h"Go to the source code of this file.
Functions | |
| void | usDelay (uint32_t Count) |
| void | ADC_disable (ADC_Handle adcHandle) |
| Disables the analog-to-digital converter (ADC) More... | |
| void | ADC_disableBandGap (ADC_Handle adcHandle) |
| Disables the analog-to-digital converter (ADC) band gap circuit. More... | |
| void | ADC_disableInt (ADC_Handle adcHandle, const ADC_IntNumber_e intNumber) |
| Disables the analog-to-digital converter (ADC) interrupt. More... | |
| void | ADC_disableRefBuffers (ADC_Handle adcHandle) |
| Disables the analog-to-digital converter (ADC) reference buffers circuit. More... | |
| void | ADC_enable (ADC_Handle adcHandle) |
| Enables the analog-to-digital converter (ADC) More... | |
| void | ADC_enableBandGap (ADC_Handle adcHandle) |
| Enables the analog-to-digital converter (ADC) band gap circuit. More... | |
| void | ADC_enableInt (ADC_Handle adcHandle, const ADC_IntNumber_e intNumber) |
| Enables the analog-to-digital converter (ADC) interrupt. More... | |
| void | ADC_enableRefBuffers (ADC_Handle adcHandle) |
| Enables the analog-to-digital converter (ADC) reference buffers circuit. More... | |
| ADC_Handle | ADC_init (void *pMemory, const size_t numBytes) |
| Initializes the analog-to-digital converter (ADC) object handle. More... | |
| void | ADC_powerDown (ADC_Handle adcHandle) |
| Powers down the analog-to-digital converter (ADC) More... | |
| void | ADC_powerUp (ADC_Handle adcHandle) |
| Powers up the analog-to-digital converter (ADC) More... | |
| void | ADC_reset (ADC_Handle adcHandle) |
| Resets the analog-to-digital converter (ADC) More... | |
| void | ADC_setSampleOverlapMode (ADC_Handle adcHandle, ADC_ADCCTL2_ADCNONOVERLAP_e OverLap) |
| void | ADC_setIntMode (ADC_Handle adcHandle, const ADC_IntNumber_e intNumber, const ADC_IntMode_e intMode) |
| Sets the interrupt mode. More... | |
| void | ADC_setIntPulseGenMode (ADC_Handle adcHandle, const ADC_IntPulseGenMode_e pulseMode) |
| Sets the interrupt pulse generation mode. More... | |
| void | ADC_setIntSrc (ADC_Handle adcHandle, const ADC_IntNumber_e intNumber, const ADC_IntSrc_e intSrc) |
| Sets the interrupt source. More... | |
| void | ADC_setSampleMode (ADC_Handle adcHandle, const ADC_SampleMode_e sampleMode) |
| Sets the sample mode. More... | |
| void | ADC_setSocChanNumber (ADC_Handle adcHandle, const ADC_SocNumber_e socNumber, const ADC_SocChanNumber_e chanNumber) |
| Sets the start-of-conversion (SOC) channel number. More... | |
| void | ADC_setSocSampleDelay (ADC_Handle adcHandle, const ADC_SocNumber_e socNumber, const ADC_SocSampleDelay_e sampleDelay) |
| Sets the start-of-conversion (SOC) sample delay. More... | |
| void | ADC_setSocTrigSrc (ADC_Handle adcHandle, const ADC_SocNumber_e socNumber, const ADC_SocTrigSrc_e trigSrc) |
| Sets the start-of-conversion (SOC) trigger source. More... | |
| void | ADC_setSocFrc (ADC_Handle adcHandle, const ADC_SocFrc_e socFrc) |
| Sets the start-of-conversion (SOC) force register. More... | |
| void | ADC_setSocFrcWord (ADC_Handle adcHandle, const uint16_t socFrc) |
| Sets the entire start of conversion (SOC) force register. More... | |
| void | ADC_setTempSensorSrc (ADC_Handle adcHandle, const ADC_TempSensorSrc_e sensorSrc) |
| Sets the temperature sensor source. More... | |
| void | ADC_setVoltRefSrc (ADC_Handle adcHandle, const ADC_VoltageRefSrc_e voltSrc) |
| Sets the voltage reference source. More... | |
| ADC_DivideSelect_e | ADC_getDivideSelect (ADC_Handle adcHandle) |
| Gets the analog-to-digital converter (ADC) divide select value. More... | |
| void | ADC_setDivideSelect (ADC_Handle adcHandle, const ADC_DivideSelect_e divSelect) |
| Sets the analog-to-digital converter (ADC) divide select value. More... | |
| void | ADC_enableNoOverlapMode (ADC_Handle adcHandle) |
| Enables no overlap mode. More... | |
| void | ADC_disableNoOverlapMode (ADC_Handle adcHandle) |
| Disables no overlap mode. More... | |
| void | ADC_setupSocTrigSrc (ADC_Handle adcHandle, const ADC_SocNumber_e socNumber, const ADC_IntTriggerSOC_e intTrigSrc) |
| Sets the start of conversion (SOC) trigger source. More... | |
| void | ADC_setOffTrim (ADC_Handle adcHandle, const uint16_t offtrim) |
| Sets the offset trim register. More... | |
| void | ADC_enableVoltRefLoConv (ADC_Handle adcHandle) |
| Enables conversion of the voltage reference low signal for calibration. More... | |
| void | ADC_disableVoltRefLoConv (ADC_Handle adcHandle) |
| Disables conversion of the voltage reference low signal for calibration. More... | |
Contains the various functions related to the analog-to-digital converter (ADC) object.
(C) Copyright 2015, Texas Instruments, Inc.
Definition in file adc.c.
| void ADC_setSampleOverlapMode | ( | ADC_Handle | adcHandle, |
| ADC_ADCCTL2_ADCNONOVERLAP_e | OverLap | ||
| ) |
Definition at line 257 of file adc.c.
References ADC_ADCCTL2_ADCNONOVERLAP_BITS, ADC_ADCCTL2_Overlap, _ADC_Obj_::ADCCTL2, DISABLE_PROTECTED_REGISTER_WRITE_MODE, and ENABLE_PROTECTED_REGISTER_WRITE_MODE.
| void usDelay | ( | uint32_t | Count | ) |
1.8.9.1