|
MotorWare f2806x Driver API Documentation
|
Contains the various functions related to the comparator (COMP) object. More...
#include "sw/drivers/comp/src/32b/f28x/f2806x/comp.h"Go to the source code of this file.
Functions | |
| void | usDelay (uint32_t Count) |
| void | COMP_disable (COMP_Handle compHandle) |
| Disables the comparator (COMP) More... | |
| void | COMP_disableDac (COMP_Handle compHandle) |
| Disables the DAC. More... | |
| void | COMP_enable (COMP_Handle compHandle) |
| Enables the comparator (COMP) More... | |
| void | COMP_enableDac (COMP_Handle compHandle) |
| Enables the DAC. More... | |
| COMP_Handle | COMP_init (void *pMemory, const size_t numBytes) |
| Initializes the comparator (COMP) object handle. More... | |
Contains the various functions related to the comparator (COMP) object.
(C) Copyright 2015, Texas Instruments, Inc.
Definition in file comp.c.
| void usDelay | ( | uint32_t | Count | ) |
1.8.9.1