|
MotorWare f2806x Driver API Documentation
|
Contains the various functions related to the central processing unit (CPU) object. More...
#include "sw/drivers/cpu/src/32b/f28x/f2806x/cpu.h"Go to the source code of this file.
Functions | |
| void | CPU_clearIntFlags (CPU_Handle cpuHandle) |
| Clears all interrupt flags. More... | |
| void | CPU_disableDebugInt (CPU_Handle cpuHandle) |
| Disables the debug interrupt. More... | |
| void | CPU_disableGlobalInts (CPU_Handle cpuHandle) |
| Disables global interrupts. More... | |
| void | CPU_disableInt (CPU_Handle cpuHandle, const CPU_IntNumber_e intNumber) |
| Disables a specified interrupt number. More... | |
| void | CPU_disableInts (CPU_Handle cpuHandle) |
| Disables all interrupts. More... | |
| void | CPU_disableProtectedRegisterWrite (CPU_Handle cpuHandle) |
| Disables protected register writes. More... | |
| void | CPU_enableDebugInt (CPU_Handle cpuHandle) |
| Enables the debug interrupt. More... | |
| void | CPU_enableGlobalInts (CPU_Handle cpuHandle) |
| Enables global interrupts. More... | |
| void | CPU_enableInt (CPU_Handle cpuHandle, const CPU_IntNumber_e intNumber) |
| Enables a specified interrupt number. More... | |
| void | CPU_enableProtectedRegisterWrite (CPU_Handle cpuHandle) |
| Enables protected register writes. More... | |
| CPU_Handle | CPU_init (void *pMemory, const size_t numBytes) |
| Initializes the central processing unit (CPU) object handle. More... | |
Variables | |
| CPU_Obj | cpu |
| Defines the CPU object. More... | |
Contains the various functions related to the central processing unit (CPU) object.
(C) Copyright 2015, Texas Instruments, Inc.
Definition in file cpu.c.
1.8.9.1