|
MotorWare f2806x Driver API Documentation
|
Contains public interface to various functions related to the DRV8301 object. More...
#include "sw/drivers/spi/src/32b/f28x/f2806x/spi.h"#include "sw/drivers/gpio/src/32b/f28x/f2806x/gpio.h"Go to the source code of this file.
Data Structures | |
| struct | _DRV_SPI_8301_Stat1_t_ |
| struct | _DRV_SPI_8301_Stat2_t_ |
| struct | _DRV_SPI_8301_CTRL1_t_ |
| struct | _DRV_SPI_8301_CTRL2_t_ |
| struct | _DRV_SPI_8301_Vars_t_ |
| struct | _DRV8301_Obj_ |
| Defines the DRV8301 object. More... | |
Macros | |
| #define | DRV8301_ADDR_MASK (0x7800) |
| Defines the address mask. More... | |
| #define | DRV8301_DATA_MASK (0x07FF) |
| Defines the data mask. More... | |
| #define | DRV8301_RW_MASK (0x8000) |
| Defines the R/W mask. More... | |
| #define | DRV8301_FAULT_TYPE_MASK (0x07FF) |
| Defines the R/W mask. More... | |
| #define | DRV8301_STATUS1_FETLC_OC_BITS (1 << 0) |
| Defines the location of the FETLC_OC (FET Low side, Phase C Over Current) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_FETHC_OC_BITS (1 << 1) |
| Defines the location of the FETLC_OC (FET High side, Phase C Over Current) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_FETLB_OC_BITS (1 << 2) |
| Defines the location of the FETLC_OC (FET Low side, Phase B Over Current) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_FETHB_OC_BITS (1 << 3) |
| Defines the location of the FETLC_OC (FET High side, Phase B Over Current) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_FETLA_OC_BITS (1 << 4) |
| Defines the location of the FETLC_OC (FET Low side, Phase A Over Current) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_FETHA_OC_BITS (1 << 5) |
| Defines the location of the FETLC_OC (FET High side, Phase A Over Current) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_OTW_BITS (1 << 6) |
| Defines the location of the OTW (Over Temperature Warning) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_OTSD_BITS (1 << 7) |
| Defines the location of the OTSD (Over Temperature Shut Down) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_PVDD_UV_BITS (1 << 8) |
| Defines the location of the PVDD_UV (Power supply Vdd, Under Voltage) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_GVDD_UV_BITS (1 << 9) |
| Defines the location of the GVDD_UV (DRV8301 Vdd, Under Voltage) bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS1_FAULT_BITS (1 << 10) |
| Defines the location of the FAULT bits in the Status 1 register. More... | |
| #define | DRV8301_STATUS2_ID_BITS (15 << 0) |
| Defines the location of the Device ID bits in the Status 2 register. More... | |
| #define | DRV8301_STATUS2_GVDD_OV_BITS (1 << 7) |
| Defines the location of the GVDD_OV (DRV8301 Vdd, Over Voltage) bits in the Status 2 register. More... | |
| #define | DRV8301_CTRL1_GATE_CURRENT_BITS (3 << 0) |
| Defines the location of the GATE_CURRENT bits in the Control 1 register. More... | |
| #define | DRV8301_CTRL1_GATE_RESET_BITS (1 << 2) |
| Defines the location of the GATE_RESET bits in the Control 1 register. More... | |
| #define | DRV8301_CTRL1_PWM_MODE_BITS (1 << 3) |
| Defines the location of the PWM_MODE bits in the Control 1 register. More... | |
| #define | DRV8301_CTRL1_OC_MODE_BITS (3 << 4) |
| Defines the location of the OC_MODE bits in the Control 1 register. More... | |
| #define | DRV8301_CTRL1_OC_ADJ_SET_BITS (31 << 6) |
| Defines the location of the OC_ADJ bits in the Control 1 register. More... | |
| #define | DRV8301_CTRL2_OCTW_SET_BITS (3 << 0) |
| Defines the location of the OCTW_SET bits in the Control 2 register. More... | |
| #define | DRV8301_CTRL2_GAIN_BITS (3 << 2) |
| Defines the location of the GAIN bits in the Control 2 register. More... | |
| #define | DRV8301_CTRL2_DC_CAL_1_BITS (1 << 4) |
| Defines the location of the DC_CAL_1 bits in the Control 2 register. More... | |
| #define | DRV8301_CTRL2_DC_CAL_2_BITS (1 << 5) |
| Defines the location of the DC_CAL_2 bits in the Control 2 register. More... | |
| #define | DRV8301_CTRL2_OC_TOFF_BITS (1 << 6) |
| Defines the location of the OC_TOFF bits in the Control 2 register. More... | |
Typedefs | |
| typedef struct _DRV_SPI_8301_Stat1_t_ | DRV_SPI_8301_Stat1_t_ |
| typedef struct _DRV_SPI_8301_Stat2_t_ | DRV_SPI_8301_Stat2_t_ |
| typedef struct _DRV_SPI_8301_CTRL1_t_ | DRV_SPI_8301_CTRL1_t_ |
| typedef struct _DRV_SPI_8301_CTRL2_t_ | DRV_SPI_8301_CTRL2_t_ |
| typedef struct _DRV_SPI_8301_Vars_t_ | DRV_SPI_8301_Vars_t |
| typedef struct _DRV8301_Obj_ | DRV8301_Obj |
| Defines the DRV8301 object. More... | |
| typedef struct _DRV8301_Obj_ * | DRV8301_Handle |
| Defines the DRV8301 handle. More... | |
| typedef uint16_t | DRV8301_Word_t |
| Defines the DRV8301 Word type. More... | |
Functions | |
| static DRV8301_Word_t | DRV8301_buildCtrlWord (const DRV8301_CtrlMode_e ctrlMode, const DRV8301_RegName_e regName, const uint16_t data) |
| Builds the control word. More... | |
| DRV8301_DcCalMode_e | DRV8301_getDcCalMode (DRV8301_Handle handle, const DRV8301_ShuntAmpNumber_e ampNumber) |
| Gets the DC calibration mode. More... | |
| void | DRV8301_enable (DRV8301_Handle handle) |
| Enables the DRV8301. More... | |
| DRV8301_FaultType_e | DRV8301_getFaultType (DRV8301_Handle handle) |
| Gets the fault type. More... | |
| uint16_t | DRV8301_getId (DRV8301_Handle handle) |
| Gets the device ID. More... | |
| DRV8301_VdsLevel_e | DRV8301_getOcLevel (DRV8301_Handle handle) |
| Gets the over current level. More... | |
| DRV8301_OcMode_e | DRV8301_getOcMode (DRV8301_Handle handle) |
| Gets the over current mode. More... | |
| DRV8301_OcOffTimeMode_e | DRV8301_getOcOffTimeMode (DRV8301_Handle handle) |
| Gets the over current off time mode. More... | |
| DRV8301_OcTwMode_e | DRV8301_getOcTwMode (DRV8301_Handle handle) |
| Gets the over current, temperature warning mode. More... | |
| DRV8301_PeakCurrent_e | DRV8301_getPeakCurrent (DRV8301_Handle handle) |
| Gets the peak current value. More... | |
| DRV8301_PwmMode_e | DRV8301_getPwmMode (DRV8301_Handle handle) |
| Gets the PWM mode. More... | |
| DRV8301_ShuntAmpGain_e | DRV8301_getShuntAmpGain (DRV8301_Handle handle) |
| Gets the shunt amplifier gain value. More... | |
| uint16_t | DRV8301_getStatusRegister1 (DRV8301_Handle handle) |
| Gets the status register 1 value. More... | |
| uint16_t | DRV8301_getStatusRegister2 (DRV8301_Handle handle) |
| Gets the status register 2 value. More... | |
| DRV8301_Handle | DRV8301_init (void *pMemory, const size_t numBytes) |
| Initializes the DRV8301 object. More... | |
| bool | DRV8301_isFault (DRV8301_Handle handle) |
| Determines if DRV8301 fault has occurred. More... | |
| bool | DRV8301_isReset (DRV8301_Handle handle) |
| Determines if DRV8301 is in reset. More... | |
| uint16_t | DRV8301_readSpi (DRV8301_Handle handle, const DRV8301_RegName_e regName) |
| Reads data from the DRV8301 register. More... | |
| void | DRV8301_reset (DRV8301_Handle handle) |
| Resets the DRV8301. More... | |
| static void | DRV8301_resetEnableTimeout (DRV8301_Handle handle) |
| Resets the enable timeout flag. More... | |
| static void | DRV8301_resetRxTimeout (DRV8301_Handle handle) |
| Resets the RX fifo timeout flag. More... | |
| void | DRV8301_setDcCalMode (DRV8301_Handle handle, const DRV8301_ShuntAmpNumber_e ampNumber, const DRV8301_DcCalMode_e mode) |
| Sets the DC calibration mode. More... | |
| void | DRV8301_setGpioHandle (DRV8301_Handle handle, GPIO_Handle gpioHandle) |
| Sets the GPIO handle in the DRV8301. More... | |
| void | DRV8301_setGpioNumber (DRV8301_Handle handle, GPIO_Number_e gpioNumber) |
| Sets the GPIO number in the DRV8301. More... | |
| void | DRV8301_setOcLevel (DRV8301_Handle handle, const DRV8301_VdsLevel_e VdsLevel) |
| Sets the over current level in terms of Vds. More... | |
| void | DRV8301_setOcMode (DRV8301_Handle handle, const DRV8301_OcMode_e mode) |
| Sets the over current mode. More... | |
| void | DRV8301_setOcOffTimeMode (DRV8301_Handle handle, const DRV8301_OcOffTimeMode_e mode) |
| Sets the over current off time mode. More... | |
| void | DRV8301_setOcTwMode (DRV8301_Handle handle, const DRV8301_OcTwMode_e mode) |
| Sets the over current, temperature warning mode. More... | |
| void | DRV8301_setPeakCurrent (DRV8301_Handle handle, const DRV8301_PeakCurrent_e peakCurrent) |
| Sets the peak current value. More... | |
| void | DRV8301_setPwmMode (DRV8301_Handle handle, const DRV8301_PwmMode_e mode) |
| Sets the PWM mode. More... | |
| void | DRV8301_setShuntAmpGain (DRV8301_Handle handle, const DRV8301_ShuntAmpGain_e gain) |
| Sets the shunt amplifier gain value. More... | |
| void | DRV8301_setSpiHandle (DRV8301_Handle handle, SPI_Handle spiHandle) |
| Sets the SPI handle in the DRV8301. More... | |
| void | DRV8301_writeSpi (DRV8301_Handle handle, const DRV8301_RegName_e regName, const uint16_t data) |
| Writes data to the DRV8301 register. More... | |
| void | DRV8301_writeData (DRV8301_Handle handle, DRV_SPI_8301_Vars_t *Spi_8301_Vars) |
| Interface to all 8301 SPI variables. More... | |
| void | DRV8301_readData (DRV8301_Handle handle, DRV_SPI_8301_Vars_t *Spi_8301_Vars) |
| void | DRV8301_setupSpi (DRV8301_Handle handle, DRV_SPI_8301_Vars_t *Spi_8301_Vars) |
| Initialize the interface to all 8301 SPI variables. More... | |
Contains public interface to various functions related to the DRV8301 object.
(C) Copyright 2015, Texas Instruments, Inc.
Definition in file drv8301.h.
1.8.9.1