MotorWare f2806x Driver API Documentation
Functions
flash.c File Reference

Contains the various functions related to the flash object. More...

#include "sw/drivers/flash/src/32b/f28x/f2806x/flash.h"

Go to the source code of this file.

Functions

void FLASH_clear3VStatus (FLASH_Handle flashHandle)
 Clears the 3V status. More...
 
void FLASH_disablePipelineMode (FLASH_Handle flashHandle)
 Disables the pipeline mode. More...
 
void FLASH_enablePipelineMode (FLASH_Handle flashHandle)
 Enables the pipeline mode. More...
 
FLASH_3VStatus_e FLASH_get3VStatus (FLASH_Handle flashHandle)
 Gets the 3V status. More...
 
uint16_t FLASH_getActiveWaitCount (FLASH_Handle flashHandle)
 Gets the active wait count. More...
 
FLASH_CounterStatus_e FLASH_getActiveWaitStatus (FLASH_Handle flashHandle)
 Gets the active wait counter status. More...
 
FLASH_PowerMode_e FLASH_getPowerMode (FLASH_Handle flashHandle)
 Gets the power mode. More...
 
uint16_t FLASH_getStandbyWaitCount (FLASH_Handle flashHandle)
 Gets the standby wait count. More...
 
FLASH_CounterStatus_e FLASH_getStandbyWaitStatus (FLASH_Handle flashHandle)
 Gets the standby wait counter status. More...
 
FLASH_Handle FLASH_init (void *pMemory, const size_t numBytes)
 Initializes the flash (FLASH) handle. More...
 
void FLASH_setActiveWaitCount (FLASH_Handle flashHandle, const uint16_t count)
 Sets the active wait count. More...
 
void FLASH_setNumPagedReadWaitStates (FLASH_Handle flashHandle, const FLASH_NumPagedWaitStates_e numStates)
 Sets the number of paged read wait states. More...
 
void FLASH_setNumRandomReadWaitStates (FLASH_Handle flashHandle, const FLASH_NumRandomWaitStates_e numStates)
 Sets the number of random read wait states. More...
 
void FLASH_setOtpWaitStates (FLASH_Handle flashHandle, const FLASH_NumOtpWaitStates_e numStates)
 Sets the number of one-time programmable (OTP) wait states. More...
 
void FLASH_setPowerMode (FLASH_Handle flashHandle, const FLASH_PowerMode_e mode)
 Sets the power mode. More...
 
void FLASH_setStandbyWaitCount (FLASH_Handle flashHandle, const uint16_t count)
 Sets the standby wait count. More...
 

Detailed Description

Contains the various functions related to the flash object.

(C) Copyright 2015, Texas Instruments, Inc.

Definition in file flash.c.