MotorWare f2806x Driver API Documentation
Functions
pll.c File Reference

Contains the various functions related to the phase-locked loop (PLL) object. More...

#include "sw/drivers/pll/src/32b/f28x/f2806x/pll.h"

Go to the source code of this file.

Functions

void PLL_disable (PLL_Handle pllHandle)
 Disables the phase lock loop (PLL) More...
 
void PLL_disableClkDetect (PLL_Handle pllHandle)
 Disables the clock detect logic. More...
 
void PLL_disableNormRdy (PLL_Handle pllHandle)
 Disables the NORMRDY signal. More...
 
void PLL_disableOsc (PLL_Handle pllHandle)
 Disables the oscillator. More...
 
void PLL_enable (PLL_Handle pllHandle)
 Enables the phase lock loop (PLL) More...
 
void PLL_enableClkDetect (PLL_Handle pllHandle)
 Enables the clock detect logic. More...
 
void PLL_enableNormRdy (PLL_Handle pllHandle)
 Enables the NORMRDY signal. More...
 
void PLL_enableOsc (PLL_Handle pllHandle)
 Enables the oscillator. More...
 
PLL_ClkFreq_e PLL_getClkFreq (PLL_Handle pllHandle)
 Gets the phase lock loop (PLL) clock frequency. More...
 
PLL_ClkStatus_e PLL_getClkStatus (PLL_Handle pllHandle)
 Gets the phase lock loop (PLL) clock status. More...
 
PLL_DivideSelect_e PLL_getDivideSelect (PLL_Handle pllHandle)
 Gets the phase lock loop (PLL) divide select value. More...
 
PLL_LockStatus_e PLL_getLockStatus (PLL_Handle pllHandle)
 Gets the phase lock loop (PLL) lock status. More...
 
PLL_Handle PLL_init (void *pMemory, const size_t numBytes)
 Initializes the phase lock loop (PLL) object handle. More...
 
void PLL_resetClkDetect (PLL_Handle pllHandle)
 Resets the phase lock loop (PLL) clock detect logic. More...
 
void PLL_setClkFreq (PLL_Handle pllHandle, const PLL_ClkFreq_e clkFreq)
 Sets the phase lock loop (PLL) clock frequency. More...
 
void PLL_setDivideSelect (PLL_Handle pllHandle, const PLL_DivideSelect_e divSelect)
 Sets the phase lock loop (PLL) divide select value. More...
 
void PLL_setLockPeriod (PLL_Handle pllHandle, const uint16_t lockPeriod)
 Sets the phase lock loop (PLL) lock time. More...
 

Detailed Description

Contains the various functions related to the phase-locked loop (PLL) object.

(C) Copyright 2015, Texas Instruments, Inc.

Definition in file pll.c.