|
MotorWare f2806x Driver API Documentation
|
Contains the various functions related to the power (PWR) object. More...
#include "sw/drivers/pwr/src/32b/f28x/f2806x/pwr.h"Go to the source code of this file.
Functions | |
| void | PWR_disableBrownOutReset (PWR_Handle pwrHandle) |
| Disables the brownout reset functions. More... | |
| void | PWR_disableWatchDogInt (PWR_Handle pwrHandle) |
| Disables the watchdog interrupt. More... | |
| void | PWR_enableBrownOutReset (PWR_Handle pwrHandle) |
| Enables the brownout reset functions. More... | |
| void | PWR_enableWatchDogInt (PWR_Handle pwrHandle) |
| Enables the watchdog interrupt. More... | |
| PWR_Handle | PWR_init (void *pMemory, const size_t numBytes) |
| Initializes the power (PWR) object handle. More... | |
| void | PWR_setLowPowerMode (PWR_Handle pwrHandle, const PWR_LowPowerMode_e lowPowerMode) |
| Sets the low power mode. More... | |
| void | PWR_setNumStandByClocks (PWR_Handle pwrHandle, const PWR_NumStandByClocks_e numClkCycles) |
| Sets the number of standby clock cycles. More... | |
Contains the various functions related to the power (PWR) object.
(C) Copyright 2015, Texas Instruments, Inc.
Definition in file pwr.c.
1.8.9.1