|
MotorWare f2806x Driver API Documentation
|
Contains the various functions related to the serial communications interface (SCI) object. More...
#include "sw/drivers/sci/src/32b/f28x/f2806x/sci.h"Go to the source code of this file.
Functions | |
| void | SCI_clearAutoBaudDetect (SCI_Handle sciHandle) |
| Clears the auto baud detect mode. More... | |
| void | SCI_clearRxFifoOvf (SCI_Handle sciHandle) |
| Clears the Rx FIFO overflow flag. More... | |
| void | SCI_clearRxFifoInt (SCI_Handle sciHandle) |
| Clears the Rx FIFO interrupt flag. More... | |
| void | SCI_clearTxFifoInt (SCI_Handle sciHandle) |
| Clears the Tx FIFO interrupt flag. More... | |
| void | SCI_disable (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) interrupt. More... | |
| void | SCI_disableAutoBaudAlign (SCI_Handle sciHandle) |
| Disable the serial communications interface (SCI) auto baud alignment. More... | |
| void | SCI_disableLoopBack (SCI_Handle sciHandle) |
| Disables the serial peripheral interface (SCI) loop back mode. More... | |
| void | SCI_disableParity (SCI_Handle sciHandle) |
| Disable the parity. More... | |
| void | SCI_disableRx (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) master/slave receive mode. More... | |
| void | SCI_disableRxErrorInt (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) receive error interrupt. More... | |
| void | SCI_disableRxFifoInt (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) receive FIFO interrupt. More... | |
| void | SCI_disableRxInt (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) receive interrupt. More... | |
| void | SCI_disableSleep (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) sleep mode. More... | |
| void | SCI_disableTx (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) master/slave transmit mode. More... | |
| void | SCI_disableTxFifoEnh (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) transmit FIFO enhancements. More... | |
| void | SCI_disableTxFifoInt (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) transmit FIFO interrupt. More... | |
| void | SCI_disableTxInt (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) transmit interrupt. More... | |
| void | SCI_disableTxWake (SCI_Handle sciHandle) |
| Disables the serial communications interface (SCI) wakeup method. More... | |
| void | SCI_enable (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) More... | |
| void | SCI_enableAutoBaudAlign (SCI_Handle sciHandle) |
| Enable the serial communications interface (SCI) auto baud alignment. More... | |
| void | SCI_enableChannels (SCI_Handle sciHandle) |
| Enable the serial communications interface (SCI) transmit and receive channels. More... | |
| void | SCI_enableLoopBack (SCI_Handle sciHandle) |
| Enables the serial peripheral interface (SCI) loop back mode. More... | |
| void | SCI_enableParity (SCI_Handle sciHandle) |
| Enables the serial peripheral interface (SCI) parity. More... | |
| void | SCI_enableRx (SCI_Handle sciHandle) |
| Enables the serial peripheral interface (SCI) receiver. More... | |
| void | SCI_enableRxErrorInt (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) receive error interrupt. More... | |
| void | SCI_enableRxInt (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) receive interrupt. More... | |
| void | SCI_enableSleep (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) sleep mode. More... | |
| void | SCI_enableRxFifo (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) receive FIFO. More... | |
| void | SCI_enableRxFifoInt (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) receive FIFO interrupt. More... | |
| void | SCI_enableTx (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) masater/slave transmit mode. More... | |
| void | SCI_enableTxFifo (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) transmit FIFO. More... | |
| void | SCI_enableTxFifoEnh (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) transmit FIFO enhancements. More... | |
| void | SCI_enableTxFifoInt (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) transmit FIFO interrupt. More... | |
| void | SCI_enableTxInt (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) transmit interrupt. More... | |
| void | SCI_enableTxWake (SCI_Handle sciHandle) |
| Enables the serial communications interface (SCI) wakeup method. More... | |
| uint16_t | SCI_getDataBlocking (SCI_Handle sciHandle) |
| Gets data from the serial communications interface (Blocking) More... | |
| uint16_t | SCI_getDataNonBlocking (SCI_Handle sciHandle, uint16_t *success) |
| Read data from the serial communications interface (Non-Blocking) More... | |
| SCI_FifoStatus_e | SCI_getRxFifoStatus (SCI_Handle sciHandle) |
| Gets the serial communications interface (SCI) receive FIFO status. More... | |
| SCI_FifoStatus_e | SCI_getTxFifoStatus (SCI_Handle sciHandle) |
| Gets the serial communications interface (SCI) transmit FIFO status. More... | |
| SCI_Handle | SCI_init (void *pMemory, const size_t numBytes) |
| Initializes the serial communications interface (SCI) object handle. More... | |
| void | SCI_putDataBlocking (SCI_Handle sciHandle, uint16_t data) |
| Writes data to the serial communications interface (Blocking) More... | |
| uint16_t | SCI_putDataNonBlocking (SCI_Handle sciHandle, uint16_t data) |
| Writes data to the serial communications interface (Non-Blocking) More... | |
| void | SCI_reset (SCI_Handle sciHandle) |
| Resets the serial communications interface (SCI) More... | |
| void | SCI_resetChannels (SCI_Handle sciHandle) |
| Resets the serial communications interface (SCI) transmit and receive channels. More... | |
| void | SCI_resetRxFifo (SCI_Handle sciHandle) |
| Resets the serial communications interface (SCI) receive FIFO. More... | |
| void | SCI_resetTxFifo (SCI_Handle sciHandle) |
| Resets the serial communications interface (SCI) transmit FIFO. More... | |
| void | SCI_setBaudRate (SCI_Handle sciHandle, const SCI_BaudRate_e baudRate) |
| Sets the serial communications interface (SCI) baud rate. More... | |
| void | SCI_setCharLength (SCI_Handle sciHandle, const SCI_CharLength_e charLength) |
| Sets the serial communications interface (SCI) character length. More... | |
| void | SCI_setMode (SCI_Handle sciHandle, const SCI_Mode_e mode) |
| Sets the serial communications interface (SCI) miltprocessor mode. More... | |
| void | SCI_setNumStopBits (SCI_Handle sciHandle, const SCI_NumStopBits_e numBits) |
| Sets the serial communications interface (SCI) number of stop bits. More... | |
| void | SCI_setPriority (SCI_Handle sciHandle, const SCI_Priority_e priority) |
| Sets the serial communications interface (SCI) priority. More... | |
| void | SCI_setParity (SCI_Handle sciHandle, const SCI_Parity_e parity) |
| Sets the serial communications interface (SCI) parity. More... | |
| void | SCI_setTxDelay (SCI_Handle sciHandle, const uint_least8_t delay) |
| Sets the serial communications interface (SCI) transmit delay. More... | |
| void | SCI_setRxFifoIntLevel (SCI_Handle sciHandle, const SCI_FifoLevel_e fifoLevel) |
| Sets the serial communications interface (SCI) receive FIFO level for generating an interrupt. More... | |
| void | SCI_setTxFifoIntLevel (SCI_Handle sciHandle, const SCI_FifoLevel_e fifoLevel) |
| Sets the serial communications interface (SCI) transmit FIFO level for generating an interrupt. More... | |
Contains the various functions related to the serial communications interface (SCI) object.
(C) Copyright 2015, Texas Instruments, Inc.
Definition in file sci.c.
1.8.9.1